![]() |
![]() |
|
MSPM0G3507SensoredFOCMotorControlLibrary
1.0
|
userInputPinCfg structure More...
#include <appInputCtrlInterface.h>
Data Fields | |
| uint32_t | brakeInp: 2 |
| uint32_t | brakePinMode: 1 |
| uint32_t | reserved1: 16 |
| uint32_t | vdcFiltDis: 1 |
| uint32_t | reserved: 12 |
userInputPinCfg structure
| uint32_t userInputPinCfg::brakeInp |
Brake pin override
Referenced by update_BrakeStatus().
| uint32_t userInputPinCfg::brakePinMode |
Brake pin mode
| uint32_t userInputPinCfg::reserved1 |
Reserved
| uint32_t userInputPinCfg::vdcFiltDis |
Bus voltage filter enable
| uint32_t userInputPinCfg::reserved |
Reserved