MSPM0G1507HallSensoredTrapMotorControlLibrary  1.0
Data Structures | Macros | Enumerations | Functions
Motor Driver/DRV8316

Data Structures

struct  DRV8316_Instance
 Defines DRV8316 instance. More...
 

Macros

#define DRV8316_ADDR_MASK   (0x7E00)
 Defines the address mask.
 
#define DRV8316_DATA_MASK   (0x00FF)
 Defines the data mask.
 
#define DRV8316_DATA_TRANSMIT_TO_READ   (0x00)
 Defines the data transmitted while reading a register.
 
#define DRV8316_INITIAL_PARITY   (0x00)
 Defines the initial parity of command word.
 
#define DRV8316_PARITY_CHECK   (0x01)
 Defines the parity checking bit.
 
#define DRV8316_RIGHT_SHIFT_REGISTER   (1)
 Defines the number of bits right shifted.
 
#define DRV8316_PARITY_BIT_POSITION   (8)
 Defines the position of the parity in command word.
 
#define DRV8316_ADDR_BIT_POSITION   (9)
 Defines the position of the parity in command word.
 
#define DRV8316_SPICMD_BIT_POSITION   (15)
 Defines the position of the parity in command word.
 
#define DRV8316_CLEAR_BIT_MASK   (0x01)
 Defines the claer bit mask.
 
#define DRV8316_MAXIMUM_RESET_TIME   (40)
 Defines the time to clear the nSLEEP pin to reset faults.
 
#define DRV8316_MAXIMUM_WAKEUP_TIME   (2000)
 Defines the time to wakeup the drv after reset.
 
#define DRV8316_VOLTAGE_CONV_CONST   _IQ20(13.417)
 Defines voltage conversion constant.
 
#define DRV8316_CSA_REF_VOLTAGE   (3000)
 Defines CSA reference voltage.
 
#define DRV8316_CSAGAIN_0P15VA_IQ   _IQ20(0.15)
 Defines CSA gains 0.15 in IQ20.
 
#define DRV8316_CSAGAIN_0P3VA_IQ   _IQ20(0.3)
 Defines CSA gains 0.3 in IQ20.
 
#define DRV8316_CSAGAIN_0P6VA_IQ   _IQ20(0.6)
 Defines CSA gains 0.6 in IQ20.
 
#define DRV8316_CSAGAIN_1P2VA_IQ   _IQ20(1.2)
 Defines CSA gains 1.2 in IQ20.
 

Enumerations

enum  DRV8316_CTRL01_MASK { DRV8316_CTRL01_MASK_REG_LOCK = 0x07 << 0 }
 
enum  DRV8316_CTRL02_MASK {
  DRV8316_CTRL02_MASK_CLR_FLT = 0x01 << 0,
  DRV8316_CTRL02_MASK_PWM_MODE = 0x03 << 1,
  DRV8316_CTRL02_MASK_SLEW = 0x03 << 3,
  DRV8316_CTRL02_MASK_SDO_MODE = 0x01 << 5
}
 
enum  DRV8316_CTRL03_MASK {
  DRV8316_CTRL03_MASK_OTW_REP = 0x01 << 0,
  DRV8316_CTRL03_MASK_OVP_EN = 0x01 << 2,
  DRV8316_CTRL03_MASK_OVP_SEL = 0x01 << 3,
  DRV8316_CTRL03_MASK_PWM_100_DUTY_SEL = 0x01 << 4
}
 
enum  DRV8316_CTRL04_MASK {
  DRV8316_CTRL04_MASK_OCP_MODE = 0x03 << 0,
  DRV8316_CTRL04_MASK_OCP_LVL = 0x01 << 2,
  DRV8316_CTRL04_MASK_OCP_RETRY = 0x01 << 3,
  DRV8316_CTRL04_MASK_OCP_DEG = 0x03 << 4,
  DRV8316_CTRL04_MASK_OCP_CBC = 0x01 << 6,
  DRV8316_CTRL04_MASK_DRV_OFF = 0x01 << 7
}
 
enum  DRV8316_CTRL05_MASK {
  DRV8316_CTRL05_MASK_CSA_GAIN = 0x03 << 0,
  DRV8316_CTRL05_MASK_EN_ASR = 0x01 << 2,
  DRV8316_CTRL05_MASK_EN_AAR = 0x01 << 3,
  DRV8316_CTRL05_MASK_ILIM_RECIR = 0x01 << 6
}
 
enum  DRV8316_CTRL06_MASK {
  DRV8316_CTRL06_MASK_BUCK_DIS = 0x01 << 0,
  DRV8316_CTRL06_MASK_BUCK_SEL = 0x03 << 1,
  DRV8316_CTRL06_MASK_BUCK_CL = 0x01 << 3,
  DRV8316_CTRL06_MASK_BUCK_PS_DIS = 0x01 << 4
}
 
enum  DRV8316_CTRL10_MASK {
  DRV8316_CTRL10_MASK_DLY_TARGET = 0x0F << 0,
  DRV8316_CTRL10_MASK_DLYCMP_EN = 0x01 << 4
}
 
enum  DRV8316_CTRL01 {
  DRV8316_CTRL01_REG_UNLOCK = 0x03 << 0,
  DRV8316_CTRL01_REG_LOCK = 0x06 << 0
}
 
enum  DRV8316_CTRL02 {
  DRV8316_CTRL02_CLR_FLT = 0x01 << 0,
  DRV8316_CTRL02_PWMMODE_6x = 0x00 << 1,
  DRV8316_CTRL02_PWMMODE_6x_CL = 0x01 << 1,
  DRV8316_CTRL02_PWMMODE_3x = 0x02 << 1,
  DRV8316_CTRL02_PWMMODE_3x_CL = 0x03 << 1,
  DRV8316_CTRL02_SLEWRATE_25 = 0x00 << 3,
  DRV8316_CTRL02_SLEWRATE_50 = 0x01 << 3,
  DRV8316_CTRL02_SLEWRATE_125 = 0x02 << 3,
  DRV8316_CTRL02_SLEWRATE_200 = 0x03 << 3,
  DRV8316_CTRL02_SDO_OPEN_DRAIN_MODE = 0x00 << 5,
  DRV8316_CTRL02_SDO_PUSH_PULL_MODE = 0x01 << 5
}
 
enum  DRV8316_CTRL03 {
  DRV8316_CTRL03_OTW_REP_DISABLE = 0x00 << 0,
  DRV8316_CTRL03_OTW_REP_ENABLE = 0x01 << 0,
  DRV8316_CTRL03_OVP_DISABLE = 0x00 << 2,
  DRV8316_CTRL03_OVP_ENABLE = 0x01 << 2,
  DRV8316_CTRL03_OVP_SEL_34V = 0x00 << 3,
  DRV8316_CTRL03_OVP_SEL_22V = 0x01 << 3,
  DRV8316_CTRL03_PWM_20KHZ = 0x00 << 4,
  DRV8316_CTRL03_PWM_40KHZ = 0x01 << 4
}
 
enum  DRV8316_CTRL04 {
  DRV8316_CTRL04_OCP_LATCHED = 0x00 << 0,
  DRV8316_CTRL04_OCP_AUTO_RETRY = 0x01 << 0,
  DRV8316_CTRL04_OCP_REPORT = 0x02 << 0,
  DRV8316_CTRL04_OCP_DISABLE = 0x03 << 0,
  DRV8316_CTRL04_OCP_LVL_16A = 0x00 << 2,
  DRV8316_CTRL04_OCP_LVL_24A = 0x01 << 2,
  DRV8316_CTRL04_OCP_RETRY_5MS = 0x00 << 3,
  DRV8316_CTRL04_OCP_RETRY_500MS = 0x01 << 3,
  DRV8316_CTRL04_OCP_DEG_0P2US = 0x00 << 4,
  DRV8316_CTRL04_OCP_DEG_0P6US = 0x01 << 4,
  DRV8316_CTRL04_OCP_DEG_1P25US = 0x02 << 4,
  DRV8316_CTRL04_OCP_DEG_1P6US = 0x03 << 4,
  DRV8316_CTRL04_OCP_CBC_DISABLE = 0x00 << 6,
  DRV8316_CTRL04_OCP_CBC_ENABLE = 0x01 << 6,
  DRV8316_CTRL04_DRV_OFF_NO_ACTION = 0x00 << 7,
  DRV8316_CTRL04_DRV_OFF_LOW_POWER_MODE = 0x01 << 7
}
 
enum  DRV8316_CTRL05 {
  DRV8316_CTRL05_CSA_GAIN_0P15VA = 0x00 << 0,
  DRV8316_CTRL05_CSA_GAIN_0P3VA = 0x01 << 0,
  DRV8316_CTRL05_CSA_GAIN_0P6VA = 0x02 << 0,
  DRV8316_CTRL05_CSA_GAIN_1P2VA = 0x03 << 0,
  DRV8316_CTRL05_EN_ASR_DISABLE = 0x00 << 2,
  DRV8316_CTRL05_EN_ASR_ENABLE = 0x01 << 2,
  DRV8316_CTRL05_EN_AAR_DISABLE = 0x00 << 3,
  DRV8316_CTRL05_EN_AAR_ENABLE = 0x01 << 3,
  DRV8316_CTRL05_ILIM_RECIR_BRAKE_MODE = 0x00 << 6,
  DRV8316_CTRL05_ILIM_RECIR_COAST_MODE = 0x01 << 6
}
 
enum  DRV8316_CTRL06 {
  DRV8316_CTRL06_BUCK_DIS_ENABLE = 0x00 << 0,
  DRV8316_CTRL06_BUCK_DIS_DISABLE = 0x01 << 0,
  DRV8316_CTRL06_BUCK_SEL_3P3V = 0x00 << 1,
  DRV8316_CTRL06_BUCK_SEL_5P0V = 0x01 << 1,
  DRV8316_CTRL06_BUCK_SEL_4P0V = 0x02 << 1,
  DRV8316_CTRL06_BUCK_SEL_5P7V = 0x03 << 1,
  DRV8316_CTRL06_BUCK_CL_600MA = 0x00 << 3,
  DRV8316_CTRL06_BUCK_CL_150MA = 0x01 << 3,
  DRV8316_CTRL06_BUCK_PS_DIS_ENABLE = 0x00 << 4,
  DRV8316_CTRL06_BUCK_PS_DIS_DISABLE = 0x01 << 4
}
 
enum  DRV8316_CTRL10 {
  DRV8316_CTRL10_DLY_TARGET_0P0US = 0x00 << 0,
  DRV8316_CTRL10_DLY_TARGET_0P4US = 0x01 << 0,
  DRV8316_CTRL10_DLY_TARGET_0P6US = 0x02 << 0,
  DRV8316_CTRL10_DLY_TARGET_0P8US = 0x03 << 0,
  DRV8316_CTRL10_DLY_TARGET_1P0US = 0x04 << 0,
  DRV8316_CTRL10_DLY_TARGET_1P2US = 0x05 << 0,
  DRV8316_CTRL10_DLY_TARGET_1P4US = 0x06 << 0,
  DRV8316_CTRL10_DLY_TARGET_1P6US = 0x07 << 0,
  DRV8316_CTRL10_DLY_TARGET_1P8US = 0x08 << 0,
  DRV8316_CTRL10_DLY_TARGET_2P0US = 0x09 << 0,
  DRV8316_CTRL10_DLY_TARGET_2P2US = 0x0A << 0,
  DRV8316_CTRL10_DLY_TARGET_2P4US = 0x0B << 0,
  DRV8316_CTRL10_DLY_TARGET_2P6US = 0x0C << 0,
  DRV8316_CTRL10_DLY_TARGET_2P8US = 0x0D << 0,
  DRV8316_CTRL10_DLY_TARGET_3P0US = 0x0E << 0,
  DRV8316_CTRL10_DLY_TARGET_3P2US = 0x0F << 0,
  DRV8316_CTRL10_DLYCMP_EN_DISABLE = 0x00 << 4,
  DRV8316_CTRL10_DLYCMP_EN_ENABLE = 0x01 << 4
}
 
enum  DRV8316_SPI {
  DRV8316_SPI_READ = 1 << 15,
  DRV8316_SPI_WRITE = 0 << 15
}
 
enum  DRV8316_ADDR {
  DRV8316_ADDR_STAT_IC = 0x0,
  DRV8316_ADDR_STAT_1 = 0x1,
  DRV8316_ADDR_STAT_2 = 0x2,
  DRV8316_ADDR_CTRL_1 = 0x3,
  DRV8316_ADDR_CTRL_2 = 0x4,
  DRV8316_ADDR_CTRL_3 = 0x5,
  DRV8316_ADDR_CTRL_4 = 0x6,
  DRV8316_ADDR_CTRL_5 = 0x7,
  DRV8316_ADDR_CTRL_6 = 0x8,
  DRV8316_ADDR_CTRL_10 = 0xC
}
 
enum  DRV8316_CSAGAIN {
  DRV8316_CSAGAIN_0P15VA = 0x00 << 0,
  DRV8316_CSAGAIN_0P3VA = 0x01 << 0,
  DRV8316_CSAGAIN_0P6VA = 0x02 << 0,
  DRV8316_CSAGAIN_1P2VA = 0x03 << 0
}
 
enum  DRV8316_DRVOFF_PIN_STAT {
  DRV8316_DRVOFF_PIN_LOW = HAL_GPIO_PIN_LOW,
  DRV8316_DRVOFF_PIN_HIGH = HAL_GPIO_PIN_HIGH
}
 
enum  DRV8316_DRV_NSLEEP_STAT {
  DRV8316_DRV_NSLEEP_SLEEP = HAL_GPIO_PIN_LOW,
  DRV8316_DRV_NSLEEP_AWAKE = HAL_GPIO_PIN_HIGH
}
 

Functions

__STATIC_INLINE void DRV8316_setDrvoff (DRV8316_Instance *drvHandle, DRV8316_DRVOFF_PIN_STAT value)
 set drvoff More...
 
__STATIC_INLINE void DRV8316_setnSleep (DRV8316_Instance *drvHandle, DRV8316_DRV_NSLEEP_STAT value)
 set nSleep More...
 
void DRV8316_init (DRV8316_Instance *drvHandle)
 initialize the drv8316 module More...
 
uint16_t DRV8316_SPIWrite (DRV8316_Instance *drvHandle, DRV8316_ADDR addr, uint8_t data)
 write data to spi More...
 
uint16_t DRV8316_SPIRead (DRV8316_Instance *drvHandle, DRV8316_ADDR addr)
 write data to spi More...
 
void DRV8316_enable (DRV8316_Instance *drvHandle)
 Enable DRV. More...
 
void DRV8316_updateCTRLRegs (DRV8316_Instance *drvHandle, DRV8316_ADDR regAddr, uint16_t value, uint16_t mask)
 update the drv registers More...
 
void DRV8316_updateCSAScaleFactor (DRV8316_Instance *drvHandle, DRV8316_CSAGAIN csa)
 updates the current gain scale factor More...
 
_iq20 DRV8316_getVoltage (HAL_ADC_CHAN chan)
 Get voltage from adc channel. More...
 
_iq20 DRV8316_getCurrent (HAL_ADC_CHAN chan, DRV8316_Instance *drvHandle, _iq20 vRef)
 Get current from adc channel. More...
 
void DRV8316_ADCVRefSel (HAL_ADC_VREF adcRef, HAL_ADC_CHAN chan, HAL_ADC_INT_VREF internalVRef, uint16_t externalVRef)
 updates the adc voltage reference More...
 
__STATIC_INLINE void DRV8316_updateSPICsagain (DRV8316_Instance *drvHandle, DRV8316_CSAGAIN csaGain)
 Update the SPI CSA gain register. More...
 
__STATIC_INLINE void DRV8316_unlockRegs (DRV8316_Instance *drvHandle)
 unlock all registers More...
 
__STATIC_INLINE void DRV8316_clearfaultBit (DRV8316_Instance *drvHandle)
 clear the status registers More...
 
__STATIC_INLINE _iq20 DRV8316_getcsaVref (uint16_t vRef)
 get Current reference in IQ20 More...
 

Detailed Description

Enumeration Type Documentation

§ DRV8316_CTRL01_MASK

Enumerator
DRV8316_CTRL01_MASK_REG_LOCK 

Defines the mask for clear fault bit.

§ DRV8316_CTRL02_MASK

Enumerator
DRV8316_CTRL02_MASK_CLR_FLT 

Defines the mask for clear fault bit.

DRV8316_CTRL02_MASK_PWM_MODE 

Defines the mask for pwm mode selection bit.

DRV8316_CTRL02_MASK_SLEW 

Defines the mask for slew rate selection bit.

DRV8316_CTRL02_MASK_SDO_MODE 

Defines the mask for SDO mode selection bit.

§ DRV8316_CTRL03_MASK

Enumerator
DRV8316_CTRL03_MASK_OTW_REP 

Defines the mask for over temp warning bit.

DRV8316_CTRL03_MASK_OVP_EN 

Defines the mask for over voltage protection enable bit.

DRV8316_CTRL03_MASK_OVP_SEL 

Defines the mask for over voltage protection level setting bit.

DRV8316_CTRL03_MASK_PWM_100_DUTY_SEL 

Defines the mask for frequency selection bit.

§ DRV8316_CTRL04_MASK

Enumerator
DRV8316_CTRL04_MASK_OCP_MODE 

Defines the mask for over current protection mode selection bit.

DRV8316_CTRL04_MASK_OCP_LVL 

Defines the mask for over current protection level setting bit.

DRV8316_CTRL04_MASK_OCP_RETRY 

Defines the mask for over current protection retry time setting bit.

DRV8316_CTRL04_MASK_OCP_DEG 

Defines the mask for over current protection deglitch time setting bit.

DRV8316_CTRL04_MASK_OCP_CBC 

Defines the mask for over current protection pwm cycle operation bit.

DRV8316_CTRL04_MASK_DRV_OFF 

Defines the mask for drvoff bit.

§ DRV8316_CTRL05_MASK

Enumerator
DRV8316_CTRL05_MASK_CSA_GAIN 

Defines the mask for CSA gain setting bit.

DRV8316_CTRL05_MASK_EN_ASR 

Defines the mask for Active Synchronous Rectification Enable bit.

DRV8316_CTRL05_MASK_EN_AAR 

Defines the mask for Active Asynshronous Rectification Enable bit.

DRV8316_CTRL05_MASK_ILIM_RECIR 

Defines the mask for Current Limit Recirculation Settings bit.

§ DRV8316_CTRL06_MASK

Enumerator
DRV8316_CTRL06_MASK_BUCK_DIS 

Defines the mask for buck disable bit.

DRV8316_CTRL06_MASK_BUCK_SEL 

Defines the mask for buck voltage selection bit.

DRV8316_CTRL06_MASK_BUCK_CL 

Defines the mask for buck current limit setting bit.

DRV8316_CTRL06_MASK_BUCK_PS_DIS 

Defines the mask for buck power sequence disable bit.

§ DRV8316_CTRL10_MASK

Enumerator
DRV8316_CTRL10_MASK_DLY_TARGET 

Defines the mask for delay target bit.

DRV8316_CTRL10_MASK_DLYCMP_EN 

Defines the mask for driver delay compensation enable bit.

§ DRV8316_CTRL01

Enumerator
DRV8316_CTRL01_REG_UNLOCK 

unlock all registers

DRV8316_CTRL01_REG_LOCK 

lock all registers

§ DRV8316_CTRL02

Enumerator
DRV8316_CTRL02_CLR_FLT 

clear the latched faults

DRV8316_CTRL02_PWMMODE_6x 

set 6x pwm mode

DRV8316_CTRL02_PWMMODE_6x_CL 

set 6x pwm mode with current limit

DRV8316_CTRL02_PWMMODE_3x 

set 3x pwm mode

DRV8316_CTRL02_PWMMODE_3x_CL 

set 3x pwm mode with current limit

DRV8316_CTRL02_SLEWRATE_25 

set slew rate to 25V/us

DRV8316_CTRL02_SLEWRATE_50 

set slew rate to 50V/us

DRV8316_CTRL02_SLEWRATE_125 

set slew rate to 125V/us

DRV8316_CTRL02_SLEWRATE_200 

set slew rate to 200V/us

DRV8316_CTRL02_SDO_OPEN_DRAIN_MODE 

set SDO in open drain mode

DRV8316_CTRL02_SDO_PUSH_PULL_MODE 

set SDO in push pull mode

§ DRV8316_CTRL03

Enumerator
DRV8316_CTRL03_OTW_REP_DISABLE 

Disable over temperature warning.

DRV8316_CTRL03_OTW_REP_ENABLE 

Enable over temperature warning.

DRV8316_CTRL03_OVP_DISABLE 

Disable over voltage protection.

DRV8316_CTRL03_OVP_ENABLE 

Enable over voltage protection.

DRV8316_CTRL03_OVP_SEL_34V 

over voltage protection limit set to 34V

DRV8316_CTRL03_OVP_SEL_22V 

over voltage protection limit set to 22V

DRV8316_CTRL03_PWM_20KHZ 

PMW Freq at 100% duty is set to 20KHz.

DRV8316_CTRL03_PWM_40KHZ 

PMW Freq at 100% duty is set to 40KHz.

§ DRV8316_CTRL04

Enumerator
DRV8316_CTRL04_OCP_LATCHED 

set over current fault to latched

DRV8316_CTRL04_OCP_AUTO_RETRY 

set over current fault to automatic retry

DRV8316_CTRL04_OCP_REPORT 

report over current fault

DRV8316_CTRL04_OCP_DISABLE 

disable over current fault

DRV8316_CTRL04_OCP_LVL_16A 

set over current protection level to 16A

DRV8316_CTRL04_OCP_LVL_24A 

set over current protection level to 24A

DRV8316_CTRL04_OCP_RETRY_5MS 

set over current protection retry time to 5ms

DRV8316_CTRL04_OCP_RETRY_500MS 

set over current protection retry time to 500ms

DRV8316_CTRL04_OCP_DEG_0P2US 

set over current protection deglitch time to 0.2us

DRV8316_CTRL04_OCP_DEG_0P6US 

set over current protection deglitch time to 0.6us

DRV8316_CTRL04_OCP_DEG_1P25US 

set over current protection deglitch time to 1.25us

DRV8316_CTRL04_OCP_DEG_1P6US 

set over current protection deglitch time to 1.6us

DRV8316_CTRL04_OCP_CBC_DISABLE 

set over current protection pwm cycle operation dsiable

DRV8316_CTRL04_OCP_CBC_ENABLE 

set over current protection pwm cycle operation enable

DRV8316_CTRL04_DRV_OFF_NO_ACTION 

enable DRV

DRV8316_CTRL04_DRV_OFF_LOW_POWER_MODE 

enter DRV into low power mode

§ DRV8316_CTRL05

Enumerator
DRV8316_CTRL05_CSA_GAIN_0P15VA 

set CSAGAIN to 0.15V/A

DRV8316_CTRL05_CSA_GAIN_0P3VA 

set CSAGAIN to 0.3V/A

DRV8316_CTRL05_CSA_GAIN_0P6VA 

set CSAGAIN to 0.6V/A

DRV8316_CTRL05_CSA_GAIN_1P2VA 

set CSAGAIN to 1.2V/A

DRV8316_CTRL05_EN_ASR_DISABLE 

disable Active synchronous rectification

DRV8316_CTRL05_EN_ASR_ENABLE 

enable Active synchronous rectification

DRV8316_CTRL05_EN_AAR_DISABLE 

disable Active asynchronous rectification

DRV8316_CTRL05_EN_AAR_ENABLE 

enable Active asynchronous rectification

DRV8316_CTRL05_ILIM_RECIR_BRAKE_MODE 

set braking type to brake mode

DRV8316_CTRL05_ILIM_RECIR_COAST_MODE 

set braking type to coast mode

§ DRV8316_CTRL06

Enumerator
DRV8316_CTRL06_BUCK_DIS_ENABLE 

enable buck regulator

DRV8316_CTRL06_BUCK_DIS_DISABLE 

disable buck regulator

DRV8316_CTRL06_BUCK_SEL_3P3V 

set buck voltage selection to 3.3V

DRV8316_CTRL06_BUCK_SEL_5P0V 

set buck voltage selection to 5.0V

DRV8316_CTRL06_BUCK_SEL_4P0V 

set buck voltage selection to 4.0V

DRV8316_CTRL06_BUCK_SEL_5P7V 

set buck voltage selection to 5.7V

DRV8316_CTRL06_BUCK_CL_600MA 

set buck current limit to 600mA

DRV8316_CTRL06_BUCK_CL_150MA 

set buck current limit to 150mA

DRV8316_CTRL06_BUCK_PS_DIS_ENABLE 

enable buck power sequencing

DRV8316_CTRL06_BUCK_PS_DIS_DISABLE 

disable buck power sequencing

§ DRV8316_CTRL10

Enumerator
DRV8316_CTRL10_DLY_TARGET_0P0US 

Delay Target 0.0us.

DRV8316_CTRL10_DLY_TARGET_0P4US 

Delay Target 0.4us.

DRV8316_CTRL10_DLY_TARGET_0P6US 

Delay Target 0.6us.

DRV8316_CTRL10_DLY_TARGET_0P8US 

Delay Target 0.8us.

DRV8316_CTRL10_DLY_TARGET_1P0US 

Delay Target 1.0us.

DRV8316_CTRL10_DLY_TARGET_1P2US 

Delay Target 1.2us.

DRV8316_CTRL10_DLY_TARGET_1P4US 

Delay Target 1.4us.

DRV8316_CTRL10_DLY_TARGET_1P6US 

Delay Target 1.6us.

DRV8316_CTRL10_DLY_TARGET_1P8US 

Delay Target 1.8us.

DRV8316_CTRL10_DLY_TARGET_2P0US 

Delay Target 2.0us.

DRV8316_CTRL10_DLY_TARGET_2P2US 

Delay Target 2.2us.

DRV8316_CTRL10_DLY_TARGET_2P4US 

Delay Target 2.4us.

DRV8316_CTRL10_DLY_TARGET_2P6US 

Delay Target 2.6us.

DRV8316_CTRL10_DLY_TARGET_2P8US 

Delay Target 2.8us.

DRV8316_CTRL10_DLY_TARGET_3P0US 

Delay Target 3.0us.

DRV8316_CTRL10_DLY_TARGET_3P2US 

Delay Target 3.2us.

DRV8316_CTRL10_DLYCMP_EN_DISABLE 

disable driver delay compensation

DRV8316_CTRL10_DLYCMP_EN_ENABLE 

enable driver delay compensation

§ DRV8316_SPI

Enumerator
DRV8316_SPI_READ 

DRV8316 SPI read command.

DRV8316_SPI_WRITE 

DRV8316 SPI write command.

§ DRV8316_ADDR

Enumerator
DRV8316_ADDR_STAT_IC 

Address of Static Register 0.

DRV8316_ADDR_STAT_1 

Address of Static Register 1.

DRV8316_ADDR_STAT_2 

Address of Static Register 2.

DRV8316_ADDR_CTRL_1 

Address of Control Register 1.

DRV8316_ADDR_CTRL_2 

Address of Control Register 2.

DRV8316_ADDR_CTRL_3 

Address of Control Register 3.

DRV8316_ADDR_CTRL_4 

Address of Control Register 4.

DRV8316_ADDR_CTRL_5 

Address of Control Register 5.

DRV8316_ADDR_CTRL_6 

Address of Control Register 6.

DRV8316_ADDR_CTRL_10 

Address of Control Register 10.

§ DRV8316_CSAGAIN

Enumerator
DRV8316_CSAGAIN_0P15VA 

Define DRV8316 CSA GAIN 0.15 Setting.

DRV8316_CSAGAIN_0P3VA 

Define DRV8316 CSA GAIN 0.3 Setting.

DRV8316_CSAGAIN_0P6VA 

Define DRV8316 CSA GAIN 0.6 Setting.

DRV8316_CSAGAIN_1P2VA 

Define DRV8316 CSA GAIN 1.2 Setting.

§ DRV8316_DRVOFF_PIN_STAT

Enumerator
DRV8316_DRVOFF_PIN_LOW 

Define DRVOFF PIN LOW.

DRV8316_DRVOFF_PIN_HIGH 

Define DRVOFF PIN HIGH.

§ DRV8316_DRV_NSLEEP_STAT

Enumerator
DRV8316_DRV_NSLEEP_SLEEP 

Define NSLEEP PIN LOW.

DRV8316_DRV_NSLEEP_AWAKE 

Define NSLEEP PIN HIGH.

Function Documentation

§ DRV8316_setDrvoff()

__STATIC_INLINE void DRV8316_setDrvoff ( DRV8316_Instance drvHandle,
DRV8316_DRVOFF_PIN_STAT  value 
)

set drvoff

Parameters
[in]drvHandleThe drv instance
[in]valuedrvoff value

References DRV8316_DRVOFF_PIN_HIGH, DRV8316_DRVOFF_PIN_LOW, DRV8316_Instance::drvoff, HAL_GPIO_PIN_HIGH, HAL_GPIO_PIN_LOW, and HAL_writeGPIOPin().

Referenced by DRV8316_enable().

§ DRV8316_setnSleep()

__STATIC_INLINE void DRV8316_setnSleep ( DRV8316_Instance drvHandle,
DRV8316_DRV_NSLEEP_STAT  value 
)

§ DRV8316_init()

void DRV8316_init ( DRV8316_Instance drvHandle)

§ DRV8316_SPIWrite()

uint16_t DRV8316_SPIWrite ( DRV8316_Instance drvHandle,
DRV8316_ADDR  addr,
uint8_t  data 
)

write data to spi

Parameters
[in]drvHandleThe drv instance
[in]addrSPI register address
[in]datadata transmitted
Returns
Return

References DRV8316_SPI_WRITE, DRV8316_Instance::spiChan, and DRV8316_Instance::spiCs.

Referenced by DRV8316_setnSleep(), and DRV8316_updateCTRLRegs().

§ DRV8316_SPIRead()

uint16_t DRV8316_SPIRead ( DRV8316_Instance drvHandle,
DRV8316_ADDR  addr 
)

write data to spi

Parameters
[in]drvHandleThe drv instance
[in]addrSPI register address
Returns
Return

References DRV8316_SPI_READ, DRV8316_Instance::spiChan, and DRV8316_Instance::spiCs.

Referenced by DRV8316_setnSleep(), and DRV8316_updateCTRLRegs().

§ DRV8316_enable()

void DRV8316_enable ( DRV8316_Instance drvHandle)

§ DRV8316_updateCTRLRegs()

void DRV8316_updateCTRLRegs ( DRV8316_Instance drvHandle,
DRV8316_ADDR  regAddr,
uint16_t  value,
uint16_t  mask 
)

update the drv registers

Parameters
[in]drvHandleThe drv instance
[in]regAddrThe register to be updated
[in]valuenew value of the bits to be updated
[in]maskmask for the bit to be updated

References DRV8316_SPIRead(), and DRV8316_SPIWrite().

Referenced by DRV8316_clearfaultBit(), DRV8316_setnSleep(), DRV8316_unlockRegs(), and DRV8316_updateSPICsagain().

§ DRV8316_updateCSAScaleFactor()

void DRV8316_updateCSAScaleFactor ( DRV8316_Instance drvHandle,
DRV8316_CSAGAIN  csa 
)

updates the current gain scale factor

Parameters
[in]drvHandleThe drv instance
[in]csaDRV8316 CSA gain value

References DRV8316_Instance::csa_sf, DRV8316_CSAGAIN_0P15VA, DRV8316_CSAGAIN_0P15VA_IQ, DRV8316_CSAGAIN_0P3VA, DRV8316_CSAGAIN_0P3VA_IQ, DRV8316_CSAGAIN_0P6VA, DRV8316_CSAGAIN_0P6VA_IQ, DRV8316_CSAGAIN_1P2VA, and DRV8316_CSAGAIN_1P2VA_IQ.

Referenced by DRV8316_setnSleep().

§ DRV8316_getVoltage()

_iq20 DRV8316_getVoltage ( HAL_ADC_CHAN  chan)

Get voltage from adc channel.

Parameters
[in]chanThe ADC channel name
Returns
Return

References DRV8316_VOLTAGE_CONV_CONST, and HAL_getIQ20VoltageFromADC().

Referenced by DRV8316_setnSleep().

§ DRV8316_getCurrent()

_iq20 DRV8316_getCurrent ( HAL_ADC_CHAN  chan,
DRV8316_Instance drvHandle,
_iq20  vRef 
)

Get current from adc channel.

Parameters
[in]chanThe ADC channel name
[in]drvHandleThe drv instance
[in]vRefvoltage reference for current
Returns
Return

References DRV8316_Instance::csa_sf, and HAL_getIQ20VoltageFromADC().

Referenced by DRV8316_setnSleep().

§ DRV8316_ADCVRefSel()

void DRV8316_ADCVRefSel ( HAL_ADC_VREF  adcRef,
HAL_ADC_CHAN  chan,
HAL_ADC_INT_VREF  internalVRef,
uint16_t  externalVRef 
)

updates the adc voltage reference

Parameters
[in]adcRefADC voltage reference
[in]chanADC channel name
[in]internalVRefInternal reference voltage
[in]externalVRefExternal reference voltage

References HAL_ADC_VREF_EXTERNAL, HAL_ADC_VREF_INTERNAL, HAL_ADC_VREF_VDDA, HAL_setADCVRefExternal(), HAL_setADCVRefInternal(), and HAL_setADCVRefVDDA().

Referenced by DRV8316_setnSleep().

§ DRV8316_updateSPICsagain()

__STATIC_INLINE void DRV8316_updateSPICsagain ( DRV8316_Instance drvHandle,
DRV8316_CSAGAIN  csaGain 
)

Update the SPI CSA gain register.

Parameters
[in]drvHandleThe drv instance
[in]csaGainThe CSA gain value

References DRV8316_ADDR_CTRL_5, DRV8316_CTRL05_MASK_CSA_GAIN, and DRV8316_updateCTRLRegs().

§ DRV8316_unlockRegs()

__STATIC_INLINE void DRV8316_unlockRegs ( DRV8316_Instance drvHandle)

unlock all registers

Parameters
[in]drvHandleThe drv instance

References DRV8316_ADDR_CTRL_1, DRV8316_CTRL01_MASK_REG_LOCK, DRV8316_CTRL01_REG_UNLOCK, and DRV8316_updateCTRLRegs().

Referenced by DRV8316_enable().

§ DRV8316_clearfaultBit()

__STATIC_INLINE void DRV8316_clearfaultBit ( DRV8316_Instance drvHandle)

clear the status registers

Parameters
[in]drvHandleThe drv instance

References DRV8316_ADDR_CTRL_2, DRV8316_CTRL02_CLR_FLT, DRV8316_CTRL02_MASK_CLR_FLT, and DRV8316_updateCTRLRegs().

Referenced by DRV8316_enable().

§ DRV8316_getcsaVref()

__STATIC_INLINE _iq20 DRV8316_getcsaVref ( uint16_t  vRef)

get Current reference in IQ20

Parameters
[in]vRefCSA reference voltage in milli volts
Returns
_iq20 CSA reference voltage in _iq20 format
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale