MSPM0C1106HallSensoredTrapMotorControlLibrary  1.0
Data Fields
DRV8300_Instance Struct Reference

Defines DRV8300 instance. More...

#include <drv8300.h>

Data Fields

HAL_GPIO_OUT led
 
_iq20 csa_sf
 
_iq20 csaVRef
 
HAL_ADC_CHAN Vsen
 
HAL_ADC_CHAN VsenA
 
HAL_ADC_CHAN VsenB
 
HAL_ADC_CHAN VsenC
 
HAL_ADC_CHAN IsenA
 
HAL_ADC_CHAN IsenB
 
HAL_ADC_CHAN IsenC
 

Detailed Description

Defines DRV8300 instance.

Field Documentation

§ led

HAL_GPIO_OUT DRV8300_Instance::led

HAL output pin connected to the motor driver's LED pin

§ csa_sf

_iq20 DRV8300_Instance::csa_sf

Scale factor used to cache values needed to calculate current

Referenced by DRV8300_getCurrent(), and DRV8300_updateCSAScaleFactor().

§ csaVRef

_iq20 DRV8300_Instance::csaVRef

Scale factor used to cache values needed to calculate current

§ Vsen

HAL_ADC_CHAN DRV8300_Instance::Vsen

ADc channels used to measure bus voltage

Referenced by DRV8300_init().

§ VsenA

HAL_ADC_CHAN DRV8300_Instance::VsenA

ADc channels used to measure phase A voltage

Referenced by DRV8300_init().

§ VsenB

HAL_ADC_CHAN DRV8300_Instance::VsenB

ADc channels used to measure phase B voltage

Referenced by DRV8300_init().

§ VsenC

HAL_ADC_CHAN DRV8300_Instance::VsenC

ADc channels used to measure phase C voltage

Referenced by DRV8300_init().

§ IsenA

HAL_ADC_CHAN DRV8300_Instance::IsenA

ADc channels used to measure phase A current

Referenced by DRV8300_init().

§ IsenB

HAL_ADC_CHAN DRV8300_Instance::IsenB

ADc channels used to measure phase B current

Referenced by DRV8300_init().

§ IsenC

HAL_ADC_CHAN DRV8300_Instance::IsenC

ADc channels used to measure phase C current

Referenced by DRV8300_init().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale