MSPM0L111X Driver Library  2.05.01.00
Macros
DL_INTERRUPT_GROUP_INTERRUPTS
Collaboration diagram for DL_INTERRUPT_GROUP_INTERRUPTS:

Macros

#define DL_INTERRUPT_GROUP0_WWDT0   (CPUSS_INT_GROUP_IMASK_INT_INT0)
 WWDT0 Interrupt in Group 0.
 
#define DL_INTERRUPT_GROUP0_WWDT1   (CPUSS_INT_GROUP_IMASK_INT_INT1)
 WWDT1 Interrupt in Group 0.
 
#define DL_INTERRUPT_GROUP0_DEBUGSS   (CPUSS_INT_GROUP_IMASK_INT_INT2)
 DEBUGSS Interrupt in Group 0.
 
#define DL_INTERRUPT_GROUP0_FLASH   (CPUSS_INT_GROUP_IMASK_INT_INT3)
 FLASH Interrupt in Group 0.
 
#define DL_INTERRUPT_GROUP0_WUC_FSUB0   (CPUSS_INT_GROUP_IMASK_INT_INT4)
 Generic event subscriber 0 in Group 0.
 
#define DL_INTERRUPT_GROUP0_WUC_FSUB1   (CPUSS_INT_GROUP_IMASK_INT_INT5)
 Generic event subscriber 1 in Group 0.
 
#define DL_INTERRUPT_GROUP0_PMCU   (CPUSS_INT_GROUP_IMASK_INT_INT6)
 PMCU (system controller) in Group 0.
 
#define DL_INTERRUPT_GROUP1_GPIOA   (CPUSS_INT_GROUP_IMASK_INT_INT0)
 GPIOA Interrupt in Group 1.
 
#define DL_INTERRUPT_GROUP1_GPIOB   (CPUSS_INT_GROUP_IMASK_INT_INT1)
 GPIOB Interrupt in Group 1. More...
 
#define DL_INTERRUPT_GROUP1_COMP0   (CPUSS_INT_GROUP_IMASK_INT_INT2)
 COMP0 Interrupt in Group 1. More...
 
#define DL_INTERRUPT_GROUP1_COMP1   (CPUSS_INT_GROUP_IMASK_INT_INT3)
 COMP1 Interrupt in Group 1. More...
 
#define DL_INTERRUPT_GROUP1_COMP2   (CPUSS_INT_GROUP_IMASK_INT_INT4)
 COMP2 Interrupt in Group 1. More...
 
#define DL_INTERRUPT_GROUP1_TRNG   (CPUSS_INT_GROUP_IMASK_INT_INT5)
 TRNG Interrupt in Group 1. More...
 

Detailed Description

Macro Definition Documentation

§ DL_INTERRUPT_GROUP1_GPIOB

#define DL_INTERRUPT_GROUP1_GPIOB   (CPUSS_INT_GROUP_IMASK_INT_INT1)

GPIOB Interrupt in Group 1.

Note
This is a device specific interrupt. Please consult the device TRM to determine if the interrupt is enabled as part of Group 1 interrupts.

§ DL_INTERRUPT_GROUP1_COMP0

#define DL_INTERRUPT_GROUP1_COMP0   (CPUSS_INT_GROUP_IMASK_INT_INT2)

COMP0 Interrupt in Group 1.

Note
This is a device specific interrupt. Please consult the device TRM to determine if the interrupt is enabled as part of Group 1 interrupts.

§ DL_INTERRUPT_GROUP1_COMP1

#define DL_INTERRUPT_GROUP1_COMP1   (CPUSS_INT_GROUP_IMASK_INT_INT3)

COMP1 Interrupt in Group 1.

Note
This is a device specific interrupt. Please consult the device TRM to determine if the interrupt is enabled as part of Group 1 interrupts.

§ DL_INTERRUPT_GROUP1_COMP2

#define DL_INTERRUPT_GROUP1_COMP2   (CPUSS_INT_GROUP_IMASK_INT_INT4)

COMP2 Interrupt in Group 1.

Note
This is a device specific interrupt. Please consult the device TRM to determine if the interrupt is enabled as part of Group 1 interrupts.

§ DL_INTERRUPT_GROUP1_TRNG

#define DL_INTERRUPT_GROUP1_TRNG   (CPUSS_INT_GROUP_IMASK_INT_INT5)

TRNG Interrupt in Group 1.

Note
This is a device specific interrupt. Please consult the device TRM to determine if the interrupt is enabled as part of Group 1 interrupts.
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale