![]() |
![]() |
|
MSPM0GX51X Driver Library
2.05.01.00
|
Configuration struct for DL_Timer_initTimerMode. More...
#include <dl_timer.h>
Data Fields | |
| DL_TIMER_TIMER_MODE | timerMode |
| uint32_t | period |
| DL_TIMER | startTimer |
| DL_TIMER_INTERM_INT | genIntermInt |
| uint32_t | counterVal |
Configuration struct for DL_Timer_initTimerMode.
| DL_TIMER_TIMER_MODE DL_Timer_TimerConfig::timerMode |
One shot or Periodic mode configuration. One of DL_TIMER_TIMER_MODE
| uint32_t DL_Timer_TimerConfig::period |
Actual period will be period_actual=(period +1)T_TIMCLK where T_TIMCLK is the period of the timer source clock.
| DL_TIMER_INTERM_INT DL_Timer_TimerConfig::genIntermInt |
Generate intermediate counter interrupt DL_TIMER_INTERM_INT
| uint32_t DL_Timer_TimerConfig::counterVal |
Counter value when intermediate interrupt should be generated. This member must be set to 0 when genIntermInt == DL_TIMER_INTERM_INT_DISABLED