MSPM0C110X Driver Library  2.05.01.00
Modules | Data Structures | Macros | Enumerations | Functions
Serial Peripheral Interface (SPI)
Collaboration diagram for Serial Peripheral Interface (SPI):

Modules

 DL_SPI_CD_MODE
 
 DL_SPI_INTERRUPT
 
 DL_SPI_DMA_INTERRUPT_RX
 

Data Structures

struct  DL_SPI_Config
 Configuration struct for DL_SPI_init. More...
 
struct  DL_SPI_ClockConfig
 Configuration struct for DL_SPI_setClockConfig. More...
 
struct  DL_SPI_backupConfig
 Configuration structure to backup SPI peripheral state before going to STOP/STANDBY mode. Used by DL_SPI_saveConfiguration and DL_SPI_restoreConfiguration. More...
 

Macros

#define DL_SPI_DMA_INTERRUPT_TX   (SPI_DMA_TRIG_TX_IMASK_TX_SET)
 SPI interrupt for enabling SPI transmit as DMA trigger.
 

Enumerations

enum  DL_SPI_DMA_IIDX_RX {
  DL_SPI_DMA_IIDX_RX_TRIGGER = SPI_DMA_TRIG_RX_IIDX_STAT_RX_EVT,
  DL_SPI_DMA_IIDX_RX_TIMEOUT_TRIGGER = SPI_DMA_TRIG_RX_IIDX_STAT_RTOUT_EVT
}
 
enum  DL_SPI_DMA_IIDX_TX { DL_SPI_DMA_IIDX_TX_TRIGGER = SPI_DMA_TRIG_TX_IIDX_STAT_TX_EVT }
 
enum  DL_SPI_PARITY {
  DL_SPI_PARITY_EVEN,
  DL_SPI_PARITY_ODD,
  DL_SPI_PARITY_NONE = (SPI_CTL1_PREN_DISABLE | SPI_CTL1_PTEN_DISABLE)
}
 
enum  DL_SPI_FRAME_FORMAT {
  DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA1,
  DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA0,
  DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA1,
  DL_SPI_FRAME_FORMAT_TI_SYNC = (SPI_CTL0_FRF_TI_SYNC)
}
 
enum  DL_SPI_MODE {
  DL_SPI_MODE_CONTROLLER = (SPI_CTL1_CP_ENABLE),
  DL_SPI_MODE_PERIPHERAL = (SPI_CTL1_CP_DISABLE)
}
 
enum  DL_SPI_BIT_ORDER {
  DL_SPI_BIT_ORDER_MSB_FIRST = (SPI_CTL1_MSB_ENABLE),
  DL_SPI_BIT_ORDER_LSB_FIRST = (SPI_CTL1_MSB_DISABLE)
}
 
enum  DL_SPI_DATA_SIZE {
  DL_SPI_DATA_SIZE_4 = (SPI_CTL0_DSS_DSS_4),
  DL_SPI_DATA_SIZE_5 = (SPI_CTL0_DSS_DSS_5),
  DL_SPI_DATA_SIZE_6 = (SPI_CTL0_DSS_DSS_6),
  DL_SPI_DATA_SIZE_7 = (SPI_CTL0_DSS_DSS_7),
  DL_SPI_DATA_SIZE_8 = (SPI_CTL0_DSS_DSS_8),
  DL_SPI_DATA_SIZE_9 = (SPI_CTL0_DSS_DSS_9),
  DL_SPI_DATA_SIZE_10 = (SPI_CTL0_DSS_DSS_10),
  DL_SPI_DATA_SIZE_11 = (SPI_CTL0_DSS_DSS_11),
  DL_SPI_DATA_SIZE_12 = (SPI_CTL0_DSS_DSS_12),
  DL_SPI_DATA_SIZE_13 = (SPI_CTL0_DSS_DSS_13),
  DL_SPI_DATA_SIZE_14 = (SPI_CTL0_DSS_DSS_14),
  DL_SPI_DATA_SIZE_15 = (SPI_CTL0_DSS_DSS_15),
  DL_SPI_DATA_SIZE_16 = (SPI_CTL0_DSS_DSS_16)
}
 
enum  DL_SPI_CHIP_SELECT {
  DL_SPI_CHIP_SELECT_0 = (SPI_CTL0_CSSEL_CSSEL_0),
  DL_SPI_CHIP_SELECT_1 = (SPI_CTL0_CSSEL_CSSEL_1),
  DL_SPI_CHIP_SELECT_2 = (SPI_CTL0_CSSEL_CSSEL_2),
  DL_SPI_CHIP_SELECT_3 = (SPI_CTL0_CSSEL_CSSEL_3),
  DL_SPI_CHIP_SELECT_NONE = (0)
}
 
enum  DL_SPI_TX_FIFO_LEVEL {
  DL_SPI_TX_FIFO_LEVEL_3_4_EMPTY = SPI_IFLS_TXIFLSEL_LVL_3_4,
  DL_SPI_TX_FIFO_LEVEL_1_2_EMPTY = SPI_IFLS_TXIFLSEL_LVL_1_2,
  DL_SPI_TX_FIFO_LEVEL_1_4_EMPTY = SPI_IFLS_TXIFLSEL_LVL_1_4,
  DL_SPI_TX_FIFO_LEVEL_EMPTY = SPI_IFLS_TXIFLSEL_LVL_EMPTY,
  DL_SPI_TX_FIFO_LEVEL_ONE_FRAME = SPI_IFLS_TXIFLSEL_LEVEL_1
}
 
enum  DL_SPI_RX_FIFO_LEVEL {
  DL_SPI_RX_FIFO_LEVEL_ONE_FRAME = SPI_IFLS_RXIFLSEL_LEVEL_1,
  DL_SPI_RX_FIFO_LEVEL_FULL = SPI_IFLS_RXIFLSEL_LVL_FULL,
  DL_SPI_RX_FIFO_LEVEL_3_4_FULL = SPI_IFLS_RXIFLSEL_LVL_3_4,
  DL_SPI_RX_FIFO_LEVEL_1_2_FULL = SPI_IFLS_RXIFLSEL_LVL_1_2,
  DL_SPI_RX_FIFO_LEVEL_1_4_FULL = SPI_IFLS_RXIFLSEL_LVL_1_4
}
 
enum  DL_SPI_IIDX {
  DL_SPI_IIDX_DMA_DONE_TX = SPI_CPU_INT_IIDX_STAT_DMA_DONE_TX_EVT,
  DL_SPI_IIDX_DMA_DONE_RX = SPI_CPU_INT_IIDX_STAT_DMA_DONE_RX_EVT,
  DL_SPI_IIDX_IDLE = SPI_CPU_INT_IIDX_STAT_IDLE_EVT,
  DL_SPI_IIDX_TX_EMPTY = SPI_CPU_INT_IIDX_STAT_TX_EMPTY,
  DL_SPI_IIDX_TX = SPI_CPU_INT_IIDX_STAT_TX_EVT,
  DL_SPI_IIDX_RX = SPI_CPU_INT_IIDX_STAT_RX_EVT,
  DL_SPI_IIDX_RX_TIMEOUT = SPI_CPU_INT_IIDX_STAT_RTOUT_EVT,
  DL_SPI_IIDX_RX_FULL = SPI_CPU_INT_IIDX_STAT_RXFULL_EVT,
  DL_SPI_IIDX_TX_UNDERFLOW = SPI_CPU_INT_IIDX_STAT_TXFIFO_UNF_EVT,
  DL_SPI_IIDX_PARITY_ERROR = SPI_CPU_INT_IIDX_STAT_PER_EVT,
  DL_SPI_IIDX_RX_OVERFLOW = SPI_CPU_INT_IIDX_STAT_RXFIFO_OFV_EVT
}
 
enum  DL_SPI_CLOCK_DIVIDE_RATIO {
  DL_SPI_CLOCK_DIVIDE_RATIO_1 = SPI_CLKDIV_RATIO_DIV_BY_1,
  DL_SPI_CLOCK_DIVIDE_RATIO_2 = SPI_CLKDIV_RATIO_DIV_BY_2,
  DL_SPI_CLOCK_DIVIDE_RATIO_3 = SPI_CLKDIV_RATIO_DIV_BY_3,
  DL_SPI_CLOCK_DIVIDE_RATIO_4 = SPI_CLKDIV_RATIO_DIV_BY_4,
  DL_SPI_CLOCK_DIVIDE_RATIO_5 = SPI_CLKDIV_RATIO_DIV_BY_5,
  DL_SPI_CLOCK_DIVIDE_RATIO_6 = SPI_CLKDIV_RATIO_DIV_BY_6,
  DL_SPI_CLOCK_DIVIDE_RATIO_7 = SPI_CLKDIV_RATIO_DIV_BY_7,
  DL_SPI_CLOCK_DIVIDE_RATIO_8 = SPI_CLKDIV_RATIO_DIV_BY_8
}
 
enum  DL_SPI_CLOCK {
  DL_SPI_CLOCK_BUSCLK = SPI_CLKSEL_SYSCLK_SEL_ENABLE,
  DL_SPI_CLOCK_MFCLK = SPI_CLKSEL_MFCLK_SEL_ENABLE,
  DL_SPI_CLOCK_LFCLK = SPI_CLKSEL_LFCLK_SEL_ENABLE
}
 

Functions

void DL_SPI_init (SPI_Regs *spi, const DL_SPI_Config *config)
 Initialize the SPI peripheral. More...
 
__STATIC_INLINE void DL_SPI_enablePower (SPI_Regs *spi)
 Enables the Peripheral Write Enable (PWREN) register for the SPI. More...
 
__STATIC_INLINE void DL_SPI_disablePower (SPI_Regs *spi)
 Disables the Peripheral Write Enable (PWREN) register for the SPI. More...
 
__STATIC_INLINE bool DL_SPI_isPowerEnabled (const SPI_Regs *spi)
 Returns if the Peripheral Write Enable (PWREN) register for the SPI is enabled. More...
 
__STATIC_INLINE void DL_SPI_reset (SPI_Regs *spi)
 Resets spi peripheral. More...
 
__STATIC_INLINE bool DL_SPI_isReset (const SPI_Regs *spi)
 Returns if spi peripheral was reset. More...
 
__STATIC_INLINE void DL_SPI_enable (SPI_Regs *spi)
 Enable the SPI peripheral. More...
 
__STATIC_INLINE bool DL_SPI_isEnabled (const SPI_Regs *spi)
 Checks if the SPI peripheral is enabled. More...
 
__STATIC_INLINE void DL_SPI_disable (SPI_Regs *spi)
 Disable the SPI peripheral. More...
 
void DL_SPI_setClockConfig (SPI_Regs *spi, const DL_SPI_ClockConfig *config)
 Configure SPI source clock. More...
 
void DL_SPI_getClockConfig (const SPI_Regs *spi, DL_SPI_ClockConfig *config)
 Get SPI source clock configuration. More...
 
__STATIC_INLINE bool DL_SPI_isBusy (const SPI_Regs *spi)
 Checks if the SPI is busy transmitting. More...
 
__STATIC_INLINE bool DL_SPI_isTXFIFOEmpty (const SPI_Regs *spi)
 Checks if the TX FIFO is empty. More...
 
__STATIC_INLINE bool DL_SPI_isTXFIFOFull (const SPI_Regs *spi)
 Checks if the TX FIFO is full. More...
 
__STATIC_INLINE bool DL_SPI_isRXFIFOEmpty (const SPI_Regs *spi)
 Checks if the RX FIFO is empty. More...
 
__STATIC_INLINE bool DL_SPI_isRXFIFOFull (const SPI_Regs *spi)
 Checks if the RX FIFO is full. More...
 
__STATIC_INLINE void DL_SPI_setParity (SPI_Regs *spi, DL_SPI_PARITY parity)
 Sets the parity configuration used for transactions. More...
 
__STATIC_INLINE DL_SPI_PARITY DL_SPI_getParity (const SPI_Regs *spi)
 Get the current receive and transmit parity configuration. More...
 
__STATIC_INLINE void DL_SPI_enableReceiveParity (SPI_Regs *spi)
 Enables receive parity. More...
 
__STATIC_INLINE void DL_SPI_disableReceiveParity (SPI_Regs *spi)
 Disables receive parity. More...
 
__STATIC_INLINE bool DL_SPI_isReceiveParityEnabled (const SPI_Regs *spi)
 Checks if receive parity is enabled. More...
 
__STATIC_INLINE void DL_SPI_enableTransmitParity (SPI_Regs *spi)
 Enables transmit parity. More...
 
__STATIC_INLINE void DL_SPI_disableTransmitParity (SPI_Regs *spi)
 Disables transmit parity. More...
 
__STATIC_INLINE bool DL_SPI_isTransmitParityEnabled (const SPI_Regs *spi)
 Checks if transmit parity is enabled. More...
 
__STATIC_INLINE void DL_SPI_setFrameFormat (SPI_Regs *spi, DL_SPI_FRAME_FORMAT frameFormat)
 Set the frame format to use. More...
 
__STATIC_INLINE DL_SPI_FRAME_FORMAT DL_SPI_getFrameFormat (const SPI_Regs *spi)
 Get the frame format configuration. More...
 
__STATIC_INLINE void DL_SPI_setDataSize (SPI_Regs *spi, DL_SPI_DATA_SIZE dataSize)
 Set the size for transfers. More...
 
__STATIC_INLINE DL_SPI_DATA_SIZE DL_SPI_getDataSize (const SPI_Regs *spi)
 Get the configured size for transfers. More...
 
__STATIC_INLINE void DL_SPI_setMode (SPI_Regs *spi, DL_SPI_MODE mode)
 Set whether the device should be in controller/peripheral mode. More...
 
__STATIC_INLINE DL_SPI_MODE DL_SPI_getMode (const SPI_Regs *spi)
 Get the current mode for the SPI (controller/peripheral) More...
 
__STATIC_INLINE void DL_SPI_setBitOrder (SPI_Regs *spi, DL_SPI_BIT_ORDER bitOrder)
 Set the bit order used for transfers. More...
 
__STATIC_INLINE DL_SPI_BIT_ORDER DL_SPI_getBitOrder (const SPI_Regs *spi)
 Get the current bit order used for transfers. More...
 
__STATIC_INLINE void DL_SPI_enableLoopbackMode (SPI_Regs *spi)
 Enables loopback mode. More...
 
__STATIC_INLINE void DL_SPI_disableLoopbackMode (SPI_Regs *spi)
 Disables loopback mode. More...
 
__STATIC_INLINE bool DL_SPI_isLoopbackModeEnabled (const SPI_Regs *spi)
 Checks if the loopback mode is enabled. More...
 
__STATIC_INLINE void DL_SPI_setRepeatTransmit (SPI_Regs *spi, uint32_t numRepeats)
 Set counter for repeated transmit. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRepeatTransmit (const SPI_Regs *spi)
 Get counter for repeated transmit. More...
 
__STATIC_INLINE void DL_SPI_enablePeripheralAlignDataOnChipSelect (SPI_Regs *spi)
 Enables data alignment on chip select for peripherals. More...
 
__STATIC_INLINE void DL_SPI_disablePeripheralAlignDataOnChipSelect (SPI_Regs *spi)
 Disables data alignment on chip select for peripherals. More...
 
__STATIC_INLINE bool DL_SPI_isPeripheralAlignDataOnChipSelectEnabled (const SPI_Regs *spi)
 Checks if data alignment on chip select for peripherals is enabled. More...
 
__STATIC_INLINE void DL_SPI_enablePacking (SPI_Regs *spi)
 Enables packing feature. More...
 
__STATIC_INLINE void DL_SPI_disablePacking (SPI_Regs *spi)
 Disables packing feature. More...
 
__STATIC_INLINE bool DL_SPI_isPackingEnabled (const SPI_Regs *spi)
 Checks if packing feature is enabled. More...
 
__STATIC_INLINE void DL_SPI_setChipSelect (SPI_Regs *spi, DL_SPI_CHIP_SELECT chipSelect)
 Set chip select used for controller or peripheral mode. More...
 
__STATIC_INLINE DL_SPI_CHIP_SELECT DL_SPI_getChipSelect (const SPI_Regs *spi)
 Get chip select used for controller or peripheral mode. More...
 
__STATIC_INLINE void DL_SPI_setPeripheralReceiveTimeout (SPI_Regs *spi, uint32_t timeout)
 Set peripheral receive timeout. More...
 
__STATIC_INLINE uint32_t DL_SPI_getPeripheralReceiveTimeout (const SPI_Regs *spi)
 Get peripheral receive timeout. More...
 
__STATIC_INLINE void DL_SPI_setControllerCommandDataModeConfig (SPI_Regs *spi, uint32_t config)
 Configure the command/data mode. More...
 
__STATIC_INLINE uint32_t DL_SPI_getControllerCommandDataModeConfig (const SPI_Regs *spi)
 Get the command/data mode configuration. More...
 
__STATIC_INLINE void DL_SPI_enableControllerCommandDataMode (SPI_Regs *spi)
 Enables command/data mode. More...
 
__STATIC_INLINE void DL_SPI_disableControllerCommandDataMode (SPI_Regs *spi)
 Disables command/data mode. More...
 
__STATIC_INLINE bool DL_SPI_isControllerCommandDataModeEnabled (const SPI_Regs *spi)
 Checks if command/data mode is enabled. More...
 
__STATIC_INLINE void DL_SPI_enablePeripheralDataOutput (SPI_Regs *spi)
 Enables peripheral data output. More...
 
__STATIC_INLINE void DL_SPI_disablePeripheralDataOutput (SPI_Regs *spi)
 Disables peripheral data output. More...
 
__STATIC_INLINE bool DL_SPI_isPeripheralDataOutputEnabled (const SPI_Regs *spi)
 Checks if peripheral data output is enabled. More...
 
__STATIC_INLINE void DL_SPI_setDelayedSampling (SPI_Regs *spi, uint32_t delay)
 Set the delay sampling. More...
 
__STATIC_INLINE uint32_t DL_SPI_getDelayedSampling (const SPI_Regs *spi)
 Get the delay sampling. More...
 
__STATIC_INLINE void DL_SPI_setFIFOThreshold (SPI_Regs *spi, DL_SPI_RX_FIFO_LEVEL rxThreshold, DL_SPI_TX_FIFO_LEVEL txThreshold)
 Set the RX and TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE DL_SPI_TX_FIFO_LEVEL DL_SPI_getTXFIFOThreshold (const SPI_Regs *spi)
 Get the TX FIFO interrupt threshold level. More...
 
__STATIC_INLINE DL_SPI_RX_FIFO_LEVEL DL_SPI_getRXFIFOThreshold (const SPI_Regs *spi)
 Get the RX FIFO interrupt threshold level. More...
 
__STATIC_INLINE void DL_SPI_setBitRateSerialClockDivider (SPI_Regs *spi, uint32_t SCR)
 Set the SPI bit rate serial clock divider (SCR) More...
 
__STATIC_INLINE uint32_t DL_SPI_getBitRateSerialClockDivider (const SPI_Regs *spi)
 Get the SPI bit rate serial clock divider (SCR) More...
 
__STATIC_INLINE void DL_SPI_transmitData8 (SPI_Regs *spi, uint8_t data)
 Writes 8-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE void DL_SPI_transmitData16 (SPI_Regs *spi, uint16_t data)
 Writes 16-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE void DL_SPI_transmitData32 (SPI_Regs *spi, uint32_t data)
 Writes 32-bit data into the TX FIFO for transmit. More...
 
__STATIC_INLINE uint8_t DL_SPI_receiveData8 (const SPI_Regs *spi)
 Reads 8-bit data from the RX FIFO. More...
 
__STATIC_INLINE uint16_t DL_SPI_receiveData16 (const SPI_Regs *spi)
 Reads 16-bit data from the RX FIFO. More...
 
__STATIC_INLINE uint32_t DL_SPI_receiveData32 (const SPI_Regs *spi)
 Reads 32-bit data from the RX FIFO. More...
 
__STATIC_INLINE void DL_SPI_enableInterrupt (SPI_Regs *spi, uint32_t interruptMask)
 Enable SPI interrupts. More...
 
__STATIC_INLINE void DL_SPI_disableInterrupt (SPI_Regs *spi, uint32_t interruptMask)
 Disable SPI interrupts. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledInterrupts (const SPI_Regs *spi, uint32_t interruptMask)
 Check which SPI interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledInterruptStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of enabled SPI interrupts. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawInterruptStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of any SPI interrupt. More...
 
__STATIC_INLINE DL_SPI_IIDX DL_SPI_getPendingInterrupt (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt. More...
 
__STATIC_INLINE void DL_SPI_clearInterruptStatus (SPI_Regs *spi, uint32_t interruptMask)
 Clear pending SPI interrupts. More...
 
void DL_SPI_transmitDataBlocking8 (SPI_Regs *spi, uint8_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
void DL_SPI_transmitDataBlocking16 (SPI_Regs *spi, uint16_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
void DL_SPI_transmitDataBlocking32 (SPI_Regs *spi, uint32_t data)
 Blocks to ensure transmit is ready before sending data. More...
 
uint8_t DL_SPI_receiveDataBlocking8 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
uint16_t DL_SPI_receiveDataBlocking16 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
uint32_t DL_SPI_receiveDataBlocking32 (const SPI_Regs *spi)
 Blocks to ensure receive is ready before reading data. More...
 
bool DL_SPI_transmitDataCheck8 (SPI_Regs *spi, uint8_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_transmitDataCheck16 (SPI_Regs *spi, uint16_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_transmitDataCheck32 (SPI_Regs *spi, uint32_t data)
 Checks the TX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck8 (const SPI_Regs *spi, uint8_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck16 (const SPI_Regs *spi, uint16_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
bool DL_SPI_receiveDataCheck32 (const SPI_Regs *spi, uint32_t *buffer)
 Checks the RX FIFO before trying to transmit data. More...
 
uint32_t DL_SPI_drainRXFIFO8 (const SPI_Regs *spi, uint8_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 8 bit access. More...
 
uint32_t DL_SPI_drainRXFIFO16 (const SPI_Regs *spi, uint16_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 16 bit access. More...
 
uint32_t DL_SPI_drainRXFIFO32 (const SPI_Regs *spi, uint32_t *buffer, uint32_t maxCount)
 Read all available data out of the RX FIFO using 32 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO8 (SPI_Regs *spi, const uint8_t *buffer, uint32_t count)
 Fill the TX FIFO using 8 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO16 (SPI_Regs *spi, const uint16_t *buffer, uint32_t count)
 Fill the TX FIFO using 16 bit access. More...
 
uint32_t DL_SPI_fillTXFIFO32 (SPI_Regs *spi, const uint32_t *buffer, uint32_t count)
 Fill the TX FIFO using 32 bit access. More...
 
__STATIC_INLINE void DL_SPI_enableDMAReceiveEvent (SPI_Regs *spi, uint32_t interrupt)
 Enable SPI interrupt for triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_enableDMATransmitEvent (SPI_Regs *spi)
 Enable SPI interrupt for triggering the DMA transmit event. More...
 
__STATIC_INLINE void DL_SPI_disableDMAReceiveEvent (SPI_Regs *spi, uint32_t interrupt)
 Disables SPI interrupt from triggering the DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_disableDMATransmitEvent (SPI_Regs *spi)
 Disables SPI interrupt from triggering the DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEvent (const SPI_Regs *spi, uint32_t interruptMask)
 Check which SPI interrupt for DMA receive events is enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEvent (const SPI_Regs *spi)
 Check if SPI interrupt for DMA transmit event is enabled. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEventStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of enabled SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEventStatus (const SPI_Regs *spi)
 Check interrupt flag of enabled SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawDMAReceiveEventStatus (const SPI_Regs *spi, uint32_t interruptMask)
 Check interrupt flag of any SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE uint32_t DL_SPI_getRawDMATransmitEventStatus (const SPI_Regs *spi)
 Check interrupt flag of any SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE DL_SPI_DMA_IIDX_RX DL_SPI_getPendingDMAReceiveEvent (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt for DMA receive event. More...
 
__STATIC_INLINE DL_SPI_DMA_IIDX_TX DL_SPI_getPendingDMATransmitEvent (const SPI_Regs *spi)
 Get highest priority pending SPI interrupt for DMA transmit event. More...
 
__STATIC_INLINE void DL_SPI_clearDMAReceiveEventStatus (SPI_Regs *spi, uint32_t interruptMask)
 Clear pending SPI interrupts for DMA receive event. More...
 
__STATIC_INLINE void DL_SPI_clearDMATransmitEventStatus (SPI_Regs *spi)
 Clear pending SPI interrupt for DMA transmit event. More...
 
bool DL_SPI_saveConfiguration (const SPI_Regs *spi, DL_SPI_backupConfig *ptr)
 Save SPI configuration before entering a power loss state. More...
 
bool DL_SPI_restoreConfiguration (SPI_Regs *spi, DL_SPI_backupConfig *ptr)
 Restore SPI configuration after leaving a power loss state. More...
 

Detailed Description

Overview

The Serial Peripheral Interface Driver Library allows full configuration of the MSPM0 SPI module. The serial peripheral interface (SPI) module provides a standardized serial interface to transfer data between MSPM0 devices and other external devices with SPI interface.


Enumeration Type Documentation

§ DL_SPI_DMA_IIDX_RX

Enumerator
DL_SPI_DMA_IIDX_RX_TRIGGER 

SPI interrupt index for enabling SPI receive as DMA trigger

DL_SPI_DMA_IIDX_RX_TIMEOUT_TRIGGER 

SPI interrupt index for enabling SPI receive timeout as DMA trigger

§ DL_SPI_DMA_IIDX_TX

Enumerator
DL_SPI_DMA_IIDX_TX_TRIGGER 

SPI interrupt index for enabling SPI transmit as DMA trigger

§ DL_SPI_PARITY

Enumerator
DL_SPI_PARITY_EVEN 

Use even parity, enable transmit and receive parity

DL_SPI_PARITY_ODD 

Use odd parity, enable transmit and receive parity

DL_SPI_PARITY_NONE 

Disable receive and transmit parity

§ DL_SPI_FRAME_FORMAT

Enumerator
DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA0 

Motorola 3 Wire with Polarity 0, Phase 0

DL_SPI_FRAME_FORMAT_MOTO3_POL0_PHA1 

Motorola 3 Wire with Polarity 0, Phase 1

DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA0 

Motorola 3 Wire with Polarity 1, Phase 0

DL_SPI_FRAME_FORMAT_MOTO3_POL1_PHA1 

Motorola 3 Wire with Polarity 1, Phase 1

DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA0 

Motorola 4 Wire with Polarity 0, Phase 0

DL_SPI_FRAME_FORMAT_MOTO4_POL0_PHA1 

Motorola 4 Wire with Polarity 0, Phase 1

DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA0 

Motorola 4 Wire with Polarity 1, Phase 0

DL_SPI_FRAME_FORMAT_MOTO4_POL1_PHA1 

Motorola 4 Wire with Polarity 1, Phase 1

DL_SPI_FRAME_FORMAT_TI_SYNC 

TI Sync Frame Format

§ DL_SPI_MODE

Enumerator
DL_SPI_MODE_CONTROLLER 

Controller mode

DL_SPI_MODE_PERIPHERAL 

Peripheral mode

§ DL_SPI_BIT_ORDER

Enumerator
DL_SPI_BIT_ORDER_MSB_FIRST 

MSB First

DL_SPI_BIT_ORDER_LSB_FIRST 

LSB First

§ DL_SPI_DATA_SIZE

Enumerator
DL_SPI_DATA_SIZE_4 

Data size 4 bits

DL_SPI_DATA_SIZE_5 

Data size 5 bits

DL_SPI_DATA_SIZE_6 

Data size 6 bits

DL_SPI_DATA_SIZE_7 

Data size 7 bits

DL_SPI_DATA_SIZE_8 

Data size 8 bits

DL_SPI_DATA_SIZE_9 

Data size 9 bits

DL_SPI_DATA_SIZE_10 

Data size 10 bits

DL_SPI_DATA_SIZE_11 

Data size 11 bits

DL_SPI_DATA_SIZE_12 

Data size 12 bits

DL_SPI_DATA_SIZE_13 

Data size 13 bits

DL_SPI_DATA_SIZE_14 

Data size 14 bits

DL_SPI_DATA_SIZE_15 

Data size 15 bits

DL_SPI_DATA_SIZE_16 

Data size 16 bits

§ DL_SPI_CHIP_SELECT

Enumerator
DL_SPI_CHIP_SELECT_0 

Chip Select 0

DL_SPI_CHIP_SELECT_1 

Chip Select 1

DL_SPI_CHIP_SELECT_2 

Chip Select 2

DL_SPI_CHIP_SELECT_3 

Chip Select 3

DL_SPI_CHIP_SELECT_NONE 

No chip select

§ DL_SPI_TX_FIFO_LEVEL

Enumerator
DL_SPI_TX_FIFO_LEVEL_3_4_EMPTY 

Interrupt triggers when TX FIFO <= 3/4 empty

DL_SPI_TX_FIFO_LEVEL_1_2_EMPTY 

Interrupt triggers when TX FIFO <= 1/2 empty (default)

DL_SPI_TX_FIFO_LEVEL_1_4_EMPTY 

Interrupt triggers when TX FIFO <= 1/4 empty

DL_SPI_TX_FIFO_LEVEL_EMPTY 

Interrupt triggers when TX FIFO is empty

DL_SPI_TX_FIFO_LEVEL_ONE_FRAME 

Interrupt triggers when TX FIFO has >= 1 frame free. Should be used with DMA

§ DL_SPI_RX_FIFO_LEVEL

Enumerator
DL_SPI_RX_FIFO_LEVEL_ONE_FRAME 

Interrupt triggers when RX FIFO contains >= 1 frame. Should be used with DMA

DL_SPI_RX_FIFO_LEVEL_FULL 

Interrupt triggers when RX FIFO is full

DL_SPI_RX_FIFO_LEVEL_3_4_FULL 

Interrupt triggers when RX FIFO >= 3/4 full

DL_SPI_RX_FIFO_LEVEL_1_2_FULL 

Interrupt triggers when RX FIFO >= 1/2 full (default)

DL_SPI_RX_FIFO_LEVEL_1_4_FULL 

Interrupt triggers when RX FIFO >= 1/4 full

§ DL_SPI_IIDX

Enumerator
DL_SPI_IIDX_DMA_DONE_TX 

SPI interrupt index for DMA Done 1 event for transmit

DL_SPI_IIDX_DMA_DONE_RX 

SPI interrupt index for DMA Done 1 event for receive

DL_SPI_IIDX_IDLE 

SPI interrupt index for SPI to signal it has finished transfers and changed into idle mode

DL_SPI_IIDX_TX_EMPTY 

SPI interrupt index for transmit FIFO empty

DL_SPI_IIDX_TX 

SPI interrupt index for transmit FIFO

DL_SPI_IIDX_RX 

SPI interrupt index for receive FIFO

DL_SPI_IIDX_RX_TIMEOUT 

SPI interrupt index for receive timeout

DL_SPI_IIDX_RX_FULL 

SPI interrupt index for receive FIFO full

DL_SPI_IIDX_TX_UNDERFLOW 

SPI interrupt index for transmit FIFO underflow

DL_SPI_IIDX_PARITY_ERROR 

SPI interrupt index for parity error

DL_SPI_IIDX_RX_OVERFLOW 

SPI interrupt index for receive FIFO overflow

§ DL_SPI_CLOCK_DIVIDE_RATIO

Enumerator
DL_SPI_CLOCK_DIVIDE_RATIO_1 

SPI source clock divide ratio set to 1

DL_SPI_CLOCK_DIVIDE_RATIO_2 

SPI source clock divide ratio set to 2

DL_SPI_CLOCK_DIVIDE_RATIO_3 

SPI source clock divide ratio set to 3

DL_SPI_CLOCK_DIVIDE_RATIO_4 

SPI source clock divide ratio set to 4

DL_SPI_CLOCK_DIVIDE_RATIO_5 

SPI source clock divide ratio set to 5

DL_SPI_CLOCK_DIVIDE_RATIO_6 

SPI source clock divide ratio set to 6

DL_SPI_CLOCK_DIVIDE_RATIO_7 

SPI source clock divide ratio set to 7

DL_SPI_CLOCK_DIVIDE_RATIO_8 

SPI source clock divide ratio set to 8

§ DL_SPI_CLOCK

Enumerator
DL_SPI_CLOCK_BUSCLK 

Selects BUSCLK as the clock source

DL_SPI_CLOCK_MFCLK 

Selects MFCLK as the clock source

DL_SPI_CLOCK_LFCLK 

Selects LFCLK as the clock source

Function Documentation

§ DL_SPI_init()

void DL_SPI_init ( SPI_Regs *  spi,
const DL_SPI_Config config 
)

Initialize the SPI peripheral.

Initializes all the common configurable options for the SPI peripheral. Any other custom configuration can be done after calling this API. The SPI is not enabled in this API.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]configConfiguration for SPI peripheral

§ DL_SPI_enablePower()

__STATIC_INLINE void DL_SPI_enablePower ( SPI_Regs *  spi)

Enables the Peripheral Write Enable (PWREN) register for the SPI.

Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.

Note
For power savings, please refer to DL_SPI_enable
Parameters
spiPointer to the register overlay for the peripheral

§ DL_SPI_disablePower()

__STATIC_INLINE void DL_SPI_disablePower ( SPI_Regs *  spi)

Disables the Peripheral Write Enable (PWREN) register for the SPI.

When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.

Note
This API does not provide large power savings. For power savings, please refer to DL_SPI_enable
Parameters
spiPointer to the register overlay for the peripheral

§ DL_SPI_isPowerEnabled()

__STATIC_INLINE bool DL_SPI_isPowerEnabled ( const SPI_Regs *  spi)

Returns if the Peripheral Write Enable (PWREN) register for the SPI is enabled.

Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.

When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.

Parameters
spiPointer to the register overlay for the peripheral
Returns
true if peripheral register access is enabled
false if peripheral register access is disabled

§ DL_SPI_reset()

__STATIC_INLINE void DL_SPI_reset ( SPI_Regs *  spi)

Resets spi peripheral.

Parameters
spiPointer to the register overlay for the peripheral

§ DL_SPI_isReset()

__STATIC_INLINE bool DL_SPI_isReset ( const SPI_Regs *  spi)

Returns if spi peripheral was reset.

Parameters
spiPointer to the register overlay for the peripheral
Returns
true if peripheral was reset
false if peripheral wasn't reset

§ DL_SPI_enable()

__STATIC_INLINE void DL_SPI_enable ( SPI_Regs *  spi)

Enable the SPI peripheral.

Parameters
[in]spiPointer to the register overlay for the peripheral

§ DL_SPI_isEnabled()

__STATIC_INLINE bool DL_SPI_isEnabled ( const SPI_Regs *  spi)

Checks if the SPI peripheral is enabled.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the enabled status of the SPI
Return values
trueThe SPI peripheral is enabled
falseThe SPI peripheral is disabled

§ DL_SPI_disable()

__STATIC_INLINE void DL_SPI_disable ( SPI_Regs *  spi)

Disable the SPI peripheral.

Parameters
[in]spiPointer to the register overlay for the peripheral

References DL_SPI_getClockConfig(), and DL_SPI_setClockConfig().

§ DL_SPI_setClockConfig()

void DL_SPI_setClockConfig ( SPI_Regs *  spi,
const DL_SPI_ClockConfig config 
)

Configure SPI source clock.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]configPointer to the clock configuration struct DL_SPI_ClockConfig.

Referenced by DL_SPI_disable().

§ DL_SPI_getClockConfig()

void DL_SPI_getClockConfig ( const SPI_Regs *  spi,
DL_SPI_ClockConfig config 
)

Get SPI source clock configuration.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]configPointer to the clock configuration struct DL_SPI_ClockConfig.

Referenced by DL_SPI_disable().

§ DL_SPI_isBusy()

__STATIC_INLINE bool DL_SPI_isBusy ( const SPI_Regs *  spi)

Checks if the SPI is busy transmitting.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the busy status of the SPI
Return values
trueThe SPI is transmitting
falseThe SPI is idle

§ DL_SPI_isTXFIFOEmpty()

__STATIC_INLINE bool DL_SPI_isTXFIFOEmpty ( const SPI_Regs *  spi)

Checks if the TX FIFO is empty.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the empty status of the TX FIFO
Return values
trueThe TX FIFO is empty
falseThe TX FIFO is not empty

§ DL_SPI_isTXFIFOFull()

__STATIC_INLINE bool DL_SPI_isTXFIFOFull ( const SPI_Regs *  spi)

Checks if the TX FIFO is full.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the full status of the TX FIFO
Return values
trueThe TX FIFO is full
falseThe TX FIFO is not full

§ DL_SPI_isRXFIFOEmpty()

__STATIC_INLINE bool DL_SPI_isRXFIFOEmpty ( const SPI_Regs *  spi)

Checks if the RX FIFO is empty.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the empty status of the RX FIFO
Return values
trueThe RX FIFO is empty
falseThe RX FIFO is not empty

§ DL_SPI_isRXFIFOFull()

__STATIC_INLINE bool DL_SPI_isRXFIFOFull ( const SPI_Regs *  spi)

Checks if the RX FIFO is full.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
Returns the full status of the RX FIFO
Return values
trueThe RX FIFO is full
falseThe RX FIFO is not full

§ DL_SPI_setParity()

__STATIC_INLINE void DL_SPI_setParity ( SPI_Regs *  spi,
DL_SPI_PARITY  parity 
)

Sets the parity configuration used for transactions.

This API sets the configuration for both receive parity and transmit parity. This includes which bit is used, and whether even or odd parity is set.

To individually enable or dsiable the receive or transmit parity, refer to the APIs listed below.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]parityParity configuration to use. One of DL_SPI_PARITY.
See also
DL_SPI_init
DL_SPI_enableReceiveParity
DL_SPI_disableReceiveParity
DL_SPI_enableTransmitParity
DL_SPI_disableTransmitParity

References DL_Common_updateReg().

§ DL_SPI_getParity()

__STATIC_INLINE DL_SPI_PARITY DL_SPI_getParity ( const SPI_Regs *  spi)

Get the current receive and transmit parity configuration.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The current parity configuration being used
Return values
Oneof DL_SPI_PARITY

§ DL_SPI_enableReceiveParity()

__STATIC_INLINE void DL_SPI_enableReceiveParity ( SPI_Regs *  spi)

Enables receive parity.

This API only enables receive parity, it does not configure the parity mode used.

Parameters
[in]spipointer to the register overlay for the peripheral
See also
DL_SPI_setParity

§ DL_SPI_disableReceiveParity()

__STATIC_INLINE void DL_SPI_disableReceiveParity ( SPI_Regs *  spi)

Disables receive parity.

This API only disable receive parity, it does not configure the parity mode used.

Parameters
[in]spipointer to the register overlay for the peripheral
See also
DL_SPI_setParity

§ DL_SPI_isReceiveParityEnabled()

__STATIC_INLINE bool DL_SPI_isReceiveParityEnabled ( const SPI_Regs *  spi)

Checks if receive parity is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
If receive parity is enabled
Return values
trueReceive parity is enabled
falseReceive parity is disabled

§ DL_SPI_enableTransmitParity()

__STATIC_INLINE void DL_SPI_enableTransmitParity ( SPI_Regs *  spi)

Enables transmit parity.

This API only enables transmit parity, it does not configure the parity mode used.

Parameters
[in]spipointer to the register overlay for the peripheral
See also
DL_SPI_setParity

§ DL_SPI_disableTransmitParity()

__STATIC_INLINE void DL_SPI_disableTransmitParity ( SPI_Regs *  spi)

Disables transmit parity.

This API only disables transmit parity, it does not configure the parity mode used.

Parameters
[in]spipointer to the register overlay for the peripheral
See also
DL_SPI_setParity

§ DL_SPI_isTransmitParityEnabled()

__STATIC_INLINE bool DL_SPI_isTransmitParityEnabled ( const SPI_Regs *  spi)

Checks if transmit parity is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
If transmit parity is enabled
Return values
trueTransmit parity is enabled
falseTransmit parity is disabled

§ DL_SPI_setFrameFormat()

__STATIC_INLINE void DL_SPI_setFrameFormat ( SPI_Regs *  spi,
DL_SPI_FRAME_FORMAT  frameFormat 
)

Set the frame format to use.

Configures the frame format to use for transactions. If you are using chip select you must use one of the Motorola 4 wire frame formats.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]frameFormatFrame format to use. One of DL_SPI_FRAME_FORMAT.
See also
DL_SPI_init

References DL_Common_updateReg().

§ DL_SPI_getFrameFormat()

__STATIC_INLINE DL_SPI_FRAME_FORMAT DL_SPI_getFrameFormat ( const SPI_Regs *  spi)

Get the frame format configuration.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The current frame format being used
Return values
Oneof DL_SPI_FRAME_FORMAT

§ DL_SPI_setDataSize()

__STATIC_INLINE void DL_SPI_setDataSize ( SPI_Regs *  spi,
DL_SPI_DATA_SIZE  dataSize 
)

Set the size for transfers.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]dataSizeNumber of bits used in a transfer. One of DL_SPI_DATA_SIZE
See also
DL_SPI_init

References DL_Common_updateReg().

§ DL_SPI_getDataSize()

__STATIC_INLINE DL_SPI_DATA_SIZE DL_SPI_getDataSize ( const SPI_Regs *  spi)

Get the configured size for transfers.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The currently configured size for transfers
Return values
Oneof DL_SPI_DATA_SIZE

§ DL_SPI_setMode()

__STATIC_INLINE void DL_SPI_setMode ( SPI_Regs *  spi,
DL_SPI_MODE  mode 
)

Set whether the device should be in controller/peripheral mode.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]modeMode to configure the SPI into. One of DL_SPI_MODE.
See also
DL_SPI_init

References DL_Common_updateReg().

§ DL_SPI_getMode()

__STATIC_INLINE DL_SPI_MODE DL_SPI_getMode ( const SPI_Regs *  spi)

Get the current mode for the SPI (controller/peripheral)

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The currently configured mode for the SPI (controller/peripheral)
Return values
Oneof DL_SPI_MODE.

§ DL_SPI_setBitOrder()

__STATIC_INLINE void DL_SPI_setBitOrder ( SPI_Regs *  spi,
DL_SPI_BIT_ORDER  bitOrder 
)

Set the bit order used for transfers.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]bitOrderOrder for bits to be sent out during transfer. One of DL_SPI_BIT_ORDER.
See also
DL_SPI_init

References DL_Common_updateReg().

§ DL_SPI_getBitOrder()

__STATIC_INLINE DL_SPI_BIT_ORDER DL_SPI_getBitOrder ( const SPI_Regs *  spi)

Get the current bit order used for transfers.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The currently configured bit order
Return values
Oneof DL_SPI_BIT_ORDER.

§ DL_SPI_enableLoopbackMode()

__STATIC_INLINE void DL_SPI_enableLoopbackMode ( SPI_Regs *  spi)

Enables loopback mode.

Enables the loopback mode. When enabled, the output of the transmit serial shifter is connected to the input of the receive serial shifter internally.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_disableLoopbackMode()

__STATIC_INLINE void DL_SPI_disableLoopbackMode ( SPI_Regs *  spi)

Disables loopback mode.

Disables the loopback mode. When disabled, the transmit serial shifter and receive serial shifter are not connected internally.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_isLoopbackModeEnabled()

__STATIC_INLINE bool DL_SPI_isLoopbackModeEnabled ( const SPI_Regs *  spi)

Checks if the loopback mode is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The status of the loopback mode
Return values
trueif loopback mode is enabled
falseif loopback mode is disabled

§ DL_SPI_setRepeatTransmit()

__STATIC_INLINE void DL_SPI_setRepeatTransmit ( SPI_Regs *  spi,
uint32_t  numRepeats 
)

Set counter for repeated transmit.

Repeated transmit allows you to send the same data multiple times. This is essentially the same as writing the data into the transmit buffer repeatedly.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]numRepeatsnumber of times to repeat the transfer. Should be a value between 0-255.
  • 0 disables the repeated transfer
  • 1-255 repeats that many times. So will be sent numRepeats + 1 times in total.

References DL_Common_updateReg().

§ DL_SPI_getRepeatTransmit()

__STATIC_INLINE uint32_t DL_SPI_getRepeatTransmit ( const SPI_Regs *  spi)

Get counter for repeated transmit.

Repeated transmit allows you to send the same data multiple times. This is essentially the same as writing the data into the transmit buffer repeatedly.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
Number of repeats used for transfer
Return values
0Repeated transfer is disabled
1-255Repeat that many times.

§ DL_SPI_enablePeripheralAlignDataOnChipSelect()

__STATIC_INLINE void DL_SPI_enablePeripheralAlignDataOnChipSelect ( SPI_Regs *  spi)

Enables data alignment on chip select for peripherals.

When enabled, the receieve bit counter is cleared automatically when the chip select gets set inactive. This helps the peripheral synchronize again to the controller in case of a disturbance or glitch on the clock line or during initialization.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_disablePeripheralAlignDataOnChipSelect()

__STATIC_INLINE void DL_SPI_disablePeripheralAlignDataOnChipSelect ( SPI_Regs *  spi)

Disables data alignment on chip select for peripherals.

When disable, the receieve bit counter is not cleared automatically when the chip select gets set inactive.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_isPeripheralAlignDataOnChipSelectEnabled()

__STATIC_INLINE bool DL_SPI_isPeripheralAlignDataOnChipSelectEnabled ( const SPI_Regs *  spi)

Checks if data alignment on chip select for peripherals is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The status of data alignment on chip select
Return values
trueData alignment on chip select is enabled
falseData alignment on chip select is disabled

§ DL_SPI_enablePacking()

__STATIC_INLINE void DL_SPI_enablePacking ( SPI_Regs *  spi)

Enables packing feature.

When enabled, two entries of the RX FIFO are returned as a 32-bit value. When reading the TX FIFO, if the last write to that field was a 32-bit write, those 32-bits will be returned. When writing to the TX FIFO, a 32-bit write will be written as one FIFO entry.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_disablePacking()

__STATIC_INLINE void DL_SPI_disablePacking ( SPI_Regs *  spi)

Disables packing feature.

When disabled, 1 entry of the RX FIFO is returned as a 16-bit value. When reading the TX FIFO, if the last write to that field was a 16-bit write, those 16-bits wil be returned. When writing to the TX FIFO, a 32-bit write will be written as two FIFO entries.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_isPackingEnabled()

__STATIC_INLINE bool DL_SPI_isPackingEnabled ( const SPI_Regs *  spi)

Checks if packing feature is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
If packing is enabled
Return values
truePacking is enabled
falsePacking is disabled

§ DL_SPI_setChipSelect()

__STATIC_INLINE void DL_SPI_setChipSelect ( SPI_Regs *  spi,
DL_SPI_CHIP_SELECT  chipSelect 
)

Set chip select used for controller or peripheral mode.

Choose which chip select should be used for data transfer. User must ensure one of the 4-wire frame formats were selected using DL_SPI_init or DL_SPI_setFrameFormat.

This API is for both controller and peripheral modes, and the chip select can be changed in the application by calling this API.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]chipSelectthe chip select pin to use. One of DL_SPI_CHIP_SELECT.

References DL_Common_updateReg().

§ DL_SPI_getChipSelect()

__STATIC_INLINE DL_SPI_CHIP_SELECT DL_SPI_getChipSelect ( const SPI_Regs *  spi)

Get chip select used for controller or peripheral mode.

This API is for both controller and peripheral modes.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The current chip selected used for data transfer
Return values
Oneof DL_SPI_CHIP_SELECT.

§ DL_SPI_setPeripheralReceiveTimeout()

__STATIC_INLINE void DL_SPI_setPeripheralReceiveTimeout ( SPI_Regs *  spi,
uint32_t  timeout 
)

Set peripheral receive timeout.

Sets the number of clock cycles before a receive timeout occurs.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]timeoutNumber of clock cycles before a receive timeout occurs. Must be between 0-63.
  • 0 Disables receive timeout
  • 1-63 Number of clock cycles before timeout

References DL_Common_updateReg().

§ DL_SPI_getPeripheralReceiveTimeout()

__STATIC_INLINE uint32_t DL_SPI_getPeripheralReceiveTimeout ( const SPI_Regs *  spi)

Get peripheral receive timeout.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The current amount of cycles used for a peripheral timeout
Return values
0indicating that receive timeout is disabled
1-63number of clock cycles before a receive timeout occurs

§ DL_SPI_setControllerCommandDataModeConfig()

__STATIC_INLINE void DL_SPI_setControllerCommandDataModeConfig ( SPI_Regs *  spi,
uint32_t  config 
)

Configure the command/data mode.

Command/data mode allows the hardware to control the C/D pin to indicate whether the data being transferred is a command or just data. The C/D pin is low for commands and high for data.

You can use this API to manually set the C/D pin by passing in DL_SPI_CD_MODE_DATA or DL_SPI_CD_MODE_COMMAND. You can also have the C/D pin switch automatically by passing in how many bytes are part of the command transfer. The C/D pin will stay low until that many bytes are sent out and then automatically switch to high.

This is only relevant when in controller mode.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]configconfiguration for command/data mode. One of:
  • DL_SPI_CD_MODE_DATA
  • DL_SPI_CD_MODE_COMMAND
  • A value between 1-14 to indicate how many bytes should be sent as command

References DL_Common_updateReg().

§ DL_SPI_getControllerCommandDataModeConfig()

__STATIC_INLINE uint32_t DL_SPI_getControllerCommandDataModeConfig ( const SPI_Regs *  spi)

Get the command/data mode configuration.

Returns the current configuration for command/data mode. When using the automatic C/D pin the value read back will be the number of command bytes remaining to be sent.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The current configuration for command/data mode
Return values
DL_SPI_CD_MODE_DATAif in manual data mode
DL_SPI_CD_MODE_COMMANDif in manual command mode
1-14indicating how many command bytes still need to be sent

§ DL_SPI_enableControllerCommandDataMode()

__STATIC_INLINE void DL_SPI_enableControllerCommandDataMode ( SPI_Regs *  spi)

Enables command/data mode.

When command/data mode is enabled, the C/D pin is used to differentiate between command and data during the transaction.

Parameters
[in]spipointer to the register overlay for the peripheral
See also
DL_SPI_setControllerCommandDataModeConfig

§ DL_SPI_disableControllerCommandDataMode()

__STATIC_INLINE void DL_SPI_disableControllerCommandDataMode ( SPI_Regs *  spi)

Disables command/data mode.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_isControllerCommandDataModeEnabled()

__STATIC_INLINE bool DL_SPI_isControllerCommandDataModeEnabled ( const SPI_Regs *  spi)

Checks if command/data mode is enabled.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The status of command/data mode
Return values
trueCommand/data mode is enabled
falseCommand/data mode is disabled

§ DL_SPI_enablePeripheralDataOutput()

__STATIC_INLINE void DL_SPI_enablePeripheralDataOutput ( SPI_Regs *  spi)

Enables peripheral data output.

When peripheral data output is enabled, the peripheral can drive the POCI output pin. This will cause problems if all peripherals have their RXD lines tied together and the controller is trying to broadcast a message to all peripherals while ensuring only one peripheral drives data onto its serial output line.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_disablePeripheralDataOutput()

__STATIC_INLINE void DL_SPI_disablePeripheralDataOutput ( SPI_Regs *  spi)

Disables peripheral data output.

When peripheral data output is disabled, the peripheral cannot drive the POCI output pin. This allows multiple peripherals that have their RXD lines tied together to receive a broadcasted message from a controller.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral

§ DL_SPI_isPeripheralDataOutputEnabled()

__STATIC_INLINE bool DL_SPI_isPeripheralDataOutputEnabled ( const SPI_Regs *  spi)

Checks if peripheral data output is enabled.

This is only relevant when in peripheral mode.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
If peripheral data output is enabled
Return values
trueif peripheral data output is enabled
falseif peripheral data output is disabled

§ DL_SPI_setDelayedSampling()

__STATIC_INLINE void DL_SPI_setDelayedSampling ( SPI_Regs *  spi,
uint32_t  delay 
)

Set the delay sampling.

In controller mode only, the data on the input pin will be delayed sampled by the defined SPI clock cycles. The delay can be adjusted in steps of SPI input clock steps. The maximum allowed delay should not exceed the length of one data frame

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]delayThe number of SPI clock cycles to delay sampling on input pin. Value between 0-15.

References DL_Common_updateReg().

§ DL_SPI_getDelayedSampling()

__STATIC_INLINE uint32_t DL_SPI_getDelayedSampling ( const SPI_Regs *  spi)

Get the delay sampling.

In controller mode only, the data on the input pin will be delayed sampled by the defined SPI clock cycles. The delay can be adjusted in steps of SPI input clock steps. The maximum allowed delay should not exceed the length of one data frame

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The amount of delay sampling on the input pin in SPI clock cycles.
Return values
0- 15. The amount of delay sampling in SPI clock cycles.

§ DL_SPI_setFIFOThreshold()

__STATIC_INLINE void DL_SPI_setFIFOThreshold ( SPI_Regs *  spi,
DL_SPI_RX_FIFO_LEVEL  rxThreshold,
DL_SPI_TX_FIFO_LEVEL  txThreshold 
)

Set the RX and TX FIFO interrupt threshold level.

Select the threshold for the receive and transmit FIFO interrupts. The interrupts are generated based on a transition through a level rather than being based on the level. That is, the interrupts are generated when the fill level progresses through the trigger level.

For example, if the trigger level is set to the half-way mark, the interrupt is triggered when the FIFO becomes half empty/full.

Out of reset, the FIFOs are triggered to interrupt at half-way mark.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]rxThresholdOne of DL_SPI_RX_FIFO_LEVEL
[in]txThresholdOne of DL_SPI_TX_FIFO_LEVEL

References DL_Common_updateReg().

§ DL_SPI_getTXFIFOThreshold()

__STATIC_INLINE DL_SPI_TX_FIFO_LEVEL DL_SPI_getTXFIFOThreshold ( const SPI_Regs *  spi)

Get the TX FIFO interrupt threshold level.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The TX FIFO interrupt threshold level
Return values
Oneof DL_SPI_TX_FIFO_LEVEL

§ DL_SPI_getRXFIFOThreshold()

__STATIC_INLINE DL_SPI_RX_FIFO_LEVEL DL_SPI_getRXFIFOThreshold ( const SPI_Regs *  spi)

Get the RX FIFO interrupt threshold level.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The RX FIFO interrupt threshold level
Return values
Oneof DL_SPI_RX_FIFO_LEVEL

§ DL_SPI_setBitRateSerialClockDivider()

__STATIC_INLINE void DL_SPI_setBitRateSerialClockDivider ( SPI_Regs *  spi,
uint32_t  SCR 
)

Set the SPI bit rate serial clock divider (SCR)

The SPI includes a programmable bit rate clock divider and prescaler to generate the serial output clock. The bit rates are supported up to FUNCCLK/2. The functional clock selection depends on the specific device, please refer to the device datasheet and PMU/Clock section.

The SPI output bit rate is calculated with the following formula: SPI bit rate = (SPI functional clock) / ((1 + SCR)*2) Given this formula, the SCR can be calculated: SCR = (SPI functional clock) / ((2 * SPI bit rate) - 1)

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]SCRThe SPI serial clock divider. Value between 0-1023.

References DL_Common_updateReg().

§ DL_SPI_getBitRateSerialClockDivider()

__STATIC_INLINE uint32_t DL_SPI_getBitRateSerialClockDivider ( const SPI_Regs *  spi)

Get the SPI bit rate serial clock divider (SCR)

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The current bit rate serial clock divider
Return values
TheSPI SCR. Value from 0-1023

§ DL_SPI_transmitData8()

__STATIC_INLINE void DL_SPI_transmitData8 ( SPI_Regs *  spi,
uint8_t  data 
)

Writes 8-bit data into the TX FIFO for transmit.

Puts the data into the TX FIFO without checking its status. Use if already sure the TX FIFO has space for the write. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_transmitDataBlocking8
DL_SPI_transmitDataCheck8

§ DL_SPI_transmitData16()

__STATIC_INLINE void DL_SPI_transmitData16 ( SPI_Regs *  spi,
uint16_t  data 
)

Writes 16-bit data into the TX FIFO for transmit.

Puts the data into the TX FIFO without checking its status. Use if already sure the TX FIFO has space for the write. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_transmitDataBlocking16
DL_SPI_transmitDataCheck16

§ DL_SPI_transmitData32()

__STATIC_INLINE void DL_SPI_transmitData32 ( SPI_Regs *  spi,
uint32_t  data 
)

Writes 32-bit data into the TX FIFO for transmit.

Puts the data into the TX FIFO without checking its status. Use if already sure the TX FIFO has space for the write. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: If packing is enabled by calling DL_SPI_enablePacking prior to calling this API, then a 32-bit write will be written as one FIFO entry. If packing is disabled, then a 32-bit write will be written as two FIFO entries.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_enablePacking
DL_SPI_transmitDataBlocking32
DL_SPI_transmitDataCheck32

§ DL_SPI_receiveData8()

__STATIC_INLINE uint8_t DL_SPI_receiveData8 ( const SPI_Regs *  spi)

Reads 8-bit data from the RX FIFO.

Reads the data from the RX FIFO without checking its status. Use if already sure the RX FIFO has data available. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
See also
DL_SPI_receiveDataBlocking8
DL_SPI_receiveDataCheck8

§ DL_SPI_receiveData16()

__STATIC_INLINE uint16_t DL_SPI_receiveData16 ( const SPI_Regs *  spi)

Reads 16-bit data from the RX FIFO.

Reads the data from the RX FIFO without checking its status. Use if already sure the RX FIFO has data available. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
See also
DL_SPI_receiveDataBlocking16
DL_SPI_receiveDataCheck16

§ DL_SPI_receiveData32()

__STATIC_INLINE uint32_t DL_SPI_receiveData32 ( const SPI_Regs *  spi)

Reads 32-bit data from the RX FIFO.

Reads the data from the RX FIFO without checking its status. Use if already sure the RX FIFO has data available. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: Requires that packing has been enabled by calling DL_SPI_enablePacking prior to calling this API. When packing is enabled, two entries of the RX FIFO are returned as a 32-bit value.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
Precondition
DL_SPI_enablePacking
See also
DL_SPI_receiveDataBlocking32
DL_SPI_receiveDataCheck32

§ DL_SPI_enableInterrupt()

__STATIC_INLINE void DL_SPI_enableInterrupt ( SPI_Regs *  spi,
uint32_t  interruptMask 
)

Enable SPI interrupts.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to enable. Bitwise OR of DL_SPI_INTERRUPT.

§ DL_SPI_disableInterrupt()

__STATIC_INLINE void DL_SPI_disableInterrupt ( SPI_Regs *  spi,
uint32_t  interruptMask 
)

Disable SPI interrupts.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to disable. Bitwise OR of DL_SPI_INTERRUPT.

§ DL_SPI_getEnabledInterrupts()

__STATIC_INLINE uint32_t DL_SPI_getEnabledInterrupts ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check which SPI interrupts are enabled.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_INTERRUPT.
Returns
Which of the requested SPI interrupts are enabled
Return values
BitwiseOR of DL_SPI_INTERRUPT values

§ DL_SPI_getEnabledInterruptStatus()

__STATIC_INLINE uint32_t DL_SPI_getEnabledInterruptStatus ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check interrupt flag of enabled SPI interrupts.

Checks if any of the SPI interrupts that were previously enabled are pending.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_INTERRUPT.
Returns
Which of the requested SPI interrupts are pending
Return values
BitwiseOR of DL_SPI_INTERRUPT values
See also
DL_SPI_enableInterrupt

§ DL_SPI_getRawInterruptStatus()

__STATIC_INLINE uint32_t DL_SPI_getRawInterruptStatus ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check interrupt flag of any SPI interrupt.

Checks if any of the SPI interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_INTERRUPT.
Returns
Which of the requested SPI interrupts are pending
Return values
BitwiseOR of DL_SPI_INTERRUPT values

§ DL_SPI_getPendingInterrupt()

__STATIC_INLINE DL_SPI_IIDX DL_SPI_getPendingInterrupt ( const SPI_Regs *  spi)

Get highest priority pending SPI interrupt.

Checks if any of the SPI interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The highest priority pending SPI interrupt. One of DL_SPI_IIDX

§ DL_SPI_clearInterruptStatus()

__STATIC_INLINE void DL_SPI_clearInterruptStatus ( SPI_Regs *  spi,
uint32_t  interruptMask 
)

§ DL_SPI_transmitDataBlocking8()

void DL_SPI_transmitDataBlocking8 ( SPI_Regs *  spi,
uint8_t  data 
)

Blocks to ensure transmit is ready before sending data.

Puts the data into the TX FIFO after blocking to ensure the TX FIFO is not full. Will wait indefinitely until there is space in the TX FIFO. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_transmitData8
DL_SPI_transmitDataCheck8

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_transmitDataBlocking16()

void DL_SPI_transmitDataBlocking16 ( SPI_Regs *  spi,
uint16_t  data 
)

Blocks to ensure transmit is ready before sending data.

Puts the data into the TX FIFO after blocking to ensure the TX FIFO is not full. Will wait indefinitely until there is space in the TX FIFO. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_transmitData16
DL_SPI_transmitDataCheck16

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_transmitDataBlocking32()

void DL_SPI_transmitDataBlocking32 ( SPI_Regs *  spi,
uint32_t  data 
)

Blocks to ensure transmit is ready before sending data.

Puts the data into the TX FIFO after blocking to ensure the TX FIFO is not full. Will wait indefinitely until there is space in the TX FIFO. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: If packing is enabled by calling DL_SPI_enablePacking prior to calling this API, then a 32-bit write will be written as one FIFO entry. If packing is disabled, then a 32-bit write will be written as two FIFO entries.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
See also
DL_SPI_enablePacking
DL_SPI_transmitData32
DL_SPI_transmitDataCheck32

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataBlocking8()

uint8_t DL_SPI_receiveDataBlocking8 ( const SPI_Regs *  spi)

Blocks to ensure receive is ready before reading data.

Reads the data from the RX FIFO after blocking to ensure the RX FIFO is not empty. Will wait indefinitely until there is data in the RX FIFO. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
See also
DL_SPI_transmitData8
DL_SPI_transmitDataCheck8

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataBlocking16()

uint16_t DL_SPI_receiveDataBlocking16 ( const SPI_Regs *  spi)

Blocks to ensure receive is ready before reading data.

Reads the data from the RX FIFO after blocking to ensure the RX FIFO is not empty. Will wait indefinitely until there is data in the RX FIFO. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
See also
DL_SPI_transmitData16
DL_SPI_transmitDataCheck16

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataBlocking32()

uint32_t DL_SPI_receiveDataBlocking32 ( const SPI_Regs *  spi)

Blocks to ensure receive is ready before reading data.

Reads the data from the RX FIFO after blocking to ensure the RX FIFO is not empty. Will wait indefinitely until there is data in the RX FIFO. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: Requires that packing has been enabled by calling DL_SPI_enablePacking prior to calling this API. When packing is enabled, two entries of the RX FIFO are returned as a 32-bit value.

Parameters
[in]spipointer to the register overlay for the peripheral
Returns
The data in the RX FIFO
Precondition
DL_SPI_enablePacking
See also
DL_SPI_transmitData32
DL_SPI_transmitDataCheck32

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_transmitDataCheck8()

bool DL_SPI_transmitDataCheck8 ( SPI_Regs *  spi,
uint8_t  data 
)

Checks the TX FIFO before trying to transmit data.

Checks if the TX FIFO is already full before trying to add new data to the FIFO. Exits immediately if full rather than trying to block. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
Returns
If the transmit occurred
Return values
trueif data was added to the TX FIFO
falseif the TX FIFO was full and data was not added
See also
DL_SPI_transmitData8
DL_SPI_transmitDataBlocking8

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_transmitDataCheck16()

bool DL_SPI_transmitDataCheck16 ( SPI_Regs *  spi,
uint16_t  data 
)

Checks the TX FIFO before trying to transmit data.

Checks if the TX FIFO is already full before trying to add new data to the FIFO. Exits immediately if full rather than trying to block. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
Returns
If the transmit occurred
Return values
trueif data was added to the TX FIFO
falseif the TX FIFO was full and data was not added
See also
DL_SPI_transmitData16
DL_SPI_transmitDataBlocking16

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_transmitDataCheck32()

bool DL_SPI_transmitDataCheck32 ( SPI_Regs *  spi,
uint32_t  data 
)

Checks the TX FIFO before trying to transmit data.

Checks if the TX FIFO is already full before trying to add new data to the FIFO. Exits immediately if full rather than trying to block. See related APIs for additional transmit options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: If packing is enabled by calling DL_SPI_enablePacking prior to calling this API, then a 32-bit write will be written as one FIFO entry. If packing is disabled, then a 32-bit write will be written as two FIFO entries.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]datadata to send
Returns
If the transmit occurred
Return values
trueif data was added to the TX FIFO
falseif the TX FIFO was full and data was not added
See also
DL_SPI_enablePacking
DL_SPI_transmitData32
DL_SPI_transmitDataBlocking32

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataCheck8()

bool DL_SPI_receiveDataCheck8 ( const SPI_Regs *  spi,
uint8_t *  buffer 
)

Checks the RX FIFO before trying to transmit data.

Checks if the RX FIFO is already empty before trying to read new data from the FIFO. Exits immediately if empty rather than trying to block. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 8 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]buffera buffer to write the received data into
Returns
If the receive occurred
Return values
trueif data was read from the RX FIFO
falseif the RX FIFO was empty and data was not read
See also
DL_SPI_receiveData8
DL_SPI_receiveDataBlocking8

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataCheck16()

bool DL_SPI_receiveDataCheck16 ( const SPI_Regs *  spi,
uint16_t *  buffer 
)

Checks the RX FIFO before trying to transmit data.

Checks if the RX FIFO is already empty before trying to read new data from the FIFO. Exits immediately if empty rather than trying to block. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 16 bits.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]buffera buffer to write the received data into
Returns
If the receive occurred
Return values
trueif data was read from the RX FIFO
falseif the RX FIFO was empty and data was not read
See also
DL_SPI_receiveData16
DL_SPI_receiveDataBlocking16

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_receiveDataCheck32()

bool DL_SPI_receiveDataCheck32 ( const SPI_Regs *  spi,
uint32_t *  buffer 
)

Checks the RX FIFO before trying to transmit data.

Checks if the RX FIFO is already empty before trying to read new data from the FIFO. Exits immediately if empty rather than trying to block. See related APIs for additional receive options.

Can be used for any data transfers that are less than or equal to 32 bits.

NOTE: Requires that packing has been enabled by calling DL_SPI_enablePacking prior to calling this API. When packing is enabled, two entries of the RX FIFO are returned as a 32-bit value.

Parameters
[in]spipointer to the register overlay for the peripheral
[in]buffera buffer to write the received data into
Returns
If the receive occurred
Return values
trueif data was read from the RX FIFO
falseif the RX FIFO was empty and data was not read
Precondition
DL_SPI_enablePacking
See also
DL_SPI_receiveData32
DL_SPI_receiveDataBlocking32

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_drainRXFIFO8()

uint32_t DL_SPI_drainRXFIFO8 ( const SPI_Regs *  spi,
uint8_t *  buffer,
uint32_t  maxCount 
)

Read all available data out of the RX FIFO using 8 bit access.

Parameters
[in]spiPointer to the register overlay for the peripheral
[out]bufferBuffer to write received data into
[in]maxCountMax number of bytes to read from the RX FIFO
Returns
Number of bytes read from the RX FIFO

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_drainRXFIFO16()

uint32_t DL_SPI_drainRXFIFO16 ( const SPI_Regs *  spi,
uint16_t *  buffer,
uint32_t  maxCount 
)

Read all available data out of the RX FIFO using 16 bit access.

Parameters
[in]spiPointer to the register overlay for the peripheral
[out]bufferBuffer to write received data into
[in]maxCountMax number of halfwords to read from the RX FIFO
Returns
Number of halfwords read from the RX FIFO

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_drainRXFIFO32()

uint32_t DL_SPI_drainRXFIFO32 ( const SPI_Regs *  spi,
uint32_t *  buffer,
uint32_t  maxCount 
)

Read all available data out of the RX FIFO using 32 bit access.

NOTE: Requires that packing has been enabled by calling DL_SPI_enablePacking prior to calling this API. When packing is enabled, two entries of the RX FIFO are returned as a 32-bit value.

Parameters
[in]spiPointer to the register overlay for the peripheral
[out]bufferBuffer to write received data into
[in]maxCountMax number of words to read from the RX FIFO
Returns
Number of words read from the RX FIFO
Precondition
DL_SPI_enablePacking

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_fillTXFIFO8()

uint32_t DL_SPI_fillTXFIFO8 ( SPI_Regs *  spi,
const uint8_t *  buffer,
uint32_t  count 
)

Fill the TX FIFO using 8 bit access.

Continuously write data into the TX FIFO until it is filled up or count has been reached.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]bufferBuffer of data to write to the TX FIFO
[in]countMax number of bytes to write to the TX FIFO
Returns
Number of bytes written to the TX FIFO

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_fillTXFIFO16()

uint32_t DL_SPI_fillTXFIFO16 ( SPI_Regs *  spi,
const uint16_t *  buffer,
uint32_t  count 
)

Fill the TX FIFO using 16 bit access.

Continuously write data into the TX FIFO until it is filled up or count has been reached.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]bufferBuffer of data to write to the TX FIFO
[in]countMax number of halfwords to write to the TX FIFO
Returns
Number of halfwords written to the TX FIFO

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_fillTXFIFO32()

uint32_t DL_SPI_fillTXFIFO32 ( SPI_Regs *  spi,
const uint32_t *  buffer,
uint32_t  count 
)

Fill the TX FIFO using 32 bit access.

Continuously write data into the TX FIFO until it is filled up or count has been reached.

NOTE: If packing is enabled by calling DL_SPI_enablePacking prior to calling this API, then a 32-bit write will be written as one FIFO entry. If packing is disabled, then a 32-bit write will be written as two FIFO entries.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]bufferBuffer of data to write to the TX FIFO
[in]countMax number of words to write to the TX FIFO
Returns
Number of words written to the TX FIFO
See also
DL_SPI_enablePacking

Referenced by DL_SPI_clearInterruptStatus().

§ DL_SPI_enableDMAReceiveEvent()

__STATIC_INLINE void DL_SPI_enableDMAReceiveEvent ( SPI_Regs *  spi,
uint32_t  interrupt 
)

Enable SPI interrupt for triggering the DMA receive event.

Enables the SPI interrupt to be used as the condition to generate an event to directly trigger the DMA. This API configures the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Note
Only one interrupt source should be enabled at a time.
Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptInterrupt to enable as the trigger condition for the DMA. One of DL_SPI_DMA_INTERRUPT_RX.

§ DL_SPI_enableDMATransmitEvent()

__STATIC_INLINE void DL_SPI_enableDMATransmitEvent ( SPI_Regs *  spi)

Enable SPI interrupt for triggering the DMA transmit event.

Enables the SPI interrupt to be used as the condition to generate an event to directly trigger the DMA. This API configures the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Note
DMA_TRIG_TX only has one transmit interrupt source
Parameters
[in]spiPointer to the register overlay for the peripheral

§ DL_SPI_disableDMAReceiveEvent()

__STATIC_INLINE void DL_SPI_disableDMAReceiveEvent ( SPI_Regs *  spi,
uint32_t  interrupt 
)

Disables SPI interrupt from triggering the DMA receive event.

Disables the SPI interrupt as the condition to generate an event to directly trigger the DMA. This API configures the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptInterrupt to disable as the trigger condition for the DMA. One of DL_SPI_DMA_INTERRUPT_RX.

§ DL_SPI_disableDMATransmitEvent()

__STATIC_INLINE void DL_SPI_disableDMATransmitEvent ( SPI_Regs *  spi)

Disables SPI interrupt from triggering the DMA transmit event.

Disables the SPI interrupt as the condition to generate an event to directly trigger the DMA. This API configures the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Note
DMA_TRIG_TX only has one transmit interrupt source
Parameters
[in]spiPointer to the register overlay for the peripheral

§ DL_SPI_getEnabledDMAReceiveEvent()

__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEvent ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check which SPI interrupt for DMA receive events is enabled.

This API checks the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_DMA_INTERRUPT_RX.
Note
Only one interrupt source should be enabled at a time.
Returns
Which of the requested SPI interrupts is enabled
Return values
Oneof DL_SPI_DMA_INTERRUPT_RX

§ DL_SPI_getEnabledDMATransmitEvent()

__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEvent ( const SPI_Regs *  spi)

Check if SPI interrupt for DMA transmit event is enabled.

This API checks the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The requested SPI interrupt status
Return values
DL_SPI_DMA_INTERRUPT_TXif enabled, 0 if not enabled

§ DL_SPI_getEnabledDMAReceiveEventStatus()

__STATIC_INLINE uint32_t DL_SPI_getEnabledDMAReceiveEventStatus ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check interrupt flag of enabled SPI interrupt for DMA receive event.

Checks if any of the SPI interrupts for the DMA receive event that were previously enabled are pending. This API checks the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_DMA_INTERRUPT_RX.
Note
Only one interrupt source should be enabled at a time.
Returns
The requested SPI interrupt status
Return values
Oneof DL_SPI_DMA_INTERRUPT_RX
See also
DL_SPI_enableDMAReceiveEvent

§ DL_SPI_getEnabledDMATransmitEventStatus()

__STATIC_INLINE uint32_t DL_SPI_getEnabledDMATransmitEventStatus ( const SPI_Regs *  spi)

Check interrupt flag of enabled SPI interrupt for DMA transmit event.

Checks if the SPI interrupt for the DMA transmit event that was previously enabled is pending. This API checks the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The requested SPI interrupt status
Return values
DL_SPI_DMA_INTERRUPT_TXif enabled, 0 if not enabled
See also
DL_SPI_enableDMATransmitEvent

§ DL_SPI_getRawDMAReceiveEventStatus()

__STATIC_INLINE uint32_t DL_SPI_getRawDMAReceiveEventStatus ( const SPI_Regs *  spi,
uint32_t  interruptMask 
)

Check interrupt flag of any SPI interrupt for DMA receive event.

Checks if any of the SPI interrupts for DMA receive event are pending. Interrupts do not have to be previously enabled. This API checks the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to check. Bitwise OR of DL_SPI_DMA_INTERRUPT_RX.
Returns
Which of the requested SPI interrupts are pending
Return values
BitwiseOR of DL_SPI_DMA_INTERRUPT_RX values

§ DL_SPI_getRawDMATransmitEventStatus()

__STATIC_INLINE uint32_t DL_SPI_getRawDMATransmitEventStatus ( const SPI_Regs *  spi)

Check interrupt flag of any SPI interrupt for DMA transmit event.

Checks if any of the SPI interrupts for DMA transmit event are pending. Interrupts do not have to be previously enabled. This API checks the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The requested SPI interrupt status
Return values
DL_SPI_DMA_INTERRUPT_TXif enabled, 0 if not enabled

§ DL_SPI_getPendingDMAReceiveEvent()

__STATIC_INLINE DL_SPI_DMA_IIDX_RX DL_SPI_getPendingDMAReceiveEvent ( const SPI_Regs *  spi)

Get highest priority pending SPI interrupt for DMA receive event.

Checks if any of the SPI interrupts for DMA receive event are pending. Interrupts do not have to be previously enabled. This API checks the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The highest priority pending SPI interrupt
Return values
Oneof DL_SPI_DMA_IIDX_RX

§ DL_SPI_getPendingDMATransmitEvent()

__STATIC_INLINE DL_SPI_DMA_IIDX_TX DL_SPI_getPendingDMATransmitEvent ( const SPI_Regs *  spi)

Get highest priority pending SPI interrupt for DMA transmit event.

Checks if the SPI interrupt for DMA transmit event is pending. Interrupts do not have to be previously enabled. This API checks the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Returns
The highest priority pending SPI interrupt
Return values
DL_SPI_DMA_IIDX_TXif pending, 0 if not pending

§ DL_SPI_clearDMAReceiveEventStatus()

__STATIC_INLINE void DL_SPI_clearDMAReceiveEventStatus ( SPI_Regs *  spi,
uint32_t  interruptMask 
)

Clear pending SPI interrupts for DMA receive event.

This API checks the DMA_TRIG_RX register, which is the event publisher used for triggering the DMA to do a receive data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]interruptMaskBit mask of interrupts to clear. Bitwise OR of DL_SPI_DMA_INTERRUPT_RX.

§ DL_SPI_clearDMATransmitEventStatus()

__STATIC_INLINE void DL_SPI_clearDMATransmitEventStatus ( SPI_Regs *  spi)

Clear pending SPI interrupt for DMA transmit event.

This API checks the DMA_TRIG_TX register, which is the event publisher used for triggering the DMA to do a transmit data transfer.

Parameters
[in]spiPointer to the register overlay for the peripheral
Note
DMA_TRIG_TX only has one transmit interrupt source

References DL_SPI_restoreConfiguration(), and DL_SPI_saveConfiguration().

§ DL_SPI_saveConfiguration()

bool DL_SPI_saveConfiguration ( const SPI_Regs *  spi,
DL_SPI_backupConfig ptr 
)

Save SPI configuration before entering a power loss state.

Some MSPM0G peripherals residing in PD1 domain do not retain register contents when entering STOP or STANDBY modes. Please refer to the datasheet for the full list of peripheral instances that exhibit this behavior.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]ptrConfiguration backup setup structure. See DL_SPI_backupConfig.
Return values
FALSEif a configuration already exists in ptr (will not be overwritten). TRUE if a configuration was successfully saved
See also
DL_SPI_restoreConfiguration

Referenced by DL_SPI_clearDMATransmitEventStatus().

§ DL_SPI_restoreConfiguration()

bool DL_SPI_restoreConfiguration ( SPI_Regs *  spi,
DL_SPI_backupConfig ptr 
)

Restore SPI configuration after leaving a power loss state.

Some MSPM0G peripherals residing in PD1 domain do not retain register contents when entering STOP or STANDBY modes. Please refer to the datasheet for the full list of peripheral instances that exhibit this behavior.

Parameters
[in]spiPointer to the register overlay for the peripheral
[in]ptrConfiguration backup setup structure. See DL_SPI_backupConfig.
Return values
FALSEif a configuration does not exist in ptr (will not be loaded). TRUE if a configuration successfully loaded
See also
DL_SPI_saveConfiguration

Referenced by DL_SPI_clearDMATransmitEventStatus().

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale