#include <stdint.h>
#include <ti/devices/msp/msp.h>
Go to the source code of this file.
§ DL_CORE_getImplementer()
| __STATIC_INLINE uint32_t DL_CORE_getImplementer |
( |
void |
| ) |
|
Get the implementer code for the processor.
- Returns
- The implementer code
- Return values
-
§ DL_CORE_getVariant()
| __STATIC_INLINE uint32_t DL_CORE_getVariant |
( |
void |
| ) |
|
Get the major revision number 'n' in the 'npm' revision status.
- Returns
- The major revision number
- Return values
-
§ DL_CORE_getArchitecture()
| __STATIC_INLINE uint32_t DL_CORE_getArchitecture |
( |
void |
| ) |
|
Get the architecture of the processor.
- Returns
- Value that defines the architecture of the processor
- Return values
-
| 0x0C | for ARMv6-M architecture |
§ DL_CORE_getPartNumber()
| __STATIC_INLINE uint32_t DL_CORE_getPartNumber |
( |
void |
| ) |
|
Get part number of the processor (not the device)
- Returns
- Value that defines the processor
- Return values
-
§ DL_CORE_getRevision()
| __STATIC_INLINE uint32_t DL_CORE_getRevision |
( |
void |
| ) |
|
Get the minor revision number 'm' in the 'npm' revision status.
- Returns
- The minor revision number
- Return values
-
§ DL_CORE_configInstruction()
| __STATIC_INLINE void DL_CORE_configInstruction |
( |
uint32_t |
icache, |
|
|
uint32_t |
prefetch, |
|
|
uint32_t |
litCache |
|
) |
| |
Configures instruction caching in flash accesses and instruction prefetch to flash.
- Parameters
-
Referenced by DL_FactoryRegion_getBOOTCRCData(), DL_FactoryRegion_getBSLPinI2CSCLFunction(), DL_FactoryRegion_getBSLPinI2CSCLPad(), DL_FactoryRegion_getBSLPinI2CSDAFunction(), DL_FactoryRegion_getBSLPinI2CSDAPad(), DL_FactoryRegion_getBSLPinInvokeGPIOLevel(), DL_FactoryRegion_getBSLPinInvokeGPIOModule(), DL_FactoryRegion_getBSLPinInvokeGPIOModulePad(), DL_FactoryRegion_getBSLPinInvokeGPIOPin(), DL_FactoryRegion_getBSLPinUARTRXDFunction(), DL_FactoryRegion_getBSLPinUARTRXDPad(), DL_FactoryRegion_getBSLPinUARTTXDFunction(), DL_FactoryRegion_getBSLPinUARTTXDPad(), DL_FactoryRegion_getDATAFlashSize(), DL_FactoryRegion_getMAINFlashSize(), DL_FactoryRegion_getManufacturerCode(), DL_FactoryRegion_getNumBanks(), DL_FactoryRegion_getPartNumber(), DL_FactoryRegion_getSRAMFlashSize(), DL_FactoryRegion_getTemperatureVoltage(), DL_FactoryRegion_getTraceID(), DL_FactoryRegion_getUserIDMajorRev(), DL_FactoryRegion_getUserIDMinorRev(), DL_FactoryRegion_getUserIDPart(), DL_FactoryRegion_getUserIDVariant(), and DL_FactoryRegion_getVersion().
§ DL_CORE_getInstructionConfig()
| __STATIC_INLINE uint32_t DL_CORE_getInstructionConfig |
( |
void |
| ) |
|
Returns instruction caching, prefetch, and literal cache configuration.
- Returns
- Bitwise OR of DL_CORE_CACHE and DL_CORE_PREFETCH and DL_CORE_LITERAL_CACHE
Referenced by DL_FactoryRegion_getBOOTCRCData(), DL_FactoryRegion_getBSLPinI2CSCLFunction(), DL_FactoryRegion_getBSLPinI2CSCLPad(), DL_FactoryRegion_getBSLPinI2CSDAFunction(), DL_FactoryRegion_getBSLPinI2CSDAPad(), DL_FactoryRegion_getBSLPinInvokeGPIOLevel(), DL_FactoryRegion_getBSLPinInvokeGPIOModule(), DL_FactoryRegion_getBSLPinInvokeGPIOModulePad(), DL_FactoryRegion_getBSLPinInvokeGPIOPin(), DL_FactoryRegion_getBSLPinUARTRXDFunction(), DL_FactoryRegion_getBSLPinUARTRXDPad(), DL_FactoryRegion_getBSLPinUARTTXDFunction(), DL_FactoryRegion_getBSLPinUARTTXDPad(), DL_FactoryRegion_getDATAFlashSize(), DL_FactoryRegion_getMAINFlashSize(), DL_FactoryRegion_getManufacturerCode(), DL_FactoryRegion_getNumBanks(), DL_FactoryRegion_getPartNumber(), DL_FactoryRegion_getSRAMFlashSize(), DL_FactoryRegion_getTemperatureVoltage(), DL_FactoryRegion_getTraceID(), DL_FactoryRegion_getUserIDMajorRev(), DL_FactoryRegion_getUserIDMinorRev(), DL_FactoryRegion_getUserIDPart(), DL_FactoryRegion_getUserIDVariant(), and DL_FactoryRegion_getVersion().