MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Structures | Enumerations | Variables
appUserOutputs.h File Reference

Detailed Description

Application Outputs Module.


Overview

Handles the output variables for user to understand


#include "stdint.h"
#include "mcLib.h"
Include dependency graph for appUserOutputs.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  OUTPUTS_CURRENT_PI_T
 PI Current output structure. More...
 
struct  OUTPUTS_PI_T
 PI output structure. More...
 
struct  OUTPUT_DQ_T
 DQ structure. More...
 
struct  appVersion
 appVersion structure More...
 
union  APP_VERSION_T
 appVersion register More...
 
struct  USER_STATUS_INTERFACE_T
 User output structure. More...
 

Enumerations

enum  MOTOR_STATE_TYPES_T {
  MOTOR_IDLE = 0,
  MOTOR_ISD = 1,
  MOTOR_TRISTATE = 2,
  MOTOR_BRAKE_ON_START = 3,
  MOTOR_IPD = 4,
  MOTOR_SLOW_FIRST_CYCLE = 5,
  MOTOR_ALIGN = 6,
  MOTOR_OPEN_LOOP = 7,
  MOTOR_CLOSE_LOOP_UNALIGNED = 8,
  MOTOR_CLOSE_LOOP_ALIGNED = 9,
  MOTOR_CLOSE_LOOP_ACTIVE_BRAKING = 10,
  MOTOR_SOFT_STOP = 11,
  MOTOR_BRAKE_ON_STOP = 12,
  MOTOR_FAULT = 13,
  MOTOR_MAX = 0xFFFF
}
 Motor states. More...
 
enum  USER_FAULT_TYPES {
  NO_FAULTS = 0,
  FAULT_MOTOR_STALL = 1,
  FAULT_VOLTAGE_OUT_OF_BOUNDS = 2,
  FAULT_LOAD_STALL = 3,
  FAULT_HARDWARE_OVER_CURRENT = 4,
  FAULT_HV_DIE = 5,
  FAULT_NONE = 0xFFFF
}
 Fault types. More...
 
enum  IPD_IDENTIFIED_SECTOR_T {
  Ac = 0,
  aC = 1,
  Bc = 2,
  bC = 3,
  aB = 4,
  Ab = 5,
  IPD_IDENTIFIED_SECTOR_MAX = 0xFFFFFFFF
}
 IPD identified sector types. More...
 

Variables

USER_STATUS_INTERFACE_TpUserStatusRegs
 pointer to userOutputs
 

Enumeration Type Documentation

§ MOTOR_STATE_TYPES_T

Motor states.

Enumerator
MOTOR_IDLE 

Motor Idle state

MOTOR_ISD 

Motor in ISD state

MOTOR_TRISTATE 

Motor in Tristate state

MOTOR_BRAKE_ON_START 

Motor in Brake on start state

MOTOR_IPD 

Motor in IPD state

MOTOR_SLOW_FIRST_CYCLE 

Motor in Slow first cycle state

MOTOR_ALIGN 

Motor in align state

MOTOR_OPEN_LOOP 

Motor in open loop state

MOTOR_CLOSE_LOOP_UNALIGNED 

Motor in close loop unaligned state

MOTOR_CLOSE_LOOP_ALIGNED 

Motor in close loop aligned state

MOTOR_CLOSE_LOOP_ACTIVE_BRAKING 

Motor in active brake state

MOTOR_SOFT_STOP 

Motor in soft stop state

MOTOR_BRAKE_ON_STOP 

Motor in brake on stop state

MOTOR_FAULT 

Motor in fault state

MOTOR_MAX 

Motor Max State

§ USER_FAULT_TYPES

Fault types.

Enumerator
NO_FAULTS 

No Fault

FAULT_MOTOR_STALL 

Motor Stall detected

FAULT_VOLTAGE_OUT_OF_BOUNDS 

Voltage out of bounds detected

FAULT_LOAD_STALL 

Motor startup fault detected

FAULT_HARDWARE_OVER_CURRENT 

Over current fault detected

FAULT_HV_DIE 

HVDie Fault

FAULT_NONE 

Fault Max

§ IPD_IDENTIFIED_SECTOR_T

IPD identified sector types.

Enumerator
Ac 

IPD sector Ac

aC 

IPD sector aC

Bc 

IPD sector Bc

bC 

IPD sector bC

aB 

IPD sector aB

Ab 

IPD sector Ab

IPD_IDENTIFIED_SECTOR_MAX 

Max number of IPD sector

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale