MSPM0G3507SensorlessFOCMotorControlLibrary  1.0
Data Fields
userInputMotorStartUp2 Struct Reference

userInputMotorStartUp2 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t thetaErrRampRate: 3
 
uint32_t FirstCycFreqSel: 1
 
uint32_t slowFirstCycFreq: 4
 
uint32_t alignAngle: 5
 
uint32_t olClHandOffThr: 5
 
uint32_t autoHandOffEn: 1
 
uint32_t olAcc2: 4
 
uint32_t olAcc1: 4
 
uint32_t olILimit: 5
 

Detailed Description

userInputMotorStartUp2 structure

Field Documentation

§ thetaErrRampRate

uint32_t userInputMotorStartUp2::thetaErrRampRate

Ramp rate for reducing difference between estimated theta and open loop theta

§ FirstCycFreqSel

uint32_t userInputMotorStartUp2::FirstCycFreqSel

First cycle frequency in open loop for align, double align and IPD startup options

§ slowFirstCycFreq

uint32_t userInputMotorStartUp2::slowFirstCycFreq

Frequency of first cycle in close loop startup (% of MAX_SPEED)

§ alignAngle

uint32_t userInputMotorStartUp2::alignAngle

Align angle

§ olClHandOffThr

uint32_t userInputMotorStartUp2::olClHandOffThr

Open to close loop handoff threshold (% of MAX_SPEED)

Referenced by update_MotorStartUp2Config().

§ autoHandOffEn

uint32_t userInputMotorStartUp2::autoHandOffEn

Auto handoff enable

§ olAcc2

uint32_t userInputMotorStartUp2::olAcc2

Open loop acceleration coefficient A2

Referenced by update_MotorStartUp2Config(), and update_RvsDrvConfig().

§ olAcc1

uint32_t userInputMotorStartUp2::olAcc1

Open loop acceleration coefficient A1

Referenced by update_RvsDrvConfig().

§ olILimit

uint32_t userInputMotorStartUp2::olILimit

Open loop current limit


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale