MSPM0G3507SensoredFOCMotorControlLibrary  1.0
Data Fields
userInputPinCfg Struct Reference

userInputPinCfg structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t brakeInp: 2
 
uint32_t brakePinMode: 1
 
uint32_t reserved1: 16
 
uint32_t vdcFiltDis: 1
 
uint32_t reserved: 12
 

Detailed Description

userInputPinCfg structure

Field Documentation

§ brakeInp

uint32_t userInputPinCfg::brakeInp

Brake pin override

Referenced by update_BrakeStatus().

§ brakePinMode

uint32_t userInputPinCfg::brakePinMode

Brake pin mode

§ reserved1

uint32_t userInputPinCfg::reserved1

Reserved

§ vdcFiltDis

uint32_t userInputPinCfg::vdcFiltDis

Bus voltage filter enable

§ reserved

uint32_t userInputPinCfg::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale