MSPM0G3507SensoredFOCMotorControlLibrary  1.0
Data Structures | Functions
fluxWeak.h File Reference

Detailed Description

fluxWeak Module


Overview


#include "mcLib.h"
#include "motor.h"
#include "pi.h"
#include "main.h"
Include dependency graph for fluxWeak.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  FLUX_WEAK_T
 Flux Weakening Working Structure. More...
 

Functions

void fluxWeakInit (FLUX_WEAK_T *pFluxWeak)
 Flux weakening Init. More...
 
void fluxWeakRun (FLUX_WEAK_T *pFluxWeak)
 Flux weakening Run. More...
 

Function Documentation

§ fluxWeakInit()

void fluxWeakInit ( FLUX_WEAK_T pFluxWeak)

Flux weakening Init.

Parameters
[in]*pFluxWeakInput Pointer

References FLUX_WEAK_T::idRef, FLUX_WEAK_T::piFluxWeak, and piInit().

Referenced by idRefInit().

§ fluxWeakRun()

void fluxWeakRun ( FLUX_WEAK_T pFluxWeak)

Flux weakening Run.

Parameters
[in]*pFluxWeakInput Pointer

References FLUX_WEAK_T::idRef, PI_T::out, FLUX_WEAK_T::piFluxWeak, and piRun_LowPriority().

Referenced by idRefLowPriorityRun().

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale