![]() |
![]() |
|
MSPM0L111X TI-Driver Library
2.05.00.05
|
I2CTarget Parameters. More...
#include <I2CTarget.h>

Data Fields | |
| I2CTarget_EventCallbackFxn | eventCallbackFxn |
| uint_least16_t | targetAddress |
| void * | custom |
I2CTarget Parameters.
I2CTarget parameters are used to with the I2CTarget_open() call. Default values for these parameters are set using I2CTarget_Params_init().
| I2CTarget_EventCallbackFxn I2CTarget_Params::eventCallbackFxn |
Interrupt context event callback for the user
| uint_least16_t I2CTarget_Params::targetAddress |
Device's own address on the I2C bus
| void* I2CTarget_Params::custom |
Custom argument used by driver implementation