![]() |
![]() |
|
MSPM0GX51X Driver Library
2.05.00.05
|
Functions | |
| __STATIC_INLINE void | DL_Common_updateReg (volatile uint32_t *reg, uint32_t val, uint32_t mask) |
| Writes value to specified register - retaining bits unaffected by mask. More... | |
| void | DL_Common_delayCycles (uint32_t cycles) |
| Consumes the number of CPU cycles specified. More... | |
APIs used across multiple DriverLib modules
| __STATIC_INLINE void DL_Common_updateReg | ( | volatile uint32_t * | reg, |
| uint32_t | val, | ||
| uint32_t | mask | ||
| ) |
Writes value to specified register - retaining bits unaffected by mask.
| [in] | reg | Pointer to the register overlay for the peripheral. |
| [in] | val | Value to be written to the register. |
| [in] | mask | Mask defines which bits will be altered. |
References DL_Common_delayCycles().
Referenced by DL_ADC12_configHwAverage(), DL_ADC12_disableForcingSYSOSCOnInRunMode(), DL_ADC12_disableForcingSYSOSCOnInStopMode(), DL_ADC12_initSeqSample(), DL_ADC12_initSingleSample(), DL_ADC12_setDMASamplesCnt(), DL_ADC12_setEndAddress(), DL_ADC12_setPowerDownMode(), DL_ADC12_setStartAddress(), DL_AESADV_resumeAADPhase(), DL_AESADV_resumeDataPhase(), DL_AESADV_setCCMCounterWidth(), DL_AESADV_setCCMTagWidth(), DL_AESADV_setCounterWidth(), DL_AESADV_setDirection(), DL_AESADV_setFeedbackWidth(), DL_AESADV_setKeySize(), DL_AESADV_setMode(), DL_COMP_init(), DL_COMP_refVoltageInit(), DL_COMP_setBlankingSource(), DL_COMP_setCompMode(), DL_COMP_setDACCode0(), DL_COMP_setDACCode1(), DL_COMP_setDACControl(), DL_COMP_setDACInput(), DL_COMP_setEnabledInputChannels(), DL_COMP_setHysteresis(), DL_COMP_setNegativeChannelInput(), DL_COMP_setOutputInterruptEdge(), DL_COMP_setOutputPolarity(), DL_COMP_setPositiveChannelInput(), DL_COMP_setReferenceCompTerminal(), DL_COMP_setReferenceMode(), DL_COMP_setReferenceSource(), DL_DAC12_configDataFormat(), DL_DAC12_setAmplifier(), DL_DAC12_setFIFOThreshold(), DL_DAC12_setFIFOTriggerSource(), DL_DAC12_setReferenceVoltageSource(), DL_DAC12_setSampleRate(), DL_DMA_configMode(), DL_DMA_Full_Ch_setEarlyInterruptThreshold(), DL_DMA_setBurstSize(), DL_DMA_setDestIncrement(), DL_DMA_setDestWidth(), DL_DMA_setExtendedMode(), DL_DMA_setSrcIncrement(), DL_DMA_setSrcWidth(), DL_DMA_setTransferMode(), DL_DMA_setTrigger(), DL_FlashCTL_setBankSelect(), DL_FlashCTL_setRegionSelect(), DL_GPIO_configSubscriber(), DL_GPIO_disableDMAAccess(), DL_GPIO_enableDMAAccess(), DL_GPIO_setWakeupCompareValue(), DL_KEYSTORECTL_setDestinationKeySize(), DL_KEYSTORECTL_setDestinationKeySlot(), DL_KEYSTORECTL_setNumberOf256Keys(), DL_KEYSTORECTL_setSourceKeySize(), DL_KEYSTORECTL_setSourceKeySlot(), DL_RTC_Common_getPublisherChanID(), DL_RTC_Common_setAlarm1DayOfMonthBCD(), DL_RTC_Common_setAlarm1DayOfMonthBinary(), DL_RTC_Common_setAlarm1DayOfWeekBCD(), DL_RTC_Common_setAlarm1DayOfWeekBinary(), DL_RTC_Common_setAlarm2DayOfMonthBCD(), DL_RTC_Common_setAlarm2DayOfMonthBinary(), DL_RTC_Common_setAlarm2DayOfWeekBCD(), DL_RTC_Common_setAlarm2DayOfWeekBinary(), DL_RTC_Common_setCalendarDayOfMonthBCD(), DL_RTC_Common_setCalendarDayOfMonthBinary(), DL_RTC_Common_setCalendarDayOfWeekBCD(), DL_RTC_Common_setCalendarDayOfWeekBinary(), DL_RTC_Common_setIntervalAlarm(), DL_RTC_Common_setOffsetCalibrationAdjValue(), DL_RTC_Common_setOffsetCalibrationFrequency(), DL_RTC_Common_setPeriodicAlarm0(), DL_RTC_Common_setPeriodicAlarm1(), DL_RTC_Common_setPeriodicAlarm2(), DL_SYSCTL_configSYSOSCUserTrim(), DL_SYSCTL_enableExternalClock(), DL_SYSCTL_setFCCPeriods(), DL_SYSCTL_setFlashDEDErrorBehavior(), DL_SYSCTL_setFlashWaitState(), DL_SYSCTL_setHFCLKDividerForMFPCLK(), DL_SYSCTL_setHFXTFrequencyRange(), DL_SYSCTL_setHFXTStartupTime(), DL_SYSCTL_setMCLKDivider(), DL_SYSCTL_setMFPCLKSource(), DL_SYSCTL_setShutdownStorageByte(), DL_SYSCTL_setSRAMBank1PowerLevelInRUN(), DL_SYSCTL_setSRAMBank1PowerLevelInSTOP(), DL_SYSCTL_setSYSOSCFreq(), DL_SYSCTL_setULPCLKDivider(), DL_SYSCTL_setVBOOSTConfig(), DL_SYSCTL_setWWDT0ErrorBehavior(), DL_SYSCTL_setWWDT1ErrorBehavior(), DL_Timer_configCrossTriggerEnable(), DL_Timer_configCrossTriggerInputCond(), DL_Timer_configCrossTriggerSrc(), DL_Timer_configFaultCounter(), DL_Timer_configFaultOutputAction(), DL_Timer_setCCPOutputDisabled(), DL_Timer_setCCPOutputDisabledAdv(), DL_Timer_setCounterControl(), DL_Timer_setCounterMode(), DL_Timer_setCounterRepeatMode(), DL_Timer_setCounterValueAfterEnable(), DL_Timer_setDebugReleaseBehavior(), DL_Timer_setExternalTriggerEvent(), and DL_Timer_setFaultConfig().
| void DL_Common_delayCycles | ( | uint32_t | cycles | ) |
Consumes the number of CPU cycles specified.
| [in] | cycles | Floor number of cycles to delay. Specifying zero will result in the maximum possible delay. Note that guarantees at least this number of cycles will be delayed, not that exactly this number of cycles will be delayed. If a more precise number of cycle delay value is needed, GPTimer is recommended. |
Typical variance from this function is 10 cycles or less assuming that the function is located in flash and that caching is enabled. Disabling caching may result in wait-states when fetching from flash. Other variance occurs due:
Referenced by DL_Common_updateReg().