![]() |
![]() |
|
MSPM0C110X Driver Library
2.05.00.05
|
Functions | |
| __STATIC_INLINE uint16_t | DL_FactoryRegion_getMAINFlashSize (void) |
| Get the size of the MAIN Flash region. More... | |
| __STATIC_INLINE uint16_t | DL_FactoryRegion_getSRAMFlashSize (void) |
| Get the size of the SRAM region. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getDATAFlashSize (void) |
| Get the size of the DATA Flash region. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getNumBanks (void) |
| Get the number of Flash banks on the device. More... | |
| __STATIC_INLINE uint32_t | DL_FactoryRegion_getTraceID (void) |
| Get the trace ID of the device. More... | |
| __STATIC_INLINE uint16_t | DL_FactoryRegion_getManufacturerCode (void) |
| Get JEDEC bank and company code. More... | |
| __STATIC_INLINE uint16_t | DL_FactoryRegion_getPartNumber (void) |
| Get the part number of the device. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getVersion (void) |
| Get the version of the device. More... | |
| __STATIC_INLINE uint16_t | DL_FactoryRegion_getUserIDPart (void) |
| Get the bit pattern identifying the part. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getUserIDVariant (void) |
| Get the bit pattern identifying a variant of a part. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getUserIDMinorRev (void) |
| Get the value that preserves compatibility with lesser minorrev values. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getUserIDMajorRev (void) |
| Get the value that preserves compatibility with lesser majorrev values. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinUARTRXDPad (void) |
| Get the UART RXD PIN used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinUARTRXDFunction (void) |
| Get the UART RXD Pin function selection value used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinUARTTXDPad (void) |
| Get the UART TXD PIN used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinUARTTXDFunction (void) |
| Get the UART TXD Pin function selection value used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinI2CSDAPad (void) |
| Get the I2C SDA Pin used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinI2CSDAFunction (void) |
| Get the I2C SDA Pin function selection value used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinI2CSCLPad (void) |
| Get the I2C SCL Pin used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinI2CSCLFunction (void) |
| Get the I2C SCL Pin function selection value used by BSL. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinInvokeGPIOLevel (void) |
| Get the GPIO level used by BSL pin invocation. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinInvokeGPIOPin (void) |
| Get the GPIO Pin selection value used by BSL pin invocation. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinInvokeGPIOModule (void) |
| Get the GPIO module selection used by BSL pin invocation. More... | |
| __STATIC_INLINE uint8_t | DL_FactoryRegion_getBSLPinInvokeGPIOModulePad (void) |
| Get the BSL invocation pin number. More... | |
| __STATIC_INLINE uint32_t | DL_FactoryRegion_getTemperatureVoltage (void) |
| Get the ADC conversion results of temperature sensor output voltage. More... | |
| __STATIC_INLINE uint32_t | DL_FactoryRegion_getBOOTCRCData (void) |
| Get the BOOTCRC value. More... | |
| __STATIC_INLINE float | DL_FactoryRegion_getADCOffset (void) |
| Get the ADC offset value. More... | |
| __STATIC_INLINE uint16_t DL_FactoryRegion_getMAINFlashSize | ( | void | ) |
Get the size of the MAIN Flash region.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
Referenced by DL_FlashCTL_getFlashSectorNumberInBank().
| __STATIC_INLINE uint16_t DL_FactoryRegion_getSRAMFlashSize | ( | void | ) |
Get the size of the SRAM region.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getDATAFlashSize | ( | void | ) |
Get the size of the DATA Flash region.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getNumBanks | ( | void | ) |
Get the number of Flash banks on the device.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
Referenced by DL_FlashCTL_getFlashSectorNumberInBank().
| __STATIC_INLINE uint32_t DL_FactoryRegion_getTraceID | ( | void | ) |
Get the trace ID of the device.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint16_t DL_FactoryRegion_getManufacturerCode | ( | void | ) |
Get JEDEC bank and company code.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint16_t DL_FactoryRegion_getPartNumber | ( | void | ) |
Get the part number of the device.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getVersion | ( | void | ) |
Get the version of the device.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint16_t DL_FactoryRegion_getUserIDPart | ( | void | ) |
Get the bit pattern identifying the part.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getUserIDVariant | ( | void | ) |
Get the bit pattern identifying a variant of a part.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getUserIDMinorRev | ( | void | ) |
Get the value that preserves compatibility with lesser minorrev values.
Monotonic increasing value indicating a new revision that preserves compatibility with lesser minorrev values. New capability may be introduced such that lesser minorrev numbers may not be compatible with greater if the new capability is used
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getUserIDMajorRev | ( | void | ) |
Get the value that preserves compatibility with lesser majorrev values.
Monotonic increasing value indicating a new revision significant enough that users of the device may have to revise PCB or or software design
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinUARTRXDPad | ( | void | ) |
Get the UART RXD PIN used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinUARTRXDFunction | ( | void | ) |
Get the UART RXD Pin function selection value used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinUARTTXDPad | ( | void | ) |
Get the UART TXD PIN used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinUARTTXDFunction | ( | void | ) |
Get the UART TXD Pin function selection value used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinI2CSDAPad | ( | void | ) |
Get the I2C SDA Pin used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinI2CSDAFunction | ( | void | ) |
Get the I2C SDA Pin function selection value used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinI2CSCLPad | ( | void | ) |
Get the I2C SCL Pin used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinI2CSCLFunction | ( | void | ) |
Get the I2C SCL Pin function selection value used by BSL.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinInvokeGPIOLevel | ( | void | ) |
Get the GPIO level used by BSL pin invocation.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinInvokeGPIOPin | ( | void | ) |
Get the GPIO Pin selection value used by BSL pin invocation.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinInvokeGPIOModule | ( | void | ) |
Get the GPIO module selection used by BSL pin invocation.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint8_t DL_FactoryRegion_getBSLPinInvokeGPIOModulePad | ( | void | ) |
Get the BSL invocation pin number.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE uint32_t DL_FactoryRegion_getTemperatureVoltage | ( | void | ) |
Get the ADC conversion results of temperature sensor output voltage.
Returns the temperature sensor output voltage at the factory trim temperature in ADC result code format. This ADC result code is based upon 12-bit sampling mode together with the 1.4-V internal voltage reference.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
Referenced by DL_SYSCTL_getTempCalibrationConstant().
| __STATIC_INLINE uint32_t DL_FactoryRegion_getBOOTCRCData | ( | void | ) |
Get the BOOTCRC value.
The 32-bit CRC of all locations in OPEN including reserved locations.
References DL_CORE_CACHE_DISABLED, DL_CORE_configInstruction(), DL_CORE_getInstructionConfig(), DL_CORE_LITERAL_CACHE_ENABLED, and DL_CORE_PREFETCH_ENABLED.
| __STATIC_INLINE float DL_FactoryRegion_getADCOffset | ( | void | ) |
Get the ADC offset value.
Workaround for errata on MSPM0C110x devices: ADC_ERR_06 0x41C40040 is expected to point to factory region reserved0 bit
Referenced by DL_ADC12_getADCOffsetCalibration().