MSPM0C1105_C1106 Driver Library  2.05.00.05
Modules | Macros | Enumerations | Functions
Low Frequeuncy Sub-System (LFSS)
Collaboration diagram for Low Frequeuncy Sub-System (LFSS):

Modules

 DL_LFSS_TAMPERIO_INTERRUPT
 
 DL_LFSS_TAMPERIO_EVENT
 

Macros

#define LFSS_TAMPER_IO_PIN_ENABLE   0x1
 Individual Tamper IO pin enable.
 
#define LFSS_TAMPER_IO_PIN_MASK   0x1
 Individual Tamper IO pin mask.
 

Enumerations

enum  DL_LFSS_TAMPERIO {
  DL_LFSS_TAMPERIO_0 = 0x0000,
  DL_LFSS_TAMPERIO_1 = 0x0001,
  DL_LFSS_TAMPERIO_2 = 0x0002,
  DL_LFSS_TAMPERIO_3 = 0x0003,
  DL_LFSS_TAMPERIO_4 = 0x0004,
  DL_LFSS_TAMPERIO_5 = 0x0005,
  DL_LFSS_TAMPERIO_6 = 0x0006,
  DL_LFSS_TAMPERIO_7 = 0x0007,
  DL_LFSS_TAMPERIO_8 = 0x0008,
  DL_LFSS_TAMPERIO_9 = 0x0009,
  DL_LFSS_TAMPERIO_10 = 0x000A,
  DL_LFSS_TAMPERIO_11 = 0x000B,
  DL_LFSS_TAMPERIO_12 = 0x000C,
  DL_LFSS_TAMPERIO_13 = 0x000D,
  DL_LFSS_TAMPERIO_14 = 0x000E,
  DL_LFSS_TAMPERIO_15 = 0x000F
}
 
enum  DL_LFSS_TAMPERIO_VALUE {
  DL_LFSS_TAMPERIO_VALUE_0 = 0x00000,
  DL_LFSS_TAMPERIO_VALUE_1 = 0x0001
}
 
enum  DL_LFSS_TAMPERIO_OUTPUT_SOURCE {
  DL_LFSS_TAMPERIO_OUTPUT_SOURCE_TOUT = LFSS_TIOCTL_TOUTSEL_TOUT,
  DL_LFSS_TAMPERIO_OUTPUT_SOURCE_LFCLK = LFSS_TIOCTL_TOUTSEL_LFCLKEXT,
  DL_LFSS_TAMPERIO_OUTPUT_SOURCE_HEARTBEAT = LFSS_TIOCTL_TOUTSEL_HEARTBEAT,
  DL_LFSS_TAMPERIO_OUTPUT_SOURCE_TIME_STAMP_EVENT = LFSS_TIOCTL_TOUTSEL_TSEVTSTAT
}
 
enum  DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH {
  DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_NONE = LFSS_TIOCTL_FILTEREN_NO_FLT,
  DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_30_USEC = LFSS_TIOCTL_FILTEREN_FLT_1,
  DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_100_USEC = LFSS_TIOCTL_FILTEREN_FLT_2,
  DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_200_USEC = LFSS_TIOCTL_FILTEREN_FLT_3
}
 
enum  DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY {
  DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_DISABLE = LFSS_TIOCTL_POLARITY_DISABLE,
  DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_RISE = LFSS_TIOCTL_POLARITY_RISE,
  DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_FALL = LFSS_TIOCTL_POLARITY_FALL,
  DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_BOTH = LFSS_TIOCTL_POLARITY_BOTH
}
 
enum  DL_LFSS_TAMPERIO_MODE {
  DL_LFSS_TAMPERIO_MODE_TAMPER = LFSS_TIOCTL_IOMUX_TAMPER,
  DL_LFSS_TAMPERIO_MODE_IOMUX = LFSS_TIOCTL_IOMUX_IOMUX
}
 
enum  DL_LFSS_HEARTBEAT_INTERVAL {
  DL_LFSS_HEARTBEAT_INTERVAL_0_125_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT0P125,
  DL_LFSS_HEARTBEAT_INTERVAL_0_25_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT0P25,
  DL_LFSS_HEARTBEAT_INTERVAL_05_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT0P5,
  DL_LFSS_HEARTBEAT_INTERVAL_1_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT1,
  DL_LFSS_HEARTBEAT_INTERVAL_2_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT2,
  DL_LFSS_HEARTBEAT_INTERVAL_4_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT4,
  DL_LFSS_HEARTBEAT_INTERVAL_8_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT8,
  DL_LFSS_HEARTBEAT_INTERVAL_16_SEC = LFSS_HEARTBEAT_HBINTERVAL_HBINT16
}
 
enum  DL_LFSS_HEARTBEAT_PULSE_WIDTH {
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_1_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH1,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_2_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH2,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_4_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH4,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_8_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH8,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_16_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH16,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_32_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH32,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_64_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH64,
  DL_LFSS_HEARTBEAT_PULSE_WIDTH_128_MSEC = LFSS_HEARTBEAT_HBWIDTH_HBPWDTH128
}
 
enum  DL_LFSS_HEARTBEAT_MODE {
  DL_LFSS_HEARTBEAT_MODE_DISABLED = LFSS_HEARTBEAT_HBMODE_HB_DIS,
  DL_LFSS_HEARTBEAT_MODE_ALWAYS_ON = LFSS_HEARTBEAT_HBMODE_HB_ALLWAYS,
  DL_LFSS_HEARTBEAT_MODE_TIME_STAMP = LFSS_HEARTBEAT_HBMODE_HB_TS,
  DL_LFSS_HEARTBEAT_MODE_POWER_FAIL = LFSS_HEARTBEAT_HBMODE_HB_VDDFAIL
}
 
enum  DL_LFSS_TAMPERIO_IIDX {
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_0 = LFSS_CPU_INT_IIDX_STAT_TIO0,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_1 = LFSS_CPU_INT_IIDX_STAT_TIO1,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_2 = LFSS_CPU_INT_IIDX_STAT_TIO2,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_3 = LFSS_CPU_INT_IIDX_STAT_TIO3,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_4 = LFSS_CPU_INT_IIDX_STAT_TIO4,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_5 = LFSS_CPU_INT_IIDX_STAT_TIO5,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_6 = LFSS_CPU_INT_IIDX_STAT_TIO6,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_7 = LFSS_CPU_INT_IIDX_STAT_TIO7,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_8 = LFSS_CPU_INT_IIDX_STAT_TIO8,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_9 = LFSS_CPU_INT_IIDX_STAT_TIO9,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_10 = LFSS_CPU_INT_IIDX_STAT_TIO10,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_11 = LFSS_CPU_INT_IIDX_STAT_TIO11,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_12 = LFSS_CPU_INT_IIDX_STAT_TIO12,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_13 = LFSS_CPU_INT_IIDX_STAT_TIO13,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_14 = LFSS_CPU_INT_IIDX_STAT_TIO14,
  DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_15 = LFSS_CPU_INT_IIDX_STAT_TIO15
}
 
enum  DL_LFSS_SCRATCHPAD_MEM_WORD {
  DL_LFSS_SCRATCHPAD_MEM_WORD_0 = 0x0000,
  DL_LFSS_SCRATCHPAD_MEM_WORD_1 = 0x0001,
  DL_LFSS_SCRATCHPAD_MEM_WORD_2 = 0x0002,
  DL_LFSS_SCRATCHPAD_MEM_WORD_3 = 0x0003,
  DL_LFSS_SCRATCHPAD_MEM_WORD_4 = 0x0004,
  DL_LFSS_SCRATCHPAD_MEM_WORD_5 = 0x0005,
  DL_LFSS_SCRATCHPAD_MEM_WORD_6 = 0x0006,
  DL_LFSS_SCRATCHPAD_MEM_WORD_7 = 0x0007
}
 
enum  DL_LFSS_SCRATCHPAD_MEM_BYTE {
  DL_LFSS_SCRATCHPAD_MEM_BYTE_0 = 0x0000,
  DL_LFSS_SCRATCHPAD_MEM_BYTE_1 = 0x0001,
  DL_LFSS_SCRATCHPAD_MEM_BYTE_2 = 0x0002,
  DL_LFSS_SCRATCHPAD_MEM_BYTE_3 = 0x0003
}
 
enum  DL_LFSS_IWDT_CLOCK_DIVIDE {
  DL_LFSS_IWDT_CLOCK_DIVIDE_1 = 0x00000000,
  DL_LFSS_IWDT_CLOCK_DIVIDE_2 = 0x00000001,
  DL_LFSS_IWDT_CLOCK_DIVIDE_3 = 0x00000002,
  DL_LFSS_IWDT_CLOCK_DIVIDE_4 = 0x00000003,
  DL_LFSS_IWDT_CLOCK_DIVIDE_5 = 0x00000004,
  DL_LFSS_IWDT_CLOCK_DIVIDE_6 = 0x00000005,
  DL_LFSS_IWDT_CLOCK_DIVIDE_7 = 0x00000006,
  DL_LFSS_IWDT_CLOCK_DIVIDE_8 = 0x00000007
}
 
enum  DL_LFSS_IWDT_TIMER_PERIOD {
  DL_LFSS_IWDT_TIMER_PERIOD_6_BITS = LFSS_WDTCTL_PER_PER_EN_6,
  DL_LFSS_IWDT_TIMER_PERIOD_8_BITS = LFSS_WDTCTL_PER_PER_EN_8,
  DL_LFSS_IWDT_TIMER_PERIOD_10_BITS = LFSS_WDTCTL_PER_PER_EN_10,
  DL_LFSS_IWDT_TIMER_PERIOD_12_BITS = LFSS_WDTCTL_PER_PER_EN_12,
  DL_LFSS_IWDT_TIMER_PERIOD_15_BITS = LFSS_WDTCTL_PER_PER_EN_15,
  DL_LFSS_IWDT_TIMER_PERIOD_18_BITS = LFSS_WDTCTL_PER_PER_EN_18,
  DL_LFSS_IWDT_TIMER_PERIOD_21_BITS = LFSS_WDTCTL_PER_PER_EN_21,
  DL_LFSS_IWDT_TIMER_PERIOD_25_BITS = LFSS_WDTCTL_PER_PER_EN_25
}
 

Functions

__STATIC_INLINE void DL_LFSS_TamperIO_enableOutputInversion (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Enable output inversion for the specified Tamper IO. More...
 
__STATIC_INLINE bool DL_LFSS_TamperIO_isOutputInversionEnabled (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Checks if output inversion is enabled for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableOutputInversion (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Disable output inversion for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setOutputSource (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO, DL_LFSS_TAMPERIO_OUTPUT_SOURCE source)
 Selects the source for the tamper output (TOUT) control for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_OUTPUT_SOURCE DL_LFSS_TamperIO_getOutputSource (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the source for the tamper output (TOUT) control for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setGlitchFilterWidth (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO, DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH width)
 Selects the filter width for the digital glitch filter for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH DL_LFSS_TamperIO_getGlitchFilterWidth (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the filter width for the digital glitch filter for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setEdgeDetectionPolarity (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO, DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY polarity)
 Selects the edge detection polarity for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY DL_LFSS_TamperIO_getEdgeDetectionPolarity (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the edge detection polarity for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableInternalPullUp (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Enable internal pull-up resistor for the specified Tamper IO. More...
 
__STATIC_INLINE bool DL_LFSS_TamperIO_isInternalPullUpEnabled (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Checks if internal pull-up resistor is enabled for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableInternalPullUp (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Disable internal pull-up resistor for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableInternalPullDown (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Enable internal pull-down resistor for the specified Tamper IO. More...
 
__STATIC_INLINE bool DL_LFSS_TamperIO_isInternalPullDownEnabled (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Checks if internal pull-down resistor is enabled for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableInternalPullDown (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Disable internal pull-down resistor for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableInput (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Enable input path for the specified Tamper IO. More...
 
__STATIC_INLINE bool DL_LFSS_TamperIO_isInputEnabled (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Checks if input is enabled for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableInput (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Disable input path for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setMode (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO, DL_LFSS_TAMPERIO_MODE mode)
 Selects the mode for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_MODE DL_LFSS_TamperIO_getMode (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the mode for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableOutput (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Enable data output for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableOutput (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Disable data output for the specified Tamper IO. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_isOutputEnabled (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Checks if data output for the specified Tamper IO is enabled. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setOutputValue (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO, DL_LFSS_TAMPERIO_VALUE outVal)
 Enable data output value as zero for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_VALUE DL_LFSS_TamperIO_getOutputValue (LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the output data value for the specified Tamper IO. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_VALUE DL_LFSS_TamperIO_getInputValue (const LFSS_Regs *lfss, DL_LFSS_TAMPERIO tamperIO)
 Gets the input data value for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatInterval (LFSS_Regs *lfss, DL_LFSS_HEARTBEAT_INTERVAL interval)
 Sets the interval for the heart beat generator. More...
 
__STATIC_INLINE DL_LFSS_HEARTBEAT_INTERVAL DL_LFSS_TamperIO_getHeartBeatInterval (const LFSS_Regs *lfss)
 Gets the interval for the heart beat generator. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatPulseWidth (LFSS_Regs *lfss, DL_LFSS_HEARTBEAT_PULSE_WIDTH width)
 Sets the pulse width for the heart beat generator. More...
 
__STATIC_INLINE DL_LFSS_HEARTBEAT_PULSE_WIDTH DL_LFSS_TamperIO_getHeartBeatPulseWidth (const LFSS_Regs *lfss)
 Gets the pulse width for the heart beat generator. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatMode (LFSS_Regs *lfss, DL_LFSS_HEARTBEAT_MODE mode)
 Sets the mode for the heart beat generator. More...
 
__STATIC_INLINE DL_LFSS_HEARTBEAT_MODE DL_LFSS_TamperIO_getHeartBeatMode (const LFSS_Regs *lfss)
 Gets the pulse mode for the heart beat generator. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableWriteProtectLock (LFSS_Regs *lfss)
 Enable write protection lock of the TIOCTL and HEARTBEAT registers from accidental updates. More...
 
__STATIC_INLINE bool DL_LFSS_TamperIO_isWriteProtectLockEnabled (const LFSS_Regs *lfss)
 Checks if write protection lock of the TIOCTL and HEARTBEAT registers is enabled for the specified Tamper IO. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableWriteProtectLock (LFSS_Regs *lfss)
 Disable write protection lock of the TIOCTL and HEARTBEAT registers. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_enableModule (LFSS_Regs *lfss)
 Enables the Watchdog module. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_disableModule (LFSS_Regs *lfss)
 Disables the Watchdog module. More...
 
__STATIC_INLINE bool DL_LFSS_IWDT_isModuleEnabled (const LFSS_Regs *lfss)
 Returns if Watchdog module is on. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_enableFreeRun (LFSS_Regs *lfss)
 Enables the Watchdog free run control. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_disableFreeRun (LFSS_Regs *lfss)
 Disables the Watchdog free run control. More...
 
__STATIC_INLINE bool DL_LFSS_IWDT_isFreeRunEnabled (const LFSS_Regs *lfss)
 Returns if Watchdog free run control is enabled. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_setClockDivider (LFSS_Regs *lfss, DL_LFSS_IWDT_CLOCK_DIVIDE divider)
 Sets the clock divider for the WDT module. More...
 
__STATIC_INLINE DL_LFSS_IWDT_CLOCK_DIVIDE DL_LFSS_IWDT_getClockDivider (const LFSS_Regs *lfss)
 Gets the clock divider for the WDT module. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_setTimerPeriod (LFSS_Regs *lfss, DL_LFSS_IWDT_TIMER_PERIOD period)
 Sets the timer period for the WDT module. More...
 
__STATIC_INLINE DL_LFSS_IWDT_TIMER_PERIOD DL_LFSS_IWDT_getTimerPeriod (const LFSS_Regs *lfss)
 Get the timer period for the WDT module. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_restart (LFSS_Regs *lfss)
 Restarts the Watchdog. More...
 
__STATIC_INLINE bool DL_LFSS_IWDT_isWatchdogRunning (const LFSS_Regs *lfss)
 Returns if Watchdog module is running. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_enableWriteProtect (LFSS_Regs *lfss)
 Enable write protection lock of the WDTEN and WDTCTL registers from accidental updates. More...
 
__STATIC_INLINE bool DL_LFSS_IWDT_isWriteProtectEnabled (const LFSS_Regs *lfss)
 Checks if write protection lock of the WDTEN and WDTCTL registers is enabled. More...
 
__STATIC_INLINE void DL_LFSS_IWDT_disableWriteProtect (LFSS_Regs *lfss)
 Disable write protection lock of the WDTEN and WDTCTL registers. More...
 
__STATIC_INLINE void DL_LFSS_writeScratchPadData32 (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, uint32_t data)
 Write a word in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_writeScratchPadData8 (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex, uint32_t data)
 Write to a single byte in scratch pad memory. More...
 
__STATIC_INLINE uint32_t DL_LFSS_readScratchPadDataWord (const LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex)
 Read the specified word in scratch pad memory. More...
 
__STATIC_INLINE uint8_t DL_LFSS_readScratchPadDataByte (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Read the specified byte in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_enableScratchPadWriteProtectByte (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Enable write protection lock of the specified byte in scratch pad memory from accidental updates. More...
 
__STATIC_INLINE bool DL_LFSS_isScratchPadWriteProtectByteEnabled (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Checks if write protection is enabled for the specified byte in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_disableScratchPadWriteProtectByte (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Disable write protection lock of the specified byte in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_enableScratchPadTamperEraseByte (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Enable tamper erase of the specified byte in scratch pad memory. More...
 
__STATIC_INLINE bool DL_LFSS_isScratchPadTamperEraseByteEnabled (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Checks if tamper erase is enabled for the specified byte in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_disableScratchPadTamperEraseByte (LFSS_Regs *lfss, DL_LFSS_SCRATCHPAD_MEM_WORD memIndex, DL_LFSS_SCRATCHPAD_MEM_BYTE byteIndex)
 Disable tamper erase of the specified byte in scratch pad memory. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableInterrupt (LFSS_Regs *lfss, uint32_t interruptMask)
 Enable LFSS Tamper Interrupts. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableInterrupt (LFSS_Regs *lfss, uint32_t interruptMask)
 Disable LFSS Tamper interrupts. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledInterrupts (const LFSS_Regs *lfss, uint32_t interruptMask)
 Check which LFSS Tamper interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledInterruptStatus (const LFSS_Regs *lfss, uint32_t interruptMask)
 Check interrupt flag of enabled LFSS Tamper interrupts. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getRawInterruptStatus (const LFSS_Regs *lfss, uint32_t interruptMask)
 Check interrupt flag of any LFSS Tamper interrupt. More...
 
__STATIC_INLINE DL_LFSS_TAMPERIO_IIDX DL_LFSS_TamperIO_getPendingInterrupt (const LFSS_Regs *lfss)
 Get highest priority pending LFSS interrupt. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_clearInterruptStatus (LFSS_Regs *lfss, uint32_t interruptMask)
 Clear pending LFSS Tamper interrupts. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_enableEvent (LFSS_Regs *lfss, uint32_t eventMask)
 Enable LFSS Tamper event. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_disableEvent (LFSS_Regs *lfss, uint32_t eventMask)
 Disable LFSS Tamper event. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledEvents (const LFSS_Regs *lfss, uint32_t eventMask)
 Check which LFSS Tamper events are enabled. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledEventStatus (const LFSS_Regs *lfss, uint32_t eventMask)
 Check event flag of enabled LFSS Tamper event. More...
 
__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getRawEventsStatus (const LFSS_Regs *lfss, uint32_t eventMask)
 Check interrupt flag of any LFSS Tamper event. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_clearEventsStatus (LFSS_Regs *lfss, uint32_t eventMask)
 Clear pending LFSS Tamper events. More...
 
__STATIC_INLINE void DL_LFSS_TamperIO_setPublisherChanID (LFSS_Regs *lfss, uint8_t chanID)
 Sets the LFSS Tamper event publisher channel ID. More...
 
__STATIC_INLINE uint8_t DL_LFSS_TamperIO_getPublisherChanID (const LFSS_Regs *lfss)
 Gets the event publisher channel ID. More...
 
__STATIC_INLINE void DL_LFSS_reset (LFSS_Regs *lfss)
 Requests a reset to the LFSS module. More...
 

Detailed Description

Overview

The Low Frequency Sub-System (LFSS) Driver Library allows full configuration of the MSPM0 LFSS module. The LFSS IP enables a separate, dedicated battery supply used for maintaining continuous operation of real time clock (RTC), tamper detection input / output (TIO) module, an independent asynchronous watchdog timer (IWDT) and a small scratchpad memory storage (SPM).


Enumeration Type Documentation

§ DL_LFSS_TAMPERIO

Enumerator
DL_LFSS_TAMPERIO_0 

LFSS Tamper IO 0

DL_LFSS_TAMPERIO_1 

LFSS Tamper IO 1

DL_LFSS_TAMPERIO_2 

LFSS Tamper IO 2

DL_LFSS_TAMPERIO_3 

LFSS Tamper IO 3

DL_LFSS_TAMPERIO_4 

LFSS Tamper IO 4

DL_LFSS_TAMPERIO_5 

LFSS Tamper IO 5

DL_LFSS_TAMPERIO_6 

LFSS Tamper IO 6

DL_LFSS_TAMPERIO_7 

LFSS Tamper IO 7

DL_LFSS_TAMPERIO_8 

LFSS Tamper IO 8

DL_LFSS_TAMPERIO_9 

LFSS Tamper IO 9

DL_LFSS_TAMPERIO_10 

LFSS Tamper IO 10

DL_LFSS_TAMPERIO_11 

LFSS Tamper IO 11

DL_LFSS_TAMPERIO_12 

LFSS Tamper IO 12

DL_LFSS_TAMPERIO_13 

LFSS Tamper IO 13

DL_LFSS_TAMPERIO_14 

LFSS Tamper IO 14

DL_LFSS_TAMPERIO_15 

LFSS Tamper IO 15

§ DL_LFSS_TAMPERIO_VALUE

Enumerator
DL_LFSS_TAMPERIO_VALUE_0 

LFSS Tamper IO Value is 0

DL_LFSS_TAMPERIO_VALUE_1 

LFSS Tamper IO Value is 1

§ DL_LFSS_TAMPERIO_OUTPUT_SOURCE

Enumerator
DL_LFSS_TAMPERIO_OUTPUT_SOURCE_TOUT 

The TOUT register is the source for the tamper output (TOUT) control

DL_LFSS_TAMPERIO_OUTPUT_SOURCE_LFCLK 

LFCLK is the source for the tamper output (TOUT) control

DL_LFSS_TAMPERIO_OUTPUT_SOURCE_HEARTBEAT 

The heart beat generator is the source for the tamper output (TOUT) control

DL_LFSS_TAMPERIO_OUTPUT_SOURCE_TIME_STAMP_EVENT 

The time stamp event is the source for the tamper output (TOUT) control

§ DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH

Enumerator
DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_NONE 

No filtering on the Tamper IO beyond CDS synchronization sample

DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_30_USEC 

Pulses on the Tamper IO less than 30us are filtered

DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_100_USEC 

Pulses on the Tamper IO less than 100us are filtered

DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH_200_USEC 

Pulses on the Tamper IO less than 200us are filtered

§ DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY

Enumerator
DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_DISABLE 

Edge detection polarity is disabled

DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_RISE 

Enables rising edge detection of input event

DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_FALL 

Enables falling edge detection of input event

DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY_BOTH 

Enables both rising and falling edge detection of input event

§ DL_LFSS_TAMPERIO_MODE

Enumerator
DL_LFSS_TAMPERIO_MODE_TAMPER 

The Tamper IO is set to tamper mode

DL_LFSS_TAMPERIO_MODE_IOMUX 

The Tamper IO is set to IOMUX mode

§ DL_LFSS_HEARTBEAT_INTERVAL

Enumerator
DL_LFSS_HEARTBEAT_INTERVAL_0_125_SEC 

Heart beat generator interval is 0.125 sec

DL_LFSS_HEARTBEAT_INTERVAL_0_25_SEC 

Heart beat generator interval is 0.25 sec

DL_LFSS_HEARTBEAT_INTERVAL_05_SEC 

Heart beat generator interval is 0.5 sec

DL_LFSS_HEARTBEAT_INTERVAL_1_SEC 

Heart beat generator interval is 1 sec

DL_LFSS_HEARTBEAT_INTERVAL_2_SEC 

Heart beat generator interval is 2 sec

DL_LFSS_HEARTBEAT_INTERVAL_4_SEC 

Heart beat generator interval is 4 sec

DL_LFSS_HEARTBEAT_INTERVAL_8_SEC 

Heart beat generator interval is 8 sec

DL_LFSS_HEARTBEAT_INTERVAL_16_SEC 

Heart beat generator interval is 16 sec

§ DL_LFSS_HEARTBEAT_PULSE_WIDTH

Enumerator
DL_LFSS_HEARTBEAT_PULSE_WIDTH_1_MSEC 

Heart beat generator pulse width is 1 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_2_MSEC 

Heart beat generator pulse width is 2 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_4_MSEC 

Heart beat generator pulse width is 4 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_8_MSEC 

Heart beat generator pulse width is 8 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_16_MSEC 

Heart beat generator pulse width is 16 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_32_MSEC 

Heart beat generator pulse width is 32 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_64_MSEC 

Heart beat generator pulse width is 64 msec

DL_LFSS_HEARTBEAT_PULSE_WIDTH_128_MSEC 

Heart beat generator pulse width is 128 msec

§ DL_LFSS_HEARTBEAT_MODE

Enumerator
DL_LFSS_HEARTBEAT_MODE_DISABLED 

Heart beat generator mode is disabled

DL_LFSS_HEARTBEAT_MODE_ALWAYS_ON 

Heart beat generator mode is always enabled

DL_LFSS_HEARTBEAT_MODE_TIME_STAMP 

Heart beat generator mode is enabled when time stamp event is detected

DL_LFSS_HEARTBEAT_MODE_POWER_FAIL 

Heart beat generator mode is enabled when the main power supply fails

§ DL_LFSS_TAMPERIO_IIDX

Enumerator
DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_0 

LFSS Tamper interrupt index for Tamper IO 0

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_1 

LFSS Tamper interrupt index for Tamper IO 1

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_2 

LFSS Tamper interrupt index for Tamper IO 2

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_3 

LFSS Tamper interrupt index for Tamper IO 3

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_4 

LFSS Tamper interrupt index for Tamper IO 4

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_5 

LFSS Tamper interrupt index for Tamper IO 5

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_6 

LFSS Tamper interrupt index for Tamper IO 6

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_7 

LFSS Tamper interrupt index for Tamper IO 7

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_8 

LFSS Tamper interrupt index for Tamper IO 8

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_9 

LFSS Tamper interrupt index for Tamper IO 9

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_10 

LFSS Tamper interrupt index for Tamper IO 10

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_11 

LFSS Tamper interrupt index for Tamper IO 11

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_12 

LFSS Tamper interrupt index for Tamper IO 12

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_13 

LFSS Tamper interrupt index for Tamper IO 13

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_14 

LFSS Tamper interrupt index for Tamper IO 14

DL_LFSS_TAMPERIO_IIDX_TAMPER_IO_15 

LFSS Tamper interrupt index for Tamper IO 15

§ DL_LFSS_SCRATCHPAD_MEM_WORD

Enumerator
DL_LFSS_SCRATCHPAD_MEM_WORD_0 

LFSS Scratch Pad memory word 0

DL_LFSS_SCRATCHPAD_MEM_WORD_1 

LFSS Scratch Pad memory word 1

DL_LFSS_SCRATCHPAD_MEM_WORD_2 

LFSS Scratch Pad memory word 2

DL_LFSS_SCRATCHPAD_MEM_WORD_3 

LFSS Scratch Pad memory word 3

DL_LFSS_SCRATCHPAD_MEM_WORD_4 

LFSS Scratch Pad memory word 4

DL_LFSS_SCRATCHPAD_MEM_WORD_5 

LFSS Scratch Pad memory word 5

DL_LFSS_SCRATCHPAD_MEM_WORD_6 

LFSS Scratch Pad memory word 6

DL_LFSS_SCRATCHPAD_MEM_WORD_7 

LFSS Scratch Pad memory word 7

§ DL_LFSS_SCRATCHPAD_MEM_BYTE

Enumerator
DL_LFSS_SCRATCHPAD_MEM_BYTE_0 

LFSS Scratch Pad memory byte 0 of the given Scratch Pad memory word

DL_LFSS_SCRATCHPAD_MEM_BYTE_1 

LFSS Scratch Pad memory byte 1 of the given Scratch Pad memory word

DL_LFSS_SCRATCHPAD_MEM_BYTE_2 

LFSS Scratch Pad memory byte 2 of the given Scratch Pad memory word

DL_LFSS_SCRATCHPAD_MEM_BYTE_3 

LFSS Scratch Pad memory byte 3 of the given Scratch Pad memory word

§ DL_LFSS_IWDT_CLOCK_DIVIDE

Enumerator
DL_LFSS_IWDT_CLOCK_DIVIDE_1 

WDT Clock divide by 1

DL_LFSS_IWDT_CLOCK_DIVIDE_2 

WDT Clock divide by 2

DL_LFSS_IWDT_CLOCK_DIVIDE_3 

WDT Clock divide by 3

DL_LFSS_IWDT_CLOCK_DIVIDE_4 

WDT Clock divide by 4

DL_LFSS_IWDT_CLOCK_DIVIDE_5 

WDT Clock divide by 5

DL_LFSS_IWDT_CLOCK_DIVIDE_6 

WDT Clock divide by 6

DL_LFSS_IWDT_CLOCK_DIVIDE_7 

WDT Clock divide by 7

DL_LFSS_IWDT_CLOCK_DIVIDE_8 

WDT Clock divide by 8

§ DL_LFSS_IWDT_TIMER_PERIOD

Enumerator
DL_LFSS_IWDT_TIMER_PERIOD_6_BITS 

WDT 2^6 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_8_BITS 

WDT 2^8 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_10_BITS 

WDT 2^10 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_12_BITS 

WDT 2^12 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_15_BITS 

WDT 2^15 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_18_BITS 

WDT 2^18 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_21_BITS 

WDT 2^21 timer period count

DL_LFSS_IWDT_TIMER_PERIOD_25_BITS 

WDT 2^25 timer period count

Function Documentation

§ DL_LFSS_TamperIO_enableOutputInversion()

__STATIC_INLINE void DL_LFSS_TamperIO_enableOutputInversion ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Enable output inversion for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

§ DL_LFSS_TamperIO_isOutputInversionEnabled()

__STATIC_INLINE bool DL_LFSS_TamperIO_isOutputInversionEnabled ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Checks if output inversion is enabled for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
Returns
Returns if output inversion is enabled
Return values
trueOutput inversion for the Tamper I/O is enabled
falseOutput inversion for the Tamper I/O is disabled

§ DL_LFSS_TamperIO_disableOutputInversion()

__STATIC_INLINE void DL_LFSS_TamperIO_disableOutputInversion ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Disable output inversion for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO

§ DL_LFSS_TamperIO_setOutputSource()

__STATIC_INLINE void DL_LFSS_TamperIO_setOutputSource ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO,
DL_LFSS_TAMPERIO_OUTPUT_SOURCE  source 
)

Selects the source for the tamper output (TOUT) control for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
[in]sourceThe source for the tamper output control. One of DL_LFSS_TAMPERIO_OUTPUT_SOURCE.

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getOutputSource()

__STATIC_INLINE DL_LFSS_TAMPERIO_OUTPUT_SOURCE DL_LFSS_TamperIO_getOutputSource ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the source for the tamper output (TOUT) control for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The output source of the tamper IO
Return values
Oneof DL_LFSS_TAMPERIO_OUTPUT_SOURCE

§ DL_LFSS_TamperIO_setGlitchFilterWidth()

__STATIC_INLINE void DL_LFSS_TamperIO_setGlitchFilterWidth ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO,
DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH  width 
)

Selects the filter width for the digital glitch filter for the specified Tamper IO.

The tamper event detection allows to configure one or more tamper IO’s to trigger a timestamp event and to generate an interrupt to the CPU. To minimize false triggers, a digital filter circuit is inserted into the IO path. Only pulses that are longer than the configured filter width will be registered as a tamper event.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
[in]widthThe width of the digital glitch filter. Pulses smaller than this width will be filtered. One of DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH.

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getGlitchFilterWidth()

__STATIC_INLINE DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH DL_LFSS_TamperIO_getGlitchFilterWidth ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the filter width for the digital glitch filter for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The digital glitch filter width
Return values
Oneof DL_LFSS_TAMPERIO_GLITCH_FILTER_WIDTH

§ DL_LFSS_TamperIO_setEdgeDetectionPolarity()

__STATIC_INLINE void DL_LFSS_TamperIO_setEdgeDetectionPolarity ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO,
DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY  polarity 
)

Selects the edge detection polarity for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
[in]polarityThe edge detection polarity. One of DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY.

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getEdgeDetectionPolarity()

__STATIC_INLINE DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY DL_LFSS_TamperIO_getEdgeDetectionPolarity ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the edge detection polarity for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The edge detection polarity for the specified Tamper IO
Return values
Oneof DL_LFSS_TAMPERIO_EDGE_DETECTION_POLARITY

§ DL_LFSS_TamperIO_enableInternalPullUp()

__STATIC_INLINE void DL_LFSS_TamperIO_enableInternalPullUp ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Enable internal pull-up resistor for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

§ DL_LFSS_TamperIO_isInternalPullUpEnabled()

__STATIC_INLINE bool DL_LFSS_TamperIO_isInternalPullUpEnabled ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Checks if internal pull-up resistor is enabled for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
Returns
Returns the internal pull-up resistor enabled status
Return values
trueInternal pull-up resistor for the Tamper I/O is enabled
falseInternal pull-up resistor for the Tamper I/O is disabled

§ DL_LFSS_TamperIO_disableInternalPullUp()

__STATIC_INLINE void DL_LFSS_TamperIO_disableInternalPullUp ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Disable internal pull-up resistor for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO

§ DL_LFSS_TamperIO_enableInternalPullDown()

__STATIC_INLINE void DL_LFSS_TamperIO_enableInternalPullDown ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Enable internal pull-down resistor for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

§ DL_LFSS_TamperIO_isInternalPullDownEnabled()

__STATIC_INLINE bool DL_LFSS_TamperIO_isInternalPullDownEnabled ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Checks if internal pull-down resistor is enabled for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
Returns
Returns the internal pull-down resistor enabled status
Return values
trueInternal pull-down resistor for the Tamper I/O is enabled
falseInternal pull-down resistor for the Tamper I/O is disabled

§ DL_LFSS_TamperIO_disableInternalPullDown()

__STATIC_INLINE void DL_LFSS_TamperIO_disableInternalPullDown ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Disable internal pull-down resistor for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO

§ DL_LFSS_TamperIO_enableInput()

__STATIC_INLINE void DL_LFSS_TamperIO_enableInput ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Enable input path for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

§ DL_LFSS_TamperIO_isInputEnabled()

__STATIC_INLINE bool DL_LFSS_TamperIO_isInputEnabled ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Checks if input is enabled for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
Returns
Returns the input enabled status
Return values
trueInput for the Tamper I/O is enabled
falseInput for the Tamper I/O is disabled

§ DL_LFSS_TamperIO_disableInput()

__STATIC_INLINE void DL_LFSS_TamperIO_disableInput ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Disable input path for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO

§ DL_LFSS_TamperIO_setMode()

__STATIC_INLINE void DL_LFSS_TamperIO_setMode ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO,
DL_LFSS_TAMPERIO_MODE  mode 
)

Selects the mode for the specified Tamper IO.

The tamper IOs have two modes of operation:

  • In IOMUX mode (DL_LFSS_TAMPERIO_MODE_IOMUX), the tamper IO input and output path are connected to the SoC IOMUX module and the IO can be used as a second function.
  • In tamper mode (DL_LFSS_TAMPERIO_MODE_TAMPER), the tamper IO is completely controlled by the VBAT IP and will remain functional during the power loss of the main supply or during SHUTDOWN mode.
Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO
[in]modeThe mode for the specified tamper IO. One of DL_LFSS_TAMPERIO_MODE.

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getMode()

__STATIC_INLINE DL_LFSS_TAMPERIO_MODE DL_LFSS_TamperIO_getMode ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the mode for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The mode for the specified Tamper IO
Return values
Oneof DL_LFSS_TAMPERIO_MODE

§ DL_LFSS_TamperIO_enableOutput()

__STATIC_INLINE void DL_LFSS_TamperIO_enableOutput ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Enable data output for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

References LFSS_TAMPER_IO_PIN_ENABLE.

§ DL_LFSS_TamperIO_disableOutput()

__STATIC_INLINE void DL_LFSS_TamperIO_disableOutput ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Disable data output for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.

References LFSS_TAMPER_IO_PIN_ENABLE.

§ DL_LFSS_TamperIO_isOutputEnabled()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_isOutputEnabled ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Checks if data output for the specified Tamper IO is enabled.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
If data output for the specified Tamper IO is enabled
Return values
trueData output for the tamper IO is enabled
falseData output for the tamper IO is disabled

References LFSS_TAMPER_IO_PIN_ENABLE, and LFSS_TAMPER_IO_PIN_MASK.

§ DL_LFSS_TamperIO_setOutputValue()

__STATIC_INLINE void DL_LFSS_TamperIO_setOutputValue ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO,
DL_LFSS_TAMPERIO_VALUE  outVal 
)

Enable data output value as zero for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO to configure. One of DL_LFSS_TAMPERIO.
[in]outValThe data value to set the tamper IO output to. One of DL_LFSS_TAMPERIO_VALUE.

References DL_Common_updateReg(), and LFSS_TAMPER_IO_PIN_MASK.

§ DL_LFSS_TamperIO_getOutputValue()

__STATIC_INLINE DL_LFSS_TAMPERIO_VALUE DL_LFSS_TamperIO_getOutputValue ( LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the output data value for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The output data value for the specified tamper IO
Return values
Oneof DL_LFSS_TAMPERIO_VALUE

References LFSS_TAMPER_IO_PIN_MASK.

§ DL_LFSS_TamperIO_getInputValue()

__STATIC_INLINE DL_LFSS_TAMPERIO_VALUE DL_LFSS_TamperIO_getInputValue ( const LFSS_Regs *  lfss,
DL_LFSS_TAMPERIO  tamperIO 
)

Gets the input data value for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]tamperIOSpecifies the tamper IO. One of DL_LFSS_TAMPERIO
Returns
The input data value for the specified tamper IO
Return values
Oneof DL_LFSS_TAMPERIO_VALUE

References LFSS_TAMPER_IO_PIN_MASK.

§ DL_LFSS_TamperIO_setHeartBeatInterval()

__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatInterval ( LFSS_Regs *  lfss,
DL_LFSS_HEARTBEAT_INTERVAL  interval 
)

Sets the interval for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]intervalThe interval of the heart beat generator. One of DL_LFSS_HEARTBEAT_INTERVAL

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getHeartBeatInterval()

__STATIC_INLINE DL_LFSS_HEARTBEAT_INTERVAL DL_LFSS_TamperIO_getHeartBeatInterval ( const LFSS_Regs *  lfss)

Gets the interval for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
The interval for the heart beat generator.
Return values
Oneof DL_LFSS_HEARTBEAT_INTERVAL

§ DL_LFSS_TamperIO_setHeartBeatPulseWidth()

__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatPulseWidth ( LFSS_Regs *  lfss,
DL_LFSS_HEARTBEAT_PULSE_WIDTH  width 
)

Sets the pulse width for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]widthThe pulse width of the heart beat generator. One of DL_LFSS_HEARTBEAT_PULSE_WIDTH

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getHeartBeatPulseWidth()

__STATIC_INLINE DL_LFSS_HEARTBEAT_PULSE_WIDTH DL_LFSS_TamperIO_getHeartBeatPulseWidth ( const LFSS_Regs *  lfss)

Gets the pulse width for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
The pulse width for the heart beat generator.
Return values
Oneof DL_LFSS_HEARTBEAT_PULSE_WIDTH

§ DL_LFSS_TamperIO_setHeartBeatMode()

__STATIC_INLINE void DL_LFSS_TamperIO_setHeartBeatMode ( LFSS_Regs *  lfss,
DL_LFSS_HEARTBEAT_MODE  mode 
)

Sets the mode for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]modeThe mode of the heart beat generator. One of DL_LFSS_HEARTBEAT_MODE

References DL_Common_updateReg().

§ DL_LFSS_TamperIO_getHeartBeatMode()

__STATIC_INLINE DL_LFSS_HEARTBEAT_MODE DL_LFSS_TamperIO_getHeartBeatMode ( const LFSS_Regs *  lfss)

Gets the pulse mode for the heart beat generator.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
The pulse mode for the heart beat generator.
Return values
Oneof DL_LFSS_HEARTBEAT_MODE

§ DL_LFSS_TamperIO_enableWriteProtectLock()

__STATIC_INLINE void DL_LFSS_TamperIO_enableWriteProtectLock ( LFSS_Regs *  lfss)

Enable write protection lock of the TIOCTL and HEARTBEAT registers from accidental updates.

When enabled, the TIOCTL and HEARTBEAT registers will have read-only access.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral

§ DL_LFSS_TamperIO_isWriteProtectLockEnabled()

__STATIC_INLINE bool DL_LFSS_TamperIO_isWriteProtectLockEnabled ( const LFSS_Regs *  lfss)

Checks if write protection lock of the TIOCTL and HEARTBEAT registers is enabled for the specified Tamper IO.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
Returns the enabled status of the write protection lock
Return values
trueWrite protection lock is enabled
falseWrite protection lock is disabled

§ DL_LFSS_TamperIO_disableWriteProtectLock()

__STATIC_INLINE void DL_LFSS_TamperIO_disableWriteProtectLock ( LFSS_Regs *  lfss)

Disable write protection lock of the TIOCTL and HEARTBEAT registers.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral

§ DL_LFSS_IWDT_enableModule()

__STATIC_INLINE void DL_LFSS_IWDT_enableModule ( LFSS_Regs *  lfss)

Enables the Watchdog module.

Parameters
lfssPointer to the register overlay for the peripheral

§ DL_LFSS_IWDT_disableModule()

__STATIC_INLINE void DL_LFSS_IWDT_disableModule ( LFSS_Regs *  lfss)

Disables the Watchdog module.

Parameters
lfssPointer to the register overlay for the peripheral

§ DL_LFSS_IWDT_isModuleEnabled()

__STATIC_INLINE bool DL_LFSS_IWDT_isModuleEnabled ( const LFSS_Regs *  lfss)

Returns if Watchdog module is on.

Parameters
lfssPointer to the register overlay for the peripheral
Returns
true Watchdog is enabled
false Watchdog is disabled

§ DL_LFSS_IWDT_enableFreeRun()

__STATIC_INLINE void DL_LFSS_IWDT_enableFreeRun ( LFSS_Regs *  lfss)

Enables the Watchdog free run control.

When enabled, the Watchdog will continue to free run and ignores the state of the CPU halted debug state

Parameters
lfssPointer to the register overlay for the peripheral

§ DL_LFSS_IWDT_disableFreeRun()

__STATIC_INLINE void DL_LFSS_IWDT_disableFreeRun ( LFSS_Regs *  lfss)

Disables the Watchdog free run control.

Parameters
lfssPointer to the register overlay for the peripheral

§ DL_LFSS_IWDT_isFreeRunEnabled()

__STATIC_INLINE bool DL_LFSS_IWDT_isFreeRunEnabled ( const LFSS_Regs *  lfss)

Returns if Watchdog free run control is enabled.

Parameters
lfssPointer to the register overlay for the peripheral
Returns
true Watchdog free run control is enabled
false Watchdog free run control is disabled

§ DL_LFSS_IWDT_setClockDivider()

__STATIC_INLINE void DL_LFSS_IWDT_setClockDivider ( LFSS_Regs *  lfss,
DL_LFSS_IWDT_CLOCK_DIVIDE  divider 
)

Sets the clock divider for the WDT module.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]dividerThe WDT clock divider to set. One of DL_LFSS_IWDT_CLOCK_DIVIDE.

References DL_Common_updateReg().

§ DL_LFSS_IWDT_getClockDivider()

__STATIC_INLINE DL_LFSS_IWDT_CLOCK_DIVIDE DL_LFSS_IWDT_getClockDivider ( const LFSS_Regs *  lfss)

Gets the clock divider for the WDT module.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
The clock divider for the WDT module
Return values
Oneof DL_LFSS_IWDT_CLOCK_DIVIDE

§ DL_LFSS_IWDT_setTimerPeriod()

__STATIC_INLINE void DL_LFSS_IWDT_setTimerPeriod ( LFSS_Regs *  lfss,
DL_LFSS_IWDT_TIMER_PERIOD  period 
)

Sets the timer period for the WDT module.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]periodThe WDT timer period to set. One of DL_LFSS_IWDT_TIMER_PERIOD.

References DL_Common_updateReg().

§ DL_LFSS_IWDT_getTimerPeriod()

__STATIC_INLINE DL_LFSS_IWDT_TIMER_PERIOD DL_LFSS_IWDT_getTimerPeriod ( const LFSS_Regs *  lfss)

Get the timer period for the WDT module.

Parameters
[in]lfssPointer to the register overlay for peripheral
Returns
The current timer period for the WDT module
Return values
Oneof DL_LFSS_IWDT_TIMER_PERIOD

§ DL_LFSS_IWDT_restart()

__STATIC_INLINE void DL_LFSS_IWDT_restart ( LFSS_Regs *  lfss)

Restarts the Watchdog.

Parameters
[in]lfssPointer to the register overlay for peripheral

§ DL_LFSS_IWDT_isWatchdogRunning()

__STATIC_INLINE bool DL_LFSS_IWDT_isWatchdogRunning ( const LFSS_Regs *  lfss)

Returns if Watchdog module is running.

Parameters
lfssPointer to the register overlay for the peripheral
Returns
true Watchdog module is running
false Watchdog counter has stopped

§ DL_LFSS_IWDT_enableWriteProtect()

__STATIC_INLINE void DL_LFSS_IWDT_enableWriteProtect ( LFSS_Regs *  lfss)

Enable write protection lock of the WDTEN and WDTCTL registers from accidental updates.

When enabled, the WDTEN and WDTCTL registers will have read-only access.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral

§ DL_LFSS_IWDT_isWriteProtectEnabled()

__STATIC_INLINE bool DL_LFSS_IWDT_isWriteProtectEnabled ( const LFSS_Regs *  lfss)

Checks if write protection lock of the WDTEN and WDTCTL registers is enabled.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
Returns
Returns the enabled status of the write protection lock
Return values
trueWrite protection lock is enabled
falseWrite protection lock is disabled

§ DL_LFSS_IWDT_disableWriteProtect()

__STATIC_INLINE void DL_LFSS_IWDT_disableWriteProtect ( LFSS_Regs *  lfss)

Disable write protection lock of the WDTEN and WDTCTL registers.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral

§ DL_LFSS_writeScratchPadData32()

__STATIC_INLINE void DL_LFSS_writeScratchPadData32 ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
uint32_t  data 
)

Write a word in scratch pad memory.

The VBAT scratch pad memory is register based memory that will retain data as long as VBAT is supplied. Refer to the device TRM for details on the specific size and implementation of the scratch pad memory.

This API wil write 32-bit data to the selected word in the scratch pad memory.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word to write to. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]dataThe 32-bit data to write to the specified scratch pad memory word. Value in range of [0x0, 0xFFFFFFF].

§ DL_LFSS_writeScratchPadData8()

__STATIC_INLINE void DL_LFSS_writeScratchPadData8 ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex,
uint32_t  data 
)

Write to a single byte in scratch pad memory.

The VBAT scratch pad memory is register based memory that will retain data as long as VBAT is supplied. Refer to the device TRM for details on the specific size and implementation of the scratch pad memory.

This API will write 8-bit data to the selected byte in the scratch pad memory. The byte to write to is given in context of the scratch pad memory word that contains that byte. For example, to write to BYTE5 of scratch pad memory, the user will call this API with parameters DL_LFSS_SCRATCHPAD_MEM_WORD_1 and DL_LFSS_SCRATCHPAD_MEM_BYTE_1.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word to write to. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified scratch pad memory byte to write to. One of DL_LFSS_SCRATCHPAD_MEM_BYTE
[in]dataThe 8-bit data to write to the specified scratch pad memory byte. Value in range of [0x0, 0xFF].

References DL_Common_updateReg().

§ DL_LFSS_readScratchPadDataWord()

__STATIC_INLINE uint32_t DL_LFSS_readScratchPadDataWord ( const LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex 
)

Read the specified word in scratch pad memory.

The VBAT scratch pad memory is register based memory that will retain data as long as VBAT is supplied. Refer to the device TRM for details on the specific size and implementation of the scratch pad memory.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word to read. One of DL_LFSS_SCRATCHPAD_MEM_WORD
Returns
The 32-bit data in the specified scratch pad memory word

§ DL_LFSS_readScratchPadDataByte()

__STATIC_INLINE uint8_t DL_LFSS_readScratchPadDataByte ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Read the specified byte in scratch pad memory.

The VBAT scratch pad memory is register based memory that will retain data as long as VBAT is supplied. Refer to the device TRM for details on the specific size and implementation of the scratch pad memory.

This API will read 8-bit data from the selected byte in the scratch pad memory. The byte to read to is given in context of the scratch pad memory word that contains that byte. For example, to read BYTE5 of scratch pad memory, the user will call this API with parameters DL_LFSS_SCRATCHPAD_MEM_WORD_1 and DL_LFSS_SCRATCHPAD_MEM_BYTE_1.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word to read. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified scratch pad memory byte to read. One of DL_LFSS_SCRATCHPAD_MEM_BYTE
Returns
The 8-bit data in the specified scratch pad memory byte

§ DL_LFSS_enableScratchPadWriteProtectByte()

__STATIC_INLINE void DL_LFSS_enableScratchPadWriteProtectByte ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Enable write protection lock of the specified byte in scratch pad memory from accidental updates.

When enabled, the specified byte in scratch pad memory will have read-only access.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified byte in scratch pad memory word to enable write protection for

§ DL_LFSS_isScratchPadWriteProtectByteEnabled()

__STATIC_INLINE bool DL_LFSS_isScratchPadWriteProtectByteEnabled ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Checks if write protection is enabled for the specified byte in scratch pad memory.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified scratch pad memory byte. One of DL_LFSS_SCRATCHPAD_MEM_BYTE
Returns
Returns if write protection is enabled for the specified byte
Return values
trueWrite protection for the specified byte is enabled
falseWrite protection for the specified byte is disabled

§ DL_LFSS_disableScratchPadWriteProtectByte()

__STATIC_INLINE void DL_LFSS_disableScratchPadWriteProtectByte ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Disable write protection lock of the specified byte in scratch pad memory.

When disables, the specified byte in scratch pad memory will have read-only access.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified byte in scratch pad memory word to disable write protection for. One of DL_LFSS_SCRATCHPAD_MEM_BYTE

§ DL_LFSS_enableScratchPadTamperEraseByte()

__STATIC_INLINE void DL_LFSS_enableScratchPadTamperEraseByte ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Enable tamper erase of the specified byte in scratch pad memory.

When enabled, the specified byte in scratch pad memory will be erased in the event of a tamper detect.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified byte in scratch pad memory word to enable tamper erase for. One of DL_LFSS_SCRATCHPAD_MEM_BYTE

§ DL_LFSS_isScratchPadTamperEraseByteEnabled()

__STATIC_INLINE bool DL_LFSS_isScratchPadTamperEraseByteEnabled ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Checks if tamper erase is enabled for the specified byte in scratch pad memory.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified byte in scratch pad memory byte. One of DL_LFSS_SCRATCHPAD_MEM_BYTE
Returns
Returns if tamper erase is enabled for the specified byte
Return values
trueTamper erase for the specified byte is enabled
falsetamper erase for the specified byte is disabled

§ DL_LFSS_disableScratchPadTamperEraseByte()

__STATIC_INLINE void DL_LFSS_disableScratchPadTamperEraseByte ( LFSS_Regs *  lfss,
DL_LFSS_SCRATCHPAD_MEM_WORD  memIndex,
DL_LFSS_SCRATCHPAD_MEM_BYTE  byteIndex 
)

Disable tamper erase of the specified byte in scratch pad memory.

The specified byte in scratch pad memory will not be erased in the event of a tamper detect.

Parameters
[in]lfssPointer to the register overlay for the LFSS peripheral
[in]memIndexThe specified scratch pad memory word to write to. One of DL_LFSS_SCRATCHPAD_MEM_WORD
[in]byteIndexThe specified byte in scratch pad memory word to disable tamper erase for. One of DL_LFSS_SCRATCHPAD_MEM_BYTE

§ DL_LFSS_TamperIO_enableInterrupt()

__STATIC_INLINE void DL_LFSS_TamperIO_enableInterrupt ( LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Enable LFSS Tamper Interrupts.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to enable. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT.

§ DL_LFSS_TamperIO_disableInterrupt()

__STATIC_INLINE void DL_LFSS_TamperIO_disableInterrupt ( LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Disable LFSS Tamper interrupts.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to enable. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT

§ DL_LFSS_TamperIO_getEnabledInterrupts()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledInterrupts ( const LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Check which LFSS Tamper interrupts are enabled.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to check. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT
Returns
Which of the requested LFSS interrupts are enabled
Return values
LogicalOR of DL_LFSS_TAMPERIO_INTERRUPT values

§ DL_LFSS_TamperIO_getEnabledInterruptStatus()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledInterruptStatus ( const LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Check interrupt flag of enabled LFSS Tamper interrupts.

Checks if any of the LFSS Tamper interrupts that were previously enabled are pending.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to check. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT
Returns
Which of the requested LFSS Tamper interrupts are pending
Return values
LogicalOR of DL_LFSS_TAMPERIO_INTERRUPT values
See also
DL_LFSS_TAMPERIO_enableInterrupt

§ DL_LFSS_TamperIO_getRawInterruptStatus()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getRawInterruptStatus ( const LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Check interrupt flag of any LFSS Tamper interrupt.

Checks if any of the LFSS Tamper interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to check. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT
Returns
Which of the requested LFSS Tamper interrupts are pending
Return values
LogicalOR of DL_LFSS_TAMPERIO_INTERRUPT values

§ DL_LFSS_TamperIO_getPendingInterrupt()

__STATIC_INLINE DL_LFSS_TAMPERIO_IIDX DL_LFSS_TamperIO_getPendingInterrupt ( const LFSS_Regs *  lfss)

Get highest priority pending LFSS interrupt.

Checks if any of the LFSS interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
Returns
The highest priority pending LFSS Tamper interrupt
Return values
Oneof DL_LFSS_TAMPERIO_IIDX

§ DL_LFSS_TamperIO_clearInterruptStatus()

__STATIC_INLINE void DL_LFSS_TamperIO_clearInterruptStatus ( LFSS_Regs *  lfss,
uint32_t  interruptMask 
)

Clear pending LFSS Tamper interrupts.

Parameters
[in]lfssPointer to the register overlay for the LFSS Tamper peripheral
[in]interruptMaskBit mask of interrupts to check. Logical OR of DL_LFSS_TAMPERIO_INTERRUPT

§ DL_LFSS_TamperIO_enableEvent()

__STATIC_INLINE void DL_LFSS_TamperIO_enableEvent ( LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Enable LFSS Tamper event.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to enable. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.

§ DL_LFSS_TamperIO_disableEvent()

__STATIC_INLINE void DL_LFSS_TamperIO_disableEvent ( LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Disable LFSS Tamper event.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to enable. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.

§ DL_LFSS_TamperIO_getEnabledEvents()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledEvents ( const LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Check which LFSS Tamper events are enabled.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to check. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.
Returns
Which of the requested LFSS Tamper interrupts are enabled
Return values
BitwiseOR of DL_LFSS_TAMPERIO_EVENT values

§ DL_LFSS_TamperIO_getEnabledEventStatus()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getEnabledEventStatus ( const LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Check event flag of enabled LFSS Tamper event.

Checks if any of the LFSS Tamper events that were previously enabled are pending.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to check. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.
Returns
Which of the requested LFSS Tamper interrupts are pending
Return values
BitwiseOR of DL_LFSS_TAMPERIO_EVENT values
See also
DL_LFSS_TamperIO_enableInterrupt

§ DL_LFSS_TamperIO_getRawEventsStatus()

__STATIC_INLINE uint32_t DL_LFSS_TamperIO_getRawEventsStatus ( const LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Check interrupt flag of any LFSS Tamper event.

Checks if any events are pending. Events do not have to be previously enabled.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to check. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.
Returns
Which of the requested LFSS Tamper interrupts are pending
Return values
BitwiseOR of DL_LFSS_TAMPERIO_EVENT values

§ DL_LFSS_TamperIO_clearEventsStatus()

__STATIC_INLINE void DL_LFSS_TamperIO_clearEventsStatus ( LFSS_Regs *  lfss,
uint32_t  eventMask 
)

Clear pending LFSS Tamper events.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]eventMaskBit mask of interrupts to clear. Bitwise OR of DL_LFSS_TAMPERIO_EVENT.

§ DL_LFSS_TamperIO_setPublisherChanID()

__STATIC_INLINE void DL_LFSS_TamperIO_setPublisherChanID ( LFSS_Regs *  lfss,
uint8_t  chanID 
)

Sets the LFSS Tamper event publisher channel ID.

Parameters
[in]lfssPointer to the register overlay for the peripheral
[in]chanIDChannel ID number. Valid range 0-15. If ChanID == 0 publisher is disconnected.

§ DL_LFSS_TamperIO_getPublisherChanID()

__STATIC_INLINE uint8_t DL_LFSS_TamperIO_getPublisherChanID ( const LFSS_Regs *  lfss)

Gets the event publisher channel ID.

Parameters
[in]lfssPointer to the register overlay for the peripheral
Returns
Event publisher channel ID

§ DL_LFSS_reset()

__STATIC_INLINE void DL_LFSS_reset ( LFSS_Regs *  lfss)

Requests a reset to the LFSS module.

Parameters
[in]lfssPointer to the register overlay for the peripheral
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale