MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
ramSpeedCtrl Struct Reference

ramSpeedCtrl structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t speedInput: 15
 
uint32_t reserved: 17
 

Detailed Description

ramSpeedCtrl structure

Field Documentation

§ speedInput

uint32_t ramSpeedCtrl::speedInput

Speed Input

§ reserved

uint32_t ramSpeedCtrl::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale