MSPM0G3519SensorlessFOCMotorControlLibrary  1.0
Data Fields
MOTOR_T Struct Reference

Motor structure. More...

#include <motor.h>

Collaboration diagram for MOTOR_T:
Collaboration graph
[legend]

Data Fields

int16_t polePairs
 
int32_t rs
 
int32_t LdDt
 
int32_t LqDt
 
int32_t L0Dt
 
int32_t L1Dt
 
int32_t Ke
 
IQ_NUM_T InvKe
 
_Bool saliency
 

Detailed Description

Motor structure.

Field Documentation

§ polePairs

int16_t MOTOR_T::polePairs

Pole Pairs

§ rs

int32_t MOTOR_T::rs

Phase Resistance

§ LdDt

int32_t MOTOR_T::LdDt

D-Axis Inductance / Sampling Time

§ LqDt

int32_t MOTOR_T::LqDt

Q-Axis Inductance / Sampling Time

§ L0Dt

int32_t MOTOR_T::L0Dt

Common mode Inductance / Sampling Time

§ L1Dt

int32_t MOTOR_T::L1Dt

Differential mode Inductance / Sampling Time

§ Ke

int32_t MOTOR_T::Ke

BEMF Constant

§ InvKe

IQ_NUM_T MOTOR_T::InvKe

Inverse of BEMF Constant

§ saliency

_Bool MOTOR_T::saliency

Saliency: Defines SPMSM or IPMSM


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale