![]() |
![]() |
|
MSPM0G3507SensorlessFOCMotorControlLibrary
1.0
|


Go to the source code of this file.
Data Structures | |
| struct | CURRENT_OFFSET_T |
| Current offset structure. More... | |
| struct | measureCurrentFlags |
| measureCurrentFlags structure More... | |
| union | MEASURE_CURRENT_FLAGS_T |
| Measure current flag. More... | |
| struct | HAL_MEASURE_CURRENT_T |
| Measure current structure. More... | |
| struct | HAL_MEASURE_VOLTAGE_T |
| Measure voltage structure. More... | |
| struct | HAL_MEASURE_MOTOR_INPUTS_T |
| Measure motor inputs structure. More... | |
Macros | |
| #define | HAL_CURRENT_OFFSET_MEAS_BITS 5 |
| Current offset averaging factor 2^n. | |
| #define | HAL_CURRENT_OFFSET_MEAS_COUNT (1 << HAL_CURRENT_OFFSET_MEAS_BITS) |
| Current offset averaging counts. | |
| #define | INV_VDC_IQ_SCALING 25 |
| Inverse Vdc scaling. | |
Functions | |
| void | inputsInit (HAL_MEASURE_MOTOR_INPUTS_T *pMotorInputs) |
| Initializes motor iputs. More... | |
| void | measureCurrentOffset (HAL_MEASURE_MOTOR_INPUTS_T *pMotorInputs) |
| Measures offset of current input. More... | |
| _Bool | getMeasureOffsetStatus (HAL_MEASURE_MOTOR_INPUTS_T *pMotorInputs) |
| Status of offset measurement. More... | |
Variables | |
| HAL_MEASURE_MOTOR_INPUTS_T * | g_pMotorInputs |
| Extern motor inputs. | |
| enum VOLTAGE_GAIN_TYPES |
| enum CURRENT_SHUNT_TYPES |
HAL measurement types.
ADC sampling ratio types.
| void inputsInit | ( | HAL_MEASURE_MOTOR_INPUTS_T * | pMotorInputs | ) |
Initializes motor iputs.
| [in] | pMotorInputs | Pointer to motor input |
References MEASURE_CURRENT_FLAGS_T::b, HAL_MEASURE_MOTOR_INPUTS_T::current, HAL_MEASURE_CURRENT_T::currentShunt, FALSE, HAL_MEASURE_CURRENT_T::flags, HAL_MEASURE_CURRENT_T::i1Sum, HAL_MEASURE_CURRENT_T::i2Sum, HAL_MEASURE_CURRENT_T::iaSum, HAL_MEASURE_CURRENT_T::ibADC0Sum, HAL_MEASURE_CURRENT_T::ibADC1Sum, HAL_MEASURE_CURRENT_T::icSum, measureCurrentFlags::offsetAB_CStatus, measureCurrentFlags::offsetGainStatus, HAL_MEASURE_CURRENT_T::offsetMeasCount, measureCurrentFlags::offsetStatus, measureCurrentFlags::threeShuntDynamic, and measureCurrentFlags::threeShuntDynamicSet.
Referenced by measureCurrentOffset().
| void measureCurrentOffset | ( | HAL_MEASURE_MOTOR_INPUTS_T * | pMotorInputs | ) |
Measures offset of current input.
| [in] | pMotorInputs | Pointer to motor input |
References MC_ABC_T::a, MC_ABC_T::b, MEASURE_CURRENT_FLAGS_T::b, MC_ABC_T::c, COMPUTE_OFFSET, HAL_MEASURE_MOTOR_INPUTS_T::current, CURRENT_SINGLE_SHUNT, CURRENT_THREE_SHUNT_A_BC, CURRENT_THREE_SHUNT_AB_C, CURRENT_THREE_SHUNT_DYNAMIC, CURRENT_TWO_SHUNT_A_B, CURRENT_TWO_SHUNT_B_C, HAL_MEASURE_CURRENT_T::currentShunt, HAL_MEASURE_CURRENT_T::currentShuntSet, HAL_MEASURE_CURRENT_T::flags, HAL_CURRENT_OFFSET_MEAS_BITS, HAL_CURRENT_OFFSET_MEAS_COUNT, HAL_SetPhaseCurrentChannels(), CURRENT_OFFSET_T::i1Offset, HAL_MEASURE_CURRENT_T::i1Sum, CURRENT_OFFSET_T::i2Offset, HAL_MEASURE_CURRENT_T::i2Sum, HAL_MEASURE_CURRENT_T::iabcRaw, CURRENT_OFFSET_T::iaOffset, HAL_MEASURE_CURRENT_T::iaSum, CURRENT_OFFSET_T::ibADC0Offset, HAL_MEASURE_CURRENT_T::ibADC0Sum, CURRENT_OFFSET_T::ibADC1Offset, HAL_MEASURE_CURRENT_T::ibADC1Sum, CURRENT_OFFSET_T::icOffset, HAL_MEASURE_CURRENT_T::icSum, HAL_MEASURE_CURRENT_T::iFirstSample, inputsInit(), HAL_MEASURE_CURRENT_T::iSecondSample, OFFSET_COMPLETE, OFFSET_INIT, measureCurrentFlags::offsetAB_CStatus, HAL_MEASURE_CURRENT_T::offsetGainIMaxBy1, measureCurrentFlags::offsetGainStatus, HAL_MEASURE_CURRENT_T::offsetMeasCount, measureCurrentFlags::offsetStatus, HAL_MEASURE_CURRENT_T::state, and TRUE.
|
inline |
Status of offset measurement.
| [in] | pMotorInputs | Pointer to motor input |
| true | Offset measurement completed |
| false | Offset measurement not completed |
References MEASURE_CURRENT_FLAGS_T::b, HAL_MEASURE_MOTOR_INPUTS_T::current, HAL_MEASURE_CURRENT_T::flags, and measureCurrentFlags::offsetStatus.
Referenced by HAL_ReadCurrents().