MSPM0G3519SensoredFOCMotorControlLibrary  1.0
Data Fields
ramAlgoDebugCtrl1 Struct Reference

ramAlgoDebugCtrl1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t reserved1: 31
 
uint32_t clearFlt: 1
 

Detailed Description

ramAlgoDebugCtrl1 structure

Field Documentation

§ reserved1

uint32_t ramAlgoDebugCtrl1::reserved1

Reserved

§ clearFlt

uint32_t ramAlgoDebugCtrl1::clearFlt

Clears all faults

Referenced by faultReportClear(), and FOC_fault_Recovery().


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale