MSPM0G3507SensoredFOCMotorControlLibrary  1.0
Data Fields
userInputMiscAlgo Struct Reference

userInputMiscAlgo1 structure More...

#include <appInputCtrlInterface.h>

Data Fields

uint32_t brkCurrPersist: 2
 
uint32_t reserved2: 3
 
uint32_t reserved1: 1
 
uint32_t clSlowAcc: 4
 
uint32_t reserved: 22
 

Detailed Description

userInputMiscAlgo1 structure

Field Documentation

§ brkCurrPersist

uint32_t userInputMiscAlgo::brkCurrPersist

Persistence time for declaring motor is stopped after applying brake

§ reserved2

uint32_t userInputMiscAlgo::reserved2

Minimum BEMF for handoff

§ reserved1

uint32_t userInputMiscAlgo::reserved1

Reserved

§ clSlowAcc

uint32_t userInputMiscAlgo::clSlowAcc

Close loop acceleration when estimator is not yet fully aligned

Referenced by update_MiscAlgoConfig().

§ reserved

uint32_t userInputMiscAlgo::reserved

Reserved


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale