MSPM0C110X Driver Library  2.05.00.05
Modules | Enumerations | Functions
General Purpose Input/Output (GPIO)
Collaboration diagram for General Purpose Input/Output (GPIO):

Modules

 DL_GPIO_PIN
 
 DL_GPIO_EDGE_POLARITY
 
 DL_GPIO_INPUT_FILTER
 

Enumerations

enum  DL_GPIO_INVERSION {
  DL_GPIO_INVERSION_ENABLE = IOMUX_PINCM_INV_ENABLE,
  DL_GPIO_INVERSION_DISABLE = IOMUX_PINCM_INV_DISABLE
}
 
enum  DL_GPIO_DRIVE_STRENGTH {
  DL_GPIO_DRIVE_STRENGTH_LOW = IOMUX_PINCM_DRV_DRVVAL0,
  DL_GPIO_DRIVE_STRENGTH_HIGH = IOMUX_PINCM_DRV_DRVVAL1
}
 
enum  DL_GPIO_RESISTOR {
  DL_GPIO_RESISTOR_NONE,
  DL_GPIO_RESISTOR_PULL_UP,
  DL_GPIO_RESISTOR_PULL_DOWN
}
 
enum  DL_GPIO_HYSTERESIS {
  DL_GPIO_HYSTERESIS_ENABLE = IOMUX_PINCM_HYSTEN_ENABLE,
  DL_GPIO_HYSTERESIS_DISABLE = IOMUX_PINCM_HYSTEN_DISABLE
}
 
enum  DL_GPIO_WAKEUP {
  DL_GPIO_WAKEUP_ENABLE = IOMUX_PINCM_WUEN_ENABLE,
  DL_GPIO_WAKEUP_DISABLE = IOMUX_PINCM_WUEN_DISABLE,
  DL_GPIO_WAKEUP_ON_0 = (IOMUX_PINCM_WUEN_ENABLE | IOMUX_PINCM_WCOMP_MATCH0),
  DL_GPIO_WAKEUP_ON_1 = (IOMUX_PINCM_WUEN_ENABLE | IOMUX_PINCM_WCOMP_MATCH1)
}
 
enum  DL_GPIO_WAKEUP_COMPARE_VALUE {
  DL_GPIO_WAKEUP_COMPARE_VALUE_0 = IOMUX_PINCM_WCOMP_MATCH0,
  DL_GPIO_WAKEUP_COMPARE_VALUE_1 = IOMUX_PINCM_WCOMP_MATCH1
}
 
enum  DL_GPIO_HIZ {
  DL_GPIO_HIZ_ENABLE = IOMUX_PINCM_HIZ1_ENABLE,
  DL_GPIO_HIZ_DISABLE = IOMUX_PINCM_HIZ1_DISABLE
}
 
enum  DL_GPIO_EVENT_ROUTE {
  DL_GPIO_EVENT_ROUTE_1 = 0,
  DL_GPIO_EVENT_ROUTE_2 = 12
}
 
enum  DL_GPIO_PUBLISHER_INDEX {
  DL_GPIO_PUBLISHER_INDEX_0 = 0,
  DL_GPIO_PUBLISHER_INDEX_1 = 1
}
 
enum  DL_GPIO_SUBSCRIBER_INDEX {
  DL_GPIO_SUBSCRIBER_INDEX_0 = 0,
  DL_GPIO_SUBSCRIBER_INDEX_1 = 1
}
 
enum  DL_GPIO_SUBSCRIBER_OUT_POLICY {
  DL_GPIO_SUBSCRIBER_OUT_POLICY_SET = GPIO_SUB0CFG_OUTPOLICY_SET,
  DL_GPIO_SUBSCRIBER_OUT_POLICY_CLEAR = GPIO_SUB0CFG_OUTPOLICY_CLR,
  DL_GPIO_SUBSCRIBER_OUT_POLICY_TOGGLE = GPIO_SUB0CFG_OUTPOLICY_TOGGLE
}
 
enum  DL_GPIO_SUBSCRIBERx_PIN {
  DL_GPIO_SUBSCRIBER0_PIN_0 = 0x00000000,
  DL_GPIO_SUBSCRIBER0_PIN_1 = 0x00010000,
  DL_GPIO_SUBSCRIBER0_PIN_2 = 0x00020000,
  DL_GPIO_SUBSCRIBER0_PIN_3 = 0x00030000,
  DL_GPIO_SUBSCRIBER0_PIN_4 = 0x00040000,
  DL_GPIO_SUBSCRIBER0_PIN_5 = 0x00050000,
  DL_GPIO_SUBSCRIBER0_PIN_6 = 0x00060000,
  DL_GPIO_SUBSCRIBER0_PIN_7 = 0x00070000,
  DL_GPIO_SUBSCRIBER0_PIN_8 = 0x00080000,
  DL_GPIO_SUBSCRIBER0_PIN_9 = 0x00090000,
  DL_GPIO_SUBSCRIBER0_PIN_10 = 0x000A0000,
  DL_GPIO_SUBSCRIBER0_PIN_11 = 0x000B0000,
  DL_GPIO_SUBSCRIBER0_PIN_12 = 0x000C0000,
  DL_GPIO_SUBSCRIBER0_PIN_13 = 0x000D0000,
  DL_GPIO_SUBSCRIBER0_PIN_14 = 0x000E0000,
  DL_GPIO_SUBSCRIBER0_PIN_15 = 0x000F0000,
  DL_GPIO_SUBSCRIBER1_PIN_16 = 0x00000000,
  DL_GPIO_SUBSCRIBER1_PIN_17 = 0x00010000,
  DL_GPIO_SUBSCRIBER1_PIN_18 = 0x00020000,
  DL_GPIO_SUBSCRIBER1_PIN_19 = 0x00030000,
  DL_GPIO_SUBSCRIBER1_PIN_20 = 0x00040000,
  DL_GPIO_SUBSCRIBER1_PIN_21 = 0x00050000,
  DL_GPIO_SUBSCRIBER1_PIN_22 = 0x00060000,
  DL_GPIO_SUBSCRIBER1_PIN_23 = 0x00070000,
  DL_GPIO_SUBSCRIBER1_PIN_24 = 0x00080000,
  DL_GPIO_SUBSCRIBER1_PIN_25 = 0x00090000,
  DL_GPIO_SUBSCRIBER1_PIN_26 = 0x000A0000,
  DL_GPIO_SUBSCRIBER1_PIN_27 = 0x000B0000,
  DL_GPIO_SUBSCRIBER1_PIN_28 = 0x000C0000,
  DL_GPIO_SUBSCRIBER1_PIN_29 = 0x000D0000,
  DL_GPIO_SUBSCRIBER1_PIN_30 = 0x000E0000,
  DL_GPIO_SUBSCRIBER1_PIN_31 = 0x000F0000
}
 
enum  DL_GPIO_IIDX {
  DL_GPIO_IIDX_NO_INTR = GPIO_CPU_INT_IIDX_STAT_NO_INTR,
  DL_GPIO_IIDX_DIO0 = GPIO_CPU_INT_IIDX_STAT_DIO0,
  DL_GPIO_IIDX_DIO1 = GPIO_CPU_INT_IIDX_STAT_DIO1,
  DL_GPIO_IIDX_DIO2 = GPIO_CPU_INT_IIDX_STAT_DIO2,
  DL_GPIO_IIDX_DIO3 = GPIO_CPU_INT_IIDX_STAT_DIO3,
  DL_GPIO_IIDX_DIO4 = GPIO_CPU_INT_IIDX_STAT_DIO4,
  DL_GPIO_IIDX_DIO5 = GPIO_CPU_INT_IIDX_STAT_DIO5,
  DL_GPIO_IIDX_DIO6 = GPIO_CPU_INT_IIDX_STAT_DIO6,
  DL_GPIO_IIDX_DIO7 = GPIO_CPU_INT_IIDX_STAT_DIO7,
  DL_GPIO_IIDX_DIO8 = GPIO_CPU_INT_IIDX_STAT_DIO8,
  DL_GPIO_IIDX_DIO9 = GPIO_CPU_INT_IIDX_STAT_DIO9,
  DL_GPIO_IIDX_DIO10 = GPIO_CPU_INT_IIDX_STAT_DIO10,
  DL_GPIO_IIDX_DIO11 = GPIO_CPU_INT_IIDX_STAT_DIO11,
  DL_GPIO_IIDX_DIO12 = GPIO_CPU_INT_IIDX_STAT_DIO12,
  DL_GPIO_IIDX_DIO13 = GPIO_CPU_INT_IIDX_STAT_DIO13,
  DL_GPIO_IIDX_DIO14 = GPIO_CPU_INT_IIDX_STAT_DIO14,
  DL_GPIO_IIDX_DIO15 = GPIO_CPU_INT_IIDX_STAT_DIO15,
  DL_GPIO_IIDX_DIO16 = GPIO_CPU_INT_IIDX_STAT_DIO16,
  DL_GPIO_IIDX_DIO17 = GPIO_CPU_INT_IIDX_STAT_DIO17,
  DL_GPIO_IIDX_DIO18 = GPIO_CPU_INT_IIDX_STAT_DIO18,
  DL_GPIO_IIDX_DIO19 = GPIO_CPU_INT_IIDX_STAT_DIO19,
  DL_GPIO_IIDX_DIO20 = GPIO_CPU_INT_IIDX_STAT_DIO20,
  DL_GPIO_IIDX_DIO21 = GPIO_CPU_INT_IIDX_STAT_DIO21,
  DL_GPIO_IIDX_DIO22 = GPIO_CPU_INT_IIDX_STAT_DIO22,
  DL_GPIO_IIDX_DIO23 = GPIO_CPU_INT_IIDX_STAT_DIO23,
  DL_GPIO_IIDX_DIO24 = GPIO_CPU_INT_IIDX_STAT_DIO24,
  DL_GPIO_IIDX_DIO25 = GPIO_CPU_INT_IIDX_STAT_DIO25,
  DL_GPIO_IIDX_DIO26 = GPIO_CPU_INT_IIDX_STAT_DIO26,
  DL_GPIO_IIDX_DIO27 = GPIO_CPU_INT_IIDX_STAT_DIO27,
  DL_GPIO_IIDX_DIO28 = GPIO_CPU_INT_IIDX_STAT_DIO28,
  DL_GPIO_IIDX_DIO29 = GPIO_CPU_INT_IIDX_STAT_DIO29,
  DL_GPIO_IIDX_DIO30 = GPIO_CPU_INT_IIDX_STAT_DIO30,
  DL_GPIO_IIDX_DIO31 = GPIO_CPU_INT_IIDX_STAT_DIO31
}
 

Functions

__STATIC_INLINE void DL_GPIO_enablePower (GPIO_Regs *gpio)
 Enables the Peripheral Write Enable (PWREN) register for the GPIO. More...
 
__STATIC_INLINE void DL_GPIO_disablePower (GPIO_Regs *gpio)
 Disables the Peripheral Write Enable (PWREN) register for the GPIO. More...
 
__STATIC_INLINE bool DL_GPIO_isPowerEnabled (GPIO_Regs *gpio)
 Returns if the Peripheral Write Enable (PWREN) register for the GPIO is enabled. More...
 
__STATIC_INLINE void DL_GPIO_reset (GPIO_Regs *gpio)
 Resets gpio peripheral. More...
 
__STATIC_INLINE bool DL_GPIO_isReset (GPIO_Regs *gpio)
 Returns if gpio peripheral was reset. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalOutput (uint32_t pincmIndex)
 Configures a pin as a basic GPIO output. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalOutputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ)
 Configures a pin as a GPIO output. More...
 
__STATIC_INLINE void DL_GPIO_setDigitalInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor)
 Configures internal resistor for digital pin. More...
 
__STATIC_INLINE void DL_GPIO_setAnalogInternalResistor (uint32_t pincmIndex, DL_GPIO_RESISTOR internalResistor)
 Configures internal resistor for analog pin. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalInput (uint32_t pincmIndex)
 Configures a pin as a basic GPIO input. More...
 
__STATIC_INLINE void DL_GPIO_initDigitalInputFeatures (uint32_t pincmIndex, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup)
 Configures a pin as a GPIO input. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral output functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_DRIVE_STRENGTH driveStrength, DL_GPIO_HIZ hiZ)
 Configure a pin to operate with peripheral output functionality with optional features. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralInputFunction (uint32_t pincmIndex, uint32_t function)
 Configure a pin to operate with peripheral input functionality. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralInputFunctionFeatures (uint32_t pincmIndex, uint32_t function, DL_GPIO_INVERSION inversion, DL_GPIO_RESISTOR internalResistor, DL_GPIO_HYSTERESIS hysteresis, DL_GPIO_WAKEUP wakeup)
 Configure a pin to operate with peripheral input functionality with optional features. More...
 
__STATIC_INLINE void DL_GPIO_initPeripheralAnalogFunction (uint32_t pincmIndex)
 Configure a pin to operate with analog functionality. More...
 
__STATIC_INLINE void DL_GPIO_enableWakeUp (uint32_t pincmIndex)
 Set GPIO pin's wakeup enable bit. More...
 
__STATIC_INLINE void DL_GPIO_disableWakeUp (uint32_t pincmIndex)
 Clear GPIO pin's wakeup enable bit. More...
 
__STATIC_INLINE bool DL_GPIO_isWakeUpEnabled (uint32_t pincmIndex)
 Returns if GPIO pin's wake up bit is enabled. More...
 
__STATIC_INLINE void DL_GPIO_setWakeupCompareValue (uint32_t pincmIndex, DL_GPIO_WAKEUP_COMPARE_VALUE value)
 Set the compare value to use for wake for the specified pin. More...
 
__STATIC_INLINE DL_GPIO_WAKEUP_COMPARE_VALUE DL_GPIO_getWakeupCompareValue (uint32_t pincmIndex)
 Get the compare value to use for wake for the specified pin. More...
 
__STATIC_INLINE bool DL_GPIO_isWakeStateGenerated (uint32_t pincmIndex)
 Checks if the GPIO pin's Wake State bit is active. More...
 
__STATIC_INLINE uint32_t DL_GPIO_readPins (GPIO_Regs *gpio, uint32_t pins)
 Read a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_writePins (GPIO_Regs *gpio, uint32_t pins)
 Write a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_writePinsVal (GPIO_Regs *gpio, uint32_t pinsMask, uint32_t pinsVal)
 Update the value of one or more GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_setPins (GPIO_Regs *gpio, uint32_t pins)
 Set a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_clearPins (GPIO_Regs *gpio, uint32_t pins)
 Clear a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_togglePins (GPIO_Regs *gpio, uint32_t pins)
 Toggle a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_enableOutput (GPIO_Regs *gpio, uint32_t pins)
 Enable output on a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_disableOutput (GPIO_Regs *gpio, uint32_t pins)
 Disable output on a group of GPIO pins. More...
 
__STATIC_INLINE void DL_GPIO_enableDMAAccess (GPIO_Regs *gpio, uint32_t pins)
 Enable DMA access on a group of pins. More...
 
__STATIC_INLINE void DL_GPIO_disableDMAAccess (GPIO_Regs *gpio, uint32_t pins)
 Disable DMA access on a group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_isDMAccessEnabled (GPIO_Regs *gpio, uint32_t pins)
 Check if DMA access is enabled on a group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setLowerPinsPolarity (GPIO_Regs *gpio, uint32_t polarity)
 Set the polarity of all bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setUpperPinsPolarity (GPIO_Regs *gpio, uint32_t polarity)
 Set the polarity of all bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsPolarity (GPIO_Regs *gpio)
 Get the polarity of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsPolarity (GPIO_Regs *gpio)
 Get the polarity of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setLowerPinsInputFilter (GPIO_Regs *gpio, uint32_t filter)
 Set the input filter of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_setUpperPinsInputFilter (GPIO_Regs *gpio, uint32_t filter)
 Set the input filter of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsInputFilter (GPIO_Regs *gpio)
 Get the input filter of bits [0, 15] in the group of pins. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsInputFilter (GPIO_Regs *gpio)
 Get the input filter of bits [16, 31] in the group of pins. More...
 
__STATIC_INLINE void DL_GPIO_enableGlobalFastWake (GPIO_Regs *gpio)
 Enable Global Fast Wake. More...
 
__STATIC_INLINE void DL_GPIO_disableGlobalFastWake (GPIO_Regs *gpio)
 Disable Global Fast Wake. More...
 
__STATIC_INLINE void DL_GPIO_enableFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Enable fast wake for pins. More...
 
__STATIC_INLINE void DL_GPIO_disableFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Disable fast wake for pins. More...
 
__STATIC_INLINE void DL_GPIO_enableHiZ (uint32_t pincmIndex)
 Enable Hi-Z for the pin. More...
 
__STATIC_INLINE void DL_GPIO_disableHiZ (uint32_t pincmIndex)
 Disable Hi-Z for the pin. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledFastWakePins (GPIO_Regs *gpio, uint32_t pins)
 Check which pins have fast wake feature enabled. More...
 
__STATIC_INLINE void DL_GPIO_enableInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Enable GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_disableInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Disable GPIO interrupts. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterrupts (GPIO_Regs *gpio, uint32_t pins)
 Check which GPIO interrupts are enabled. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Check interrupt flag of enabled GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_setInterrupt (GPIO_Regs *gpio, uint32_t pins)
 Set interrupt flag of any GPIO. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getRawInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Check interrupt flag of any GPIO interrupt. More...
 
__STATIC_INLINE DL_GPIO_IIDX DL_GPIO_getPendingInterrupt (GPIO_Regs *gpio)
 Get highest priority pending GPIO interrupt. More...
 
__STATIC_INLINE void DL_GPIO_clearInterruptStatus (GPIO_Regs *gpio, uint32_t pins)
 Clear pending GPIO interrupts. More...
 
__STATIC_INLINE void DL_GPIO_configSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, DL_GPIO_SUBSCRIBER_OUT_POLICY policy, DL_GPIO_SUBSCRIBERx_PIN pinIndex)
 Configures GPIO subscriber. This API preserves enable/disbale status of subscriber. More...
 
__STATIC_INLINE void DL_GPIO_enableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Enables GPIO subscriber. More...
 
__STATIC_INLINE void DL_GPIO_disableSubscriber (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Disables GPIO subscriber. More...
 
__STATIC_INLINE bool DL_GPIO_isSubscriberEnabled (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Returns if GPIO subscriber is enabled. More...
 
__STATIC_INLINE void DL_GPIO_setPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index, uint8_t chanID)
 Sets the event publisher channel id. More...
 
__STATIC_INLINE uint8_t DL_GPIO_getPublisherChanID (GPIO_Regs *gpio, DL_GPIO_PUBLISHER_INDEX index)
 Gets the event publisher channel id. More...
 
__STATIC_INLINE void DL_GPIO_setSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index, uint8_t chanID)
 Sets the event subscriber channel id. More...
 
__STATIC_INLINE uint8_t DL_GPIO_getSubscriberChanID (GPIO_Regs *gpio, DL_GPIO_SUBSCRIBER_INDEX index)
 Gets the event subscriber channel id. More...
 
__STATIC_INLINE void DL_GPIO_enableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Enables GPIO events. More...
 
__STATIC_INLINE void DL_GPIO_disableEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Disable GPIO events. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledEvents (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Check which GPIO events are enabled. More...
 
__STATIC_INLINE uint32_t DL_GPIO_getEnabledEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Checks if any of the GPIO events which were previously enabled are pending. More...
 
__STATIC_INLINE void DL_GPIO_clearEventStatus (GPIO_Regs *gpio, DL_GPIO_EVENT_ROUTE index, uint32_t pins)
 Clear pending GPIO event. More...
 

Detailed Description

Overview

The GPIO Driver Library allows full configuration of the MSPM0 GPIO module. The GPIO peripheral provides the user with a means to write data out and read data in to and from the device pins. It also provides a way to detect wakeup events while the device is in a low power state.


Enumeration Type Documentation

§ DL_GPIO_INVERSION

Enumerator
DL_GPIO_INVERSION_ENABLE 

Enable Inversion

DL_GPIO_INVERSION_DISABLE 

Disable Inversion

§ DL_GPIO_DRIVE_STRENGTH

Enumerator
DL_GPIO_DRIVE_STRENGTH_LOW 

Disable High-Drive Strength

DL_GPIO_DRIVE_STRENGTH_HIGH 

Enable High-Drive (where allowed)

§ DL_GPIO_RESISTOR

Enumerator
DL_GPIO_RESISTOR_NONE 

Use no pull up/pull down resistors on pin

DL_GPIO_RESISTOR_PULL_UP 

Use a pull up resistor on the pin

DL_GPIO_RESISTOR_PULL_DOWN 

Use a pull down resistor on the pin

§ DL_GPIO_HYSTERESIS

Enumerator
DL_GPIO_HYSTERESIS_ENABLE 

Enable Hysteresis on pin

DL_GPIO_HYSTERESIS_DISABLE 

Disable Hysteresis on pin

§ DL_GPIO_WAKEUP

Enumerator
DL_GPIO_WAKEUP_ENABLE 

Wakeup enabled

DL_GPIO_WAKEUP_DISABLE 

Wakeup disabled

DL_GPIO_WAKEUP_ON_0 

Wakeup when pin changes to 0

DL_GPIO_WAKEUP_ON_1 

Wakeup when pin changes to 1

§ DL_GPIO_WAKEUP_COMPARE_VALUE

Enumerator
DL_GPIO_WAKEUP_COMPARE_VALUE_0 

Wakeup compare value of 0

DL_GPIO_WAKEUP_COMPARE_VALUE_1 

Wakeup compare value of 1

§ DL_GPIO_HIZ

Enumerator
DL_GPIO_HIZ_ENABLE 

Enable Hi-Z on pin

DL_GPIO_HIZ_DISABLE 

Disable Hi-Z on pin

§ DL_GPIO_EVENT_ROUTE

Enumerator
DL_GPIO_EVENT_ROUTE_1 

GPIO event route 1

DL_GPIO_EVENT_ROUTE_2 

GPIO event route 2

§ DL_GPIO_PUBLISHER_INDEX

Enumerator
DL_GPIO_PUBLISHER_INDEX_0 

GPIO Publisher index 0

DL_GPIO_PUBLISHER_INDEX_1 

GPIO Publisher index 1

§ DL_GPIO_SUBSCRIBER_INDEX

Enumerator
DL_GPIO_SUBSCRIBER_INDEX_0 

GPIO Subscriber index 0

DL_GPIO_SUBSCRIBER_INDEX_1 

GPIO Subscriber index 1

§ DL_GPIO_SUBSCRIBER_OUT_POLICY

Enumerator
DL_GPIO_SUBSCRIBER_OUT_POLICY_SET 

GPIO is set

DL_GPIO_SUBSCRIBER_OUT_POLICY_CLEAR 

GPIO is cleared

DL_GPIO_SUBSCRIBER_OUT_POLICY_TOGGLE 

GPIO is toggled

§ DL_GPIO_SUBSCRIBERx_PIN

Enumerator
DL_GPIO_SUBSCRIBER0_PIN_0 

Selects DIO 0 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_1 

Selects DIO 1 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_2 

Selects DIO 2 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_3 

Selects DIO 3 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_4 

Selects DIO 4 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_5 

Selects DIO 5 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_6 

Selects DIO 6 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_7 

Selects DIO 7 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_8 

Selects DIO 8 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_9 

Selects DIO 9 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_10 

Selects DIO 10 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_11 

Selects DIO 11 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_12 

Selects DIO 12 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_13 

Selects DIO 13 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_14 

Selects DIO 14 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER0_PIN_15 

Selects DIO 15 when Subscriber index 0 is selected

DL_GPIO_SUBSCRIBER1_PIN_16 

Selects DIO 16 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_17 

Selects DIO 17 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_18 

Selects DIO 18 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_19 

Selects DIO 19 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_20 

Selects DIO 20 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_21 

Selects DIO 21 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_22 

Selects DIO 22 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_23 

Selects DIO 23 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_24 

Selects DIO 24 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_25 

Selects DIO 25 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_26 

Selects DIO 26 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_27 

Selects DIO 27 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_28 

Selects DIO 28 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_29 

Selects DIO 29 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_30 

Selects DIO 30 when Subscriber index 1 is selected

DL_GPIO_SUBSCRIBER1_PIN_31 

Selects DIO 31 when Subscriber index 1 is selected

§ DL_GPIO_IIDX

Enumerator
DL_GPIO_IIDX_NO_INTR 

Interrupt index for no interrupt

DL_GPIO_IIDX_DIO0 

Interrupt index for GPIO DIO0

DL_GPIO_IIDX_DIO1 

Interrupt index for GPIO DIO1

DL_GPIO_IIDX_DIO2 

Interrupt index for GPIO DIO2

DL_GPIO_IIDX_DIO3 

Interrupt index for GPIO DIO3

DL_GPIO_IIDX_DIO4 

Interrupt index for GPIO DIO4

DL_GPIO_IIDX_DIO5 

Interrupt index for GPIO DIO5

DL_GPIO_IIDX_DIO6 

Interrupt index for GPIO DIO6

DL_GPIO_IIDX_DIO7 

Interrupt index for GPIO DIO7

DL_GPIO_IIDX_DIO8 

Interrupt index for GPIO DIO8

DL_GPIO_IIDX_DIO9 

Interrupt index for GPIO DIO9

DL_GPIO_IIDX_DIO10 

Interrupt index for GPIO DIO10

DL_GPIO_IIDX_DIO11 

Interrupt index for GPIO DIO11

DL_GPIO_IIDX_DIO12 

Interrupt index for GPIO DIO12

DL_GPIO_IIDX_DIO13 

Interrupt index for GPIO DIO13

DL_GPIO_IIDX_DIO14 

Interrupt index for GPIO DIO14

DL_GPIO_IIDX_DIO15 

Interrupt index for GPIO DIO15

DL_GPIO_IIDX_DIO16 

Interrupt index for GPIO DIO16

DL_GPIO_IIDX_DIO17 

Interrupt index for GPIO DIO17

DL_GPIO_IIDX_DIO18 

Interrupt index for GPIO DIO18

DL_GPIO_IIDX_DIO19 

Interrupt index for GPIO DIO19

DL_GPIO_IIDX_DIO20 

Interrupt index for GPIO DIO20

DL_GPIO_IIDX_DIO21 

Interrupt index for GPIO DIO21

DL_GPIO_IIDX_DIO22 

Interrupt index for GPIO DIO22

DL_GPIO_IIDX_DIO23 

Interrupt index for GPIO DIO23

DL_GPIO_IIDX_DIO24 

Interrupt index for GPIO DIO24

DL_GPIO_IIDX_DIO25 

Interrupt index for GPIO DIO25

DL_GPIO_IIDX_DIO26 

Interrupt index for GPIO DIO26

DL_GPIO_IIDX_DIO27 

Interrupt index for GPIO DIO27

DL_GPIO_IIDX_DIO28 

Interrupt index for GPIO DIO28

DL_GPIO_IIDX_DIO29 

Interrupt index for GPIO DIO29

DL_GPIO_IIDX_DIO30 

Interrupt index for GPIO DIO30

DL_GPIO_IIDX_DIO31 

Interrupt index for GPIO DIO31

Function Documentation

§ DL_GPIO_enablePower()

__STATIC_INLINE void DL_GPIO_enablePower ( GPIO_Regs *  gpio)

Enables the Peripheral Write Enable (PWREN) register for the GPIO.

Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.

Parameters
gpioPointer to the register overlay for the peripheral

§ DL_GPIO_disablePower()

__STATIC_INLINE void DL_GPIO_disablePower ( GPIO_Regs *  gpio)

Disables the Peripheral Write Enable (PWREN) register for the GPIO.

When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.

Note
This API does not provide large power savings.
Parameters
gpioPointer to the register overlay for the peripheral

§ DL_GPIO_isPowerEnabled()

__STATIC_INLINE bool DL_GPIO_isPowerEnabled ( GPIO_Regs *  gpio)

Returns if the Peripheral Write Enable (PWREN) register for the GPIO is enabled.

Before any peripheral registers can be configured by software, the peripheral itself must be enabled by writing the ENABLE bit together with the appropriate KEY value to the peripheral's PWREN register.

When the PWREN.ENABLE bit is cleared, the peripheral's registers are not accessible for read/write operations.

Parameters
gpioPointer to the register overlay for the peripheral
Returns
true if peripheral register access is enabled
false if peripheral register access is disabled

§ DL_GPIO_reset()

__STATIC_INLINE void DL_GPIO_reset ( GPIO_Regs *  gpio)

Resets gpio peripheral.

Parameters
gpioPointer to the register overlay for the peripheral

§ DL_GPIO_isReset()

__STATIC_INLINE bool DL_GPIO_isReset ( GPIO_Regs *  gpio)

Returns if gpio peripheral was reset.

Parameters
gpioPointer to the register overlay for the peripheral
Returns
true if peripheral was reset
false if peripheral wasn't reset

§ DL_GPIO_initDigitalOutput()

__STATIC_INLINE void DL_GPIO_initDigitalOutput ( uint32_t  pincmIndex)

Configures a pin as a basic GPIO output.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.

§ DL_GPIO_initDigitalOutputFeatures()

__STATIC_INLINE void DL_GPIO_initDigitalOutputFeatures ( uint32_t  pincmIndex,
DL_GPIO_INVERSION  inversion,
DL_GPIO_RESISTOR  internalResistor,
DL_GPIO_DRIVE_STRENGTH  driveStrength,
DL_GPIO_HIZ  hiZ 
)

Configures a pin as a GPIO output.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
[in]inversionEnable Inversion of the pin output. One of DL_GPIO_INVERSION.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.
[in]driveStrengthEnable High-Drive for the pin. One of DL_GPIO_DRIVE_STRENGTH.
[in]hiZEnable/disable Hi-Z for the pin. One of DL_GPIO_HIZ.

§ DL_GPIO_setDigitalInternalResistor()

__STATIC_INLINE void DL_GPIO_setDigitalInternalResistor ( uint32_t  pincmIndex,
DL_GPIO_RESISTOR  internalResistor 
)

Configures internal resistor for digital pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.

§ DL_GPIO_setAnalogInternalResistor()

__STATIC_INLINE void DL_GPIO_setAnalogInternalResistor ( uint32_t  pincmIndex,
DL_GPIO_RESISTOR  internalResistor 
)

Configures internal resistor for analog pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.

§ DL_GPIO_initDigitalInput()

__STATIC_INLINE void DL_GPIO_initDigitalInput ( uint32_t  pincmIndex)

Configures a pin as a basic GPIO input.

Configures the pin as a basic GPIO input. If you want to use additional features of the input mode, refer to DL_GPIO_initDigitalInputFeatures.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.

§ DL_GPIO_initDigitalInputFeatures()

__STATIC_INLINE void DL_GPIO_initDigitalInputFeatures ( uint32_t  pincmIndex,
DL_GPIO_INVERSION  inversion,
DL_GPIO_RESISTOR  internalResistor,
DL_GPIO_HYSTERESIS  hysteresis,
DL_GPIO_WAKEUP  wakeup 
)

Configures a pin as a GPIO input.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
[in]inversionEnable Inversion of the pin input. One of DL_GPIO_INVERSION.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.
[in]hysteresisEnable/disable Hysteresis on the pin. One of DL_GPIO_HYSTERESIS.
[in]wakeupConfigure wakeup behavior for the pin. One of DL_GPIO_WAKEUP.

§ DL_GPIO_initPeripheralFunction()

__STATIC_INLINE void DL_GPIO_initPeripheralFunction ( uint32_t  pincmIndex,
uint32_t  function 
)

Configure a pin to operate with peripheral functionality.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the peripheral functionality for
[in]functionFunction to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file.

§ DL_GPIO_initPeripheralOutputFunction()

__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunction ( uint32_t  pincmIndex,
uint32_t  function 
)

Configure a pin to operate with peripheral output functionality.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the peripheral functionality for
[in]functionFunction to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file.

§ DL_GPIO_initPeripheralOutputFunctionFeatures()

__STATIC_INLINE void DL_GPIO_initPeripheralOutputFunctionFeatures ( uint32_t  pincmIndex,
uint32_t  function,
DL_GPIO_INVERSION  inversion,
DL_GPIO_RESISTOR  internalResistor,
DL_GPIO_DRIVE_STRENGTH  driveStrength,
DL_GPIO_HIZ  hiZ 
)

Configure a pin to operate with peripheral output functionality with optional features.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the peripheral functionality for
[in]functionFunction to configure the pin for. Check definition of IOMUX_PINCMx_PF_xxx in the device header file.
[in]inversionEnable Inversion of the pin output. One of DL_GPIO_INVERSION.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.
[in]driveStrengthEnable High-Drive for the pin. One of DL_GPIO_DRIVE_STRENGTH.
[in]hiZEnable/disable Hi-Z for the pin. One of DL_GPIO_HIZ.

§ DL_GPIO_initPeripheralInputFunction()

__STATIC_INLINE void DL_GPIO_initPeripheralInputFunction ( uint32_t  pincmIndex,
uint32_t  function 
)

Configure a pin to operate with peripheral input functionality.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the peripheral functionality for
[in]functionFunction to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file.

§ DL_GPIO_initPeripheralInputFunctionFeatures()

__STATIC_INLINE void DL_GPIO_initPeripheralInputFunctionFeatures ( uint32_t  pincmIndex,
uint32_t  function,
DL_GPIO_INVERSION  inversion,
DL_GPIO_RESISTOR  internalResistor,
DL_GPIO_HYSTERESIS  hysteresis,
DL_GPIO_WAKEUP  wakeup 
)

Configure a pin to operate with peripheral input functionality with optional features.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the peripheral functionality for
[in]functionFunction to configure the pin for. See definition of IOMUX_PINCMx_PF_xxx in the device header file.
[in]inversionEnable Inversion of the pin input. One of DL_GPIO_INVERSION.
[in]internalResistorInternal resistor to use. One of DL_GPIO_RESISTOR.
[in]hysteresisEnable/disable Hystersis on the pin. One of DL_GPIO_HYSTERESIS.
[in]wakeupConfigure wakeup behavior for the pin. One of DL_GPIO_WAKEUP.

§ DL_GPIO_initPeripheralAnalogFunction()

__STATIC_INLINE void DL_GPIO_initPeripheralAnalogFunction ( uint32_t  pincmIndex)

Configure a pin to operate with analog functionality.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target pin to configure the analog functionality for

§ DL_GPIO_enableWakeUp()

__STATIC_INLINE void DL_GPIO_enableWakeUp ( uint32_t  pincmIndex)

Set GPIO pin's wakeup enable bit.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.

References DL_GPIO_WAKEUP_ENABLE.

§ DL_GPIO_disableWakeUp()

__STATIC_INLINE void DL_GPIO_disableWakeUp ( uint32_t  pincmIndex)

Clear GPIO pin's wakeup enable bit.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.

§ DL_GPIO_isWakeUpEnabled()

__STATIC_INLINE bool DL_GPIO_isWakeUpEnabled ( uint32_t  pincmIndex)

Returns if GPIO pin's wake up bit is enabled.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
Returns
True if wake up enabled on GPIO pin.

§ DL_GPIO_setWakeupCompareValue()

__STATIC_INLINE void DL_GPIO_setWakeupCompareValue ( uint32_t  pincmIndex,
DL_GPIO_WAKEUP_COMPARE_VALUE  value 
)

Set the compare value to use for wake for the specified pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
[in]valueThe wakeup compare value to set. One of DL_GPIO_WAKEUP_COMPARE_VALUE

References DL_Common_updateReg().

§ DL_GPIO_getWakeupCompareValue()

__STATIC_INLINE DL_GPIO_WAKEUP_COMPARE_VALUE DL_GPIO_getWakeupCompareValue ( uint32_t  pincmIndex)

Get the compare value to use for wake for the specified pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
Returns
The wakeup compare value for the specified pin
Return values
Oneof DL_GPIO_WAKEUP_COMPARE_VALUE

§ DL_GPIO_isWakeStateGenerated()

__STATIC_INLINE bool DL_GPIO_isWakeStateGenerated ( uint32_t  pincmIndex)

Checks if the GPIO pin's Wake State bit is active.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin.
Returns
True if 0x00002000U, False if 0x00000000U.

§ DL_GPIO_readPins()

__STATIC_INLINE uint32_t DL_GPIO_readPins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Read a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to read. Bitwise OR of DL_GPIO_PIN.
Returns
The pins (from the selection) that are currently high
Return values
BitwiseOR of DL_GPIO_PIN of pins that are currently high from the input selection.

§ DL_GPIO_writePins()

__STATIC_INLINE void DL_GPIO_writePins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Write a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to write. All enabled GPIO pins will be set to the equivalent bit value in pins.

§ DL_GPIO_writePinsVal()

__STATIC_INLINE void DL_GPIO_writePinsVal ( GPIO_Regs *  gpio,
uint32_t  pinsMask,
uint32_t  pinsVal 
)

Update the value of one or more GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsMaskThe GPIO pin(s) you want to update. Bitwise OR of DL_GPIO_PIN.
[in]pinsValValue(s) for the GPIO pin(s) you want to update. Only the values for pins specified in pinsMask will change.

§ DL_GPIO_setPins()

__STATIC_INLINE void DL_GPIO_setPins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Set a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to set high. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_clearPins()

__STATIC_INLINE void DL_GPIO_clearPins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Clear a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to clear. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_togglePins()

__STATIC_INLINE void DL_GPIO_togglePins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Toggle a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to toggle. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_enableOutput()

__STATIC_INLINE void DL_GPIO_enableOutput ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Enable output on a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to enable output. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_disableOutput()

__STATIC_INLINE void DL_GPIO_disableOutput ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Disable output on a group of GPIO pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to disable output. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_enableDMAAccess()

__STATIC_INLINE void DL_GPIO_enableDMAAccess ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Enable DMA access on a group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to toggle. Bitwise OR of DL_GPIO_PIN.

References DL_Common_updateReg().

§ DL_GPIO_disableDMAAccess()

__STATIC_INLINE void DL_GPIO_disableDMAAccess ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Disable DMA access on a group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to disable DMA access on. Bitwise OR of DL_GPIO_PIN.

References DL_Common_updateReg().

§ DL_GPIO_isDMAccessEnabled()

__STATIC_INLINE uint32_t DL_GPIO_isDMAccessEnabled ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Check if DMA access is enabled on a group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsPins to check DMA access on. Bitwise OR of DL_GPIO_PIN.
Returns
Which pins of the requested group have DMA access enabled
Return values
BitwiseOR of DL_GPIO_PIN values

§ DL_GPIO_setLowerPinsPolarity()

__STATIC_INLINE void DL_GPIO_setLowerPinsPolarity ( GPIO_Regs *  gpio,
uint32_t  polarity 
)

Set the polarity of all bits [0, 15] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]polarityBitwise OR of DL_GPIO_EDGE_POLARITY for pins [0, 15]

§ DL_GPIO_setUpperPinsPolarity()

__STATIC_INLINE void DL_GPIO_setUpperPinsPolarity ( GPIO_Regs *  gpio,
uint32_t  polarity 
)

Set the polarity of all bits [16, 31] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]polarityBitwise OR of DL_GPIO_EDGE_POLARITY for pins [16, 31]

§ DL_GPIO_getLowerPinsPolarity()

__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsPolarity ( GPIO_Regs *  gpio)

Get the polarity of bits [0, 15] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
Return values
Polaritysetting with bitwise OR of DL_GPIO_EDGE_POLARITY for pins [0, 15]

§ DL_GPIO_getUpperPinsPolarity()

__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsPolarity ( GPIO_Regs *  gpio)

Get the polarity of bits [16, 31] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
Return values
Polaritysetting with bitwise OR of DL_GPIO_EDGE_POLARITY for pins [16, 31]

§ DL_GPIO_setLowerPinsInputFilter()

__STATIC_INLINE void DL_GPIO_setLowerPinsInputFilter ( GPIO_Regs *  gpio,
uint32_t  filter 
)

Set the input filter of bits [0, 15] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]filterBitwise OR of DL_GPIO_INPUT_FILTER for pins [0, 15]

§ DL_GPIO_setUpperPinsInputFilter()

__STATIC_INLINE void DL_GPIO_setUpperPinsInputFilter ( GPIO_Regs *  gpio,
uint32_t  filter 
)

Set the input filter of bits [16, 31] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]filterBitwise OR of DL_GPIO_INPUT_FILTER for pins [16, 31]

§ DL_GPIO_getLowerPinsInputFilter()

__STATIC_INLINE uint32_t DL_GPIO_getLowerPinsInputFilter ( GPIO_Regs *  gpio)

Get the input filter of bits [0, 15] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
Return values
Inputfilter setting with bitwise OR of DL_GPIO_INPUT_FILTER for pins [0, 15]

§ DL_GPIO_getUpperPinsInputFilter()

__STATIC_INLINE uint32_t DL_GPIO_getUpperPinsInputFilter ( GPIO_Regs *  gpio)

Get the input filter of bits [16, 31] in the group of pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
Return values
Inputfilter setting with bitwise OR of DL_GPIO_INPUT_FILTER for pins [16, 31]

§ DL_GPIO_enableGlobalFastWake()

__STATIC_INLINE void DL_GPIO_enableGlobalFastWake ( GPIO_Regs *  gpio)

Enable Global Fast Wake.

Parameters
[in]gpioPointer to the register overlay for the peripheral

§ DL_GPIO_disableGlobalFastWake()

__STATIC_INLINE void DL_GPIO_disableGlobalFastWake ( GPIO_Regs *  gpio)

Disable Global Fast Wake.

Parameters
[in]gpioPointer to the register overlay for the peripheral

§ DL_GPIO_enableFastWakePins()

__STATIC_INLINE void DL_GPIO_enableFastWakePins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Enable fast wake for pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of pins to enable fast-wake feature. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_disableFastWakePins()

__STATIC_INLINE void DL_GPIO_disableFastWakePins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Disable fast wake for pins.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of pins to disable fast-wake feature. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_enableHiZ()

__STATIC_INLINE void DL_GPIO_enableHiZ ( uint32_t  pincmIndex)

Enable Hi-Z for the pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin

§ DL_GPIO_disableHiZ()

__STATIC_INLINE void DL_GPIO_disableHiZ ( uint32_t  pincmIndex)

Disable Hi-Z for the pin.

Parameters
[in]pincmIndexThe PINCM register index that maps to the target GPIO pin

§ DL_GPIO_getEnabledFastWakePins()

__STATIC_INLINE uint32_t DL_GPIO_getEnabledFastWakePins ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Check which pins have fast wake feature enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of pins to check. Bitwise OR of DL_GPIO_PIN.
Returns
Which of the requested GPIO pins have fast wake enabled
Return values
BitwiseOR of DL_GPIO_PIN values

§ DL_GPIO_enableInterrupt()

__STATIC_INLINE void DL_GPIO_enableInterrupt ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Enable GPIO interrupts.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to enable. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_disableInterrupt()

__STATIC_INLINE void DL_GPIO_disableInterrupt ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Disable GPIO interrupts.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to disable. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_getEnabledInterrupts()

__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterrupts ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Check which GPIO interrupts are enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN.
Returns
Which of the requested GPIO interrupts are enabled
Return values
BitwiseOR of DL_GPIO_PIN values

§ DL_GPIO_getEnabledInterruptStatus()

__STATIC_INLINE uint32_t DL_GPIO_getEnabledInterruptStatus ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Check interrupt flag of enabled GPIO interrupts.

Checks if any of the GPIO interrupts that were previously enabled are pending.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN.
Returns
Which of the requested GPIO interrupts are pending
Return values
BitwiseOR of DL_GPIO_PIN values
See also
DL_GPIO_enableInterrupt

§ DL_GPIO_setInterrupt()

__STATIC_INLINE void DL_GPIO_setInterrupt ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Set interrupt flag of any GPIO.

Manually set a GPIO interrupt to be pending

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to set. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_getRawInterruptStatus()

__STATIC_INLINE uint32_t DL_GPIO_getRawInterruptStatus ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Check interrupt flag of any GPIO interrupt.

Checks if any of the GPIO interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN.
Returns
Which of the requested GPIO interrupts are pending
Return values
BitwiseOR of DL_GPIO_PIN values

§ DL_GPIO_getPendingInterrupt()

__STATIC_INLINE DL_GPIO_IIDX DL_GPIO_getPendingInterrupt ( GPIO_Regs *  gpio)

Get highest priority pending GPIO interrupt.

Checks if any of the GPIO interrupts are pending. Interrupts do not have to be previously enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
Returns
The highest priority pending GPIO interrupt
Return values
Oneof DL_GPIO_IIDX

§ DL_GPIO_clearInterruptStatus()

__STATIC_INLINE void DL_GPIO_clearInterruptStatus ( GPIO_Regs *  gpio,
uint32_t  pins 
)

Clear pending GPIO interrupts.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]pinsBit mask of interrupts to check. Bitwise OR of DL_GPIO_PIN.

§ DL_GPIO_configSubscriber()

__STATIC_INLINE void DL_GPIO_configSubscriber ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index,
DL_GPIO_SUBSCRIBER_OUT_POLICY  policy,
DL_GPIO_SUBSCRIBERx_PIN  pinIndex 
)

Configures GPIO subscriber. This API preserves enable/disbale status of subscriber.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the subscriber event index to be configured
[in]policySpecifies the the GPIO behavior when the subscriber receives publisher event.
[in]pinIndexSpecifies the GPIO bit number which will be targeted by the subscriber action.

References DL_Common_updateReg().

§ DL_GPIO_enableSubscriber()

__STATIC_INLINE void DL_GPIO_enableSubscriber ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index 
)

Enables GPIO subscriber.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the subscriber event index to be configured

§ DL_GPIO_disableSubscriber()

__STATIC_INLINE void DL_GPIO_disableSubscriber ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index 
)

Disables GPIO subscriber.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the subscriber event index to be configured

§ DL_GPIO_isSubscriberEnabled()

__STATIC_INLINE bool DL_GPIO_isSubscriberEnabled ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index 
)

Returns if GPIO subscriber is enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the subscriber event index to be configured
Returns
true if GPIO subscriber is enabled
false if GPIO subscriber is disabled

§ DL_GPIO_setPublisherChanID()

__STATIC_INLINE void DL_GPIO_setPublisherChanID ( GPIO_Regs *  gpio,
DL_GPIO_PUBLISHER_INDEX  index,
uint8_t  chanID 
)

Sets the event publisher channel id.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]chanIDChannel ID number. Valid range 0-15. If ChanID == 0 subscriber is disconnected. Consult your device datasheet on the actual maximum number of channels.

§ DL_GPIO_getPublisherChanID()

__STATIC_INLINE uint8_t DL_GPIO_getPublisherChanID ( GPIO_Regs *  gpio,
DL_GPIO_PUBLISHER_INDEX  index 
)

Gets the event publisher channel id.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
Returns
Event publisher channel ID

§ DL_GPIO_setSubscriberChanID()

__STATIC_INLINE void DL_GPIO_setSubscriberChanID ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index,
uint8_t  chanID 
)

Sets the event subscriber channel id.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]chanIDChannel ID number. Valid range 0-15. If ChanID == 0 subscriber is disconnected. Consult your device datasheet on the actual maximum number of channels.

§ DL_GPIO_getSubscriberChanID()

__STATIC_INLINE uint8_t DL_GPIO_getSubscriberChanID ( GPIO_Regs *  gpio,
DL_GPIO_SUBSCRIBER_INDEX  index 
)

Gets the event subscriber channel id.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
Returns
Event subscriber channel ID

§ DL_GPIO_enableEvents()

__STATIC_INLINE void DL_GPIO_enableEvents ( GPIO_Regs *  gpio,
DL_GPIO_EVENT_ROUTE  index,
uint32_t  pins 
)

Enables GPIO events.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]pinsValid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31).

References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.

§ DL_GPIO_disableEvents()

__STATIC_INLINE void DL_GPIO_disableEvents ( GPIO_Regs *  gpio,
DL_GPIO_EVENT_ROUTE  index,
uint32_t  pins 
)

Disable GPIO events.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]pinsValid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31).

References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.

§ DL_GPIO_getEnabledEvents()

__STATIC_INLINE uint32_t DL_GPIO_getEnabledEvents ( GPIO_Regs *  gpio,
DL_GPIO_EVENT_ROUTE  index,
uint32_t  pins 
)

Check which GPIO events are enabled.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]pinsValid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31).
Returns
Which of the requested GPIO events are enabled
Return values
BitwiseOR of DL_GPIO_PIN values

§ DL_GPIO_getEnabledEventStatus()

__STATIC_INLINE uint32_t DL_GPIO_getEnabledEventStatus ( GPIO_Regs *  gpio,
DL_GPIO_EVENT_ROUTE  index,
uint32_t  pins 
)

Checks if any of the GPIO events which were previously enabled are pending.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]pinsValid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31).
Returns
Which of the requested GPIO events are pending
Return values
BitwiseOR of DL_GPIO_PIN values
See also
DL_GPIO_enableEvents

§ DL_GPIO_clearEventStatus()

__STATIC_INLINE void DL_GPIO_clearEventStatus ( GPIO_Regs *  gpio,
DL_GPIO_EVENT_ROUTE  index,
uint32_t  pins 
)

Clear pending GPIO event.

Parameters
[in]gpioPointer to the register overlay for the peripheral
[in]indexSpecifies the register event index to be configured
[in]pinsValid options will depend on index argument. When index == DL_GPIO_EVENT_ROUTE_1, valid pins values are bitwise OR of DL_GPIO_PIN (0-15). When index == DL_GPIO_EVENT_ROUTE_2, valid pins Bitwise OR of DL_GPIO_PIN (16-31).

References DL_GPIO_EVENT_ROUTE_1, and DL_GPIO_EVENT_ROUTE_2.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale