SensoredFOCMotorControlLibrary  1.0
Data Fields
debugEnableFlags Struct Reference

Structure for debug enable flags. More...

#include <appUserInputs.h>

Data Fields

uint16_t updatedData: 1
 
uint16_t updatedKe: 1
 

Detailed Description

Structure for debug enable flags.

Field Documentation

§ updatedData

uint16_t debugEnableFlags::updatedData

Flag to updated register data

§ updatedKe

uint16_t debugEnableFlags::updatedKe

Flag to updated Ke


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale