![]() |
![]() |
MSPM0L11XX_L13XX TI-Driver Library
2.01.00.03
|
I2C Pin Configuration. More...
#include <I2CMSPM0.h>
Data Fields | |
uint8_t | pinSDA |
uint8_t | pinSCL |
I2C Pin Configuration.
Pin configuration that holds non-default pins. The default pin configuration is typically defined in I2CMSPM0_HWAttrs placed in the board file. The pin configuration structure is used by setting the custom void pointer in the I2C_Params to point to this struct. If the custom void pointer is NULL, the I2CMSPM0_HWAttrs pin mapping will be used.
uint8_t I2CMSPM0_I2CPinCfg::pinSDA |
SDA Pincm value
uint8_t I2CMSPM0_I2CPinCfg::pinSCL |
SCL Pincm value