MSPM0G1X0X_G3X0X TI-Driver Library  2.01.00.03
Functions
Common helper functions for I2C driver
Collaboration diagram for Common helper functions for I2C driver:

Functions

void I2CSupport_controllerFinish (I2C_HWAttrs const *hwAttrs)
 Function to send a finish command to the controller module. More...
 
void I2CSupport_powerSetConstraint (void)
 Function to set power constraint.
 
void I2CSupport_powerRelConstraint (void)
 Function to release power constraint.
 
int_fast16_t I2CSupport_primeTransfer (I2C_Handle handle, I2C_Transaction *transaction)
 Function to initialize transfers. More...
 

Detailed Description

Overview

Refer to ti_drivers_I2C_Overview for a complete description of APIs and examples of use.

Function Documentation

§ I2CSupport_controllerFinish()

void I2CSupport_controllerFinish ( I2C_HWAttrs const *  hwAttrs)

Function to send a finish command to the controller module.

Parameters
[in]hwAttrsA pointer to an I2C_HWAttrs structure.

§ I2CSupport_primeTransfer()

int_fast16_t I2CSupport_primeTransfer ( I2C_Handle  handle,
I2C_Transaction transaction 
)

Function to initialize transfers.

Parameters
[in]handleAn I2C_Handle returned from I2C_open().
[in]transactionA pointer to an I2C_Transaction.
Returns
Returns a status indicating success or failure of the transfer.
Return values
I2C_STATUS_SUCCESSThe transfer was successful.
I2C_STATUS_INCOMPLETEI2C transaction is in progress or returned without completing.
I2C_STATUS_BUS_BUSYI2C bus already in use by another I2C Controller.
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale