![]() |
![]() |
MSPM0G1X0X_G3X0X TI-Driver Library
2.01.00.03
|
I2CTargetMSPM0 Hardware attributes. More...
#include <I2CTargetMSPM0.h>
Data Fields | |
I2CTARGET_BASE_HWATTRS uint8_t | sdaPincm |
uint8_t | sdaPinIndex |
uint32_t | sdaPinMux |
uint8_t | sclPincm |
uint8_t | sclPinIndex |
uint32_t | sclPinMux |
DL_I2C_CLOCK | clockSource |
DL_I2C_CLOCK_DIVIDE | clockDivider |
DL_I2C_RX_FIFO_LEVEL | rxIntFifoThr |
DL_I2C_TX_FIFO_LEVEL | txIntFifoThr |
bool | isClockStretchingEnabled |
bool | isAnalogGlitchFilterEnabled |
uint16_t | i2cClk |
I2CTargetMSPM0 Hardware attributes.
The baseAddr and intNum fields define the base address and the interrupt number of the I2C peripheral. These values are passed to driverlib APIs and therefore must be populated by driverlib macro definitions. These macros are found in the header files:
The powerMngrId is the Power driver resource ID for the I2C peripheral. These macros are defined in the device specific Power include file.
intPriority is the I2C peripheral's interrupt priority, This value is passed unmodified to Hwi_create().
sdaPinMux and sclPinMux are values drawn from the GPIO driver. They indicate the function for that specific IO pin that select I2C mode.
sdaPinMux and sclPinMux are values drawn from the GPIO driver. They indicate the function for that specific DIO pin that select I2C mode.
A sample structure is shown below:
I2CTARGET_BASE_HWATTRS uint8_t I2CTargetMSPM0_HWAttrs::sdaPincm |
< I2C base hardware attributes SDA Pincm value
uint8_t I2CTargetMSPM0_HWAttrs::sdaPinIndex |
SDA pin index
uint32_t I2CTargetMSPM0_HWAttrs::sdaPinMux |
SDA pin function
uint8_t I2CTargetMSPM0_HWAttrs::sclPincm |
SCL Pincm value
uint8_t I2CTargetMSPM0_HWAttrs::sclPinIndex |
SCL pin index
uint32_t I2CTargetMSPM0_HWAttrs::sclPinMux |
SCL pin function
DL_I2C_CLOCK I2CTargetMSPM0_HWAttrs::clockSource |
I2C clock source
DL_I2C_CLOCK_DIVIDE I2CTargetMSPM0_HWAttrs::clockDivider |
I2C clock divider to get the required bps
DL_I2C_RX_FIFO_LEVEL I2CTargetMSPM0_HWAttrs::rxIntFifoThr |
I2C receive FIFO interrupt threshold
DL_I2C_TX_FIFO_LEVEL I2CTargetMSPM0_HWAttrs::txIntFifoThr |
I2C transmit FIFO interrupt threshold
bool I2CTargetMSPM0_HWAttrs::isClockStretchingEnabled |
Clock stretching enable/disable flag
bool I2CTargetMSPM0_HWAttrs::isAnalogGlitchFilterEnabled |
Analog Glitch Filter enable/disable flag
uint16_t I2CTargetMSPM0_HWAttrs::i2cClk |
The clock must be in MHz