![]() |
![]() |
MSPM0L11XX_L13XX TI-Driver Library
2.00.01.00
|
![]() |
Macros | |
#define | GPIO_CFG_DRVSTR_MED_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
Medium drive strength is not available on MSPM0 devices. | |
#define | GPIO_CFG_INT_LOW_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
Low value interrupts are not available on MSPM0 devices. | |
#define | GPIO_CFG_INT_HIGH_INTERNAL (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED) |
High value interrupts are not available on MSPM0 devices. | |
Refer to ti_drivers_GPIO_Overview for a complete description of the GPIO driver APIs provided and examples of their use.
The definitions in this file should not be used directly. All GPIO_CFG macros should be used as-is from GPIO.h.
There are no additional configuration values or platform-specific functions for GPIOMSPM0.