MSPM0L11XX_L13XX TI-Driver Library  2.00.01.00
Macros
GPIOMSPM0.h File Reference

Detailed Description

GPIO driver implementation for MSPM0 devices.


#include <ti/drivers/GPIO.h>
Include dependency graph for GPIOMSPM0.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define GPIO_CFG_DRVSTR_MED_INTERNAL   (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED)
 Medium drive strength is not available on MSPM0 devices.
 
#define GPIO_CFG_INT_LOW_INTERNAL   (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED)
 Low value interrupts are not available on MSPM0 devices.
 
#define GPIO_CFG_INT_HIGH_INTERNAL   (GPIOMSPM0_CFG_OPTION_NOT_SUPPORTED)
 High value interrupts are not available on MSPM0 devices.
 
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale