MSPM0G1X0X_G3X0X TI-Driver Library  2.00.01.00
Modules | Data Structures | Typedefs | Enumerations | Functions
Universal Asynchronous Receiver-Transmitter (UART)
Collaboration diagram for Universal Asynchronous Receiver-Transmitter (UART):

Modules

 UART driver APIs
 
 UART driver supporting APIs
 
 UART status codes
 

Data Structures

struct  UART_Params
 UART Parameters. More...
 

Typedefs

typedef struct UART_Config_UART_Handle
 A handle that is returned from a UART_open() call.
 
typedef void(* UART_Callback) (UART_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status)
 The definition of a callback function used by the UART driver when used in UART_Mode_CALLBACK. The callback can occur in task or interrupt context. More...
 
typedef void(* UART_EventCallback) (UART_Handle handle, uint32_t event, uint32_t data, void *userArg)
 The definition of a callback function used by the UART driver. The callback can occur in task or interrupt context. More...
 

Enumerations

enum  UART_Mode {
  UART_Mode_BLOCKING = 0,
  UART_Mode_CALLBACK,
  UART_Mode_NONBLOCKING
}
 UART mode settings. More...
 
enum  UART_ReadReturnMode {
  UART_ReadReturnMode_FULL = 0,
  UART_ReadReturnMode_PARTIAL
}
 UART return mode settings. More...
 
enum  UART_DataLen {
  UART_DataLen_5 = DL_UART_WORD_LENGTH_5_BITS,
  UART_DataLen_6 = DL_UART_WORD_LENGTH_6_BITS,
  UART_DataLen_7 = DL_UART_WORD_LENGTH_7_BITS,
  UART_DataLen_8 = DL_UART_WORD_LENGTH_8_BITS
}
 UART data length settings. More...
 
enum  UART_StopBits {
  UART_StopBits_1 = DL_UART_STOP_BITS_ONE,
  UART_StopBits_2 = DL_UART_STOP_BITS_TWO
}
 UART stop bit settings. More...
 
enum  UART_Parity {
  UART_Parity_NONE = DL_UART_PARITY_NONE,
  UART_Parity_EVEN = DL_UART_PARITY_EVEN,
  UART_Parity_ODD = DL_UART_PARITY_ODD,
  UART_Parity_ZERO = DL_UART_PARITY_STICK_ZERO,
  UART_Parity_ONE = DL_UART_PARITY_STICK_ONE
}
 UART parity type settings. More...
 

Functions

void UART_Params_init (UART_Params *params)
 Function to initialize the UART_Params struct to its defaults. More...
 
UART_Handle UART_open (uint_least8_t index, UART_Params *params)
 Function to initialize a given UART peripheral. More...
 
void UART_close (UART_Handle handle)
 Function to close a UART peripheral specified by the UART handle. More...
 
int_fast16_t UART_read (UART_Handle handle, void *buf, size_t size, size_t *bytesRead)
 Function that reads data from a UART. More...
 
int_fast16_t UART_write (UART_Handle handle, const void *buf, size_t size, size_t *bytesWritten)
 Function that writes data to a UART. More...
 
int_fast16_t UART_readTimeout (UART_Handle handle, void *buf, size_t size, size_t *bytesRead, uint32_t timeout)
 UART read with timeout. Note that the timeout parameter is different from the hardware read timeout. More...
 
int_fast16_t UART_writeTimeout (UART_Handle handle, const void *buf, size_t size, size_t *bytesWritten, uint32_t timeout)
 UART write with timeout. Note that the timeout parameter is different from the hardware read timeout. More...
 
void UART_readCancel (UART_Handle handle)
 Function that cancels a UART_read() function call. More...
 
void UART_writeCancel (UART_Handle handle)
 Function that cancels a UART_write() function call. More...
 
void UART_rxDisable (UART_Handle handle)
 Function that disables collecting of RX data into the circular buffer. More...
 
void UART_rxEnable (UART_Handle handle)
 Function that enables collecting of RX data into the circular buffer. More...
 
void UART_flushRx (UART_Handle handle)
 Function to flush data in the UART RX FIFO. More...
 
void UART_getRxCount (UART_Handle handle)
 Get the number of bytes available in the circular buffer. More...
 

Detailed Description

The UART header file should be included in an application as follows:

Overview

UART has both RX and TX ring buffers for receiving/sending data. UART uses DMA to transfer data between the UART FIFOs and the RX and TX ring buffers in blocking mode. In callback mode, DMA will transfer data straight between the hardware FIFO and the source/destination buffer supplied by the application. NOTE: If the source-buffer for a TX operation resides in flash, the driver will constrain the flash to remain on during idle. The UART APIs for reading and writing data have been made more posix-like. UART provides for event notification, allowing the application to receive TX start and completion events, and RX error events.

Note
These events are synchronous to what can be observed on the data lines. A UART_STAT_TXFE_SET event will for example only occur after all data has been shifted from the hardware FIFO out onto the TX-pin. In contrast, read and write-callbacks are invoked when the driver has finished writing data into the hardware FIFO.

To use the UART driver, ensure that the correct driver library for your device is linked in and include this header file as follows:

Typedef Documentation

§ UART_Callback

typedef void(* UART_Callback) (UART_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status)

The definition of a callback function used by the UART driver when used in UART_Mode_CALLBACK. The callback can occur in task or interrupt context.

Parameters
[in]UART_HandleUART_Handle.
[in]bufPointer to read/write buffer.
[in]countNumber of elements read/written.
[in]userArgA user supplied argument specified in UART_Params.
[in]statusA UART status codes code indicating success or failure of the transfer.

§ UART_EventCallback

typedef void(* UART_EventCallback) (UART_Handle handle, uint32_t event, uint32_t data, void *userArg)

The definition of a callback function used by the UART driver. The callback can occur in task or interrupt context.

Parameters
[in]UART_HandleUART_Handle.
[in]eventUART_EVENT that has occurred.
[in]dataOne of the following
  • UART_EVENT_OVERRUN: accumulated count
  • UART_EVENT_BREAK: unused
  • UART_EVENT_PARITY: unused
  • UART_EVENT_FRAMING: unused
[in]userArgA user supplied argument specified in UART_Params.
[in]statusA UART_STATUS code indicating success or failure of the transfer.

Enumeration Type Documentation

§ UART_Mode

enum UART_Mode

UART mode settings.

This enum defines the read and write modes for the configured UART.

Enumerator
UART_Mode_BLOCKING 

UART_write() will block the calling task until all of the data can be accepted by the device driver. UART_read() will block until some data becomes available.

UART_Mode_CALLBACK 

Non-blocking, UART_write() or UART_read() will return immediately. When the transfer has finished, the callback function is called from either the caller's context or from an interrupt context.

UART_Mode_NONBLOCKING 

Non-blocking, UART_write() or UART_read() will return immediately. UART_write() will copy as much data into the transmit buffer as space allows. UART_read() will copy as much data from the receive buffer as is immediately available.

§ UART_ReadReturnMode

UART return mode settings.

This enumeration defines the return modes for UART_read().

UART_ReadReturnMode_FULL unblocks or performs a callback when the read buffer has been filled with the number of bytes passed to UART_read(). UART_ReadReturnMode_PARTIAL unblocks or performs a callback whenever a read timeout error occurs on the UART peripheral. This timeout error is not the same as the blocking read timeout in the UART_Params; the read timeout occurs if the read FIFO is non-empty and no new data has been received for a device/baudrate dependent number of clock cycles. This mode can be used when the exact number of bytes to be read is not known.

Enumerator
UART_ReadReturnMode_FULL 

Unblock/callback when buffer is full.

UART_ReadReturnMode_PARTIAL 

Unblock/callback when no new data comes in.

§ UART_DataLen

UART data length settings.

This enumeration defines the UART data lengths.

Enumerator
UART_DataLen_5 

Data length is 5 bits

UART_DataLen_6 

Data length is 6 bits

UART_DataLen_7 

Data length is 7 bits

UART_DataLen_8 

Data length is 8 bits

§ UART_StopBits

UART stop bit settings.

This enumeration defines the UART stop bits.

Enumerator
UART_StopBits_1 

One stop bit

UART_StopBits_2 

Two stop bits

§ UART_Parity

UART parity type settings.

This enumeration defines the UART parity types.

Enumerator
UART_Parity_NONE 

No parity

UART_Parity_EVEN 

Parity bit is even

UART_Parity_ODD 

Parity bit is odd

UART_Parity_ZERO 

Parity bit is always zero

UART_Parity_ONE 

Parity bit is always one

Function Documentation

§ UART_Params_init()

void UART_Params_init ( UART_Params params)

Function to initialize the UART_Params struct to its defaults.

Parameters
[in]paramsA pointer to UART_Params structure for initialization.

Defaults values are:

  • readMode = UART_Mode_BLOCKING;
  • writeMode = UART_Mode_BLOCKING;
  • eventCallback = NULL;
  • eventMask = 0;
  • readCallback = NULL;
  • writeCallback = NULL;
  • readReturnMode = UART_ReadReturnMode_PARTIAL;
  • baudRate = 9600;
  • dataLength = UART_DataLen_8;
  • stopBits = UART_StopBits_1;
  • parityType = UART_Parity_NONE;
  • userArg = NULL;

§ UART_open()

UART_Handle UART_open ( uint_least8_t  index,
UART_Params params 
)

Function to initialize a given UART peripheral.

Function to initialize a given UART peripheral specified by the particular index value.

Parameters
[in]indexLogical peripheral number for the UART indexed into the UART_config table.
[in]paramsPointer to a UART_Params structure. If NULL, default parameter values will be used. All the fields in this structure are read-only.
Returns
UART handle
See also
UART_close()

§ UART_close()

void UART_close ( UART_Handle  handle)

Function to close a UART peripheral specified by the UART handle.

Precondition
UART_open() has been called.
There are no ongoing read or write calls. Any ongoing read or write calls can be cancelled with UART_readCancel() or UART_writeCancel().
Parameters
[in]handleA UART_Handle returned from UART_open().
See also
UART_open()

§ UART_read()

int_fast16_t UART_read ( UART_Handle  handle,
void *  buf,
size_t  size,
size_t *  bytesRead 
)

Function that reads data from a UART.

UART_read() reads data from a UART controller. The destination is specified by buffer and the number of bytes to read is given by size.

In UART_Mode_BLOCKING, UART_read() blocks task execution until all the data in buffer has been read, if the read return mode is UART_ReadReturnMode_FULL. If the read return mode is UART_ReadReturnMode_PARTIAL, UART_read() returns before all the data has been read, if some data has been received, but reception has been inactive sufficiently long for a hardware read timeout to occur (e.g., for a 32-bit period). If a receive error occurs (e.g., framing, FIFO overrun), UART_read() will return with the number of bytes read up to the occurrence of the error.

In UART_Mode_CALLBACK, UART_read() does not block task execution. Instead, a callback function specified by UART_Params::readCallback is called when the transfer is finished (UART_ReadReturnMode_FULL), or reception has become inactive (UART_ReadReturnMode_PARTIAL). The callback function can occur in the caller's context or in SWI context, depending on the device-specific implementation. An unfinished asynchronous read operation must always be cancelled using UART_readCancel() before calling UART_close().

Note
It is ok to call UART_read() from its own callback function when in UART_Mode_CALLBACK.
Parameters
[in]handleA UART_Handle returned by UART_open().
[in]bufA pointer to an empty buffer to which received data should be read.
[in]sizeThe number of bytes to be read into buffer.
[out]bytesReadIf non-NULL, the location to store the number of bytes actually read into the buffer. If NULL, this parameter will be ignored. In callback mode, NULL could be passed in for this parameter, since the callback function will be passed the number of bytes read. In blocking mode, NULL can be passed, however, status should be checked in case the number of bytes requested was not received due to errors.
Returns
Returns a status indicating success or failure of the read.
Return values
UART_STATUS_SUCCESSThe call was successful.
UART_STATUS_EINUSEAnother read from the UART is currently ongoing.
UART_STATUS_ECANCELLEDIn UART_Mode_BLOCKING, the read was canceled by a call to UART_readCancel() before any data could be received.

§ UART_write()

int_fast16_t UART_write ( UART_Handle  handle,
const void *  buf,
size_t  size,
size_t *  bytesWritten 
)

Function that writes data to a UART.

UART_write() writes data from a memory buffer to the UART interface. The source is specified by buffer and the number of bytes to write is given by size.

In UART_Mode_BLOCKING, UART_write() blocks task execution until all the data in buffer has been transmitted onto the TX pin.

In UART_Mode_CALLBACK, UART_write() does not block task execution. Instead, a callback function specified by UART_Params::writeCallback is called when all data has been written to the hardware FIFO. This means that that driver is ready to accept another call to UART_write().

Note
In contrast to UART_Mode_BLOCKING, it is not guaranteed that all data has been transmitted onto the TX pin when callback is invoked.

The buffer passed to UART_write() in UART_Mode_CALLBACK is not copied. The buffer must remain coherent until all the characters have been sent (ie until the write callback has been called with a byte count equal to that passed to UART_write()). The callback function can occur in the caller's task context or in interrupt context, depending on the device implementation. An unfinished asynchronous write operation must always be cancelled using UART_writeCancel() before calling UART_close().

The bytesWritten parameter should not be NULL so the application can determine the number of bytes actually written.

Parameters
[in]handleA UART_Handle returned by UART_open().
[in]bufA read-only pointer to buffer containing data to be written to the UART.
[in]sizeThe number of bytes in the buffer that should be written to the UART.
[out]bytesWrittenIf non-NULL, the location to store the number of bytes actually written to the UART in UART_Mode_BLOCKING. In UART_Mode_CALLBACK, bytesWritten will be set to 0. If bytesWritten is NULL, this parameter will be ignored.
Returns
Returns a status indicating success or failure of the write.
Return values
UART_STATUS_SUCCESSThe call was successful.
UART_STATUS_EINUSEAnother write to the UART is currently ongoing.

§ UART_readTimeout()

int_fast16_t UART_readTimeout ( UART_Handle  handle,
void *  buf,
size_t  size,
size_t *  bytesRead,
uint32_t  timeout 
)

UART read with timeout. Note that the timeout parameter is different from the hardware read timeout.

Parameters
[in]handleUART_Handle instance from UART_open().
[in]buflocation where the data to be written.
[in]sizeamount of data to write in bytes.
[out]bytesReadIf non-NULL, the location to store the number of bytes actually read into the buffer. If NULL, this parameter will be ignored.
[in]timeoutThe number of system clock ticks to wait until all data is received. If not all requested data was received within the timeout period, an error of UART_STATUS_ETIMEOUT will be returned. This parameter is only applicable to UART_Mode_BLOCKING.
Returns
Returns a status indicating success or failure of the read.
Return values
UART_STATUS_SUCCESSThe call was successful.
UART_STATUS_EINUSEAnother read from the UART is currently ongoing.
UART_STATUS_ECANCELLEDIn UART_Mode_BLOCKING, the read was canceled by a call to UART_readCancel() before any data could be received.
UART_STATUS_ETIMEOUTThe read operation timed out.

§ UART_writeTimeout()

int_fast16_t UART_writeTimeout ( UART_Handle  handle,
const void *  buf,
size_t  size,
size_t *  bytesWritten,
uint32_t  timeout 
)

UART write with timeout. Note that the timeout parameter is different from the hardware read timeout.

Parameters
[in]handleUART_Handle instance from UART_open().
[in]buflocation to write data from.
[in]sizeamount of data to write in bytes.
[out]bytesWrittenIf non-NULL, the location to store the number of bytes actually written into the buffer. If NULL, this parameter will be ignored.
[in]timeoutThe number of system clock ticks to wait for the write to complete (UART_Mode_BLOCKING only). If the timeout expires before all bytes are written, a status of UART_STATUS_ETIMEOUT will be returned.
Returns
Returns a status indicating success or failure of the write.
Return values
UART_STATUS_SUCCESSThe call was successful.
UART_STATUS_EINUSEAnother write to the UART is currently ongoing.
UART_STATUS_ETIMEOUTThe write operation timed out.

§ UART_readCancel()

void UART_readCancel ( UART_Handle  handle)

Function that cancels a UART_read() function call.

This function cancels an asynchronous UART_read() operation in in UART_Mode_CALLBACK, or unblocks a UART_read() call in UART_Mode_BLOCKING. In UART_Mode_CALLBACK, UART_readCancel() calls the registered read callback function with the number of bytes received so far. It is the application's responsibility to check the count argument in the callback function and handle the case where only a subset of the bytes were received. The callback function will be passed a status of UART_STATUS_ECANCELLED.

In UART_Mode_BLOCKING, UART_read() will return UART_STATUS_ECANCELLED, and the bytesRead parameter will be set to the number of bytes received so far.

Parameters
[in]handleA UART_Handle returned by UART_open().

§ UART_writeCancel()

void UART_writeCancel ( UART_Handle  handle)

Function that cancels a UART_write() function call.

This function cancels an asynchronous UART_write() operation when write mode is UART_Mode_CALLBACK. In callback mode, UART_writeCancel() calls the registered write callback function no matter how many bytes were sent. It is the application's responsibility to check the count argument in the callback function and handle cases where only a subset of the bytes were sent. The callback function will be passed a status of UART_STATUS_ECANCELLED. In blocking mode, UART_write() will return UART_STATUS_ECANCELLED.

Note
The above applies to UART_writeTimeout() as well.
Parameters
[in]handleA UART_Handle returned by UART_open().

§ UART_rxDisable()

void UART_rxDisable ( UART_Handle  handle)

Function that disables collecting of RX data into the circular buffer.

The driver implementation uses a circular buffer to collect RX data while a UART_read() is not in progress. This function will disable buffering of RX data into the circular buffer. UART_read() will read directly from the UART driver's RX buffer. Disabling the circular buffer will also allow the device to go into low power modes.

Parameters
[in]handleA UART_Handle returned by UART_open().
See also
UART_rxEnable()

§ UART_rxEnable()

void UART_rxEnable ( UART_Handle  handle)

Function that enables collecting of RX data into the circular buffer.

The driver implementation uses a circular buffer to collect RX data while a UART_read() is not in progress. This function will enable buffering of RX data into the circular buffer. UART_read() will read directly from the UART drivers RX buffer. Enabling the circular buffer will also prevent the device from going into low power modes.

Parameters
[in]handleA UART_Handle returned by UART_open().
See also
UART_rxDisable()

§ UART_flushRx()

void UART_flushRx ( UART_Handle  handle)

Function to flush data in the UART RX FIFO.

Precondition
UART_open() has been called.

This function can be called to remove all data from the RX FIFO, for example, after a UART read error has occurred. All data in the RX circular buffer will be discarded.

Parameters
[in]handleA UART_Handle returned from UART_open().

§ UART_getRxCount()

void UART_getRxCount ( UART_Handle  handle)

Get the number of bytes available in the circular buffer.

Precondition
UART_open() has been called.
Parameters
[in]handleA UART_Handle returned from UART_open().
Returns
Returns the number of bytes available in the RX circular buffer.
See also
UART_rxEnable()
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale