MSPM0G1X0X_G3X0X TI-Driver Library  2.00.01.00
Data Structures | Macros | Enumerations
Collaboration diagram for ADC driver APIs:

Data Structures

struct  ADCMSPM0_HWAttrs
 ADCMSPM0 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. Currently the Single channel single conversion and the Repeat single channel conversion are supported. For the other conversion modes, user has to modify or add the needed parameters to below structure. More...
 
struct  ADCMSPM0_Object
 ADCMSPM0 Object. More...
 

Macros

#define ADC_ALL_INTERRUPTS_MASK   0xFFFFFFFFUL
 

Enumerations

enum  ADCMSPM0_Resolution_Bits {
  ADCMSPM0_RESOLUTION_12_BIT = DL_ADC12_SAMP_CONV_RES_12_BIT,
  ADCMSPM0_RESOLUTION_10_BIT = DL_ADC12_SAMP_CONV_RES_10_BIT,
  ADCMSPM0_RESOLUTION_8_BIT = DL_ADC12_SAMP_CONV_RES_8_BIT
}
 Resolution of ADC-conversion. More...
 
enum  ADCMSPM0_Reference_Source {
  ADCMSPM0_VDDA_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_VDDA,
  ADCMSPM0_INTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_INTREF,
  ADCMSPM0_EXTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_EXTREF
}
 Specifies the source of the ADC reference voltage. More...
 
enum  ADCMSPM0_Clock_Divider {
  ADCMSPM0_CLKDIV_1 = DL_ADC12_CLOCK_DIVIDE_1,
  ADCMSPM0_CLKDIV_2 = DL_ADC12_CLOCK_DIVIDE_2,
  ADCMSPM0_CLKDIV_4 = DL_ADC12_CLOCK_DIVIDE_4,
  ADCMSPM0_CLKDIV_8 = DL_ADC12_CLOCK_DIVIDE_8,
  ADCMSPM0_CLKDIV_16 = DL_ADC12_CLOCK_DIVIDE_16,
  ADCMSPM0_CLKDIV_24 = DL_ADC12_CLOCK_DIVIDE_24,
  ADCMSPM0_CLKDIV_32 = DL_ADC12_CLOCK_DIVIDE_32,
  ADCMSPM0_CLKDIV_48 = DL_ADC12_CLOCK_DIVIDE_48
}
 ADC clock-divider. More...
 
enum  ADCMSPM0_Clock_Select {
  ADCMSPM0_CLK_SYSOSC = DL_ADC12_CLOCK_SYSOSC,
  ADCMSPM0_CLK_ULPCLK = DL_ADC12_CLOCK_ULPCLK,
  ADCMSPM0_CLK_HFCLK = DL_ADC12_CLOCK_HFCLK
}
 ADC clock source select. More...
 
enum  ADCMSPM0_Freq_Range {
  ADCMSPM0_CLK_FREQ_RANGE_1TO4 = DL_ADC12_CLOCK_FREQ_RANGE_1_TO_4,
  ADCMSPM0_CLK_FREQ_RANGE_4TO8 = DL_ADC12_CLOCK_FREQ_RANGE_4_TO_8,
  ADCMSPM0_CLK_FREQ_RANGE_8TO16 = DL_ADC12_CLOCK_FREQ_RANGE_8_TO_16,
  ADCMSPM0_CLK_FREQ_RANGE_16TO20 = DL_ADC12_CLOCK_FREQ_RANGE_16_TO_20,
  ADCMSPM0_CLK_FREQ_RANGE_20TO24 = DL_ADC12_CLOCK_FREQ_RANGE_20_TO_24,
  ADCMSPM0_CLK_FREQ_RANGE_24TO32 = DL_ADC12_CLOCK_FREQ_RANGE_24_TO_32,
  ADCMSPM0_CLK_FREQ_RANGE_32TO40 = DL_ADC12_CLOCK_FREQ_RANGE_32_TO_40,
  ADCMSPM0_CLK_FREQ_RANGE_40TO48 = DL_ADC12_CLOCK_FREQ_RANGE_40_TO_48
}
 ADC clock freq range. More...
 
enum  ADCMSPM0_Conversion_Mode {
  ADCMSPM0_SINGLE_CH_SINGLE_CONV = DL_ADC12_SAMP_MODE_SINGLE,
  ADCMSPM0_MULTI_CH_SEQUENCE_CONV = DL_ADC12_SAMP_MODE_SEQUENCE
}
 ADC conversion mode. More...
 
enum  ADCMSPM0_Repeat_Conversion_Mode {
  ADCMSPM0_REPEAT_MODE_ENABLED = DL_ADC12_REPEAT_MODE_ENABLED,
  ADCMSPM0_REPEAT_MODE_DISABLED = DL_ADC12_REPEAT_MODE_DISABLED
}
 ADC Repeat conversion mode. More...
 
enum  ADCMSPM0_Sampling_Mode {
  ADCMSPM0_SAMPLING_MODE_AUTO = DL_ADC12_SAMPLING_SOURCE_AUTO,
  ADCMSPM0_SAMPLING_MODE_MANUAL = DL_ADC12_SAMPLING_SOURCE_MANUAL
}
 ADC sampling mode. More...
 
enum  ADCMSPM0_Sampling_Trg {
  ADCMSPM0_SAMPLING_TRIG_SW = DL_ADC12_TRIG_SRC_SOFTWARE,
  ADCMSPM0_SAMPLING_TRIG_EVENT = DL_ADC12_TRIG_SRC_EVENT
}
 ADC sampling trigger source. More...
 
enum  ADCMSPM0_Conv_Data_Format {
  ADCMSPM0_CONV_DATA_FORMAT_UNSIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_UNSIGNED,
  ADCMSPM0_CONV_DATA_FORMAT_SIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_SIGNED
}
 ADC conversion data format. More...
 
enum  ADCMSPM0_Sample_Timer_Source {
  ADCMSPM0_SAMP_TMR_SOURCE_SCOMP0 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0,
  ADCMSPM0_SAMP_TMR_SOURCE_SCOMP1 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP1
}
 ADC sample timer source. More...
 
enum  ADCMSPM0_Conv_Trig_Src {
  ADCMSPM0_NEXT_CONV_AUTO = DL_ADC12_TRIGGER_MODE_AUTO_NEXT,
  ADCMSPM0_NEXT_CONV_WITH_TRIG = DL_ADC12_TRIGGER_MODE_TRIGGER_NEXT
}
 ADC conversion trigger. More...
 
enum  ADCMSPM0_HW_Avg {
  ADCMSPM0_HW_AVG_ENABLED = DL_ADC12_AVERAGING_MODE_ENABLED,
  ADCMSPM0_HW_AVG_DISABLED = DL_ADC12_AVERAGING_MODE_DISABLED
}
 ADC HW averaging. More...
 
enum  ADCMSPM0_AVGN {
  ADCMSPM0_HW_AVG_NUM_ACC_DISABLED = DL_ADC12_HW_AVG_NUM_ACC_DISABLED,
  ADCMSPM0_HW_AVG_NUM_ACC_2 = DL_ADC12_HW_AVG_NUM_ACC_2,
  ADCMSPM0_HW_AVG_NUM_ACC_4 = DL_ADC12_HW_AVG_NUM_ACC_4,
  ADCMSPM0_HW_AVG_NUM_ACC_8 = DL_ADC12_HW_AVG_NUM_ACC_8,
  ADCMSPM0_HW_AVG_NUM_ACC_16 = DL_ADC12_HW_AVG_NUM_ACC_16,
  ADCMSPM0_HW_AVG_NUM_ACC_32 = DL_ADC12_HW_AVG_NUM_ACC_32,
  ADCMSPM0_HW_AVG_NUM_ACC_64 = DL_ADC12_HW_AVG_NUM_ACC_64,
  ADCMSPM0_HW_AVG_NUM_ACC_128 = DL_ADC12_HW_AVG_NUM_ACC_128
}
 Hardware averager numerator. More...
 
enum  ADCMSPM0_AVGD {
  ADCMSPM0_HW_AVG_DEN_DIV_BY_1 = DL_ADC12_HW_AVG_DEN_DIV_BY_1,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_2 = DL_ADC12_HW_AVG_DEN_DIV_BY_2,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_4 = DL_ADC12_HW_AVG_DEN_DIV_BY_4,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_8 = DL_ADC12_HW_AVG_DEN_DIV_BY_8,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_16 = DL_ADC12_HW_AVG_DEN_DIV_BY_16,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_32 = DL_ADC12_HW_AVG_DEN_DIV_BY_32,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_64 = DL_ADC12_HW_AVG_DEN_DIV_BY_64,
  ADCMSPM0_HW_AVG_DEN_DIV_BY_128 = DL_ADC12_HW_AVG_DEN_DIV_BY_128
}
 Hardware averager denominator. More...
 
enum  ADCMSPM0_Pwr_Dn_Mode {
  ADCMSPM0_Pwr_Dn_MODE_AUTO = DL_ADC12_POWER_DOWN_MODE_AUTO,
  ADCMSPM0_Pwr_Dn_MODE_MANUAL = DL_ADC12_POWER_DOWN_MODE_MANUAL
}
 ADC power down mode. More...
 
enum  ADCMSPM0_CONV_START_ADDRESS {
  ADCMSPM0_SEQ_START_ADDR_00 = DL_ADC12_SEQ_START_ADDR_00,
  ADCMSPM0_SEQ_START_ADDR_01 = DL_ADC12_SEQ_START_ADDR_01,
  ADCMSPM0_SEQ_START_ADDR_02 = DL_ADC12_SEQ_START_ADDR_02,
  ADCMSPM0_SEQ_START_ADDR_03 = DL_ADC12_SEQ_START_ADDR_03,
  ADCMSPM0_SEQ_START_ADDR_04 = DL_ADC12_SEQ_START_ADDR_04,
  ADCMSPM0_SEQ_START_ADDR_05 = DL_ADC12_SEQ_START_ADDR_05,
  ADCMSPM0_SEQ_START_ADDR_06 = DL_ADC12_SEQ_START_ADDR_06,
  ADCMSPM0_SEQ_START_ADDR_07 = DL_ADC12_SEQ_START_ADDR_07,
  ADCMSPM0_SEQ_START_ADDR_08 = DL_ADC12_SEQ_START_ADDR_08,
  ADCMSPM0_SEQ_START_ADDR_09 = DL_ADC12_SEQ_START_ADDR_09,
  ADCMSPM0_SEQ_START_ADDR_10 = DL_ADC12_SEQ_START_ADDR_10,
  ADCMSPM0_SEQ_START_ADDR_11 = DL_ADC12_SEQ_START_ADDR_11
}
 Sequence start address. More...
 
enum  ADCMSPM0_CONV_END_ADDRESS {
  ADCMSPM0_SEQ_END_ADDR_00 = DL_ADC12_SEQ_END_ADDR_00,
  ADCMSPM0_SEQ_END_ADDR_01 = DL_ADC12_SEQ_END_ADDR_01,
  ADCMSPM0_SEQ_END_ADDR_02 = DL_ADC12_SEQ_END_ADDR_02,
  ADCMSPM0_SEQ_END_ADDR_03 = DL_ADC12_SEQ_END_ADDR_03,
  ADCMSPM0_SEQ_END_ADDR_04 = DL_ADC12_SEQ_END_ADDR_04,
  ADCMSPM0_SEQ_END_ADDR_05 = DL_ADC12_SEQ_END_ADDR_05,
  ADCMSPM0_SEQ_END_ADDR_06 = DL_ADC12_SEQ_END_ADDR_06,
  ADCMSPM0_SEQ_END_ADDR_07 = DL_ADC12_SEQ_END_ADDR_07,
  ADCMSPM0_SEQ_END_ADDR_08 = DL_ADC12_SEQ_END_ADDR_08,
  ADCMSPM0_SEQ_END_ADDR_09 = DL_ADC12_SEQ_END_ADDR_09,
  ADCMSPM0_SEQ_END_ADDR_10 = DL_ADC12_SEQ_END_ADDR_10,
  ADCMSPM0_SEQ_END_ADDR_11 = DL_ADC12_SEQ_END_ADDR_11
}
 Sequence end address. More...
 

Detailed Description

This ADC driver implementation is designed to operate on a ADC peripheral for MSPM0 devices.

Refer to ADC.h for a complete description of APIs & example of use.

Macro Definition Documentation

§ ADC_ALL_INTERRUPTS_MASK

#define ADC_ALL_INTERRUPTS_MASK   0xFFFFFFFFUL

An interrupt mask for all ADC CPU interrupts

Enumeration Type Documentation

§ ADCMSPM0_Resolution_Bits

Resolution of ADC-conversion.

This sets the resolution of the ADC conversion, and will affect how long a conversion takes.

Enumerator
ADCMSPM0_RESOLUTION_12_BIT 

ADC resolution 12bit

ADCMSPM0_RESOLUTION_10_BIT 

ADC resolution 10bit

ADCMSPM0_RESOLUTION_8_BIT 

ADC resolution 8bit

§ ADCMSPM0_Reference_Source

Specifies the source of the ADC reference voltage.

The ADC reference voltage will determine the upper limit of the input voltage.

Note
The actual reference values are slightly different for each device. The function ADCMSPM0_ADCValueToMicrovolts() must be used to derive actual voltage values. Do not attempt to compare raw values between devices or derive a voltage from them yourself. The results of doing so will only be approximately correct.
Warning
Refer to the datasheet to make sure the input voltage to the ADC never exceeds the specifies limits.
Enumerator
ADCMSPM0_VDDA_REFERENCE 

ADC reference voltage VDDA

ADCMSPM0_INTERNAL_REFERENCE 

ADC reference voltage internal

ADCMSPM0_EXTERNAL_REFERENCE 

ADC reference voltage external

§ ADCMSPM0_Clock_Divider

ADC clock-divider.

This sets the clock divider value for the ADC sample clock(SAMPCLK) which can be derived from the SYSOSC/ULPCLK/HFCLK.

Enumerator
ADCMSPM0_CLKDIV_1 

Do not divide clock source

ADCMSPM0_CLKDIV_2 

Divide clock source by 2

ADCMSPM0_CLKDIV_4 

Divide clock source by 4

ADCMSPM0_CLKDIV_8 

Divide clock source by 8

ADCMSPM0_CLKDIV_16 

Divide clock source by 16

ADCMSPM0_CLKDIV_24 

Divide clock source by 24

ADCMSPM0_CLKDIV_32 

Divide clock source by 32

ADCMSPM0_CLKDIV_48 

Divide clock source by 48

§ ADCMSPM0_Clock_Select

ADC clock source select.

This selects the clock source

Enumerator
ADCMSPM0_CLK_SYSOSC 

SYSOSC is the source of ADC sample clock

ADCMSPM0_CLK_ULPCLK 

ULPCLK is the source of ADC sample clock

ADCMSPM0_CLK_HFCLK 

HFCLK is the source of ADC sample clock

§ ADCMSPM0_Freq_Range

ADC clock freq range.

This sets the clock freq range for the configured ADC clock

Enumerator
ADCMSPM0_CLK_FREQ_RANGE_1TO4 

Specifies ADC clock (ADCCLK) frequency range is from 1 MHz to 4 MHz

ADCMSPM0_CLK_FREQ_RANGE_4TO8 

Specifies ADC clock (ADCCLK) frequency range is from 4 MHz to 8 MHz

ADCMSPM0_CLK_FREQ_RANGE_8TO16 

Specifies ADC clock (ADCCLK) frequency range is from 8 MHz to 16 MHz

ADCMSPM0_CLK_FREQ_RANGE_16TO20 

Specifies ADC clock (ADCCLK) frequency range is from 16 MHz to 20 MHz

ADCMSPM0_CLK_FREQ_RANGE_20TO24 

Specifies ADC clock (ADCCLK) frequency range is from 20 MHz to 24 MHz

ADCMSPM0_CLK_FREQ_RANGE_24TO32 

Specifies ADC clock (ADCCLK) frequency range is from 24 MHz to 32 MHz

ADCMSPM0_CLK_FREQ_RANGE_32TO40 

Specifies ADC clock (ADCCLK) frequency range is from 32 MHz to 40 MHz

ADCMSPM0_CLK_FREQ_RANGE_40TO48 

Specifies ADC clock (ADCCLK) frequency range is from 40 MHz to 48 MHz

§ ADCMSPM0_Conversion_Mode

ADC conversion mode.

This sets the ADC conversion mode

Enumerator
ADCMSPM0_SINGLE_CH_SINGLE_CONV 

Single channel conversion selected

ADCMSPM0_MULTI_CH_SEQUENCE_CONV 

Multi channel conversion selected

§ ADCMSPM0_Repeat_Conversion_Mode

ADC Repeat conversion mode.

This sets the ADC repeat conversion mode to enable or disable

Enumerator
ADCMSPM0_REPEAT_MODE_ENABLED 

Enable the repetition of the selected conversion

ADCMSPM0_REPEAT_MODE_DISABLED 

Disable the repetition of the selected conversion

§ ADCMSPM0_Sampling_Mode

ADC sampling mode.

This sets the ADC sampling mode

Enumerator
ADCMSPM0_SAMPLING_MODE_AUTO 

Timer high phase is used as source of the sample signal Internal ADC sampling timer is used in this mode. It can be selected/configured from ADCMSPM0_Sample_Timer_Source.

ADCMSPM0_SAMPLING_MODE_MANUAL 

External or software trigger is used as source of the sample signal

§ ADCMSPM0_Sampling_Trg

ADC sampling trigger source.

This sets the ADC sampling trigger source

Enumerator
ADCMSPM0_SAMPLING_TRIG_SW 

Conversion is triggered by software.

ADCMSPM0_SAMPLING_TRIG_EVENT 

Conversion is triggered by hardware

§ ADCMSPM0_Conv_Data_Format

ADC conversion data format.

This sets the ADC conversion data format

Enumerator
ADCMSPM0_CONV_DATA_FORMAT_UNSIGNED 

Results are read as binary unsigned, right aligned.

ADCMSPM0_CONV_DATA_FORMAT_SIGNED 

Result are read as signed binary (2s complement), left aligned.

§ ADCMSPM0_Sample_Timer_Source

ADC sample timer source.

Selects the source of sample timer period between SCOMP0 and SCOMP1. This selection is valid when ADCMSPM0_SAMPLING_MODE_AUTO is selected as a sampling mode from ADCMSPM0_Sampling_Mode .

Enumerator
ADCMSPM0_SAMP_TMR_SOURCE_SCOMP0 

sample adc sample timer source 0

ADCMSPM0_SAMP_TMR_SOURCE_SCOMP1 

sample adc sample timer source 1

§ ADCMSPM0_Conv_Trig_Src

ADC conversion trigger.

Selects the source of the trigger to start next conversion

Enumerator
ADCMSPM0_NEXT_CONV_AUTO 

ADC triggers automaticaly to the next memory conversion register

ADCMSPM0_NEXT_CONV_WITH_TRIG 

A valid trigger will step to the next memory conversion register

§ ADCMSPM0_HW_Avg

ADC HW averaging.

Hardware Averaging enabled/disabled

Enumerator
ADCMSPM0_HW_AVG_ENABLED 

HW averaging mode enabled

ADCMSPM0_HW_AVG_DISABLED 

HW averaging mode disabled

§ ADCMSPM0_AVGN

Hardware averager numerator.

Selects number of conversions to accumulate for current MEMCTLx and then it is divided by AVGD

§ ADCMSPM0_AVGD

Hardware averager denominator.

The number to divide the accumulated value by (this is a shift).

§ ADCMSPM0_Pwr_Dn_Mode

ADC power down mode.

Selects the power down mode

Enumerator
ADCMSPM0_Pwr_Dn_MODE_AUTO 

Power down mode auto

ADCMSPM0_Pwr_Dn_MODE_MANUAL 

Power down mode manual

§ ADCMSPM0_CONV_START_ADDRESS

Sequence start address.

These bits select which MEMCTLx is used for single conversion or as first MEMCTL for sequence mode

§ ADCMSPM0_CONV_END_ADDRESS

Sequence end address.

These bits select which MEMCTLx is the last one for the sequence mode.

© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale