MSPM0L11XX_L13XX TI-Driver Library  2.00.00.03
Data Fields

Private Metadata structure for a UART instance supporting events. More...

#include <UARTSupportMSPM0.h>

Collaboration diagram for UART_EventCallback_Object:
Collaboration graph
[legend]

Data Fields

UART_EventCallback eventCallback
 
uint32_t eventMask
 

Detailed Description

Private Metadata structure for a UART instance supporting events.

Field Documentation

§ eventCallback

UART_EventCallback UART_EventCallback_Object::eventCallback

Pointer to event callback function

§ eventMask

uint32_t UART_EventCallback_Object::eventMask

Mask of events that application is interacted in


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale