MSPM0L11XX_L13XX TI-Driver Library  2.00.00.03
Data Fields

UART Global configuration. More...

#include <UARTSupportMSPM0.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

UART Global configuration.

The UART_Config structure contains a set of pointers used to characterize the UART driver implementation.

Field Documentation

§ object

void* UART_Config_::object

Pointer to a driver specific data object.

Referenced by UART_Obj_Ptr().

§ hwAttrs

void const* UART_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure.

Referenced by UART_HWAttrs_Ptr().


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale