MSPM0G1X0X_G3X0X TI-Driver Library  2.00.00.03
Data Fields
DMAMSPM0_Cfg Struct Reference

DMAMSPM0 Global configuration. More...

#include <DMAMSPM0.h>

Data Fields

void const * hwAttrs
 
void * object
 

Detailed Description

DMAMSPM0 Global configuration.

The DMAMSPM0_Cfg structure contains pointers used by the DMAMSPM0 driver.

This structure needs to be defined before calling DMAMSPM0_init() and it must not be changed thereafter.

Field Documentation

§ hwAttrs

void const* DMAMSPM0_Cfg::hwAttrs

Pointer to hardware attributes

§ object

void* DMAMSPM0_Cfg::object

Pointer to DMAMSPM0 object


The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale