MSPM0G1X0X_G3X0X TI-Driver Library
2.00.00.03
|
ADCMSPM0 Object. More...
#include <ADCMSPM0.h>
Data Fields | |
bool | isOpen |
bool | isProtected |
ADCMSPM0 Object.
The application must not access any member variables of this structure!
bool ADCMSPM0_Object::isOpen |
Flag if the instance is in use
bool ADCMSPM0_Object::isProtected |
Flag to indicate if thread safety is ensured by the driver