Function pointers to implementation/hardware specific logic.
More...
#include <UARTSupportMSPM0G1X0X_G3X0X.h>
Function pointers to implementation/hardware specific logic.
§ enable
Enable the hardware, typically called during UART_open().
- Parameters
-
[in] | handle | UART_Handle instance from UART_open(). |
[in] | params | Reference to the UART_Params struct passed in by the user. |
- Returns
- Returns true on success, else false.
§ disable
Disable the hardware, typically called during UART_close().
- Parameters
-
§ txChar
Kick the transmitter in the hardware.
- Parameters
-
§ read
int_fast16_t(* UARTSupport_Fxns::read) (UART_Handle, void *buf, size_t size, size_t *bytesRead) |
Read method to use.
- Parameters
-
[in] | handle | UART_Handle instance from UART_open(). |
[out] | buf | location to read data into. |
[in] | size | amount of data to read in bytes. |
[out] | bytesRead | If non-NULL, the location to store the number of bytes actually read into the buffer. If NULL, this parameter will be ignored. In callback mode, NULL could be passed in for this parameter, since the callback function will be passed the number of bytes read. |
- Returns
- Returns a status indicating success or failure of the read.
- Return values
-
§ write
int_fast16_t(* UARTSupport_Fxns::write) (UART_Handle, const void *buf, size_t size, size_t *bytesWritten) |
Write method to use.
- Parameters
-
[in] | handle | UART_Handle instance from UART_open(). |
[in] | buf | location to write data from. |
[in] | size | amount of data to write in bytes. |
[out] | bytesWritten | If non-NULL, the location to store the number of bytes actually written into the buffer. If NULL, this parameter will be ignored. In callback mode, NULL could be passed in for this parameter, since the callback function will be passed the number of bytes written. |
- Returns
- Returns a status indicating success or failure of the write.
- Return values
-
The documentation for this struct was generated from the following file: