![]() |
![]() |
MSPM0G1X0X_G3X0X TI-Driver Library
1.20.01.06
|
![]() |
Data Structures | |
struct | ADCMSPM0_HWAttrs |
ADCMSPM0 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. Currently the Single channel single conversion and the Repeat single channel conversion are supported. For the other conversion modes, user has to modify or add the needed parameters to below structure. More... | |
struct | ADCMSPM0_Object |
ADCMSPM0 Object. More... | |
Macros | |
#define | ADC_ALL_INTERRUPTS_MASK 0xFFFFFFFFUL |
Enumerations | |
enum | ADCMSPM0_Resolution_Bits { ADCMSPM0_RESOLUTION_12_BIT = DL_ADC12_SAMP_CONV_RES_12_BIT, ADCMSPM0_RESOLUTION_10_BIT = DL_ADC12_SAMP_CONV_RES_10_BIT, ADCMSPM0_RESOLUTION_8_BIT = DL_ADC12_SAMP_CONV_RES_8_BIT } |
Resolution of ADC-conversion. More... | |
enum | ADCMSPM0_Reference_Source { ADCMSPM0_VDDA_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_VDDA, ADCMSPM0_INTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_INTREF, ADCMSPM0_EXTERNAL_REFERENCE = DL_ADC12_REFERENCE_VOLTAGE_EXTREF } |
Specifies the source of the ADC reference voltage. More... | |
enum | ADCMSPM0_Clock_Divider { ADCMSPM0_CLKDIV_1 = DL_ADC12_CLOCK_DIVIDE_1, ADCMSPM0_CLKDIV_2 = DL_ADC12_CLOCK_DIVIDE_2, ADCMSPM0_CLKDIV_4 = DL_ADC12_CLOCK_DIVIDE_4, ADCMSPM0_CLKDIV_8 = DL_ADC12_CLOCK_DIVIDE_8, ADCMSPM0_CLKDIV_16 = DL_ADC12_CLOCK_DIVIDE_16, ADCMSPM0_CLKDIV_24 = DL_ADC12_CLOCK_DIVIDE_24, ADCMSPM0_CLKDIV_32 = DL_ADC12_CLOCK_DIVIDE_32, ADCMSPM0_CLKDIV_48 = DL_ADC12_CLOCK_DIVIDE_48 } |
ADC clock-divider. More... | |
enum | ADCMSPM0_Clock_Select { ADCMSPM0_CLK_SYSOSC = DL_ADC12_CLOCK_SYSOSC, ADCMSPM0_CLK_ULPCLK = DL_ADC12_CLOCK_ULPCLK, ADCMSPM0_CLK_HFCLK = DL_ADC12_CLOCK_HFCLK } |
ADC clock source select. More... | |
enum | ADCMSPM0_Freq_Range { ADCMSPM0_CLK_FREQ_RANGE_1TO4 = DL_ADC12_CLOCK_FREQ_RANGE_1_TO_4, ADCMSPM0_CLK_FREQ_RANGE_4TO8 = DL_ADC12_CLOCK_FREQ_RANGE_4_TO_8, ADCMSPM0_CLK_FREQ_RANGE_8TO16 = DL_ADC12_CLOCK_FREQ_RANGE_8_TO_16, ADCMSPM0_CLK_FREQ_RANGE_16TO20 = DL_ADC12_CLOCK_FREQ_RANGE_16_TO_20, ADCMSPM0_CLK_FREQ_RANGE_20TO24 = DL_ADC12_CLOCK_FREQ_RANGE_20_TO_24, ADCMSPM0_CLK_FREQ_RANGE_24TO32 = DL_ADC12_CLOCK_FREQ_RANGE_24_TO_32, ADCMSPM0_CLK_FREQ_RANGE_32TO40 = DL_ADC12_CLOCK_FREQ_RANGE_32_TO_40, ADCMSPM0_CLK_FREQ_RANGE_40TO48 = DL_ADC12_CLOCK_FREQ_RANGE_40_TO_48 } |
ADC clock freq range. More... | |
enum | ADCMSPM0_Conversion_Mode { ADCMSPM0_SINGLE_CH_SINGLE_CONV = DL_ADC12_SAMP_MODE_SINGLE, ADCMSPM0_MULTI_CH_SEQUENCE_CONV = DL_ADC12_SAMP_MODE_SEQUENCE } |
ADC conversion mode. More... | |
enum | ADCMSPM0_Repeat_Conversion_Mode { ADCMSPM0_REPEAT_MODE_ENABLED = DL_ADC12_REPEAT_MODE_ENABLED, ADCMSPM0_REPEAT_MODE_DISABLED = DL_ADC12_REPEAT_MODE_DISABLED } |
ADC Repeat conversion mode. More... | |
enum | ADCMSPM0_Sampling_Mode { ADCMSPM0_SAMPLING_MODE_AUTO = DL_ADC12_SAMPLING_SOURCE_AUTO, ADCMSPM0_SAMPLING_MODE_MANUAL = DL_ADC12_SAMPLING_SOURCE_MANUAL } |
ADC sampling mode. More... | |
enum | ADCMSPM0_Sampling_Trg { ADCMSPM0_SAMPLING_TRIG_SW = DL_ADC12_TRIG_SRC_SOFTWARE, ADCMSPM0_SAMPLING_TRIG_EVENT = DL_ADC12_TRIG_SRC_EVENT } |
ADC sampling trigger source. More... | |
enum | ADCMSPM0_Conv_Data_Format { ADCMSPM0_CONV_DATA_FORMAT_UNSIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_UNSIGNED, ADCMSPM0_CONV_DATA_FORMAT_SIGNED = DL_ADC12_SAMP_CONV_DATA_FORMAT_SIGNED } |
ADC conversion data format. More... | |
enum | ADCMSPM0_Sample_Timer_Source { ADCMSPM0_SAMP_TMR_SOURCE_SCOMP0 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP0, ADCMSPM0_SAMP_TMR_SOURCE_SCOMP1 = DL_ADC12_SAMPLE_TIMER_SOURCE_SCOMP1 } |
ADC sample timer source. More... | |
enum | ADCMSPM0_Conv_Trig_Src { ADCMSPM0_NEXT_CONV_AUTO = DL_ADC12_TRIGGER_MODE_AUTO_NEXT, ADCMSPM0_NEXT_CONV_WITH_TRIG = DL_ADC12_TRIGGER_MODE_TRIGGER_NEXT } |
ADC conversion trigger. More... | |
enum | ADCMSPM0_HW_Avg { ADCMSPM0_HW_AVG_ENABLED = DL_ADC12_AVERAGING_MODE_ENABLED, ADCMSPM0_HW_AVG_DISABLED = DL_ADC12_AVERAGING_MODE_DISABLED } |
ADC HW averaging. More... | |
enum | ADCMSPM0_AVGN { ADCMSPM0_HW_AVG_NUM_ACC_DISABLED = DL_ADC12_HW_AVG_NUM_ACC_DISABLED, ADCMSPM0_HW_AVG_NUM_ACC_2 = DL_ADC12_HW_AVG_NUM_ACC_2, ADCMSPM0_HW_AVG_NUM_ACC_4 = DL_ADC12_HW_AVG_NUM_ACC_4, ADCMSPM0_HW_AVG_NUM_ACC_8 = DL_ADC12_HW_AVG_NUM_ACC_8, ADCMSPM0_HW_AVG_NUM_ACC_16 = DL_ADC12_HW_AVG_NUM_ACC_16, ADCMSPM0_HW_AVG_NUM_ACC_32 = DL_ADC12_HW_AVG_NUM_ACC_32, ADCMSPM0_HW_AVG_NUM_ACC_64 = DL_ADC12_HW_AVG_NUM_ACC_64, ADCMSPM0_HW_AVG_NUM_ACC_128 = DL_ADC12_HW_AVG_NUM_ACC_128 } |
Hardware averager numerator. More... | |
enum | ADCMSPM0_AVGD { ADCMSPM0_HW_AVG_DEN_DIV_BY_1 = DL_ADC12_HW_AVG_DEN_DIV_BY_1, ADCMSPM0_HW_AVG_DEN_DIV_BY_2 = DL_ADC12_HW_AVG_DEN_DIV_BY_2, ADCMSPM0_HW_AVG_DEN_DIV_BY_4 = DL_ADC12_HW_AVG_DEN_DIV_BY_4, ADCMSPM0_HW_AVG_DEN_DIV_BY_8 = DL_ADC12_HW_AVG_DEN_DIV_BY_8, ADCMSPM0_HW_AVG_DEN_DIV_BY_16 = DL_ADC12_HW_AVG_DEN_DIV_BY_16, ADCMSPM0_HW_AVG_DEN_DIV_BY_32 = DL_ADC12_HW_AVG_DEN_DIV_BY_32, ADCMSPM0_HW_AVG_DEN_DIV_BY_64 = DL_ADC12_HW_AVG_DEN_DIV_BY_64, ADCMSPM0_HW_AVG_DEN_DIV_BY_128 = DL_ADC12_HW_AVG_DEN_DIV_BY_128 } |
Hardware averager denominator. More... | |
enum | ADCMSPM0_Pwr_Dn_Mode { ADCMSPM0_Pwr_Dn_MODE_AUTO = DL_ADC12_POWER_DOWN_MODE_AUTO, ADCMSPM0_Pwr_Dn_MODE_MANUAL = DL_ADC12_POWER_DOWN_MODE_MANUAL } |
ADC power down mode. More... | |
enum | ADCMSPM0_CONV_START_ADDRESS { ADCMSPM0_SEQ_START_ADDR_00 = DL_ADC12_SEQ_START_ADDR_00, ADCMSPM0_SEQ_START_ADDR_01 = DL_ADC12_SEQ_START_ADDR_01, ADCMSPM0_SEQ_START_ADDR_02 = DL_ADC12_SEQ_START_ADDR_02, ADCMSPM0_SEQ_START_ADDR_03 = DL_ADC12_SEQ_START_ADDR_03, ADCMSPM0_SEQ_START_ADDR_04 = DL_ADC12_SEQ_START_ADDR_04, ADCMSPM0_SEQ_START_ADDR_05 = DL_ADC12_SEQ_START_ADDR_05, ADCMSPM0_SEQ_START_ADDR_06 = DL_ADC12_SEQ_START_ADDR_06, ADCMSPM0_SEQ_START_ADDR_07 = DL_ADC12_SEQ_START_ADDR_07, ADCMSPM0_SEQ_START_ADDR_08 = DL_ADC12_SEQ_START_ADDR_08, ADCMSPM0_SEQ_START_ADDR_09 = DL_ADC12_SEQ_START_ADDR_09, ADCMSPM0_SEQ_START_ADDR_10 = DL_ADC12_SEQ_START_ADDR_10, ADCMSPM0_SEQ_START_ADDR_11 = DL_ADC12_SEQ_START_ADDR_11 } |
Sequence start address. More... | |
enum | ADCMSPM0_CONV_END_ADDRESS { ADCMSPM0_SEQ_END_ADDR_00 = DL_ADC12_SEQ_END_ADDR_00, ADCMSPM0_SEQ_END_ADDR_01 = DL_ADC12_SEQ_END_ADDR_01, ADCMSPM0_SEQ_END_ADDR_02 = DL_ADC12_SEQ_END_ADDR_02, ADCMSPM0_SEQ_END_ADDR_03 = DL_ADC12_SEQ_END_ADDR_03, ADCMSPM0_SEQ_END_ADDR_04 = DL_ADC12_SEQ_END_ADDR_04, ADCMSPM0_SEQ_END_ADDR_05 = DL_ADC12_SEQ_END_ADDR_05, ADCMSPM0_SEQ_END_ADDR_06 = DL_ADC12_SEQ_END_ADDR_06, ADCMSPM0_SEQ_END_ADDR_07 = DL_ADC12_SEQ_END_ADDR_07, ADCMSPM0_SEQ_END_ADDR_08 = DL_ADC12_SEQ_END_ADDR_08, ADCMSPM0_SEQ_END_ADDR_09 = DL_ADC12_SEQ_END_ADDR_09, ADCMSPM0_SEQ_END_ADDR_10 = DL_ADC12_SEQ_END_ADDR_10, ADCMSPM0_SEQ_END_ADDR_11 = DL_ADC12_SEQ_END_ADDR_11 } |
Sequence end address. More... | |
This ADC driver implementation is designed to operate on a ADC peripheral for MSPM0 devices.
Refer to ADC.h for a complete description of APIs & example of use.
#define ADC_ALL_INTERRUPTS_MASK 0xFFFFFFFFUL |
An interrupt mask for all ADC CPU interrupts
Specifies the source of the ADC reference voltage.
The ADC reference voltage will determine the upper limit of the input voltage.
Enumerator | |
---|---|
ADCMSPM0_VDDA_REFERENCE | ADC reference voltage VDDA |
ADCMSPM0_INTERNAL_REFERENCE | ADC reference voltage internal |
ADCMSPM0_EXTERNAL_REFERENCE | ADC reference voltage external |
ADC clock-divider.
This sets the clock divider value for the ADC sample clock(SAMPCLK) which can be derived from the SYSOSC/ULPCLK/HFCLK.
enum ADCMSPM0_Freq_Range |
ADC clock freq range.
This sets the clock freq range for the configured ADC clock
ADC sampling mode.
This sets the ADC sampling mode
Enumerator | |
---|---|
ADCMSPM0_SAMPLING_MODE_AUTO | Timer high phase is used as source of the sample signal Internal ADC sampling timer is used in this mode. It can be selected/configured from ADCMSPM0_Sample_Timer_Source. |
ADCMSPM0_SAMPLING_MODE_MANUAL | External or software trigger is used as source of the sample signal |
ADC sample timer source.
Selects the source of sample timer period between SCOMP0 and SCOMP1. This selection is valid when ADCMSPM0_SAMPLING_MODE_AUTO is selected as a sampling mode from ADCMSPM0_Sampling_Mode .
Enumerator | |
---|---|
ADCMSPM0_SAMP_TMR_SOURCE_SCOMP0 | sample adc sample timer source 0 |
ADCMSPM0_SAMP_TMR_SOURCE_SCOMP1 | sample adc sample timer source 1 |
enum ADCMSPM0_HW_Avg |
enum ADCMSPM0_AVGN |
Hardware averager numerator.
Selects number of conversions to accumulate for current MEMCTLx and then it is divided by AVGD
enum ADCMSPM0_AVGD |
Hardware averager denominator.
The number to divide the accumulated value by (this is a shift).
enum ADCMSPM0_Pwr_Dn_Mode |
Sequence start address.
These bits select which MEMCTLx is used for single conversion or as first MEMCTL for sequence mode
Sequence end address.
These bits select which MEMCTLx is the last one for the sequence mode.