![]() |
![]() |
|
MSPM0G1X0X_G3X0X Driver Library
1.20.01.06
|
Enumerations | |
| enum | DL_CRC_POLYNOMIAL { DL_CRC_16_POLYNOMIAL = CRC_CRCCTRL_POLYSIZE_CRC16 } |
| enum | DL_CRC_BIT { DL_CRC_BIT_REVERSED = CRC_CRCCTRL_BITREVERSE_REVERSED, DL_CRC_BIT_NOT_REVERSED = CRC_CRCCTRL_BITREVERSE_NOT_REVERSED } |
| enum | DL_CRC_INPUT_ENDIANESS { DL_CRC_INPUT_ENDIANESS_LITTLE_ENDIAN, DL_CRC_INPUT_ENDIANESS_BIG_ENDIAN = CRC_CRCCTRL_INPUT_ENDIANNESS_BIG_ENDIAN } |
| enum | DL_CRC_OUTPUT_BYTESWAP { DL_CRC_OUTPUT_BYTESWAP_ENABLED = CRC_CRCCTRL_OUTPUT_BYTESWAP_ENABLE, DL_CRC_OUTPUT_BYTESWAP_DISABLED = CRC_CRCCTRL_OUTPUT_BYTESWAP_DISABLE } |
Functions | |
| __STATIC_INLINE void | DL_CRC_enablePower (CRC_Regs *crc) |
| Enables power on crc module. More... | |
| __STATIC_INLINE void | DL_CRC_disablePower (CRC_Regs *crc) |
| Disables power on crc module. More... | |
| __STATIC_INLINE bool | DL_CRC_isPowerEnabled (CRC_Regs *crc) |
| Returns if power on crc module is enabled. More... | |
| __STATIC_INLINE void | DL_CRC_reset (CRC_Regs *crc) |
| Resets crc peripheral. More... | |
| __STATIC_INLINE bool | DL_CRC_isReset (CRC_Regs *crc) |
| Returns if crc module has been reset. More... | |
| __STATIC_INLINE void | DL_CRC_init (CRC_Regs *crc, DL_CRC_POLYNOMIAL poly, DL_CRC_BIT bitOrd, DL_CRC_INPUT_ENDIANESS inEndianness, DL_CRC_OUTPUT_BYTESWAP outByteSwap) |
| Initializes CRC. More... | |
| __STATIC_INLINE void | DL_CRC_setSeed16 (CRC_Regs *crc, uint16_t seed) |
| Initializes the seed for a 16-bit polynomial CRC calculation. More... | |
| __STATIC_INLINE void | DL_CRC_setSeed32 (CRC_Regs *crc, uint32_t seed) |
| Initializes the seed for a 32-bit polynomial CRC calculation. More... | |
| __STATIC_INLINE void | DL_CRC_feedData8 (CRC_Regs *crc, uint8_t dataIn) |
| Feeds 8-bit data into the CRC calculation. More... | |
| __STATIC_INLINE void | DL_CRC_feedData16 (CRC_Regs *crc, uint16_t dataIn) |
| Feeds 16-bit data into the CRC calculation. More... | |
| __STATIC_INLINE void | DL_CRC_feedData32 (CRC_Regs *crc, uint32_t dataIn) |
| Feeds 32-bit data into the CRC calculation. More... | |
| __STATIC_INLINE uint16_t | DL_CRC_getResult16 (CRC_Regs *crc) |
| Returns the result from the 16-bit polynomial calculation. More... | |
| __STATIC_INLINE uint32_t | DL_CRC_getResult32 (CRC_Regs *crc) |
| Returns the result from the 32-bit polynomial calculation. More... | |
| uint32_t | DL_CRC_calculateBlock32 (CRC_Regs *crc, uint32_t seed, uint32_t *ptr, uint32_t size) |
| Calculates the CRC over a range of 32-bit values. More... | |
| uint32_t | DL_CRC_calculateMemoryRange32 (CRC_Regs *crc, uint32_t seed, uint32_t *ptrStart, uint32_t *ptrEnd) |
| Calculates the CRC over a memory range. More... | |
| uint16_t | DL_CRC_calculateBlock16 (CRC_Regs *crc, uint16_t seed, uint16_t *ptr, uint16_t size) |
| Calculates the CRC over a range of 16-bit values. More... | |
| uint16_t | DL_CRC_calculateMemoryRange16 (CRC_Regs *crc, uint16_t seed, uint16_t *ptrStart, uint16_t *ptrEnd) |
| Calculates the CRC over a memory range. More... | |
| __STATIC_INLINE uintptr_t | DL_CRC_getCRCINAddr (CRC_Regs *crc) |
| Returns the address of the CRC input data register. More... | |
The CRC DriverLib allows full configuration of the MSPM0 CRC module. The cyclic redundancy check (CRC) accelerator generates signatures for a given data sequence based on the CRC16-CCITT polynomial or the CRC32-ISO3309 polynomial.
| enum DL_CRC_POLYNOMIAL |
| enum DL_CRC_BIT |
| __STATIC_INLINE void DL_CRC_enablePower | ( | CRC_Regs * | crc | ) |
Enables power on crc module.
| crc | Pointer to the register overlay for the CRC peripheral |
| __STATIC_INLINE void DL_CRC_disablePower | ( | CRC_Regs * | crc | ) |
Disables power on crc module.
| crc | Pointer to the register overlay for the CRC peripheral |
| __STATIC_INLINE bool DL_CRC_isPowerEnabled | ( | CRC_Regs * | crc | ) |
Returns if power on crc module is enabled.
| crc | Pointer to the register overlay for the CRC peripheral |
| __STATIC_INLINE void DL_CRC_reset | ( | CRC_Regs * | crc | ) |
Resets crc peripheral.
| crc | Pointer to the register overlay for the CRC peripheral |
| __STATIC_INLINE bool DL_CRC_isReset | ( | CRC_Regs * | crc | ) |
Returns if crc module has been reset.
| crc | Pointer to the register overlay for the CRC peripheral\ |
| __STATIC_INLINE void DL_CRC_init | ( | CRC_Regs * | crc, |
| DL_CRC_POLYNOMIAL | poly, | ||
| DL_CRC_BIT | bitOrd, | ||
| DL_CRC_INPUT_ENDIANESS | inEndianness, | ||
| DL_CRC_OUTPUT_BYTESWAP | outByteSwap | ||
| ) |
Initializes CRC.
| crc | Pointer to the register overlay for the CRC peripheral |
| poly | Selects CRC polynomial. One of DL_CRC_POLYNOMIAL. |
| bitOrd | Selects CRC bit order. One of DL_CRC_BIT. |
| inEndianness | Selects CRC input endianess. One of DL_CRC_INPUT_ENDIANESS. |
| outByteSwap | Selects CRC output byte swap mode. One of DL_CRC_OUTPUT_BYTESWAP. |
| __STATIC_INLINE void DL_CRC_setSeed16 | ( | CRC_Regs * | crc, |
| uint16_t | seed | ||
| ) |
Initializes the seed for a 16-bit polynomial CRC calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed for the CRC to start generating a signature from |
| __STATIC_INLINE void DL_CRC_setSeed32 | ( | CRC_Regs * | crc, |
| uint32_t | seed | ||
| ) |
Initializes the seed for a 32-bit polynomial CRC calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed for the CRC to start generating a signature from |
| __STATIC_INLINE void DL_CRC_feedData8 | ( | CRC_Regs * | crc, |
| uint8_t | dataIn | ||
| ) |
Feeds 8-bit data into the CRC calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | dataIn | 8-bit data value to add to the signature |
| __STATIC_INLINE void DL_CRC_feedData16 | ( | CRC_Regs * | crc, |
| uint16_t | dataIn | ||
| ) |
Feeds 16-bit data into the CRC calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | dataIn | 16-bit data value to add to the signature |
| __STATIC_INLINE void DL_CRC_feedData32 | ( | CRC_Regs * | crc, |
| uint32_t | dataIn | ||
| ) |
Feeds 32-bit data into the CRC calculation.
Feeds a 32-bit value into the CRC calculation. 32-bit data can only be used with the 32-bit polynomial.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | dataIn | 32 bit data value to add to the signature |
| __STATIC_INLINE uint16_t DL_CRC_getResult16 | ( | CRC_Regs * | crc | ) |
Returns the result from the 16-bit polynomial calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| __STATIC_INLINE uint32_t DL_CRC_getResult32 | ( | CRC_Regs * | crc | ) |
Returns the result from the 32-bit polynomial calculation.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
References DL_CRC_calculateBlock16(), DL_CRC_calculateBlock32(), DL_CRC_calculateMemoryRange16(), and DL_CRC_calculateMemoryRange32().
| uint32_t DL_CRC_calculateBlock32 | ( | CRC_Regs * | crc, |
| uint32_t | seed, | ||
| uint32_t * | ptr, | ||
| uint32_t | size | ||
| ) |
Calculates the CRC over a range of 32-bit values.
Uses the 32-bit polynomial to calculate the checksum over a block of values.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed for the CRC to start generating a signature from |
| [in] | ptr | A pointer to the block of code to calculate the CRC over |
| [in] | size | The size of the block of uint32_t data |
Referenced by DL_CRC_getResult32().
| uint32_t DL_CRC_calculateMemoryRange32 | ( | CRC_Regs * | crc, |
| uint32_t | seed, | ||
| uint32_t * | ptrStart, | ||
| uint32_t * | ptrEnd | ||
| ) |
Calculates the CRC over a memory range.
Calculates the checksum using the 32-bit polynomial over any memory range.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed used to start generating a signature from |
| [in] | ptrStart | A uint32_t pointer to the start of a block of code to calculate the CRC over |
| [in] | ptrEnd | A uint32_t pointer to the end of a block of code to calculate the CRC over |
Referenced by DL_CRC_getResult32().
| uint16_t DL_CRC_calculateBlock16 | ( | CRC_Regs * | crc, |
| uint16_t | seed, | ||
| uint16_t * | ptr, | ||
| uint16_t | size | ||
| ) |
Calculates the CRC over a range of 16-bit values.
Uses the 16-bit polynomial to calculate the checksum over a block of values.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed for the CRC to start generating a signature from |
| [in] | ptr | A pointer to the block of code to calculate the CRC over |
| [in] | size | The size of the block of 16-bit data |
Referenced by DL_CRC_getResult32().
| uint16_t DL_CRC_calculateMemoryRange16 | ( | CRC_Regs * | crc, |
| uint16_t | seed, | ||
| uint16_t * | ptrStart, | ||
| uint16_t * | ptrEnd | ||
| ) |
Calculates the CRC over a memory range.
Calculates the checksum using the 16-bit polynomial over any memory range.
| [in] | crc | Pointer to the register overlay for the CRC peripheral |
| [in] | seed | The seed used to start generating a signature from |
| [in] | ptrStart | A uint16_t pointer to the start of a block of code to calculate the CRC over |
| [in] | ptrEnd | A uint16_t pointer to the end of a block of code to calculate the CRC over |
Referenced by DL_CRC_getResult32().
| __STATIC_INLINE uintptr_t DL_CRC_getCRCINAddr | ( | CRC_Regs * | crc | ) |
Returns the address of the CRC input data register.
This API can be used with DL_DMA_setDestAddr to set the destination address when using DMA transfers
| [in] | crc | Pointer to the register overlay for the CRC peripheral |