MSPM0L11XX_L13XX TI-Driver Library  1.20.01.06
Modules | Macros
SPI_control command and status codes
Collaboration diagram for SPI_control command and status codes:

Modules

 Status Codes
 
 Command Codes
 

Macros

#define SPI_CMD_RESERVED   (32)
 
#define SPI_STATUS_RESERVED   (-32)
 

Detailed Description

These SPI macros are reservations for SPI.h

Macro Definition Documentation

§ SPI_CMD_RESERVED

#define SPI_CMD_RESERVED   (32)

Common SPI_control() command code reservation offset. SPI driver implementations should offset command codes with SPI_CMD_RESERVED growing positively

Example implementation specific command codes:

#define SPIXYZ_CMD_COMMAND0 SPI_CMD_RESERVED + 0
#define SPIXYZ_CMD_COMMAND1 SPI_CMD_RESERVED + 1

§ SPI_STATUS_RESERVED

#define SPI_STATUS_RESERVED   (-32)

Common SPI_control status code reservation offset. SPI driver implementations should offset status codes with SPI_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define SPIXYZ_STATUS_ERROR0 SPI_STATUS_RESERVED - 0
#define SPIXYZ_STATUS_ERROR1 SPI_STATUS_RESERVED - 1
#define SPIXYZ_STATUS_ERROR2 SPI_STATUS_RESERVED - 2
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale