Here is a list of all documented files with brief descriptions:
ADC.h | Analog to Digital Conversion (ADC) Input Driver |
ADCMSPM0.h | ADC driver implementation for the ADC peripheral on MSPM0 devices |
DMAMSPM0.h | DMA driver implementation for MSPM0 |
GPIO.h | General Purpose I/O driver interface |
GPIOMSPM0.h | GPIO driver implementation for MSPM0 devices |
I2C.h | I2C Driver |
I2CMSPM0.h | I2C driver implementation for a MSPM0 I2C controller |
I2CSupport.h | Holder of common helper functions for the I2C driver |
SPI.h | SPI Driver Interface |
SPIMSPM0.h | SPI driver implementation for MSPM0 SPI controller using the DMA controller |
UART.h | UART driver interface |
UARTMSPM0G1X0X_G3X0X.h | UART driver interface for the MSPM0G1X0X_G3X0X devices |
UARTSupportMSPM0G1X0X_G3X0X.h | UART driver support APIs for the MSPM0G1X0X_G3X0X devices |