IQMathLibrary
1.0
|
Functions to compute the base-e logarithm of an IQN number.
#include <stdint.h>
#include "../support/support.h"
#include "_IQNtables.h"
Functions | |
__STATIC_INLINE int_fast32_t | __IQNlog (int_fast32_t iqNInput, const int_fast32_t iqNMin, const int8_t q_value) |
Computes the base-e logarithm of an IQN input. More... | |
int32_t | _IQ30log (int32_t a) |
Computes the base-e logarithm of an IQ30 input. More... | |
int32_t | _IQ29log (int32_t a) |
Computes the base-e logarithm of an IQ29 input. More... | |
int32_t | _IQ28log (int32_t a) |
Computes the base-e logarithm of an IQ28 input. More... | |
int32_t | _IQ27log (int32_t a) |
Computes the base-e logarithm of an IQ27 input. More... | |
int32_t | _IQ26log (int32_t a) |
Computes the base-e logarithm of an IQ26 input. More... | |
int32_t | _IQ25log (int32_t a) |
Computes the base-e logarithm of an IQ25 input. More... | |
int32_t | _IQ24log (int32_t a) |
Computes the base-e logarithm of an IQ24 input. More... | |
int32_t | _IQ23log (int32_t a) |
Computes the base-e logarithm of an IQ23 input. More... | |
int32_t | _IQ22log (int32_t a) |
Computes the base-e logarithm of an IQ22 input. More... | |
int32_t | _IQ21log (int32_t a) |
Computes the base-e logarithm of an IQ21 input. More... | |
int32_t | _IQ20log (int32_t a) |
Computes the base-e logarithm of an IQ20 input. More... | |
int32_t | _IQ19log (int32_t a) |
Computes the base-e logarithm of an IQ19 input. More... | |
int32_t | _IQ18log (int32_t a) |
Computes the base-e logarithm of an IQ18 input. More... | |
int32_t | _IQ17log (int32_t a) |
Computes the base-e logarithm of an IQ17 input. More... | |
int32_t | _IQ16log (int32_t a) |
Computes the base-e logarithm of an IQ16 input. More... | |
int32_t | _IQ15log (int32_t a) |
Computes the base-e logarithm of an IQ15 input. More... | |
int32_t | _IQ14log (int32_t a) |
Computes the base-e logarithm of an IQ14 input. More... | |
int32_t | _IQ13log (int32_t a) |
Computes the base-e logarithm of an IQ13 input. More... | |
int32_t | _IQ12log (int32_t a) |
Computes the base-e logarithm of an IQ12 input. More... | |
int32_t | _IQ11log (int32_t a) |
Computes the base-e logarithm of an IQ11 input. More... | |
int32_t | _IQ10log (int32_t a) |
Computes the base-e logarithm of an IQ10 input. More... | |
int32_t | _IQ9log (int32_t a) |
Computes the base-e logarithm of an IQ9 input. More... | |
int32_t | _IQ8log (int32_t a) |
Computes the base-e logarithm of an IQ8 input. More... | |
int32_t | _IQ7log (int32_t a) |
Computes the base-e logarithm of an IQ7 input. More... | |
int32_t | _IQ6log (int32_t a) |
Computes the base-e logarithm of an IQ6 input. More... | |
int32_t | _IQ5log (int32_t a) |
Computes the base-e logarithm of an IQ5 input. More... | |
int32_t | _IQ4log (int32_t a) |
Computes the base-e logarithm of an IQ4 input. More... | |
int32_t | _IQ3log (int32_t a) |
Computes the base-e logarithm of an IQ3 input. More... | |
int32_t | _IQ2log (int32_t a) |
Computes the base-e logarithm of an IQ2 input. More... | |
int32_t | _IQ1log (int32_t a) |
Computes the base-e logarithm of an IQ1 input. More... | |
__STATIC_INLINE int_fast32_t __IQNlog | ( | int_fast32_t | iqNInput, |
const int_fast32_t | iqNMin, | ||
const int8_t | q_value | ||
) |
Computes the base-e logarithm of an IQN input.
iqNInput | IQN type input. |
iqNMin | Minimum parameter value. |
q_value | IQ format. |
Referenced by _IQ10log(), _IQ11log(), _IQ12log(), _IQ13log(), _IQ14log(), _IQ15log(), _IQ16log(), _IQ17log(), _IQ18log(), _IQ19log(), _IQ1log(), _IQ20log(), _IQ21log(), _IQ22log(), _IQ23log(), _IQ24log(), _IQ25log(), _IQ26log(), _IQ27log(), _IQ28log(), _IQ29log(), _IQ2log(), _IQ30log(), _IQ3log(), _IQ4log(), _IQ5log(), _IQ6log(), _IQ7log(), _IQ8log(), and _IQ9log().
int32_t _IQ30log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ30 input.
a | IQ30 type input. |
References __IQNlog().
int32_t _IQ29log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ29 input.
a | IQ29 type input. |
References __IQNlog().
int32_t _IQ28log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ28 input.
a | IQ28 type input. |
References __IQNlog().
int32_t _IQ27log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ27 input.
a | IQ27 type input. |
References __IQNlog().
int32_t _IQ26log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ26 input.
a | IQ26 type input. |
References __IQNlog().
int32_t _IQ25log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ25 input.
a | IQ25 type input. |
References __IQNlog().
int32_t _IQ24log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ24 input.
a | IQ24 type input. |
References __IQNlog().
int32_t _IQ23log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ23 input.
a | IQ23 type input. |
References __IQNlog().
int32_t _IQ22log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ22 input.
a | IQ22 type input. |
References __IQNlog().
int32_t _IQ21log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ21 input.
a | IQ21 type input. |
References __IQNlog().
int32_t _IQ20log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ20 input.
a | IQ20 type input. |
References __IQNlog().
int32_t _IQ19log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ19 input.
a | IQ19 type input. |
References __IQNlog().
int32_t _IQ18log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ18 input.
a | IQ18 type input. |
References __IQNlog().
int32_t _IQ17log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ17 input.
a | IQ17 type input. |
References __IQNlog().
int32_t _IQ16log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ16 input.
a | IQ16 type input. |
References __IQNlog().
int32_t _IQ15log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ15 input.
a | IQ15 type input. |
References __IQNlog().
int32_t _IQ14log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ14 input.
a | IQ14 type input. |
References __IQNlog().
int32_t _IQ13log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ13 input.
a | IQ13 type input. |
References __IQNlog().
int32_t _IQ12log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ12 input.
a | IQ12 type input. |
References __IQNlog().
int32_t _IQ11log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ11 input.
a | IQ11 type input. |
References __IQNlog().
int32_t _IQ10log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ10 input.
a | IQ10 type input. |
References __IQNlog().
int32_t _IQ9log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ9 input.
a | IQ9 type input. |
References __IQNlog().
int32_t _IQ8log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ8 input.
a | IQ8 type input. |
References __IQNlog().
int32_t _IQ7log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ7 input.
a | IQ7 type input. |
References __IQNlog().
int32_t _IQ6log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ6 input.
a | IQ6 type input. |
References __IQNlog().
int32_t _IQ5log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ5 input.
a | IQ5 type input. |
References __IQNlog().
int32_t _IQ4log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ4 input.
a | IQ4 type input. |
References __IQNlog().
int32_t _IQ3log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ3 input.
a | IQ3 type input. |
References __IQNlog().
int32_t _IQ2log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ2 input.
a | IQ2 type input. |
References __IQNlog().
int32_t _IQ1log | ( | int32_t | a | ) |
Computes the base-e logarithm of an IQ1 input.
a | IQ1 type input. |
References __IQNlog().