MCUSW
MCU Driver API

Introduction

Data Structures

struct  Mcu_ClockConfigType
 Structure for module clock setting. More...
 
struct  Mcu_ConfigType
 MCU CONFIG ROOT structure. More...
 

Variables

const struct Mcu_ConfigType_s McuModuleConfiguration_0
 MCU Configuration struct declaration. More...
 

Typedefs

typedef uint8 Mcu_ClockType
 This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock() More...
 
typedef uint32 Mcu_RawResetType
 This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue() More...
 
typedef uint8 Mcu_RamSectionType
 This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection() More...
 
typedef uint8 Mcu_ModeType
 This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode() More...
 
typedef const Mcu_ClockConfigType * Mcu_ClockConfigPtrType
 Pointer to Clock Config structure. More...
 

Macros

#define ARRAYSIZE(array)
 
#define MCU_E_MODE_FAILURE   0U
 

MCU Driver Module SW Version Info

Defines for MCU Driver version used for compatibility checks

#define MCU_SW_MAJOR_VERSION   (10U)
 Driver Implementation Major Version. More...
 
#define MCU_SW_MINOR_VERSION   (0U)
 Driver Implementation Minor Version. More...
 
#define MCU_SW_PATCH_VERSION   (0U)
 Driver Implementation Patch Version. More...
 

MCU Driver Module AUTOSAR Version Info

Defines for MCU Driver AUTOSAR version used for compatibility checks

#define MCU_AR_RELEASE_MAJOR_VERSION   (4U)
 AUTOSAR Major version specification implemented by MCU Driver. More...
 
#define MCU_AR_RELEASE_MINOR_VERSION   (3U)
 AUTOSAR Minor version specification implemented by MCU Driver. More...
 
#define MCU_AR_RELEASE_REVISION_VERSION   (1U)
 AUTOSAR Patch version specification implemented by MCU Driver. More...
 

MCU Driver ID Info

#define MCU_VENDOR_ID   ((uint16) 44U)
 Texas Instruments Vendor ID. More...
 
#define MCU_MODULE_ID   ((uint16) 101U)
 MCU Driver Module ID. More...
 
#define MCU_INSTANCE_ID   ((uint8) 0U)
 MCU Driver Instance ID. More...
 

MCU Error Codes

Error codes returned by MCU functions

#define MCU_E_PARAM_CONFIG   (0x0AU)
 ERROR Description: API service called with wrong configuration parameter. More...
 
#define MCU_E_PARAM_CLOCK   (0x0BU)
 ERROR Description: API service used with wrong clock value. More...
 
#define MCU_E_PARAM_MODE   (0x0CU)
 ERROR Description: API service used with wrong mode. More...
 
#define MCU_E_PARAM_RAMSECTION   (0x0DU)
 ERROR Description: API service called with invalid/wrong RAM section. More...
 
#define MCU_E_PLL_NOT_LOCKED   (0x0EU)
 ERROR Description: API service is called while PLL is not locked. More...
 
#define MCU_E_UNINIT   (0x0FU)
 ERROR Description: Mcu Driver API service is called before initialization of MCU Driver. More...
 
#define MCU_E_PARAM_POINTER   (0x10U)
 ERROR Description: API service is called with NULL/Wrong pointer. More...
 
#define MCU_E_INIT_FAILED   (0x11U)
 ERROR Description: Initialization of the MCU Driver Failed. More...
 

MCU Driver State Values

The MCU Driver State Values

#define MCU_STATUS_UNINIT   ((uint8)(0U))
 MCU driver Status uninitialized. More...
 
#define MCU_STATUS_INIT   ((uint8)(1U))
 MCU driver Status Initialized. More...
 

MCU Service Ids

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error

#define MCU_SID_INIT   (0x00U)
 Mcu_Init() API Service ID. More...
 
#define MCU_SID_INIT_RAM_SECTION   (0x01U)
 Mcu_InitRamSection() API Service ID. More...
 
#define MCU_SID_INIT_CLOCK   (0x02U)
 Mcu_InitClock() API Service ID. More...
 
#define MCU_SID_DISTRIBUTE_PLL_CLOCK   (0x03U)
 Mcu_DistributePllClock() API Service ID. More...
 
#define MCU_SID_GET_PLL_STATUS   (0x04U)
 Mcu_GetPllStatus() API Service ID. More...
 
#define MCU_SID_GET_RESET_REASON   (0x05U)
 Mcu_GetResetReason() API Service ID. More...
 
#define MCU_SID_GET_RESET_RAW_VALUE   (0x06U)
 Mcu_GetResetRawValue() API Service ID. More...
 
#define MCU_SID_PERFORM_RESET   (0x07U)
 Mcu_PerformReset() API Service ID. More...
 
#define MCU_SID_SETMODE   (0x08U)
 Mcu_SetMode() API Service ID. More...
 
#define MCU_SID_GET_VERSION_INFO   (0x09U)
 Mcu_GetVersionInfo() API Service ID. More...
 
#define MCU_SID_GET_RAM_STATE   (0x0AU)
 Mcu_GetRamState() API Service ID. More...
 

MCU Reset Modes

Reset mode enum which can be used in Mcu_PerformReset()

#define MCU_PERFORM_RESET_MODE_COLD   ((uint8) 0U)
 Initiate SW COLD RESET sequence. More...
 
#define MCU_PERFORM_RESET_MODE_WARM   ((uint8) 1U)
 Initiate SW WARM RESET sequence. More...
 

Macro Definition Documentation

◆ ARRAYSIZE

#define ARRAYSIZE (   array)
Value:
((sizeof (array) / \
sizeof ((array)[0])))

◆ MCU_SW_MAJOR_VERSION

#define MCU_SW_MAJOR_VERSION   (10U)

Driver Implementation Major Version.

◆ MCU_SW_MINOR_VERSION

#define MCU_SW_MINOR_VERSION   (0U)

Driver Implementation Minor Version.

◆ MCU_SW_PATCH_VERSION

#define MCU_SW_PATCH_VERSION   (0U)

Driver Implementation Patch Version.

◆ MCU_AR_RELEASE_MAJOR_VERSION

#define MCU_AR_RELEASE_MAJOR_VERSION   (4U)

AUTOSAR Major version specification implemented by MCU Driver.

◆ MCU_AR_RELEASE_MINOR_VERSION

#define MCU_AR_RELEASE_MINOR_VERSION   (3U)

AUTOSAR Minor version specification implemented by MCU Driver.

◆ MCU_AR_RELEASE_REVISION_VERSION

#define MCU_AR_RELEASE_REVISION_VERSION   (1U)

AUTOSAR Patch version specification implemented by MCU Driver.

◆ MCU_VENDOR_ID

#define MCU_VENDOR_ID   ((uint16) 44U)

Texas Instruments Vendor ID.

◆ MCU_MODULE_ID

#define MCU_MODULE_ID   ((uint16) 101U)

MCU Driver Module ID.

◆ MCU_INSTANCE_ID

#define MCU_INSTANCE_ID   ((uint8) 0U)

MCU Driver Instance ID.

◆ MCU_E_PARAM_CONFIG

#define MCU_E_PARAM_CONFIG   (0x0AU)

ERROR Description: API service called with wrong configuration parameter.

◆ MCU_E_PARAM_CLOCK

#define MCU_E_PARAM_CLOCK   (0x0BU)

ERROR Description: API service used with wrong clock value.

◆ MCU_E_PARAM_MODE

#define MCU_E_PARAM_MODE   (0x0CU)

ERROR Description: API service used with wrong mode.

◆ MCU_E_PARAM_RAMSECTION

#define MCU_E_PARAM_RAMSECTION   (0x0DU)

ERROR Description: API service called with invalid/wrong RAM section.

◆ MCU_E_PLL_NOT_LOCKED

#define MCU_E_PLL_NOT_LOCKED   (0x0EU)

ERROR Description: API service is called while PLL is not locked.

◆ MCU_E_UNINIT

#define MCU_E_UNINIT   (0x0FU)

ERROR Description: Mcu Driver API service is called before initialization of MCU Driver.

◆ MCU_E_PARAM_POINTER

#define MCU_E_PARAM_POINTER   (0x10U)

ERROR Description: API service is called with NULL/Wrong pointer.

◆ MCU_E_INIT_FAILED

#define MCU_E_INIT_FAILED   (0x11U)

ERROR Description: Initialization of the MCU Driver Failed.

◆ MCU_STATUS_UNINIT

#define MCU_STATUS_UNINIT   ((uint8)(0U))

MCU driver Status uninitialized.

◆ MCU_STATUS_INIT

#define MCU_STATUS_INIT   ((uint8)(1U))

MCU driver Status Initialized.

◆ MCU_SID_INIT

#define MCU_SID_INIT   (0x00U)

Mcu_Init() API Service ID.

◆ MCU_SID_INIT_RAM_SECTION

#define MCU_SID_INIT_RAM_SECTION   (0x01U)

Mcu_InitRamSection() API Service ID.

◆ MCU_SID_INIT_CLOCK

#define MCU_SID_INIT_CLOCK   (0x02U)

Mcu_InitClock() API Service ID.

◆ MCU_SID_DISTRIBUTE_PLL_CLOCK

#define MCU_SID_DISTRIBUTE_PLL_CLOCK   (0x03U)

Mcu_DistributePllClock() API Service ID.

◆ MCU_SID_GET_PLL_STATUS

#define MCU_SID_GET_PLL_STATUS   (0x04U)

Mcu_GetPllStatus() API Service ID.

◆ MCU_SID_GET_RESET_REASON

#define MCU_SID_GET_RESET_REASON   (0x05U)

Mcu_GetResetReason() API Service ID.

◆ MCU_SID_GET_RESET_RAW_VALUE

#define MCU_SID_GET_RESET_RAW_VALUE   (0x06U)

Mcu_GetResetRawValue() API Service ID.

◆ MCU_SID_PERFORM_RESET

#define MCU_SID_PERFORM_RESET   (0x07U)

Mcu_PerformReset() API Service ID.

◆ MCU_SID_SETMODE

#define MCU_SID_SETMODE   (0x08U)

Mcu_SetMode() API Service ID.

◆ MCU_SID_GET_VERSION_INFO

#define MCU_SID_GET_VERSION_INFO   (0x09U)

Mcu_GetVersionInfo() API Service ID.

◆ MCU_SID_GET_RAM_STATE

#define MCU_SID_GET_RAM_STATE   (0x0AU)

Mcu_GetRamState() API Service ID.

◆ MCU_PERFORM_RESET_MODE_COLD

#define MCU_PERFORM_RESET_MODE_COLD   ((uint8) 0U)

Initiate SW COLD RESET sequence.

◆ MCU_PERFORM_RESET_MODE_WARM

#define MCU_PERFORM_RESET_MODE_WARM   ((uint8) 1U)

Initiate SW WARM RESET sequence.

◆ MCU_E_MODE_FAILURE

#define MCU_E_MODE_FAILURE   0U

Typedef Documentation

◆ Mcu_ClockType

typedef uint8 Mcu_ClockType

This type specifies the identification (ID) for a ClockType status used by Mcu_InitClock()

◆ Mcu_RawResetType

typedef uint32 Mcu_RawResetType

This type specifies the identification (ID) for a RAW MCU reset status returned by Mcu_GetResetRawValue()

◆ Mcu_RamSectionType

typedef uint8 Mcu_RamSectionType

This type specifies the identification (ID) for a RAM section used in Mcu_InitRamSection()

◆ Mcu_ModeType

typedef uint8 Mcu_ModeType

This type specifies the identification (ID) for a MCU mode used in Mcu_SetMode()

◆ Mcu_ClockConfigPtrType

Pointer to Clock Config structure.

Variable Documentation

◆ McuModuleConfiguration_0

const struct Mcu_ConfigType_s McuModuleConfiguration_0

MCU Configuration struct declaration.