137#include "WdgIf_Types.h"
158#define WDG_SW_MAJOR_VERSION (9U)
160#define WDG_SW_MINOR_VERSION (1U)
162#define WDG_SW_PATCH_VERSION (2U)
172#define WDG_AR_RELEASE_MAJOR_VERSION (4U)
174#define WDG_AR_RELEASE_MINOR_VERSION (3U)
176#define WDG_AR_RELEASE_REVISION_VERSION (1U)
184#define WDG_VENDOR_ID ((uint16) 44U)
186#define WDG_MODULE_ID ((uint16) 102U)
188#define WDG_INSTANCE_ID ((uint8) 0U)
201#define WDG_E_DRIVER_STATE ((uint8) 0x10U)
203#define WDG_E_PARAM_MODE ((uint8) 0x11U)
205#define WDG_E_PARAM_CONFIG ((uint8) 0x12U)
207#define WDG_E_PARAM_TIMEOUT ((uint8) 0x13U)
209#define WDG_E_PARAM_POINTER ((uint8) 0x14U)
211#define WDG_E_INIT_FAILED ((uint8) 0x15U)
225#define WDG_API_INIT ((uint8) 0x00U)
227#define WDG_API_SET_MODE ((uint8) 0x01U)
229#define WDG_SET_TRIGGER_CONDITION ((uint8) 0x03U)
231#define WDG_API_GET_VERSION_INFO ((uint8) 0x04U)
233#define WDG_API_TRIGGER ((uint8) 0x05U)
235#define WDG_API_REGISTER_READBACK ((uint8) 0x06U)
245#define WDG_WINDOW_100_PERCENT ((uint32) 0x00000005U)
247#define WDG_WINDOW_50_PERCENT ((uint32) 0x00000050U)
249#define WDG_WINDOW_25_PERCENT ((uint32) 0x00000500U)
251#define WDG_WINDOW_12P5_PERCENT ((uint32) 0x00005000U)
253#define WDG_WINDOW_6P25_PERCENT ((uint32) 0x00050000U)
255#define WDG_WINDOW_3P125_PERCENT ((uint32) 0x00500000U)
259#define INIT_VAL_ZERO (0U)
312typedef struct Wdg_ConfigType_s
326typedef struct Wdg_ConfigType_PC_s
335#if (STD_ON == WDG_REGISTER_READBACK_API)
359#if (STD_ON == WDG_GET_VERSION_INFO_API)
460#if (STD_ON == WDG_REGISTER_READBACK_API)
489 WDG_APPL_DATA) regRbPtr);
This file contains generated pre compile configuration file for WDG MCAL driver.
void Wdg_Trigger(void)
This function triggers the servicing of the watchdog.
Wdg_StatusType
Watchdog driver state.
Definition Wdg.h:277
void Wdg_Init(const Wdg_ConfigType *CfgPtr)
This service initializes the WDG driver.
void Wdg_GetVersionInfo(Std_VersionInfoType *versioninfo)
This service returns the version information of this module.
void Wdg_SetTriggerCondition(uint16 timeout)
Sets the timeout value for the trigger counter.
Std_ReturnType Wdg_RegisterReadback(Wdg_RegisterReadbackType *regRbPtr)
This function reads the important registers of the hardware unit and returns the value in the structu...
Std_ReturnType Wdg_SetMode(WdgIf_ModeType Mode)
This function triggers the servicing of the watchdog.
uint32 reaction
Definition Wdg.h:292
uint16 instanceId
Definition Wdg.h:328
uint32 rtiWdKey
Definition Wdg.h:344
uint32 rtiWdStatus
Definition Wdg.h:342
Wdg_ModeInfoType fastModeCfg
Definition Wdg.h:316
uint32 rtiDwdCtrl
Definition Wdg.h:338
WdgIf_ModeType defaultMode
Definition Wdg.h:314
uint32 rtiDwdprld
Definition Wdg.h:340
uint32 initialTimeOut
Definition Wdg.h:330
Wdg_ModeInfoType slowModeCfg
Definition Wdg.h:318
uint32 timeOutVal
Definition Wdg.h:304
uint32 rtiWwdSizeCtrl
Definition Wdg.h:348
uint32 rtiWwdRxnCtrl
Definition Wdg.h:346
uint32 windowSize
Definition Wdg.h:301
@ WDG_UNINIT
Definition Wdg.h:278
@ WDG_IDLE
Definition Wdg.h:281
@ WDG_BUSY
Definition Wdg.h:284
WDG pre-compile config structure.
Definition Wdg.h:327
WDG config structure.
Definition Wdg.h:313
Mode info type.
Definition Wdg.h:291