111#include "Std_Types.h"
116#include "MemIf_Types.h"
118#include <Fls/fls_hw/ospi/V0/lldr_ospi.h>
138#define FLS_SW_MAJOR_VERSION (12U)
140#define FLS_SW_MINOR_VERSION (1U)
142#define FLS_SW_PATCH_VERSION (1U)
152#define FLS_AR_RELEASE_MAJOR_VERSION (4U)
154#define FLS_AR_RELEASE_MINOR_VERSION (3U)
156#define FLS_AR_RELEASE_REVISION_VERSION (1U)
164#define FLS_VENDOR_ID ((uint16) 44U)
166#define FLS_MODULE_ID ((uint16) 92U)
168#define FLS_INSTANCE_ID ((uint8) 0U)
189#ifndef FLS_E_PARAM_CONFIG
191#define FLS_E_PARAM_CONFIG ((uint8) 0x01U)
193#ifndef FLS_E_PARAM_ADDRESS
195#define FLS_E_PARAM_ADDRESS ((uint8) 0x02U)
197#ifndef FLS_E_PARAM_LENGTH
199#define FLS_E_PARAM_LENGTH ((uint8) 0x03U)
201#ifndef FLS_E_PARAM_DATA
203#define FLS_E_PARAM_DATA ((uint8) 0x04U)
207#define FLS_E_UNINIT ((uint8) 0x05U)
211#define FLS_E_BUSY ((uint8) 0x06U)
213#ifndef FLS_E_PARAM_POINTER
215#define FLS_E_PARAM_POINTER ((uint8) 0x0AU)
217#ifndef FLS_E_VERIFY_ERASE_FAILED
219#define FLS_E_VERIFY_ERASE_FAILED ((uint8) 0x07U)
221#ifndef FLS_E_VERIFY_WRITE_FAILED
223#define FLS_E_VERIFY_WRITE_FAILED ((uint8) 0x08U)
227#define FLS_E_TIMEOUT ((uint8) 0x09U)
232#ifndef FLS_E_ERASE_FAILED
234#define FLS_E_ERASE_FAILED ((uint8) 0x01U)
236#ifndef FLS_E_WRITE_FAILED
238#define FLS_E_WRITE_FAILED ((uint8) 0x02U)
240#ifndef FLS_E_READ_FAILED
242#define FLS_E_READ_FAILED ((uint8) 0x03U)
244#ifndef FLS_E_COMPARE_FAILED
246#define FLS_E_COMPARE_FAILED ((uint8) 0x04U)
248#ifndef FLS_E_UNEXPECTED_FLASH_ID
250#define FLS_E_UNEXPECTED_FLASH_ID ((uint8) 0x05U)
262#define FLS_SID_INIT ((uint8) 0x00U)
264#define FLS_SID_ERASE ((uint8) 0x01U)
266#define FLS_SID_WRITE ((uint8) 0x02U)
268#define FLS_SID_CANCEL ((uint8) 0x03U)
270#define FLS_SID_GET_STATUS ((uint8) 0x04U)
272#define FLS_SID_GET_JOB_RESULT ((uint8) 0x05U)
274#define FLS_SID_READ ((uint8) 0x07U)
276#define FLS_SID_COMPARE ((uint8) 0x08U)
278#define FLS_SID_SET_MODE ((uint8) 0x09U)
280#define FLS_SID_GET_VERSION_INFO ((uint8) 0x10U)
282#define FLS_SID_BLANK_CHECK ((uint8) 0x0AU)
284#define FLS_SID_MAIN_FUNCTION ((uint8) 0x06U)
345typedef struct Fls_ConfigType_s
493typedef struct FlsNorDeviceConfig_t
612 uint8 *TargetAddressPtr,
643#if (STD_ON == FLS_COMPARE_API)
676#if (STD_ON == FLS_BLANK_CHECK_API)
697#if (STD_ON == FLS_GET_STATUS_API)
721#if (STD_ON == FLS_VERSION_INFO_API)
742#if (STD_ON == FLS_GET_JOB_RESULT_API)
776#if ( FLS_CANCEL_API == STD_ON )
780#if (STD_ON == OSPI_REGISTER_READBACK_API)
808 P2VAR(CSL_ospi_flash_cfgRegs, AUTOMATIC, FLS_APPL_DATA) RegRbPtr);
This file contains generated pre compile configuration file for FLS MCAL driver.
This file contains ISR function declaration for FLS MCAL driver.
const FlsNorDeviceConfig FlsNorDevice
Std_ReturnType Fls_BlankCheck(Fls_AddressType TargetAddress, Fls_LengthType Length)
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) p...
Std_ReturnType Fls_Read(Fls_AddressType SourceAddress, uint8 *TargetAddressPtr, Fls_LengthType Length)
Reads from flash memory..
Std_ReturnType Fls_GetVersionInfo(Std_VersionInfoType *versioninfo)
This service returns the version information of this module.
MemIf_StatusType Fls_GetStatus(void)
Returns the driver state.
Std_ReturnType Fls_Erase(Fls_AddressType TargetAddress, Fls_LengthType Length)
Erases flash sector(s).
void Fls_Init(const Fls_ConfigType *ConfigPtr)
Initializes the Flash Driver.
Std_ReturnType Ospi_RegisterReadback(CSL_ospi_flash_cfgRegs *RegRbPtr)
This function reads the important registers of the hardware unit and returns the value in the structu...
MemIf_JobResultType Fls_GetJobResult(void)
Returns the result of the last job.
void Fls_MainFunction(void)
Performs the processing of jobs.
Std_ReturnType Fls_Write(Fls_AddressType TargetAddress, const uint8 *SourceAddressPtr, Fls_LengthType Length)
Writes one or more complete flash pages.
void Fls_SwitchMode(boolean dacEnable, boolean xipEnable)
Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or dis...
Std_ReturnType Fls_Compare(Fls_AddressType SourceAddress, const uint8 *TargetAddressPtr, Fls_LengthType Length)
Compares the contents of an area of flash memory with that of an application data buffer.
OSPI_xferLines
Number of lines used for OSPI read/write transaction.
Definition Fls.h:319
uint32 Fls_LengthType
Definition Fls.h:177
FLASH_Protocol
Definition Fls.h:331
void Fls_Cancel(void)
Cancels an ongoing job.
uint32 Fls_AddressType
Type of address type.
Definition Fls.h:176
uint32 blockSize
Definition Fls.h:382
uint32 NOR_OCTAL_SDR_CMD_READ_DUMMY_CYCLE
Definition Fls.h:473
uint8 NOR_CMD_SFRST
Definition Fls.h:415
uint8 NOR_VREG_OFFSET
Definition Fls.h:426
uint8 NOR_CMD_RDSR
Definition Fls.h:409
uint32 NOR_BE_SECTOR_NUM
Definition Fls.h:404
uint32 NOR_SIZE
Definition Fls.h:395
boolean dacEnable
Definition Fls.h:368
uint32 NOR_SECTOR_ERASE_TIMEOUT
Definition Fls.h:488
uint32 NOR_CMD_OCTAL_READ
Definition Fls.h:420
uint32 NOR_MANF_ID
Definition Fls.h:447
uint32 NOR_CMD_WRDIS
Definition Fls.h:408
uint32 NOR_NVREG_OFFSET
Definition Fls.h:427
uint32 NOR_CMD_EXT_OCTAL_FAST_PROG
Definition Fls.h:458
#define NOR_NUMBER_FLASH
Definition Fls_Cfg.h:193
uint32 NOR_CR_TBPARM
Definition Fls.h:452
uint32 NOR_CFG1_VREG_ADDR
Definition Fls.h:441
#define FLS_NUMBER_OF_SECTOR_CFG
Number of Sectorlist configured.
Definition Fls_Cfg.h:187
uint8 NOR_CMD_WRREG
Definition Fls.h:406
uint32 flsBaudRateDiv
Definition Fls.h:380
uint32 NOR_CMD_READ_NVCR
Definition Fls.h:468
uint32 maxWriteNormalMode
Definition Fls.h:356
Fls_AddressType sectorStartaddress
Definition Fls.h:311
uint32 NOR_SR_WIP
Definition Fls.h:449
OSPI_xferLines ospixferlines
Definition Fls.h:378
uint32 NOR_SINGLE_READ_DUMMY_CYCLE
Definition Fls.h:471
uint8 NOR_CMD_SRSTE
Definition Fls.h:414
uint32 currentSectorIndex
Definition Fls.h:363
uint32 NOR_OCTAL_READ_DUMMY_CYCLE
Definition Fls.h:475
uint32 NOR_BULK_ERASE_TIMEOUT
Definition Fls.h:490
uint32 maxReadNormalMode
Definition Fls.h:353
uint32 NOR_RDID_CMD_LENGTH_OCTAL
Definition Fls.h:485
uint32 NOR_CMD_OCTAL_O_FAST_RD
Definition Fls.h:455
Fls_LengthType numberOfSectors
Definition Fls.h:305
uint32 NOR_CFG2_NVREG_ADDR
Definition Fls.h:433
uint32 NOR_CMD_PAGE_PROG
Definition Fls.h:422
uint32 NOR_CFG3_VREG_ADDR
Definition Fls.h:443
uint8 NOR_CMD_RDREG
Definition Fls.h:411
uint32 NOR_CMD_QUAD_DDR_O_FAST_RD
Definition Fls.h:461
Fls_JobErrorNotifyType Fls_JobErrorNotification
Definition Fls.h:350
uint32 NOR_CMD_OCTAL_PROG
Definition Fls.h:423
uint32 FOUR_BYTE_ADDR_ENABLE
Definition Fls.h:391
uint32 NOR_CMD_QUAD_READ
Definition Fls.h:482
Fls_LengthType sectorPageSize
Definition Fls.h:307
uint32 NOR_SECTOR_SIZE
Definition Fls.h:394
uint32 NOR_BLOCK_SIZE
Definition Fls.h:392
uint32 NOR_NUM_PAGES_PER_BLOCK
Definition Fls.h:401
uint32 NOR_CMD_WRITE_VCR
Definition Fls.h:424
uint32 NOR_QUAD_READ_DUMMY_CYCLE
Definition Fls.h:479
uint8 NOR_CMD_WREN
Definition Fls.h:407
uint32 NOR_CFG4_NVREG_ADDR
Definition Fls.h:435
FLASH_Protocol FLS_PROTOCOL
Definition Fls.h:390
boolean xipEnable
Definition Fls.h:370
uint32 NOR_CFG1_NVREG_ADDR
Definition Fls.h:432
uint32 NOR_CFG3_NVREG_ADDR
Definition Fls.h:434
uint32 NOR_CMD_WRITE_NVCR
Definition Fls.h:467
uint32 NOR_CMD_OCTAL_DDR_IO_FAST_RD
Definition Fls.h:465
uint32 NOR_CMD_RDCR_NVOL
Definition Fls.h:454
uint32 NOR_CFG4_VREG_ADDR
Definition Fls.h:444
uint32 NOR_4K_SECT_BOT_END_OFFSET
Definition Fls.h:403
boolean dmaEnable
Definition Fls.h:384
uint32 NOR_OCTAL_READ_DUMMY_CYCLE_LC
Definition Fls.h:476
uint32 NOR_CMD_QUAD_IO_FAST_RD
Definition Fls.h:460
uint32 NOR_CFG5_VREG_ADDR
Definition Fls.h:445
uint8 NOR_ERASED_DATA
Definition Fls.h:402
boolean phyEnable
Definition Fls.h:376
uint32 NOR_CMD_READ
Definition Fls.h:418
uint32 NOR_DEVICE_ID
Definition Fls.h:448
uint32 NOR_PAGE_PROG_TIMEOUT
Definition Fls.h:487
uint32 NOR_UNIFORM_SECTOR_SIZE
Definition Fls.h:393
uint8 NOR_CMD_SECTOR_ERASE
Definition Fls.h:417
uint32 NOR_CFG5_NVREG_ADDR
Definition Fls.h:436
uint32 NOR_CMD_OCTAL_IO_FAST_RD
Definition Fls.h:456
uint32 NOR_CMD_BULK_ERASE
Definition Fls.h:405
uint32 NOR_STS2_VREG_ADDR
Definition Fls.h:439
uint32 NOR_OCTAL_READ_DUMMY_CYCLE_INDAC
Definition Fls.h:477
uint32 NOR_CFG2_VREG_ADDR
Definition Fls.h:442
uint32 NOR_CMD_QUAD_O_FAST_RD
Definition Fls.h:459
uint32 NOR_CMD_READ_ENVCR
Definition Fls.h:466
uint32 NOR_CMD_QUAD_FAST_PROG
Definition Fls.h:462
uint64 ospiClkSpeed
Definition Fls.h:372
uint8 NOR_CMD_RDID
Definition Fls.h:413
Fls_LengthType sectorSize
Definition Fls.h:309
uint32 NOR_OCTAL_DDR_CMD_READ_DUMMY_CYCLE
Definition Fls.h:474
uint32 NOR_RDID_CMD_LENGTH_SINGLE
Definition Fls.h:484
uint32 NOR_STS1_VREG_ADDR
Definition Fls.h:438
uint8 NOR_CMD_BLOCK_ERASE
Definition Fls.h:416
uint32 NOR_SR_WRPGEN
Definition Fls.h:450
uint32 NOR_SINGLE_CMD_READ_DUMMY_CYCLE
Definition Fls.h:472
uint32 NOR_NUM_BLOCKS
Definition Fls.h:398
uint32 NOR_NUM_SECTORS
Definition Fls.h:397
uint32 NOR_CMD_OCTAL_DDR_READ
Definition Fls.h:421
uint32 NOR_WRR_WRITE_TIMEOUT
Definition Fls.h:489
uint32 NOR_STS1_NVREG_ADDR
Definition Fls.h:429
uint32 NOR_CMD_OCTAL_FAST_PROG
Definition Fls.h:457
uint32 NOR_CMD_RDSR2
Definition Fls.h:410
uint32 NOR_CMD_RDCR
Definition Fls.h:412
uint32 NOR_OCTAL_READ_DUMMY_CYCLE_LC_INDAC
Definition Fls.h:478
uint32 NOR_CMD_READ_VCR
Definition Fls.h:425
uint32 NOR_CMD_QUAD_DDR_IO_READ
Definition Fls.h:480
uint32 NOR_NUM_PAGES_PER_SECTOR
Definition Fls.h:400
uint32 NOR_PAGE_SIZE
Definition Fls.h:399
uint8 NOR_CMD_WRITE_ENVCR
Definition Fls.h:469
Fls_JobEndNotifyType Fls_JobEndNotification
Definition Fls.h:347
uint32 NOR_CMD_OCTAL_DDR_O_FAST_RD
Definition Fls.h:464
uint32 NOR_CMD_FAST_READ
Definition Fls.h:419
uint32 NOR_RDID_NUM_BYTES
Definition Fls.h:446
uint32 NOR_CMD_EXT_QUAD_FAST_PROG
Definition Fls.h:463
uint32 NOR_STS2_NVREG_ADDR
Definition Fls.h:430
boolean dtrEnable
Definition Fls.h:374
uint32 NOR_NUM_4K_SECTORS
Definition Fls.h:396
uint32 NOR_CMD_QUAD_PAGE_PROG
Definition Fls.h:481
uint32 NOR_CMD_RDCR_VOL
Definition Fls.h:453
@ OSPI_XFER_LINES_SINGLE
Definition Fls.h:320
@ OSPI_XFER_LINES_DUAL
Definition Fls.h:322
@ OSPI_XFER_LINES_OCTAL
Definition Fls.h:326
@ OSPI_XFER_LINES_QUAD
Definition Fls.h:324
@ FLS_XSPI
Definition Fls.h:334
@ FLS_QSPI
Definition Fls.h:336
@ FLS_OSPI
Definition Fls.h:332
FLS Module Configuration Structure.
Definition Fls.h:346
FLS Module Flashable Sectors and pages.
Definition Fls.h:304