![]() |
MCUSW
|
This files defines FLS MCAL configuration structures
Data Structures | |
| struct | Fls_SectorType |
| FLS Module Flashable Sectors and pages. More... | |
| struct | Fls_ConfigType |
| FLS Module Configuration Structure. More... | |
| struct | FlashConfig |
| struct | FlsNorDeviceConfig |
Macros | |
| #define | FLS_PRE_COMPILE_VARIANT (STD_ON) |
| FLS Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time) | |
FLS Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| enum | OSPI_xferLines { OSPI_XFER_LINES_SINGLE = 0U , OSPI_XFER_LINES_DUAL , OSPI_XFER_LINES_QUAD , OSPI_XFER_LINES_OCTAL } |
| Number of lines used for OSPI read/write transaction. More... | |
| enum | FLASH_Protocol { FLS_OSPI = 0U , FLS_XSPI = 1U , FLS_QSPI = 2U } |
| const FlsNorDeviceConfig | FlsNorDevice |
| void | Fls_SwitchMode (boolean dacEnable, boolean xipEnable) |
| Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode) | |
| void | Fls_Init (const Fls_ConfigType *ConfigPtr) |
| Initializes the Flash Driver. | |
| Std_ReturnType | Fls_Erase (Fls_AddressType TargetAddress, Fls_LengthType Length) |
| Erases flash sector(s). | |
| Std_ReturnType | Fls_Write (Fls_AddressType TargetAddress, const uint8 *SourceAddressPtr, Fls_LengthType Length) |
| Writes one or more complete flash pages. | |
| Std_ReturnType | Fls_Read (Fls_AddressType SourceAddress, uint8 *TargetAddressPtr, Fls_LengthType Length) |
| Reads from flash memory.. | |
| Std_ReturnType | Fls_Compare (Fls_AddressType SourceAddress, const uint8 *TargetAddressPtr, Fls_LengthType Length) |
| Compares the contents of an area of flash memory with that of an application data buffer. | |
| Std_ReturnType | Fls_BlankCheck (Fls_AddressType TargetAddress, Fls_LengthType Length) |
| The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed. | |
| MemIf_StatusType | Fls_GetStatus (void) |
| Returns the driver state. | |
| Std_ReturnType | Fls_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| MemIf_JobResultType | Fls_GetJobResult (void) |
| Returns the result of the last job. | |
| void | Fls_MainFunction (void) |
| Performs the processing of jobs. | |
| void | Fls_Cancel (void) |
| Cancels an ongoing job. | |
| Std_ReturnType | Ospi_RegisterReadback (CSL_ospi_flash_cfgRegs *RegRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. | |
FLS Driver ISR category level | |
Defines for FLS Driver ISR ISR category level | |
| const struct Fls_ConfigType_s | FlsConfigSet |
| FLS Configuration struct declaration. | |
| #define | FLS_ISR_VOID (0x00U) |
| void ISR type | |
| #define | FLS_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | FLS_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
| #define | FLS_INIT_CONFIG_PC FlsConfigSet |
| Pre Compile config macro name. | |
| #define | FLS_NOR |
| FLS_MEMORY_TYPE. | |
| #define | FLS_BASE_ADDRESS (1610612736U) |
| Flash Memory start address, defines lower boundary for read/writ/erase/compare jobs. | |
| #define | FLS_BLANK_CHECK_API (STD_ON) |
| Enable/disable FLS Blank Check API. | |
| #define | FLS_COMPARE_API (STD_ON) |
| Enable/disable FLS compare API. | |
| #define | FLS_CANCEL_API (STD_ON) |
| Enable/disable FLS cancel API. | |
| #define | FLS_TIMEOUT_SUPERVISION_ENABLED (STD_OFF) |
| Enable/disable FlsTimeoutSupervisionEnabled. | |
| #define | FLS_DEV_ERROR_DETECT (STD_ON) |
| Enable/disable FLS dev detect error. | |
| #define | FLS_DRIVER_INDEX (0U) |
| Index of driver, used by FEE. | |
| #define | FLS_GET_JOB_RESULT_API (STD_ON) |
| Enable/disable FLS Fls_GetJobResult function API. | |
| #define | FLS_GET_STATUS_API (STD_ON) |
| Enable/disable FLS Fls_GetStatus function API. | |
| #define | FLS_TOTAL_SIZE (1073741824U) |
| Total amount of flash memory in bytes. | |
| #define | FLS_USE_INTERRUPTS (STD_OFF) |
| Job processing triggered by hardware interrupt. | |
| #define | FLS_ISR_TYPE (FLS_ISR_CAT2) |
| ISR type. | |
| #define | FLS_TIMEOUT_DURATION (50000U) |
| Counter ID for counter used to count wait ticks. | |
| #define | FLS_VERSION_INFO_API (STD_ON) |
| Enable/disable FLS get version info API. | |
| #define | FLS_OSPI_CTRL_BASE_ADDR (264503296U) |
| Base Address of OSPI. | |
| #define | OSPI_SAFETY_API (STD_OFF) |
| Enable/disable OSPI safety API. | |
| #define | OSPI_REGISTER_READBACK_API (STD_ON) |
| Enable/disable OSPI register read back API. | |
| #define | FLS_MAX_ERASE_TIME (1000.0) |
| Max Erase time in millisec. | |
| #define | FLS_MAX_WRITE_TIME (1000.0) |
| Max Write time in millisec. | |
| #define | FLS_NUMBER_OF_SECTOR_CFG (1U) |
| Number of Sectorlist configured. | |
| #define | FLS_OS_COUNTER_ID ((CounterType)OsCounter_0) |
| Counter ID for counter used to count wait ticks. | |
| #define | NOR_NUMBER_FLASH (1U) |
| #define | FLS_ERASE_BUF_LEN (262144U) |
| #define | FLS_READ_WRITE_BUF_LEN (768U) |
| #define | FLS_DMA_ENABLE (STD_ON) |
| Enable/disable FLS CDD DMA for indirect OSPI transfers. | |
| #define FLS_PRE_COMPILE_VARIANT (STD_ON) |
FLS Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time)
| #define FLS_ISR_VOID (0x00U) |
void ISR type
| #define FLS_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define FLS_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define FLS_INIT_CONFIG_PC FlsConfigSet |
Pre Compile config macro name.
| #define FLS_NOR |
FLS_MEMORY_TYPE.
| #define FLS_BASE_ADDRESS (1610612736U) |
Flash Memory start address, defines lower boundary for read/writ/erase/compare jobs.
| #define FLS_BLANK_CHECK_API (STD_ON) |
Enable/disable FLS Blank Check API.
| #define FLS_COMPARE_API (STD_ON) |
Enable/disable FLS compare API.
| #define FLS_CANCEL_API (STD_ON) |
Enable/disable FLS cancel API.
| #define FLS_TIMEOUT_SUPERVISION_ENABLED (STD_OFF) |
Enable/disable FlsTimeoutSupervisionEnabled.
| #define FLS_DEV_ERROR_DETECT (STD_ON) |
Enable/disable FLS dev detect error.
| #define FLS_DRIVER_INDEX (0U) |
Index of driver, used by FEE.
| #define FLS_GET_JOB_RESULT_API (STD_ON) |
Enable/disable FLS Fls_GetJobResult function API.
| #define FLS_GET_STATUS_API (STD_ON) |
Enable/disable FLS Fls_GetStatus function API.
| #define FLS_TOTAL_SIZE (1073741824U) |
Total amount of flash memory in bytes.
| #define FLS_USE_INTERRUPTS (STD_OFF) |
Job processing triggered by hardware interrupt.
| #define FLS_ISR_TYPE (FLS_ISR_CAT2) |
ISR type.
| #define FLS_TIMEOUT_DURATION (50000U) |
Counter ID for counter used to count wait ticks.
| #define FLS_VERSION_INFO_API (STD_ON) |
Enable/disable FLS get version info API.
| #define FLS_OSPI_CTRL_BASE_ADDR (264503296U) |
Base Address of OSPI.
| #define OSPI_SAFETY_API (STD_OFF) |
Enable/disable OSPI safety API.
| #define OSPI_REGISTER_READBACK_API (STD_ON) |
Enable/disable OSPI register read back API.
| #define FLS_MAX_ERASE_TIME (1000.0) |
Max Erase time in millisec.
| #define FLS_MAX_WRITE_TIME (1000.0) |
Max Write time in millisec.
| #define FLS_NUMBER_OF_SECTOR_CFG (1U) |
Number of Sectorlist configured.
| #define FLS_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
| #define NOR_NUMBER_FLASH (1U) |
| #define FLS_ERASE_BUF_LEN (262144U) |
| #define FLS_READ_WRITE_BUF_LEN (768U) |
| #define FLS_DMA_ENABLE (STD_ON) |
Enable/disable FLS CDD DMA for indirect OSPI transfers.
| enum OSPI_xferLines |
| enum FLASH_Protocol |
| void Fls_SwitchMode | ( | boolean | dacEnable, |
| boolean | xipEnable ) |
Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode)
| void Fls_Init | ( | const Fls_ConfigType * | ConfigPtr | ) |
Initializes the Flash Driver.
* Service name : Fls_Init * Syntax : void Fls_Init( const Fls_ConfigType* ConfigPtr ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : ConfigPtr - Pointer to flash driver configuration set * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Initializes the Flash Driver *
| Std_ReturnType Fls_Erase | ( | Fls_AddressType | TargetAddress, |
| Fls_LengthType | Length ) |
Erases flash sector(s).
* Service name : Fls_Erase * Syntax : Std_ReturnType Fls_Erase(Fls_AddressType TargetAddress * ,Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: erase command has been accepted * E_NOT_OK: erase command has not been accepted * Description : Erases flash sector(s). *
| Std_ReturnType Fls_Write | ( | Fls_AddressType | TargetAddress, |
| const uint8 * | SourceAddressPtr, | ||
| Fls_LengthType | Length ) |
Writes one or more complete flash pages.
* Service name : Fls_Write * Syntax : Std_ReturnType Fls_Write(Fls_AddressType TargetAddress * ,const uint8* SourceAddressPtr, * Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * SourceAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: write command has been accepted * E_NOT_OK: write command has not been accepted * Description : Writes one or more complete flash pages. *
| Std_ReturnType Fls_Read | ( | Fls_AddressType | SourceAddress, |
| uint8 * | TargetAddressPtr, | ||
| Fls_LengthType | Length ) |
Reads from flash memory..
* Service name : Fls_Read * Syntax : Std_ReturnType Fls_Read((Fls_AddressType SourceAddress * ,const uint8* TargetAddressPtr, * Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : SourceAddress - source address in flash memory. * This address offset will be added to the flash memory * base address. * TargetAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: read command has been accepted * E_NOT_OK: read command has not been accepted * Description : Reads from flash memory. *
| Std_ReturnType Fls_Compare | ( | Fls_AddressType | SourceAddress, |
| const uint8 * | TargetAddressPtr, | ||
| Fls_LengthType | Length ) |
Compares the contents of an area of flash memory with that of an application data buffer.
* Service name : Fls_Compare * Syntax : Std_ReturnType Fls_Compare * (Fls_AddressType SourceAddress, * const uint8* TargetAddressPtr, * Fls_LengthType Length) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : SourceAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * TargetAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: compare command has been accepted * E_NOT_OK: compare command has not been accepted * Description : Compares the contents of an area of flash memory * with that of an application data buffer. *
| Std_ReturnType Fls_BlankCheck | ( | Fls_AddressType | TargetAddress, |
| Fls_LengthType | Length ) |
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.
* Service name : Fls_BlankCheck * Syntax : Std_ReturnType Fls_Compare * (Fls_AddressType TargetAddress,, * Fls_LengthType Length) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0a * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * SourceAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: BlankCheck command has been accepted * E_NOT_OK: BlankCheck command has not been accepted * Description : The function Fls_BlankCheck shall verify, * whether a given memory area has been * erased but not (yet) programmed. *
| MemIf_StatusType Fls_GetStatus | ( | void | ) |
Returns the driver state.
* Service name : Fls_GetStatus * Syntax : MemIf_StatusType Fls_GetStatus( void ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : MemIf_StatusType * Description : Returns the driver state. *
| Std_ReturnType Fls_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
This service returns the version information of this module.
* Service name : Fls_GetVersionInfo * Syntax : void Fls_GetVersionInfo( Std_VersionInfoType* * versioninfo ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : versioninfo - Pointer to where to store the version * information of this module * Parameters (out) : None * Return value : None * Description : This service returns the version information of this * module *
| MemIf_JobResultType Fls_GetJobResult | ( | void | ) |
Returns the result of the last job.
* Service name : Fls_GetJobResult * Syntax : MemIf_JobResultType Fls_GetJobResult(void) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : MemIf_JobResultType * Description : Returns the result of the last job. *
| void Fls_MainFunction | ( | void | ) |
Performs the processing of jobs.
* Service name : Fls_MainFunction * Syntax : void Fls_MainFunction(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Description : Performs the processing of jobs. *
| void Fls_Cancel | ( | void | ) |
Cancels an ongoing job.
* Service name : Fls_Cancel * Syntax : void Fls_Cancel(void) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Cancels an ongoing job. *
| Std_ReturnType Ospi_RegisterReadback | ( | CSL_ospi_flash_cfgRegs * | RegRbPtr | ) |
This function reads the important registers of the hardware unit and returns the value in the structure.
This API should be called after Ospi_Init is called. Otherwise this API will return E_NOT_OK.
This API could be used to readback the register contents after Ospi_Init and then the readback value could be compared during SPI execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn't change after init based on job or channel config.
* Service name : Ospi_RegisterReadback * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (inout) : RegRbPtr - Pointer to where to store the readback * values. If this pointer is NULL_PTR, then the API * will return E_NOT_OK. * Return value : Std_ReturnType * E_OK: Register read back has been done * E_NOT_OK: Register read back failed *
| Fls_LengthType Fls_SectorType::numberOfSectors |
Number of total Sectors in the Flash Device
| Fls_LengthType Fls_SectorType::sectorPageSize |
Page size of the Flash Device
| Fls_LengthType Fls_SectorType::sectorSize |
Size of each sector in the Flash Device
| Fls_AddressType Fls_SectorType::sectorStartaddress |
Start address of first sector of the Flash Device
| Fls_JobEndNotifyType Fls_ConfigType::Fls_JobEndNotification |
Mapped to the job end notification routine provided by some upper layer module, typically the Fee module.
| Fls_JobErrorNotifyType Fls_ConfigType::Fls_JobErrorNotification |
Mapped to the job error notification routine provided by some upper layer module, typically the Fee module.
| uint32 Fls_ConfigType::maxReadNormalMode |
The maximum number of bytes to read or compare in one cycle of the flash driver's job processing function in normal mode.
| uint32 Fls_ConfigType::maxWriteNormalMode |
The maximum number of bytes to write in one cycle of the flash driver's job processing function in normal mode.
| Fls_SectorType Fls_ConfigType::sectorList[FLS_NUMBER_OF_SECTOR_CFG] |
The maximum number of bytes to write in one cycle of the flash driver's job processing function in normal mode. Using Fls Info Structure instead of this for now.
| uint32 Fls_ConfigType::currentSectorIndex |
Index of the currently active sector configuration in the sector list. This field is updated during read/write/erase operations based on the address being accessed. It helps avoid repeated traversal of the sector list and aids in boundary validation, logging, and error handling.
| boolean Fls_ConfigType::dacEnable |
Enable Direct Access Mode of Transfer in OSPI Flash
| boolean Fls_ConfigType::xipEnable |
Enable XIP mode in OSPI Flash
| uint64 Fls_ConfigType::ospiClkSpeed |
OSPI Clock Speed
| boolean Fls_ConfigType::dtrEnable |
Enable Double transfer rate protocol for OSPI.
| boolean Fls_ConfigType::phyEnable |
Enable PHY high-speed mode for DAC mode
| OSPI_xferLines Fls_ConfigType::ospixferlines |
Select the OSPI read/write transaction Lines
| uint32 Fls_ConfigType::flsBaudRateDiv |
To select the FLS baudrate Divider value
| uint32 Fls_ConfigType::blockSize |
To select OSPI block size based on variants
| boolean Fls_ConfigType::dmaEnable |
Enable DMA for OSPI read transfers
| FLASH_Protocol FlashConfig::FLS_PROTOCOL |
| uint32 FlashConfig::FOUR_BYTE_ADDR_ENABLE |
| uint32 FlashConfig::NOR_BLOCK_SIZE |
| uint32 FlashConfig::NOR_UNIFORM_SECTOR_SIZE |
| uint32 FlashConfig::NOR_SECTOR_SIZE |
| uint32 FlashConfig::NOR_SIZE |
| uint32 FlashConfig::NOR_NUM_4K_SECTORS |
| uint32 FlashConfig::NOR_NUM_SECTORS |
| uint32 FlashConfig::NOR_NUM_BLOCKS |
| uint32 FlashConfig::NOR_PAGE_SIZE |
| uint32 FlashConfig::NOR_NUM_PAGES_PER_SECTOR |
| uint32 FlashConfig::NOR_NUM_PAGES_PER_BLOCK |
| uint8 FlashConfig::NOR_ERASED_DATA |
| uint32 FlashConfig::NOR_4K_SECT_BOT_END_OFFSET |
| uint32 FlashConfig::NOR_BE_SECTOR_NUM |
| uint32 FlashConfig::NOR_CMD_BULK_ERASE |
| uint8 FlashConfig::NOR_CMD_WRREG |
| uint8 FlashConfig::NOR_CMD_WREN |
| uint32 FlashConfig::NOR_CMD_WRDIS |
| uint8 FlashConfig::NOR_CMD_RDSR |
| uint32 FlashConfig::NOR_CMD_RDSR2 |
| uint8 FlashConfig::NOR_CMD_RDREG |
| uint32 FlashConfig::NOR_CMD_RDCR |
| uint8 FlashConfig::NOR_CMD_RDID |
| uint8 FlashConfig::NOR_CMD_SRSTE |
| uint8 FlashConfig::NOR_CMD_SFRST |
| uint8 FlashConfig::NOR_CMD_BLOCK_ERASE |
| uint8 FlashConfig::NOR_CMD_SECTOR_ERASE |
| uint32 FlashConfig::NOR_CMD_READ |
| uint32 FlashConfig::NOR_CMD_FAST_READ |
| uint32 FlashConfig::NOR_CMD_OCTAL_READ |
| uint32 FlashConfig::NOR_CMD_OCTAL_DDR_READ |
| uint32 FlashConfig::NOR_CMD_PAGE_PROG |
| uint32 FlashConfig::NOR_CMD_OCTAL_PROG |
| uint32 FlashConfig::NOR_CMD_WRITE_VCR |
| uint32 FlashConfig::NOR_CMD_READ_VCR |
| uint8 FlashConfig::NOR_VREG_OFFSET |
| uint32 FlashConfig::NOR_NVREG_OFFSET |
| uint32 FlashConfig::NOR_STS1_NVREG_ADDR |
| uint32 FlashConfig::NOR_STS2_NVREG_ADDR |
| uint32 FlashConfig::NOR_CFG1_NVREG_ADDR |
| uint32 FlashConfig::NOR_CFG2_NVREG_ADDR |
| uint32 FlashConfig::NOR_CFG3_NVREG_ADDR |
| uint32 FlashConfig::NOR_CFG4_NVREG_ADDR |
| uint32 FlashConfig::NOR_CFG5_NVREG_ADDR |
| uint32 FlashConfig::NOR_STS1_VREG_ADDR |
| uint32 FlashConfig::NOR_STS2_VREG_ADDR |
| uint32 FlashConfig::NOR_CFG1_VREG_ADDR |
| uint32 FlashConfig::NOR_CFG2_VREG_ADDR |
| uint32 FlashConfig::NOR_CFG3_VREG_ADDR |
| uint32 FlashConfig::NOR_CFG4_VREG_ADDR |
| uint32 FlashConfig::NOR_CFG5_VREG_ADDR |
| uint32 FlashConfig::NOR_RDID_NUM_BYTES |
| uint32 FlashConfig::NOR_MANF_ID |
Read ID command definitions
| uint32 FlashConfig::NOR_DEVICE_ID |
| uint32 FlashConfig::NOR_SR_WIP |
| uint32 FlashConfig::NOR_SR_WRPGEN |
Status Register: Write-in-Progress bit
| uint32 FlashConfig::NOR_CR_TBPARM |
Status Register: Program enabled bit Configuration Register: TBPARM bit
| uint32 FlashConfig::NOR_CMD_RDCR_VOL |
| uint32 FlashConfig::NOR_CMD_RDCR_NVOL |
| uint32 FlashConfig::NOR_CMD_OCTAL_O_FAST_RD |
| uint32 FlashConfig::NOR_CMD_OCTAL_IO_FAST_RD |
| uint32 FlashConfig::NOR_CMD_OCTAL_FAST_PROG |
| uint32 FlashConfig::NOR_CMD_EXT_OCTAL_FAST_PROG |
| uint32 FlashConfig::NOR_CMD_QUAD_O_FAST_RD |
| uint32 FlashConfig::NOR_CMD_QUAD_IO_FAST_RD |
| uint32 FlashConfig::NOR_CMD_QUAD_DDR_O_FAST_RD |
| uint32 FlashConfig::NOR_CMD_QUAD_FAST_PROG |
| uint32 FlashConfig::NOR_CMD_EXT_QUAD_FAST_PROG |
| uint32 FlashConfig::NOR_CMD_OCTAL_DDR_O_FAST_RD |
| uint32 FlashConfig::NOR_CMD_OCTAL_DDR_IO_FAST_RD |
| uint32 FlashConfig::NOR_CMD_READ_ENVCR |
| uint32 FlashConfig::NOR_CMD_WRITE_NVCR |
| uint32 FlashConfig::NOR_CMD_READ_NVCR |
| uint8 FlashConfig::NOR_CMD_WRITE_ENVCR |
| uint32 FlashConfig::NOR_SINGLE_READ_DUMMY_CYCLE |
Dummy cycles for various Read operations
| uint32 FlashConfig::NOR_SINGLE_CMD_READ_DUMMY_CYCLE |
| uint32 FlashConfig::NOR_OCTAL_SDR_CMD_READ_DUMMY_CYCLE |
| uint32 FlashConfig::NOR_OCTAL_DDR_CMD_READ_DUMMY_CYCLE |
| uint32 FlashConfig::NOR_OCTAL_READ_DUMMY_CYCLE |
| uint32 FlashConfig::NOR_OCTAL_READ_DUMMY_CYCLE_LC |
| uint32 FlashConfig::NOR_OCTAL_READ_DUMMY_CYCLE_INDAC |
| uint32 FlashConfig::NOR_OCTAL_READ_DUMMY_CYCLE_LC_INDAC |
| uint32 FlashConfig::NOR_QUAD_READ_DUMMY_CYCLE |
| uint32 FlashConfig::NOR_CMD_QUAD_DDR_IO_READ |
| uint32 FlashConfig::NOR_CMD_QUAD_PAGE_PROG |
| uint32 FlashConfig::NOR_CMD_QUAD_READ |
| uint32 FlashConfig::NOR_RDID_CMD_LENGTH_SINGLE |
Read ID Command Lengths
| uint32 FlashConfig::NOR_RDID_CMD_LENGTH_OCTAL |
| uint32 FlashConfig::NOR_PAGE_PROG_TIMEOUT |
Timeouts (in microseconds)
| uint32 FlashConfig::NOR_SECTOR_ERASE_TIMEOUT |
| uint32 FlashConfig::NOR_WRR_WRITE_TIMEOUT |
| uint32 FlashConfig::NOR_BULK_ERASE_TIMEOUT |
| FlashConfig FlsNorDeviceConfig::flscfg[NOR_NUMBER_FLASH] |
|
extern |
|
extern |
FLS Configuration struct declaration.