![]() |
MCUSW
|
This file contains interface header for UART Complex Device Driver.
Go to the source code of this file.
MCAL Driver states | |
| #define | MCAL_STATE_RESET (0U) |
| #define | MCAL_STATE_READY (1U) |
| #define | MCAL_STATE_BUSY (2U) |
| #define | MCAL_STATE_ERROR (3U) |
| typedef uint8 | CddUartDataBufferType |
| Typedef for the data buffer elements. | |
| typedef uint8_least | CddUartDataDirectionType |
| Type for defining the direction of data transfer, i.e., sending or receival. | |
| void | Cdd_Uart_GetVersionInfo (Std_VersionInfoType *VersionInfoPtr) |
| Service for getting CDD UART version. | |
| Std_ReturnType | Cdd_Uart_RegisterReadback (uint8 ChannelID, CddUart_RegisterReadbackType *RegisterSetPtr) |
| Service for reading HW IP registers of a CDD UART instance. | |
| void | Cdd_Uart_Init (const Cdd_Uart_CfgType *ConfigurationPtr) |
| Service for CDD UART Initialization. | |
| void | Cdd_Uart_DeInit (void) |
| Service for deinitializing CDD UART. | |
| Std_ReturnType | Cdd_Uart_Write (uint8 ChannelID, CddUartDataBufferType *SrcBufferPtr, uint32 Count, uint32 Timeout) |
| Service to transmit message using UART. | |
| Std_ReturnType | Cdd_Uart_Read (uint8 ChannelID, CddUartDataBufferType *DestBufferPtr, uint32 Count, uint32 Timeout) |
| Service to read message or command from the UART. | |
| boolean | Cdd_Uart_Cancel (uint8 ChannelID, CddUartDataDirectionType TransferType) |
| Service to cancel an ongoing transaction with UART. | |
| uint32 | Cdd_Uart_GetRemainingWords (uint8 ChannelID, CddUartDataDirectionType TransferType) |
| Service to get remaining words to be transmitted from the UART for any ongoing transaction. | |
Macros | |
| #define | UART_FIFO_SIZE (64U) |
| Uart FIFO Size. | |
| #define | UART_TRANSMITEMPTY_TRIALCOUNT (3000U) |
| Timeout in ms used for TX FIFO empty at the time of delete. Three seconds is more than sufficient to transfer 64 bytes (FIFO size) at the lowest baud rate of 2400. | |
| #define | UART_STATE_RX_DISABLED (0x0U) |
| #define | UART_STATE_RX_ENABLED (0x1U) |
| #define | IS_DATA_LENGTH_VALID(dataLength) |
| Macro to check if the Data length is valid. | |
| #define | IS_STOP_BITS_VALID(stopBits) |
| Macro to check if the Number of stop bits is valid. | |
| #define | IS_PARITY_TYPE_VALID(parityType) |
| Macro to check if the Parity type is valid. | |
| #define | IS_OPER_MODE_VALID(operMode) |
| Macro to check if the Operation mode is valid. | |
| #define | IS_RXTRIG_LVL_VALID(rxTrigLvl) |
| Macro to check if the RX Trigger level is valid. | |
| #define | IS_TXTRIG_LVL_VALID(txTrigLvl) |
| Macro to check if the TX Trigger level is valid. | |
CDD UART Driver ID Info | |
name CDD UART Driver ID Info | |
| #define | CDD_UART_MODULE_ID 255U |
| CDD Module ID. | |
| #define | CDD_UART_VENDOR_ID 44U |
| Texas Instruments Vendor ID. | |
| #define | CDD_UART_INSTANCE_ID 0U |
| Texas Instruments Vendor ID. | |
CDD UART Driver Module Version Info | |
Defines for CDD Driver version used for compatibility checks | |
| #define | CDD_UART_SW_MAJOR_VERSION CDD_UART_MAJOR_VERSION |
| Driver Implementation Major Version. | |
| #define | CDD_UART_SW_MINOR_VERSION CDD_UART_MINOR_VERSION |
| Driver Implementation Minor Version. | |
| #define | CDD_UART_SW_PATCH_VERSION CDD_UART_CFG_PATCH_VERSION |
| Driver Implementation patch Version. | |
CDD UART Driver Module AUTOSAR Version Info | |
Defines for CDD Driver AUTOSAR version used for compatibility checks | |
| #define | CDD_UART_AR_RELEASE_MAJOR_VERSION 4U |
| AUTOSAR Major version specification implemented by CDD Driver. | |
| #define | CDD_UART_AR_RELEASE_MINOR_VERSION 3U |
| AUTOSAR Minor version specification implemented by CDD Driver. | |
| #define | CDD_UART_AR_RELEASE_REVISION_VERSION 1U |
| AUTOSAR Patch version specification implemented by CDD Driver. | |
CDD UART API Service ID | |
| #define | CDD_UART_INIT_SERVICE_ID 0x01U |
| API Service ID for initialization. | |
| #define | CDD_UART_GETVERSIONINFO_SERVICE_ID 0x02U |
| API Service ID for get version info. | |
| #define | CDD_UART_REGISTERREADBACK_SERVICE_ID 0x0DU |
| API Service ID for Register Readback service ID. | |
| #define | CDD_UART_READDATA_SERVICE_ID 0x03U |
| API Service ID for read API. | |
| #define | CDD_UART_WRITEDATA_SERVICE_ID 0x04U |
| API Service ID for write API. | |
| #define | CDD_UART_ERROR_SERVICE_ID 0x05U |
| API Service ID for error API. | |
| #define | CDD_UART_CANCEL_SERVICE_ID 0x06U |
| API Service ID for cancel API. | |
| #define | CDD_UART_GETREMAININGWORDS_SERVICE_ID 0x07U |
| API Service ID for get remaining words API. | |
| #define | CDD_UART_READNOTIF_SERVICE_ID 0x08U |
| API Service ID for read notification handler. | |
| #define | CDD_UART_WRITENOTIF_SERVICE_ID 0x09U |
| API Service ID for write notification handler. | |
| #define | CDD_UART_ERRORNOTIF_SERVICE_ID 0x0AU |
| API Service ID for error notification handler. | |
| #define | CDD_UART_DEINIT_SERVICE_ID 0x0BU |
| API Service ID for deinitialization. | |
| #define | CDD_UART_INTERNAL_ISR_ID 0x0CU |
| API Service ID for ISR. | |
CDD UART Error Codes | |
| #define | CDD_UART_E_UNINIT 0x01U |
| Error code indicating the UART is uninitialized. | |
| #define | CDD_UART_E_INVALID_EVENT 0x02U |
| Error code indicating an invalid event. | |
| #define | CDD_UART_E_READ_LOCKED 0x03U |
| Error code indicating UART reading mode ongoing. | |
| #define | CDD_UART_E_WRITE_LOCKED 0x04U |
| Error code indicating UART writing mode ongoing. | |
| #define | CDD_UART_E_PARAM_POINTER 0x05U |
| Error code indicating invalid parameter pointer. | |
| #define | CDD_UART_E_ALREADY_INITIALIZED 0x06U |
| Error code indicating UART is already initialized. | |
| #define | CDD_UART_E_PARAM_VALUE 0x07U |
| Error code indicating Service called with wrong param. | |
| #define | CDD_UART_E_PARAM_LENGTH 0x08U |
| Error code indicating Service called with invalid length. | |
| #define | CDD_UART_E_INVALID_CHANNEL 0x09U |
| Error code indicating invalid UART channel. | |
| #define | CDD_UART_E_INVALID_CONFIG 0x0AU |
| Error code indicating invalid UART configuration. | |
Values indicating the filled status of TX FIFO | |
| #define | UART_TX_FIFO_NOT_FULL |
| #define | UART_TX_FIFO_FULL |
Values related to status of Interrupt souces. | |
| #define | UART_INTID_MODEM_STAT |
| Values pertaining to status of UART Interrupt sources. | |
| #define | UART_INTID_TX_THRES_REACH |
| #define | UART_INTID_RX_THRES_REACH |
| #define | UART_INTID_RX_LINE_STAT_ERROR |
| #define | UART_INTID_CHAR_TIMEOUT |
| #define | UART_INTID_XOFF_SPEC_CHAR_DETECT |
| #define | UART_INTID_MODEM_SIG_STATE_CHANGE |
| #define | UART_INTR_PENDING (0U) |
| Values indicating the UART Interrupt pending status. | |
| #define | UART_NO_INTR_PENDING (1U) |
Values related to enabling/disabling of Interrupts. | |
| #define | UART_INTR_CTS (UART_IER_CTS_IT_MASK) |
| Values for enabling/disabling the interrupts of UART. | |
| #define | UART_INTR_RTS (UART_IER_RTS_IT_MASK) |
| #define | UART_INTR_XOFF (UART_IER_XOFF_IT_MASK) |
| #define | UART_INTR_SLEEPMODE (UART_IER_SLEEP_MODE_MASK) |
| #define | UART_INTR_MODEM_STAT (UART_IER_MODEM_STS_IT_MASK) |
| #define | UART_INTR_LINE_STAT (UART_IER_LINE_STS_IT_MASK) |
| #define | UART_INTR_THR (UART_IER_THR_IT_MASK) |
| #define | UART_INTR_RHR_CTI (UART_IER_RHR_IT_MASK) |
| #define | UART_INTR2_RX_EMPTY (UART_IER2_EN_RXFIFO_EMPTY_MASK) |
| #define | UART_INTR2_TX_EMPTY (UART_IER2_EN_TXFIFO_EMPTY_MASK) |
Values related to Line Status information. | |
| #define | UART_FIFO_PE_FE_BI_DETECTED (UART_LSR_RX_FIFO_STS_MASK) |
| Values pertaining to UART Line Status information. | |
| #define | UART_BREAK_DETECTED_ERROR (UART_LSR_RX_BI_MASK) |
| #define | UART_FRAMING_ERROR (UART_LSR_RX_FE_MASK) |
| #define | UART_PARITY_ERROR (UART_LSR_RX_PE_MASK) |
| #define | UART_OVERRUN_ERROR (UART_LSR_RX_OE_MASK) |