![]() |
MCUSW
|
This file contains cover page for generating doxygen API documentation.
Go to the source code of this file.
Functions | |
| void | Can_IntISR_Function (Can_ControllerInstance CanInstanceID, uint32 baseAddr) |
| This function is the ISR for CAN controller 0/INT 0. | |
| void Can_IntISR_Function | ( | Can_ControllerInstance | CanInstanceID, |
| uint32 | baseAddr ) |
This function is the ISR for CAN controller 0/INT 0.
* * Function name : Can_IntISR_Fun * Syntax : void Can_IntISR_Fun(Can_ControllerInstance CanInstanceID) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Non-Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function is the ISR for CAN controller 0/INT 0 <br> * This function should be invoked either by OS Interrupt * frame handler <br> * CAN Interrupt frame handler for Category 1 ISR *