![]() |
MCUSW
|
This file contains interface header for PWM MCAL driver.
Go to the source code of this file.
PWM Driver State Values | |
The PWM Driver State Values | |
| #define | PWM_STATUS_UNINIT ((uint8)(0U)) |
| PWM driver Status uninitialized. | |
| #define | PWM_STATUS_INIT ((uint8)(1U)) |
| PWM driver Status Initialized. | |
| #define | PWM_DUTY_0_PERCENT (0x0U) |
| 16bit value representing 0% of a period value | |
| #define | PWM_DUTY_100_PERCENT (0x8000U) |
| 16 bit value representing 100% of a period value | |
| #define | PWM_DUTY_50_PERCENT (0x4000U) |
| 16 bit value representing 50% of a period value | |
| enum | Pwm_OutputStateType { PWM_LOW = 0U , PWM_HIGH } |
| Possible output states of a PWM channel. More... | |
| enum | Pwm_EdgeNotificationType { PWM_RISING_EDGE = 1U , PWM_FALLING_EDGE = 2U , PWM_BOTH_EDGES = 3U } |
| Possible edge notification More... | |
| enum | Pwm_ChannelClassType { PWM_FIXED_PERIOD = 0U , PWM_FIXED_PERIOD_SHIFTED , PWM_VARIABLE_PERIOD } |
| Period type for pwm channels. Fixed periods prohibit changes to the period length with Pwm_SetPeriod( ). PWM_FIXED_PERIOD_SHIFTED type is not supported due to hardware restrictions of the PWM unit. More... | |
| enum | Pwm_epwmOutputCh_t { EPWM_OUTPUT_CH_A = 0U , EPWM_OUTPUT_CH_B = 1U , EPWM_OUTPUT_CH_BOTH_A_AND_B = 2U } |
| EPWM outputs in a single epwm channel. More... | |
| typedef uint32 | Pwm_PeriodType |
| typedef of period value | |
| typedef uint32 | Pwm_ChannelType |
| PWM Channel type. | |
| typedef uint32 | Pwm_FrequencyType |
| typedef of frequency value (Frequency in Hz) | |
| typedef void(* | Pwm_NotifyFuncType) (void) |
| Notification callback function pointer | |
| void | Pwm_Init (const Pwm_ConfigType *CfgPtr) |
| Service for PWM initialization. | |
| void | Pwm_DeInit (void) |
| Service for PWM de-initialization. | |
| void | Pwm_SetDutyCycle (Pwm_ChannelType ChannelNumber, uint16 DutyCycle) |
| Service for setting Duty Cycle. | |
| void | Pwm_SetPeriodAndDuty (Pwm_ChannelType ChannelNumber, Pwm_PeriodType Period, uint16 DutyCycle) |
| Service for setting Period and Duty Cycle. | |
| void | Pwm_SetOutputToIdle (Pwm_ChannelType ChannelNumber) |
| Service to set the output of a channel immediately to idle. | |
| Pwm_OutputStateType | Pwm_GetOutputState (Pwm_ChannelType ChannelNumber) |
| void | Pwm_DisableNotification (Pwm_ChannelType ChannelNumber) |
| Service to disable the Edge Notification. | |
| void | Pwm_EnableNotification (Pwm_ChannelType ChannelNumber, Pwm_EdgeNotificationType Notification) |
| Service to enable the Edge Notification. | |
| void | Pwm_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| Std_ReturnType | Pwm_RegisterReadback (Pwm_ChannelType ChannelNumber, Pwm_RegisterReadbackType *RegRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. | |
Data Structures | |
| struct | Pwm_ChannelConfigType_PC |
| Pwm channel configuration. More... | |
| struct | Pwm_ConfigType_PC |
| Pwm configuration structure. More... | |
| struct | Pwm_ChannelConfigType |
| Pwm channel configuration. More... | |
| struct | Pwm_ConfigType |
| Pwm configuration structure. More... | |
| struct | Pwm_RegisterReadbackType |
| PWM register readback structure. More... | |
Macros | |
PWM Driver Module SW Version Info | |
Defines for PWM Driver version used for compatibility checks | |
| #define | PWM_SW_MAJOR_VERSION (10U) |
| Driver Implementation Major Version. | |
| #define | PWM_SW_MINOR_VERSION (1U) |
| Driver Implementation Minor Version. | |
| #define | PWM_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. | |
PWM Driver Module AUTOSAR Version Info | |
Defines for PWM Driver AUTOSAR version used for compatibility checks | |
| #define | PWM_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by PWM Driver. | |
| #define | PWM_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by PWM Driver. | |
| #define | PWM_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by PWM Driver. | |
PWM Driver ID Info | |
| #define | PWM_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. | |
| #define | PWM_MODULE_ID ((uint16) 121U) |
| PWM Driver Module ID. | |
PWM Error Codes | |
PWM Driver Instance ID Error codes returned by PWM functions | |
| #define | PWM_E_INIT_FAILED ((uint8)(0x10U)) |
| PWM driver configuration parameter error. | |
| #define | PWM_E_UNINIT ((uint8)(0x11U)) |
| PWM driver Not initialized error. | |
| #define | PWM_E_PARAM_CHANNEL ((uint8)(0x12U)) |
| PWM driver Invalid param. | |
| #define | PWM_E_PERIOD_UNCHANGEABLE ((uint8)(0x13U)) |
| PWM driver Fixed period channel. | |
| #define | PWM_E_ALREADY_INITIALIZED ((uint8)(0x14U)) |
| PWM driver Already initialized. | |
| #define | PWM_E_PARAM_POINTER ((uint8)(0x15U)) |
| PWM driver pointer paramter error. | |
| #define | PWM_E_NOT_DISENGAGED ((uint8)(0x16U)) |
| RunTime Error: API Pwm_SetPowerState is called while the PWM module is still in use. | |
PWM Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | PWM_SID_INIT ((uint8)(0x0U)) |
| PWM driver service ID for Initialization API. | |
| #define | PWM_SID_DEINIT ((uint8)(0x1U)) |
| PWM driver service ID for De-Initialization API. | |
| #define | PWM_SID_SET_DUTY_CYCLE ((uint8)(0x2U)) |
| PWM driver service ID for set duty cycle API. | |
| #define | PWM_SID_SET_PERIOD_AND_DUTY ((uint8)(0x3U)) |
| PWM driver service ID for set duty cycle and period API. | |
| #define | PWM_SID_SET_OUTPUT_TO_IDLE ((uint8)(0x4U)) |
| PWM driver service ID for set output state to idle API. | |
| #define | PWM_SID_GET_OUTPUT_STATE ((uint8)(0x5U)) |
| PWM driver service ID for get output state API. | |
| #define | PWM_SID_DISABLE_NOTIFICATION ((uint8)(0x6U)) |
| PWM driver service ID for disable notification API. | |
| #define | PWM_SID_ENABLE_NOTIFICATION ((uint8)(0x7U)) |
| PWM driver service ID for Enable notification API. | |
| #define | PWM_SID_GET_VERSION_INFO ((uint8)(0x8U)) |
| PWM driver service ID for Get version info API. | |
| #define | PWM_SID_REGISTER_READBACK ((uint8)(0xDU)) |
| PWM driver service ID for Critical register read back API. | |