IPC module is provided as an CDD and implements IPC based on shared memory and Mailbox IP of the SoC
The IPC Driver implements interfaces specified in MCAL_CDD_IPC_Design document.
Provides methods to transport N bytes of data across core's in TDAxx class of processors. Some of the abilities of this driver are
- Send N bytes of data to other processor (s)
- Received N bytes of data from other processor (s)
- Announce Services offered by core hosting AUTOSAR to all processor (s)
- Via transmission N bytes of data
- Version
- 01.00.00
- See also
- CDD Ipc Configuration
-
MCAL_IPC_IRQ
|
| void | Cdd_IpcGetVersionInfo (Std_VersionInfoType *VersionInfoPtr) |
| | Service for getting CDD version. More...
|
| |
| void | Cdd_IpcInit (void) |
| | Service for CDD Initialization. More...
|
| |
| Std_ReturnType | Cdd_IpcDeinit (void) |
| | Service for deinitializing CDD. More...
|
| |
| Std_ReturnType | Cdd_IpcSendMsg (VAR(uint32,) chId, const void *pBuf, VAR(uint32,) bufLen) |
| | Service for sending an message to remote cores. More...
|
| |
| Std_ReturnType | Cdd_IpcReceiveMsg (VAR(uint32,) chId, void *pBuf, uint32 *bufLen) |
| | Service for reception of N bytes of data from remote cores. More...
|
| |
| Std_ReturnType | Cdd_IpcAnnounce (const UCHAR *pBuf, VAR(uint32,) chId) |
| | Service for broadcasting capabilities of this core to all other cores. More...
|
| |
| Std_ReturnType | Cdd_IpcReceiveCtrlMsg (uint32 *pRemoteProcId, uint32 *pRemoteEndPt, void *pBuf, uint32 *bufLen) |
| | Service for reception of N bytes of control message from remote cores. More...
|
| |
| Std_ReturnType | Cdd_IpcRegisterReadBack (uint32 remoteProcId, Cdd_IpcRegRbValues *pRegArgs) |
| | Service for reading the configuration registers of the MCAL modules. More...
|
| |
| boolean | Cdd_IpcIsInitDone (void) |
| | Service for checking if IPC module is initialized. More...
|
| |
| uint32 | Cdd_IpcGetMaxMsgSize (VAR(uint32,) chId) |
| | Service for checking if IPC module is initialized. More...
|
| |
| uint32 | Cdd_IpcGetMailboxStatus (VAR(uint32,) remoteProcId) |
| | Service to get Mailbox state is FULL or not. More...
|
| |
◆ CDD_IPC_SW_MAJOR_VERSION
| #define CDD_IPC_SW_MAJOR_VERSION (11U) |
Driver Implementation Major Version.
◆ CDD_IPC_SW_MINOR_VERSION
| #define CDD_IPC_SW_MINOR_VERSION (0U) |
Driver Implementation Minor Version.
◆ CDD_IPC_SW_PATCH_VERSION
| #define CDD_IPC_SW_PATCH_VERSION (0U) |
Driver Implementation patch Version.
◆ CDD_IPC_AR_RELEASE_MAJOR_VERSION
| #define CDD_IPC_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by CDD Driver.
◆ CDD_IPC_AR_RELEASE_MINOR_VERSION
| #define CDD_IPC_AR_RELEASE_MINOR_VERSION (3U) |
AUTOSAR Minor version specification implemented by CDD Driver.
◆ CDD_IPC_AR_RELEASE_REVISION_VERSION
| #define CDD_IPC_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by CDD Driver.
◆ CDD_IPC_MODULE_ID
| #define CDD_IPC_MODULE_ID ((uint16) 255U) |
◆ CDD_IPC_VENDOR_ID
| #define CDD_IPC_VENDOR_ID ((uint16) 44U) |
Texas Instruments Vendor ID.
◆ CDD_IPC_INSTANCE_ID
| #define CDD_IPC_INSTANCE_ID ((uint8) 0U) |
◆ CDD_IPC_SID_GETVERSIONINFO
| #define CDD_IPC_SID_GETVERSIONINFO (0x01U) |
API Service ID for get version info.
◆ CDD_IPC_SID_INIT
| #define CDD_IPC_SID_INIT (0x02U) |
API Service ID for initialization.
◆ CDD_IPC_SID_SEND
| #define CDD_IPC_SID_SEND (0x03U) |
API Service ID to send message to remote core.
◆ CDD_IPC_SID_RECEIVE
| #define CDD_IPC_SID_RECEIVE (0x04U) |
API Service ID to receive message from remote core.
◆ CDD_IPC_SID_ANNOUNCE
| #define CDD_IPC_SID_ANNOUNCE (0x05U) |
API Service ID to announce message all remote core.
◆ CDD_IPC_SID_INTERNAL_ISR_ID
| #define CDD_IPC_SID_INTERNAL_ISR_ID (0x06U) |
◆ CDD_IPC_SID_REG_READBACK
| #define CDD_IPC_SID_REG_READBACK (0x07U) |
API Service ID for register read back.
◆ CDD_IPC_SID_DEINIT
| #define CDD_IPC_SID_DEINIT (0x08U) |
API Service ID for De initialization.
◆ CDD_IPC_SID_CTRL_RECEIVE
| #define CDD_IPC_SID_CTRL_RECEIVE (0x09U) |
API Service ID to receive control message from remote core.
◆ CDD_IPC_SID_IS_INIT_DONE
| #define CDD_IPC_SID_IS_INIT_DONE (0x0AU) |
API Service ID to determine if module is initialized.
◆ CDD_IPC_SID_GET_MAX_MSG_SIZE
| #define CDD_IPC_SID_GET_MAX_MSG_SIZE (0x0BU) |
API Service ID to determine the maximum message size configured.
◆ CDD_IPC_SID_MAILBOX_STATE
| #define CDD_IPC_SID_MAILBOX_STATE (0x0CU) |
API Service ID to determine the state of the mailbox.
◆ CDD_IPC_E_OK
| #define CDD_IPC_E_OK (0x00U) |
◆ CDD_IPC_E_INIT_FAILED
| #define CDD_IPC_E_INIT_FAILED (0x01U) |
Error code indicating initialization failure.
◆ CDD_IPC_E_UNINIT
| #define CDD_IPC_E_UNINIT (0x02U) |
Error code indicating the IPC is uninitialized.
◆ CDD_IPC_E_PARAM_POINTER
| #define CDD_IPC_E_PARAM_POINTER (0x03U) |
Error code indicating driver is un-initialized.
◆ CDD_IPC_E_ALREADY_INITIALIZED
| #define CDD_IPC_E_ALREADY_INITIALIZED (0x04U) |
Error code indicating IPC has already been initialized.
◆ CDD_IPC_E_INVALID_CONFIG
| #define CDD_IPC_E_INVALID_CONFIG (0x05U) |
Error code indicating wrong configuration.
◆ CDD_IPC_E_SEND
| #define CDD_IPC_E_SEND (0x06U) |
Error code indicating sending of an message failed.
◆ CDD_IPC_E_RECEIVE_RETRY
| #define CDD_IPC_E_RECEIVE_RETRY (0x07U) |
Error code indicating reception of invalid message.
◆ CDD_IPC_E_NOT_SUPPORTED
| #define CDD_IPC_E_NOT_SUPPORTED (0x08U) |
Error code indicating feature is not supported.
◆ CDD_IPC_E_CALLBACK_NULL
| #define CDD_IPC_E_CALLBACK_NULL (0x09U) |
Error code indicating Callback function passed as NULL pointer.
◆ CDD_IPC_MAX_MSG_LEN
| #define CDD_IPC_MAX_MSG_LEN (496U) |
Maximum message length that can be transported.
◆ CDD_IPC_MAX_CTRL_MSG_LEN
| #define CDD_IPC_MAX_CTRL_MSG_LEN (32U) |
Maximum length of control message.
◆ CDD_IPC_MAX_RETRY_NOTIFY
| #define CDD_IPC_MAX_RETRY_NOTIFY (2U) |
Maximum number of times notify via mailbox is attempted.
In cases where the remote core is not processing mailbox notification,
the driver would attempt to notify multiple times.
◆ Cdd_Ipc_NewMessage
| typedef void(* Cdd_Ipc_NewMessage) (void) |
◆ Cdd_IpcGetVersionInfo()
| void Cdd_IpcGetVersionInfo |
( |
Std_VersionInfoType * |
VersionInfoPtr | ) |
|
Service for getting CDD version.
* Service name : Cdd_IpcGetVersionInfo
* Syntax : void Cdd_IpcGetVersionInfo(Std_VersionInfoType
* VersionInfoPtr)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_GETVERSIONINFO
* Sync/Async : Synchronous
* Reentrancy : Non Reentrant
* Parameters (in) : VersionInfoPtr - Pointer to version info element
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Service for getting CDD version.
*
◆ Cdd_IpcInit()
| void Cdd_IpcInit |
( |
void |
| ) |
|
Service for CDD Initialization.
* Service name : Cdd_IpcInit
* Syntax : Std_ReturnType Cdd_IpcInit(void)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_INIT
* Sync/Async : Synchronous
* Reentrancy : Non Reentrant
* Parameters (in) : None
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Service for CDD Initialization.
*
◆ Cdd_IpcDeinit()
| Std_ReturnType Cdd_IpcDeinit |
( |
void |
| ) |
|
Service for deinitializing CDD.
* Service name : Cdd_IpcDeinit
* Syntax : Std_ReturnType Cdd_IpcDeinit(void* ConfigPtr)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_DEINIT
* Sync/Async : Synchronous
* Reentrancy : Non-Reentrant
* Parameters (in) : ConfigPtr - Not used for now, reserved for future
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : Service for deinitializing the CDD and change the
* driver state to uninitialized
*
◆ Cdd_IpcSendMsg()
| Std_ReturnType Cdd_IpcSendMsg |
( |
VAR(uint32,) |
chId, |
|
|
const void * |
pBuf, |
|
|
VAR(uint32,) |
bufLen |
|
) |
| |
Service for sending an message to remote cores.
* Service name : Cdd_IpcSendMsg
* Syntax : Std_ReturnType Cdd_IpcSendMsg(
* uint32 chId,
* void *pBuf,
* uint32 bufLen)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_SEND
* Sync/Async : Synchronous
* Reentrancy : NonReentrant
* Parameters (in) : chId - Communication channel identifier
* : pBuf - non NULL_PTR, that describes the message to be
* sent
* : bufLen - Length in bytes and cannot exceed
* CDD_IPC_MAX_MSG_LEN
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : This API is used to transport N bytes of data across
* cores.
*
◆ Cdd_IpcReceiveMsg()
| Std_ReturnType Cdd_IpcReceiveMsg |
( |
VAR(uint32,) |
chId, |
|
|
void * |
pBuf, |
|
|
uint32 * |
bufLen |
|
) |
| |
Service for reception of N bytes of data from remote cores.
* Service name : Cdd_IpcReceiveMsg
* Syntax : Std_ReturnType Cdd_IpcReceiveMsg(
* uint32 chId,
* void *pBuf,
* uint32 bufLen)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_RECEIVE
* Sync/Async : Synchronous
* Reentrancy : NonReentrant
* Parameters (in) : chId - Communication channel identifier
* : pBuf - non NULL_PTR, that describes the memory space
* that can hold received message. The length
* shall be CDD_IPC_MAX_MSG_LEN
* : bufLen - Received message length in bytes and will not
* exceed CDD_IPC_MAX_MSG_LEN.
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : This API is used to receive message from remote core
* If there are no messages E_NOT_OK shall be
* returned.
*
*
◆ Cdd_IpcAnnounce()
| Std_ReturnType Cdd_IpcAnnounce |
( |
const UCHAR * |
pBuf, |
|
|
VAR(uint32,) |
chId |
|
) |
| |
Service for broadcasting capabilities of this core to all other cores.
* Service name : Cdd_IpcAnnounce
* Syntax : Std_ReturnType Cdd_IpcAnnounce(
* void *pBuf,
* uint32 bufLen)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_ANNOUNCE
* Sync/Async : Synchronous
* Reentrancy : NonReentrant
* Parameters (in) : pBuf - non NULL_PTR, that describes the message to be
* sent.
* : bufLen - Length in bytes and cannot exceed
* CDD_IPC_MAX_MSG_LEN
* Parameters (inout) : None
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : This API is used to announce the capability of this
* core to all other cores.
*
◆ Cdd_IpcReceiveCtrlMsg()
| Std_ReturnType Cdd_IpcReceiveCtrlMsg |
( |
uint32 * |
pRemoteProcId, |
|
|
uint32 * |
pRemoteEndPt, |
|
|
void * |
pBuf, |
|
|
uint32 * |
bufLen |
|
) |
| |
Service for reception of N bytes of control message from remote cores.
* Service name : Cdd_IpcReceiveCtrlMsg
* Syntax : Std_ReturnType Cdd_IpcReceiveCtrlMsg(
* uint32 pRemoteProcId,
* uint32 pRemoteEndPt,
* void *pBuf,
* uint32 *bufLen)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_CTRL_RECEIVE
* Sync/Async : Synchronous
* Reentrancy : NonReentrant
* Parameters (inout) : pRemoteProcId - Holds the remote processor identifier
* that iniciated this control message
* : pRemoteEndPt - Holds remote end point number that
* iniciated this control message
* : pBuf - non NULL_PTR, that describes the memory space
* that can hold received message. The length
* shall be CDD_IPC_MAX_MSG_LEN
* : bufLen - Received message length in bytes and will not
* exceed CDD_IPC_MAX_MSG_LEN.
* Parameters (in) : None
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : This API is used to receive control message from
* remote core. If there are no messages E_NOT_OK
* shall be returned.
*
*
◆ Cdd_IpcRegisterReadBack()
| Std_ReturnType Cdd_IpcRegisterReadBack |
( |
uint32 |
remoteProcId, |
|
|
Cdd_IpcRegRbValues * |
pRegArgs |
|
) |
| |
Service for reading the configuration registers of the MCAL modules.
* Service name : Cdd_RegisterReadBack
* Syntax : Std_ReturnType Cdd_RegisterReadBack(uint8* mod_name)
* Mode : Supervisor Mode (Privileged Mode)
* Service ID[hex] : None
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : None
* Parameters (inout) : pRegArgs - Pointer to structure that would hold values
* of registers read back by this API
* Parameters (out) : None
* Return value : Std_ReturnType
* Description : Service for reading the critical configuration
* registers of the Mailbox/IPC
*
◆ Cdd_IpcIsInitDone()
| boolean Cdd_IpcIsInitDone |
( |
void |
| ) |
|
Service for checking if IPC module is initialized.
* Service name : Cdd_IpcIsInitDone
* Syntax : boolean Cdd_IpcIsInitDone(void)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_IS_INIT_DONE
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : None
* Parameters (inout) : None
* Parameters (out) : None
* Return value : boolean
* Description : Returns TRUE if Cdd_ipcInit is completed else FALSE
*
◆ Cdd_IpcGetMaxMsgSize()
| uint32 Cdd_IpcGetMaxMsgSize |
( |
VAR(uint32,) |
chId | ) |
|
Service for checking if IPC module is initialized.
* Service name : Cdd_IpcGetMaxMsgSize
* Syntax : uint32 Cdd_IpcGetMaxMsgSize(uint32 chId)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_GET_MAX_MSG_SIZE
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : chId - Communication channel identifier
* Parameters (inout) : None
* Parameters (out) : None
* Return value : uint32
* Description : Returns max msg size for the specified channel
*
◆ Cdd_IpcGetMailboxStatus()
| uint32 Cdd_IpcGetMailboxStatus |
( |
VAR(uint32,) |
remoteProcId | ) |
|
Service to get Mailbox state is FULL or not.
* Service name : Cdd_IpcGetMailboxStatus
* Syntax : uint32 Cdd_IpcGetMailboxStatus(uint32 chId)
* Mode : User Mode (Non-Privileged Mode)
* Service ID[hex] : CDD_IPC_SID_MAILBOX_STATE
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Parameters (in) : remoteProcId - Remote ID
* Parameters (inout) : None
* Parameters (out) : None
* Return value : uint32
* Description : Returns the mailbox state
*