![]() |
MCUSW
|
This file contains the interface of the Ethernet driver.
Go to the source code of this file.
Macros | |
Eth Driver Module SW Version Info | |
Definitions for the Eth Driver version used for compatibility checks | |
| #define | ETH_SW_MAJOR_VERSION (10U) |
| Driver Implementation Major Version. More... | |
| #define | ETH_SW_MINOR_VERSION (0U) |
| Driver Implementation Minor Version. More... | |
| #define | ETH_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
Eth Driver Module AUTOSAR Version Info | |
Definitions for the Etj Driver AUTOSAR version used for compatibility checks | |
| #define | ETH_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by Eth Driver. More... | |
| #define | ETH_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor version specification implemented by Eth Driver. More... | |
| #define | ETH_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by Eth Driver. More... | |
Eth Driver ID Info | |
| #define | ETH_VENDOR_ID ((uint16) 44U) |
| Texas Instruments Vendor ID. More... | |
| #define | ETH_MODULE_ID ((uint16) 88U) |
| Eth Driver Module ID. More... | |
| #define | ETH_INSTANCE_ID ((uint8) 0U) |
| Eth Driver Instance ID. More... | |
Eth Error Codes | |
| #define | ETH_E_INV_CTRL_IDX ((uint8) 0x01U) |
| Invalid controller index. More... | |
| #define | ETH_E_UNINIT ((uint8) 0x02U) |
| Eth module was not initialized. More... | |
| #define | ETH_E_PARAM_POINTER ((uint8) 0x03U) |
| Invalid pointer in parameter list. More... | |
| #define | ETH_E_INV_PARAM ((uint8) 0x04U) |
| Invalid parameter. More... | |
| #define | ETH_E_INV_MODE ((uint8) 0x05U) |
| Invalid mode. More... | |
| #define | ETH_E_VIRTMAC_APIMISMATCH ((uint8) 0x07U) |
| Mismatch in API version between Eth Driver and ethernet firmware. More... | |
| #define | ETH_E_VIRTMAC_RPCCMDFAILED ((uint8) 0x08U) |
| Virtual MAC RPC command failed. More... | |
| #define | ETH_E_VIRTMAC_UNSUPPORTECLIENTNOTIFY ((uint8) 0x09U) |
| Ethernet MCAL RPC client received unhandled notify from ethernet firmware server. More... | |
| #define | ETH_E_VIRTMAC_UNSUPPORTEDSRVCMD ((uint8) 0x0AU) |
| Rpc Command sent by client not supported by server. More... | |
| #define | ETH_E_BUSY ((uint8) 0x0BU) |
| Device or resource is busy. More... | |
Eth Service Ids | |
| #define | ETH_SID_INIT ((uint8) 0x01U) |
| Eth_Init() API Service ID. More... | |
| #define | ETH_SID_SET_CONTROLLER_MODE ((uint8) 0x03U) |
| Eth_SetControllerMode() API Service ID. More... | |
| #define | ETH_SID_GET_CONTROLLER_MODE ((uint8) 0x04U) |
| Eth_GetControllerMode() API Service ID. More... | |
| #define | ETH_SID_WRITE_MII ((uint8) 0x05U) |
| Eth_WriteMii() API Service ID. More... | |
| #define | ETH_SID_READ_MII ((uint8) 0x06U) |
| Eth_ReadMii() API Service ID. More... | |
| #define | ETH_SID_GET_COUNTER_STATE ((uint8) 0x07U) |
| Eth_GetCounterState() API Service ID. More... | |
| #define | ETH_SID_GET_PHYS_ADDR ((uint8) 0x08U) |
| Eth_GetPhysAddr() API Service ID. More... | |
| #define | ETH_SID_PROVIDE_TX_BUFFER ((uint8) 0x09U) |
| Eth_ProvideTxBuffer() API Service ID. More... | |
| #define | ETH_SID_MAIN_FUNCTION ((uint8) 0x20U) |
| Eth_MainFunction() API Service ID. More... | |
| #define | ETH_SID_TRANSMIT ((uint8) 0x0AU) |
| Eth_Transmit() API Service ID. More... | |
| #define | ETH_SID_RECEIVE ((uint8) 0x0BU) |
| Eth_Receive() API Service ID. More... | |
| #define | ETH_SID_TX_CONFIRMATION ((uint8) 0x0CU) |
| Eth_TxConfirmation() API Service ID. More... | |
| #define | ETH_SID_GET_VERSION_INFO ((uint8) 0x0DU) |
| Eth_GetVersionInfo() API Service ID. More... | |
| #define | ETH_SID_RX_IRQ_HDLR ((uint8) 0x10U) |
| Eth_RxIrqHdlr_<CtrlIdx>() API Service ID. More... | |
| #define | ETH_SID_TX_IRQ_HDLR ((uint8) 0x11U) |
| Eth_TxIrqHdlr_<CtrlIdx>() API Service ID. More... | |
| #define | ETH_SID_UPDATE_PHYS_ADDR_FILTER ((uint8) 0x12U) |
| Eth_UpdatePhysAddrFilter() API Service ID. More... | |
| #define | ETH_SID_SET_PHYS_ADDR ((uint8) 0x13U) |
| Eth_SetPhysAddr() API Service ID. More... | |
| #define | ETH_SID_GET_COUNTER_VALUES ((uint8) 0x14U) |
| Eth_GetCounterValues() API Service ID. More... | |
| #define | ETH_SID_GET_RX_STATS ((uint8) 0x15U) |
| Eth_GetRxStats() API Service ID. More... | |
| #define | ETH_SID_GET_TX_STATS ((uint8) 0x1CU) |
| Eth_GetTxStats() API Service ID. More... | |
| #define | ETH_SID_GET_TXERROR_COUNTERVALUES ((uint8) 0x1DU) |
| Eth_GetTxErrorCounterValues() API Service ID. More... | |
| #define | ETH_SID_GET_CURRENT_TIME ((uint8) 0x16U) |
| Eth_GetCurrentTime() API Service ID. More... | |
| #define | ETH_SID_ENABLE_EGRESS_TIMESTAMP ((uint8) 0x17U) |
| Eth_EnableEgressTimeStamp() API Service ID. More... | |
| #define | ETH_SID_GET_EGRESS_TIMESTAMP ((uint8) 0x18U) |
| Eth_GetEgressTimeStamp() API Service ID. More... | |
| #define | ETH_SID_GET_INGRESS_TIMESTAMP ((uint8) 0x19U) |
| Eth_GetIngressTimeStamp() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_INIT ((uint8) 0x30U) |
| Eth_DispatchVirtmacInit() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_DEINIT ((uint8) 0x31U) |
| Eth_DispatchVirtmacDeinit() API Service ID. More... | |
| #define | ETH_SID_NOTIFY_VIRTMAC_MSGRECV ((uint8) 0x32U) |
| Eth_NotifyVirtmacMsgRecv() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_SUBSCRIBE_ALLTRAFFIC ((uint8) 0x33U) |
| Eth_DispatchVirtmacSubscribeAllTraffic() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_UNSUBSCRIBE_ALLTRAFFIC ((uint8) 0x34U) |
| Eth_DispatchVirtmacUnsubscribeAllTraffic() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_SUBSCRIBE_DSTMAC ((uint8) 0x35U) |
| Eth_DispatchVirtmacSubscribeDstMac() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_UNSUBSCRIBE_DSTMAC ((uint8) 0x36U) |
| Eth_DispatchVirtmacUnsubscribeDstMac() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_IPV4_MACADDR_ASSOCIATE ((uint8) 0x37U) |
| Eth_DispatchVirtmacIPv4MacAddrAssociate() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_IPV4_MACADDR_DISASSOCIATE ((uint8) 0x38U) |
| Eth_DispatchVirtmacIPv4MacAddrDisassociate() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_ADD_UNICAST_MACADDR ((uint8) 0x39U) |
| Eth_DispatchVirtmacAddUnicastMacAddr() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_ADD_MCAST_MACADDR ((uint8) 0x3AU) |
| Eth_DispatchVirtmacAddMcastMacAddr() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_DEL_MACADDR ((uint8) 0x3BU) |
| Eth_DispatchVirtmacDelMacAddr() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_ADD_VLAN ((uint8) 0x3CU) |
| Eth_DispatchVirtmacAddVlan() API Service ID. More... | |
| #define | ETH_SID_DISPATCH_VIRTMAC_DEL_VLAN ((uint8) 0x3DU) |
| Eth_DispatchVirtmacDelVlan() API Service ID. More... | |
| #define | ETH_SID_VIRTMAC_RPC_INIT ((uint8) 0x3FU) |
| Eth_VirtMacRpcInit() API Service ID. More... | |
| #define | ETH_SID_SET_BANDWIDTH_LIMIT ((uint8) 0x50U) |
| Eth_SetBandwidthLimit() API Service ID. More... | |
| #define | ETH_SID_GET_BANDWIDTH_LIMIT ((uint8) 0x51U) |
| Eth_GetBandwidthLimit() API Service ID. More... | |
| #define | ETH_SID_RELEASE_RX_BUFFER ((uint8) 0x52U) |
| Eth_ReleaseRxBuffer() API Service ID. More... | |
| #define | ETH_SID_PROVIDE_EXT_TX_BUFFER ((uint8) 0x53U) |
| Eth_ProvideExtTxBuffer() API Service ID. More... | |
| #define | ETH_SID_GET_TX_HEADER_PTR ((uint8) 0x54U) |
| Eth_GetTxHeaderPtr() API Service ID. More... | |
| #define | ETH_SID_GET_RX_HEADER_PTR ((uint8) 0x55U) |
| Eth_GetRxHeaderPtr() API Service ID. More... | |
| #define | ETH_SID_REGISTER_READBACK ((uint8) 0x56U) |
| Eth_RegisterReadback() API Service ID. More... | |
Functions | |
| void | Eth_Init (const Eth_ConfigType *CfgPtr) |
| This function initializes the driver. More... | |
| Std_ReturnType | Eth_SetControllerMode (uint8 CtrlIdx, Eth_ModeType CtrlMode) |
| This function enables / disables the indexed controller. More... | |
| Std_ReturnType | Eth_SetControllerModeByVirtMac (uint8 CtrlIdx, Eth_ModeType CtrlMode) |
| This function enables / disables the indexed controller by Eth virtmac. This is only used for recovering CPSW process. More... | |
| Std_ReturnType | Eth_GetControllerMode (uint8 CtrlIdx, Eth_ModeType *CtrlModePtr) |
| This function obtains the state of the indexed controller. More... | |
| void | Eth_GetPhysAddr (uint8 CtrlIdx, uint8 *PhysAddrPtr) |
| This function obtains the physical source address used by the indexed controller. More... | |
| void | Eth_SetPhysAddr (uint8 CtrlIdx, const uint8 *PhysAddrPtr) |
| This function sets the physical source address used by the indexed controller. More... | |
| Std_ReturnType | Eth_UpdatePhysAddrFilter (uint8 CtrlIdx, const uint8 *PhysAddrPtr, Eth_FilterActionType Action) |
| This function updates the physical source address to / from the indexed controller filter. More... | |
| Std_ReturnType | Eth_WriteMii (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal) |
| This function configures a transceiver register or triggers a function offered by the receiver Service. More... | |
| Std_ReturnType | Eth_ReadMii (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 *RegValPtr) |
| This function reads a transceiver register. More... | |
| Std_ReturnType | Eth_GetCounterValues (uint8 CtrlIdx, Eth_CounterType *CounterPtr) |
| This function reads a list with counter values of the corresponding controller. More... | |
| Std_ReturnType | Eth_GetCounterState (uint8 CtrlIdx, uint16 CtrOffs, uint32 *CtrValPtr) |
| Reads the value of a counter specified with its memory offset. More... | |
| Std_ReturnType | Eth_GetRxStats (uint8 CtrlIdx, Eth_RxStatsType *RxStats) |
| This function reads a list with RX statistics values of the corresponding controller. More... | |
| Std_ReturnType | Eth_GetTxStats (uint8 CtrlIdx, Eth_TxStatsType *TxStats) |
| This function reads a list with TX statistics values of the corresponding controller. More... | |
| Std_ReturnType | Eth_GetTxErrorCounterValues (uint8 CtrlIdx, Eth_TxErrorCounterValuesType *TxErrorCounterValues) |
| This function reads a list of values to read statistic error counter values for transmission for corresponding controller. More... | |
| Std_ReturnType | Eth_GetCurrentTime (uint8 CtrlIdx, Eth_TimeStampQualType *timeQualPtr, Eth_TimeStampType *timeStampPtr) |
| This function returns a time value out of the HW registers. More... | |
| void | Eth_EnableEgressTimeStamp (uint8 CtrlIdx, Eth_BufIdxType BufIdx) |
| This function activates egress time stamping on a dedicated message object. More... | |
| void | Eth_GetEgressTimeStamp (uint8 CtrlIdx, Eth_BufIdxType BufIdx, Eth_TimeStampQualType *timeQualPtr, Eth_TimeStampType *timeStampPtr) |
| This function reads back the egress time stamp on a dedicated message object. More... | |
| void | Eth_GetIngressTimeStamp (uint8 CtrlIdx, Eth_DataType *DataPtr, Eth_TimeStampQualType *timeQualPtr, Eth_TimeStampType *timeStampPtr) |
| This function reads back the ingress time stamp on a dedicated message object. More... | |
| BufReq_ReturnType | Eth_ProvideTxBuffer (uint8 CtrlIdx, uint8 Priority, Eth_BufIdxType *BufIdxPtr, uint8 **BufPtr, uint16 *LenBytePtr) |
| This function provides access to a transmit buffer of the specified controller. More... | |
| Std_ReturnType | Eth_Transmit (uint8 CtrlIdx, Eth_BufIdxType BufIdx, Eth_FrameType FrameType, boolean TxConfirmation, uint16 LenByte, const uint8 *PhysAddrPtr) |
| This function triggers transmission of a previously filled transmit buffer. More... | |
| void | Eth_Receive (uint8 CtrlIdx, uint8 FifoIdx, Eth_RxStatusType *RxStatusPtr) |
| This function triggers frame reception. More... | |
| void | Eth_TxConfirmation (uint8 CtrlIdx) |
| This function triggers frame transmission confirmation. More... | |
| void | Eth_GetVersionInfo (Std_VersionInfoType *VersionInfo) |
| Function returns the version information of this module. More... | |
| void | Eth_MainFunction (void) |
| The function checks for controller errors and lost frames. Used for polling state changes. Calls EthIf_CtrlModeIndication when the controller mode changed. More... | |
| Std_ReturnType | Eth_SetBandwidthLimit (uint8 CtrlIdx, uint8 QueuePrio, uint32 BandwidthLimit) |
| This function set bandwidth for a specific transmitsion queue. More... | |
| Std_ReturnType | Eth_GetBandwidthLimit (uint8 CtrlIdx, uint8 QueuePrio, uint32 *BandwidthLimitPtr) |
| This function get bandwidth for a specific transmitsion queue. More... | |
| Std_ReturnType | Eth_ReleaseRxBuffer (uint8 CtrlIdx, Eth_DataType *BufPtr) |
| This function releases an RX buffer and prepares the buffer to be reused during reception. More... | |
| BufReq_ReturnType | Eth_ProvideExtTxBuffer (uint8 CtrlIdx, uint8 Priority, Eth_BufIdxType *BufIdxPtr, Eth_DataType **BufPtr, uint16 *LenBytePtr) |
| This function provides an external buffer for frame transmission. The buffer is supposed to be locked until transmission confirmation is called. More... | |
| Std_ReturnType | Eth_GetTxHeaderPtr (uint8 CtrlIdx, uint8 BufIdx, Eth_DataType **BufPtr, uint16 *LenBytePtr) |
| This function returns the Ethernet header portion of a transmission frame. This allows the user to overwrite the Ethernet header according to his needs. Otherwise the header is written by the driver. Call this function after a call to Eth_ProvideTxBuffer or Eth_ProvideExtTxBuffer. More... | |
| Std_ReturnType | Eth_GetRxHeaderPtr (uint8 CtrlIdx, Eth_DataType **BufPtr, uint16 *LenBytePtr) |
| This function returns the pointer to the first octet of a received Ethernet frame. That allows access to the Ethernet header as well as the Ethernet payload. Call this function after the EthIf_RxIndication function is called. More... | |
| Std_ReturnType | Eth_RegisterReadback (VAR(uint8,) CtrlIdx, Eth_RegisterReadbackType *RegRbPtr) |
| This service will readback Eth registers. More... | |