![]() |
MCUSW
|
This file contains interface header for Ethernet Transceiver MCAL driver.
Go to the source code of this file.
Macros | |
EthTrcv Driver Module SW Version Info | |
Defines for ETHTRCV Driver version used for compatibility checks | |
| #define | ETHTRCV_SW_MAJOR_VERSION (10U) |
| Driver Implementation Major Version. More... | |
| #define | ETHTRCV_SW_MINOR_VERSION (0U) |
| Driver Implementation Minor Version. More... | |
| #define | ETHTRCV_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
EthTrcv Driver Module AUTOSAR Version Info | |
Defines for ETHTRCV Driver AUTOSAR version used for compatibility checks | |
| #define | ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major Version implemented. More... | |
| #define | ETHTRCV_AR_RELEASE_MINOR_VERSION (3U) |
| AUTOSAR Minor Version implemented. More... | |
| #define | ETHTRCV_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR patch Version implemented. More... | |
EthTrcv Driver ID Info | |
| #define | ETHTRCV_VENDOR_ID (44U) |
| Texas Instruments Vendor ID. More... | |
| #define | ETHTRCV_MODULE_ID (73U) |
| EthTrcv Driver ID. More... | |
| #define | ETHTRCV_INSTANCE_ID (0U) |
| EthTrcv Instace ID. More... | |
EthTrcv Driver Service Id | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| #define | ETHTRCV_INIT_ID ((uint8) 0x01U) |
| EthTrcv_Init() API Service ID. More... | |
| #define | ETHTRCV_CONTROLLER_INIT_ID ((uint8) 0x02U) |
| EthTrcv_Init() API Service ID. More... | |
| #define | ETHTRCV_SETTRCVMODE_ID ((uint8) 0x03U) |
| EthTrcv_SetTransceiverMode() API Service ID. More... | |
| #define | ETHTRCV_GETTRCVMODE_ID ((uint8) 0x04U) |
| EthTrcv_GetTransceiverMode() API Service ID. More... | |
| #define | ETHTRCV_SRTAUTONEGOTIA_ID ((uint8) 0x05U) |
| EthTrcv_StartAutoNegotiation() API Service ID. More... | |
| #define | ETHTRCV_GETLNKSTATE_ID ((uint8) 0x06U) |
| EthTrcv_GetLinkState() API Service ID. More... | |
| #define | ETHTRCV_GETBAUD_ID ((uint8) 0x07U) |
| EthTrcv_GetBaudRate() API Service ID. More... | |
| #define | ETHTRCV_GETDPLXMODE_ID ((uint8) 0x08U) |
| EthTrcv_GetDuplexMode() API Service ID. More... | |
| #define | ETHTRCV_READMIIIND_ID ((uint8) 0x09U) |
| EthTrcv_ReadMiiIndication callback() API Service ID. More... | |
| #define | ETHTRCV_WRITEMIIIND_ID ((uint8) 0x0AU) |
| EthTrcv_WriteMiiIndication callback() API Service ID. More... | |
| #define | ETHTRCV_VERSION_ID ((uint8) 0x0BU) |
| EthTrcv_GetVersionInfo() API Service ID. More... | |
| #define | ETHTRCV_MAINFCT_WRITE_ID ((uint8) 0x0CU) |
| EthTrcv_MainFunction() API Service ID. More... | |
| #define | ETHTRCV_GETTRCVWKUPMODE_ID ((uint8) 0x0DU) |
| EthTrcv_GetTransceiverWakeupMode() API Service ID. More... | |
| #define | ETHTRCV_SETTRCVWKUPMODE_ID ((uint8) 0x0EU) |
| EthTrcv_SetTransceiverWakeupMode() API Service ID. More... | |
| #define | ETHTRCV_CHKWKUP_ID ((uint8) 0x0FU) |
| EthTrcv_CheckWakeup() API Service ID. More... | |
| #define | ETHTRCV_SETPHYTESTMODE_ID ((uint8) 0x10U) |
| EthTrcv_SetPhyTestMode() API Service ID. More... | |
| #define | ETHTRCV_SETPHYLOOPBACKMODE_ID ((uint8) 0x11U) |
| EthTrcv_SetPhyLoopbackMode() API Service ID. More... | |
| #define | ETHTRCV_GETPHYSIGNALQUALITY_ID ((uint8) 0x12U) |
| EthTrcv_GetPhySignalQuality() API Service ID. More... | |
| #define | ETHTRCV_SETPHYTXMODE_ID ((uint8) 0x13U) |
| EthTrcv_SetPhyTxMode() API Service ID. More... | |
| #define | ETHTRCV_GETCABLEDIAGNOSTICSRESULT_ID ((uint8) 0x014U) |
| EthTrcv_GetCableDiagnosticsResult() API Service ID. More... | |
| #define | ETHTRCV_GETPHYIDENTIFIER_ID ((uint8) 0x015U) |
| EthTrcv_GetPhyIdentifier() API Service ID. More... | |
EthTrcv Error Codes | |
Error codes returned by EthTrcv functions | |
| #define | ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U) |
| Invalid transceiver index. More... | |
| #define | ETHTRCV_E_UNINIT ((uint8) 0x02U) |
| EthTrcv module was not initialized. More... | |
| #define | ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U) |
| #define | ETHTRCV_E_INIT_FAILED ((uint8) 0x04U) |
| #define | ETHTRCV_E_NOT_SUPPORTED ((uint8) 0x05U) |
Functions | |
| void | EthTrcv_Init (const EthTrcv_ConfigType *CfgPtr) |
| This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function. More... | |
| Std_ReturnType | EthTrcv_TransceiverInit (uint8 TrcvIdx) |
| This function initializes the Ethernet Transceiver controller. All the required initialization for the transceiver driver is performed in this function. More... | |
| Std_ReturnType | EthTrcv_SetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType CtrlMode) |
| This function enables / disables the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetTransceiverMode (uint8 TrcvIdx, EthTrcv_ModeType *TrcvModePtr) |
| This function obtains the state of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_StartAutoNegotiation (uint8 TrcvIdx) |
| This function restarts the negotiation of the transmission parameters used by the indexed. More... | |
| Std_ReturnType | EthTrcv_GetLinkState (uint8 TrcvIdx, EthTrcv_LinkStateType *LinkStatePtr) |
| This function obtains the link state of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetBaudRate (uint8 TrcvIdx, EthTrcv_BaudRateType *BaudRatePtr) |
| This function obtains the baud rate of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_GetDuplexMode (uint8 TrcvIdx, EthTrcv_DuplexModeType *DuplexModePtr) |
| This function obtains the duplex mode of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_SetPhyTestMode (uint8 TrcvIdx, EthTrcv_PhyTestModeType Mode) |
| This function Activates a given test mode. More... | |
| Std_ReturnType | EthTrcv_SetPhyLoopbackMode (uint8 TrcvIdx, EthTrcv_PhyLoopbackModeType Mode) |
| This function Activates a given loopback mode. More... | |
| Std_ReturnType | EthTrcv_GetPhySignalQuality (uint8 TrcvIdx, uint32 *SignalQualityPtr) |
| This function Obtains the current signal quality of the link of the indexed transceiver. More... | |
| Std_ReturnType | EthTrcv_SetPhyTxMode (uint8 TrcvIdx, EthTrcv_PhyTxModeType Mode) |
| This function Activates a given transmission mode. More... | |
| Std_ReturnType | EthTrcv_GetCableDiagnosticsResult (uint8 TrcvIdx, EthTrcv_CableDiagResultType *ResultPtr) |
| This function Retrieves the cable diagnostics result of a given transceiver. More... | |
| Std_ReturnType | EthTrcv_GetPhyIdentifier (uint8 TrcvIdx, uint32 *OrgUniqueIdPtr, uint8 *ModelNrPtr, uint8 *RevisionNrPtr) |
| This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802.3-2015 chapter 22.2.4.3.1 PHY Identifer. More... | |
| void | EthTrcv_GetVersionInfo (Std_VersionInfoType *VersionInfoPtr) |
| Function returns the version information of this module. More... | |
| void | EthTrcv_ReadMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal) |
| This function is called when information has been read out via MII interface. Triggered by previous Eth_ReadMii call. It can directly be called within Eth_ReadMii. More... | |
| void | EthTrcv_WriteMiiIndication (uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegId) |
| This function is called when information has been written via MII interface. Triggered by previous Eth_WriteMii call. It can directly be called within Eth_WriteMii. More... | |
| void | EthTrcv_MainFunction (void) |
| This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication when the transceiver mode changed. It stores wakeup events if EthTrcvWakeUpSupport is set to ETHTRCV_WAKEUP_BY_POLLING. More... | |