![]() |
MCUSW
|
This document details AUTOSAR BSW Flash module implementation
The Flash Driver provides services for reading, writing, erasing flash memory and Execute-in-Place (XIP) mode for external Flash Device.
The driver supports the following devices:
| Device | Flash Protocol | Boards supported |
| MT35XU512ABA1G12 | OSPI | J721E |
| S28HS512T | XSPI | J721S2, J7200, J784S4, AM62X_SK, AM62PX, J722S |
| MT25QU512ABB | QSPI | J721S2 |
The main tasks of the FLS driver are:
Please refer the Flash design, which is included as part of CSP.
The Fls Module uses internal OSPI peripheral as the serial bus to transfer data to and from the attached flash device.
Programming of clock source for the flash, is beyond the scope of this document. The Clock programming is taken care by the test application.
1 Fls instance is supported by this driver implementation.
The Fls Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Fls_Cfg.h to be present as (Configuration Folder Structure). Please refer (Build) to specify path to generated configuration. The associated Fls configuration generated files Fls_Cfg.c, and Fls_PBcfg.c to be present as shown (Configuration Folder Structure)
The following section details on the unsupported features and additional features added.
This parameter is the switch between Direct Access Mode (DAC) and Indirect Access Mode (INDAC) used by the OSPI module to communicate with the Flash Device. The Flash will be memory mapped when running in DAC mode, and execution in place will happen directly from flash memory. In INDAC mode, data transfer between system memory and external flash occurs through the internal SRAM.
This parameter is the switch to turn on or off XIP mode. Only XIP Read mode is supported in current driver. XIP mode will only be functional in DAC mode of operation.
This parameter defines the Clock Speed for the OSPI peripheral. The supported clock speeds are as follows:
This parameter is the switch between Double Transfer Rate (DTR) and Single Transfer Rate (STR) for OSPI Flash.
This parameter is the switch to turn on and off PHY mode.
Following features outlined in Specification are not supported:
As noted from the previous MCAL implementation, some of the critical configuration registers could potentially be corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection
| Description | Comments | |
| Service Name | Ospi_RegisterReadback | Can potentially be turned OFF (Refer to Design Document provided in CSP) |
| Syntax | Ospi_RegisterReadback( P2VAR(CSL_ospi_flash_cfgRegs, AUTOMATIC, SPI_APPL_DATA) RegRbPtr) | E_OK: Register read back has been done, E_NOT_OK: Register read back failed |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | None | |
| Parameters out | RegRbPtr | Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK. |
| Return Value | Std_ReturnType | E_OK, E_NOT_OK |
This API Enable Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrEnable | Fls_dataOverflowUnderflowIntrEnable Enable Under/Overflow Interrupts of the hardware unit |
| Syntax | Fls_dataOverflowUnderflowIntrEnable(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt Enabled E_NOT_OK: Interrupt Enable failed |
This API Disable Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrDisable | Spi_dataOverflowUnderflowIntrDisable Disable Under/Overflow Interrupts of the hardware unit and returns the status. |
| Syntax | Fls_dataOverflowUnderflowIntrDisable(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Disable flag for Underflow=2U Interrupt Disable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt Disabled E_NOT_OK: Interrupt Disabled failed |
This API gets status of Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrGetStatus | Fls_dataOverflowUnderflowIntrGetStatus gets status of Under/Overflow Interrupts of the hardware unit |
| Syntax | Fls_dataOverflowUnderflowIntrGetStatus(uint32 intFlags) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag |
| Parameters out | NA | |
| Return Value | ospiIrqstatus | OSPI_NO_EVENT: No underflow event OSPI_EVENT_PENDING: Underflow Event OSPI_STATUS_READ_FAIL: Status read fail |
This API clear Under/Overflow Interrupts of the hardware unit and returns the status.
| Description | Comments | |
| Service Name | Fls_dataOverflowUnderflowIntrStatusClear | Fls_dataOverflowUnderflowIntrStatusClear clear Under/Overflow Interrupts of the hardware unit and returns the status. |
| Syntax | Fls_dataOverflowUnderflowIntrStatusClear(uint32 intrFlag) | |
| Service ID | NA | |
| Sync / Async | Sync | |
| Reentrancy | Reentrant | |
| Parameter in | intrFlag | Interrupt Enable flag for Underflow=2U Interrupt Enable flag for Overflow=128U |
| Parameters out | NA | |
| Return Value | Std_ReturnType | E_OK: Interrupt status clears E_NOT_OK: Interrupt status clear failed |
The driver can have unexpected behavior and loss of functionality if unsupported values are passed into configurator or unsupported combinations are used. Below is a list of such constraints.
The Driver does not register any interrupt service routine(ISR), it’s expected that consumer of this driver registers the required interrupt handler.
The interrupt number associated with instance of the Fls is detailed in TRM. Please refer FlsApp_InterruptConfig() in fls_app_intr test application for reference.
Please note that interrupt implementation is only available when running with INDAC mode. BlankCheck and Compare APIs are not supported with interrupt mode.
The driver doesn't configure the functional clock and power for the Fls modules. It's expected that secondary boot loader(SBL) power-up the required modules. Please refer SBL documentation.
There PHY algorthm used in J7200, J721E, J721S2, and J784S4 are based on calibration algorithm. AM62AX, AM62X, AM62PX, J722S, and QSPI device on J721S2 do not have PHY tune as of now.
The Phy tune data vector must first be flashed into the last sector of flash memory, and then during first read operation, Phy tune will be calibrated.
The example application can be used as reference for this.
Some restrictions that Fls driver has right now with respect to the SoC:
Note:PHY Algorithm not validated on SMPU
Current FLS driver uses OSPI, XSPI, and QSPI protocol modes and supports the three NOR Flash devices for all devices (MT35XU512ABA1G12, S28HS512T, and MT25QU512ABB).
If variation to the supported features are needed, user will need to take care to modify the driver to accommodate changes.
J721S2 support both XSPI flash device (s28hs512t) and QSPI flash device (mt25qu512abb). The build command "FLS_PROTOCOL=qspi" and "FLS_PROTOCOL=ospi" is used to differentiate between using XSPI vs QSPI flash device. example/Fls/QSPI_Cfg has QSPI configuration files. Currently only one flash device can be used at a time on J721S2.
Refer to Build and Running the Application for QSPI build instructions.
Refer to Configuration Folder Structure for QSPI configuration folder
Please follow steps detailed in section (Build) to build library or example. Please note that OSPI Boot mode is not applicable for Fls module.
The below Fls Test Applications are available:
Please refer to Configuration Folder Structure on which of the three configuration folders each Fls Test Apllication uses.
Note: Please do a clean build (make -s allclean) when a different configuration folder is used. Each configuration folder header files have different define values.
Please follow steps detailed in section (Build) to build example
Poll Mode - Storage Mode
Test Applications fls_app_dac and fls_app_indac will run as packaged, just build and the executable will be generated.
Interrupt Mode - Storage Mode
Build fls_app_intr and run. Uses different configuration files than Poll Mode, so please build this application on a clean build.
This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.
This implementation requires one level of exclusive access to guard critical sections. Invokes SchM_Enter_Fls_FLS_EXCLUSIVE_AREA_0 (), SchM_Exit_Fls_FLS_EXCLUSIVE_AREA_0 () to enter critical section and exit.
In the example implementation (Driver File Structure SchM_Fls.c) , all the interrupts on CPU are disabled. However, disabling of the enabled Fls interrupt should suffice.
This implementation depends on MemIf module and uses its imported types such as MemIf_JobResultType, MemIf_ModeType and MemIf_StatusType.
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error.
Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Fls.h) lists the SID.
| Type of Error | Related Error code | Value (Hex) |
| API service called with wrong parameter | FLS_E_PARAM_CONFIG | 0x01 |
| API service called with wrong parameter | FLS_E_PARAM_ADDRESS | 0x02 |
| API service called with wrong parameter | FLS_E_PARAM_LENGTH | 0x03 |
| API service called with wrong parameter | FLS_E_PARAM_DATA | 0x04 |
| API service used without module initialization | FLS_E_UNINIT | 0x05 |
| API called when module is busy | FLS_E_BUSY | 0x06 |
| API called with a Null Pointer | FLS_E_PARAM_POINTER | 0x0A |
Transient errors are reported to the DET using the service Det_reportDetTransientFault(). The driver interface (Fls.h) lists the SID.
| Type of Error | Related Error code | Value (Hex) |
| Flash Erase Failed in HW | FLS_E_ERASE_FAILED | 0x01 |
| Flash Write Failed in HW | FLS_E_WRITE_FAILED | 0x02 |
| Flash Read Failed in HW | FLS_E_READ_FAILED | 0x03 |
| Flash Compare Failed in HW | FLS_E_COMPARE_FAILED | 0x04 |
| Expected HW ID not matched | FLS_E_UNEXPECTED_FLASH_ID | 0x05 |
The AUTOSAR BSW Flash Driver specification details the APIs required for Flash Driver. Please refer to (Refer to Design Document provided in CSP) for detailed API description.
Refer API Documentation for details
The example application demonstrates use of Fls module, the list below identifies key steps performed in the example. The configuration file is present at (Configuration Folder Structure).
Polled Storage Mode (fls_app_dac and fls_app_indac)
Interrupt Storage Mode (fls_app_intr)
Performance Measurements
FLS_APP_DAC:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_DAC:
Running on J7 ES
FLS_APP_DAC: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_DAC: FLS spi_test Initiating and Starting.
FLS_APP_DAC: Variant - Pre Compile being used !!!
FLS_APP_DAC: Configuring Clocks.
FLS_APP_DAC: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_DAC: DATA SIZE TEST is 0x100000
FLS_APP_DAC: Offset is 0x0
FLS_APP_DAC:
*****************Writing PHY Tune Data to last sector in memory*****************
FLS_APP_DAC: Erasing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Blank Checking
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Writing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Write 1048576 bytes at transfer rate 107557 Kbps
FLS_APP_DAC: Comparing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
*************************Writing PHY Tune Data complete*************************
FLS_APP_DAC: Erasing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Blank Checking
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Writing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Write 1048576 bytes at transfer rate 2533 Kbps
FLS_APP_DAC: Reading
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Read 1048576 bytes at transfer rate 40725 Kbps
FLS_APP_DAC: Comparing
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC: Reading
FLS_APP_DAC: Job Processing in Progress.
FLS_APP_DAC: Job Ends: SUCCESS
FLS_APP_DAC:
Read 1048576 bytes at transfer rate 41341 Kbps
FLS_APP_DAC: All tests have passed! FLS_APP_INDAC:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_INDAC:
Running on J7 ES
FLS_APP_INDAC: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_INDAC: FLS spi_test Initiating and Starting.
FLS_APP_INDAC: Variant - Pre Compile being used !!!
FLS_APP_INDAC: Configuring Clocks.
FLS_APP_INDAC: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_INDAC: DATA SIZE TEST is 0x100000
FLS_APP_INDAC: Offset is 0x0
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8912 Kbps
FLS_APP_INDAC: Cancel while Erasing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Cancel while Writing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 53350 Kbps
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Comparing.Expected to fail as data is erased.
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 8
Error ID 8
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Cancel while Comparing.Expected to fail as data is erased.
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Writing to compare again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8911 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44758 Kbps
FLS_APP_INDAC: Cancel while Reading
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 53349 Kbps
FLS_APP_INDAC:
.......................Changing mode to DAC.......................
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 20022 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
....................Changing mode to INDAC.....................
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8913 Kbps
FLS_APP_INDAC: Reading
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44756 Kbps
FLS_APP_INDAC: Comparing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Cancel Erase Job
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Blank Checking after erase cancel-----Expect to fail
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 10
Error ID 7
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Erasing again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Blank Checking after erase again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Cancel after Writing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 53350 Kbps
FLS_APP_INDAC: Comparing after write cancel---Expect to fail
FLS_APP_INDAC: Job Processing in Progress.
Det Error reported
Module ID 92
Instance ID 0
SID 8
Error ID 8
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Writing again. Will pass
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8914 Kbps
FLS_APP_INDAC: Comparing.Expected to pass since write passed.
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Erasing
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC: Writing.
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Write 1048576 bytes at transfer rate 8913 Kbps
FLS_APP_INDAC: Cancel while Reading
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 53349 Kbps
FLS_APP_INDAC: Reading again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Read 1048576 bytes at transfer rate 44751 Kbps
FLS_APP_INDAC: Cancel while Comparing
FLS_APP_INDAC: Cancel job Processing in Progress.
FLS_APP_INDAC: Error is expected as we are cancelling the operation.
FLS_APP_INDAC: Job Ends: ERROR
FLS_APP_INDAC: Comparing again
FLS_APP_INDAC: Job Processing in Progress.
FLS_APP_INDAC: Job Ends: SUCCESS
FLS_APP_INDAC:
Changing mode to DAC
FLS_APP_INDAC: FLS SPI TEST DONE!
FLS_APP_INDAC: Ospi configuration Register Readback values
FLS_APP_INDAC: CONFIG_REG : 0x81783881
FLS_APP_INDAC: DEV_INSTR_RD_CONFIG_REG : 0x1e03339d
FLS_APP_INDAC: DEV_INSTR_WR_CONFIG_REG : 0x33082
FLS_APP_INDAC: DEV_DELAY_REG : 0x300000a
FLS_APP_INDAC: DEV_SIZE_CONFIG_REG : 0x111003
FLS_APP_INDAC: SRAM_PARTITION_CFG_REG : 0x3f
FLS_APP_INDAC: DMA_PERIPH_CONFIG_REG : 0x0
FLS_APP_INDAC: MODE_BIT_CONFIG_REG : 0x200
FLS_APP_INDAC: TX_THRESH_REG : 0x1
FLS_APP_INDAC: RX_THRESH_REG : 0x1
FLS_APP_INDAC: PHY_CONFIGURATION_REG : 0x2d0021
FLS_APP_INDAC: All tests have passed! FLS_APP_INTR:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_INTR: OSPI0 controller will be configured for OSPI/XSPI flash
FLS_APP_INTR: FLS spi_test Initiating and Starting.
FLS_APP_INTR: Configuring Interrupt.
FLS_APP_INTR: Variant - Pre Compile being used !!!
FLS_APP_INTR: Configuring Clocks.
FLS_APP_INTR: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 10
SW Minor Version : 0
SW Patch Version : 0
FLS_APP_INTR: DATA SIZE TEST is 0x100000
FLS_APP_INTR: Offset is 0x0
FLS_APP_INTR: Erasing
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR: Manual comparing erased data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58417 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR: Cancel while Writing
FLS_APP_INTR: Cancel job Processing in Progress.
FLS_APP_INTR: Error is expected as we are cancelling the operation.
FLS_APP_INTR: Job Ends: ERROR
FLS_APP_INTR:
Write 1048576 bytes at transfer rate 55448 Kbps
FLS_APP_INTR: Cancel while Reading
FLS_APP_INTR: Cancel job Processing in Progress.
FLS_APP_INTR: Error is expected as we are cancelling the operation.
FLS_APP_INTR: Job Ends: ERROR
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 56766 Kbps
FLS_APP_INTR: Erasing
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR: Manual comparing erased data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58439 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR: Writing Again without Cancel
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Write 1048576 bytes at transfer rate 13121 Kbps
FLS_APP_INTR: Reading without cancel
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58452 Kbps
FLS_APP_INTR: Manual Comparing written data
FLS_APP_INTR: Calling Read to manually compare
FLS_APP_INTR: Job Processing in Progress.
FLS_APP_INTR: Job Ends: SUCCESS
FLS_APP_INTR:
Read 1048576 bytes at transfer rate 58433 Kbps
FLS_APP_INTR: Manual Comparing is Correct
FLS_APP_INTR:
Changing mode to DAC
FLS_APP_INTR: FLS SPI TEST DONE!
FLS_APP_INTR: Ospi configuration Register Readback values
FLS_APP_INTR: CONFIG_REG : 0x81783881
FLS_APP_INTR: DEV_INSTR_RD_CONFIG_REG : 0x1e03339d
FLS_APP_INTR: DEV_INSTR_WR_CONFIG_REG : 0x33082
FLS_APP_INTR: DEV_DELAY_REG : 0x300000a
FLS_APP_INTR: DEV_SIZE_CONFIG_REG : 0x111003
FLS_APP_INTR: SRAM_PARTITION_CFG_REG : 0x3f
FLS_APP_INTR: DMA_PERIPH_CONFIG_REG : 0x0
FLS_APP_INTR: MODE_BIT_CONFIG_REG : 0x200
FLS_APP_INTR: TX_THRESH_REG : 0x1
FLS_APP_INTR: RX_THRESH_REG : 0x1
FLS_APP_INTR: PHY_CONFIGURATION_REG : 0x2d0021
FLS_APP_INTR: All tests have passed! FLS_APP_XIP:
------------------FLS Sample Application - STARTS !!! ------------------
FLS_APP_XIP:
Running on J7 ES
FLS_APP_XIP: FLS spi_test Initiating and Starting.
FLS_APP_XIP: Variant - Pre Compile being used !!!
FLS_APP_XIP: Configuring Clocks.
FLS_APP_XIP: Clock Configured at 166666666Hz
FLS MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 92
SW Major Version : 1
SW Minor Version : 2
SW Patch Version : 1
FLS_APP_XIP: DATA SIZE TEST is 0x1000
FLS_APP_XIP: Offset is 0x0
FLS_APP_XIP: Erasing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Blank Checking
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Writing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Calling XIP app
MCU1_0 running
MCU1_0 reports: All tests have passed
FLS_APP_XIP: Returning from XIP app, returned value is 0xFEEDFACE
FLS_APP_XIP: Reading
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: Comparing
FLS_APP_XIP: Job Processing in Progress.
FLS_APP_XIP: Job Ends: SUCCESS
FLS_APP_XIP: DONE!